ST67W611M1 manufacturing mode


Back to main page

1. Introduction

The manufacturing mode can be used to validate a board design by measuring RF parameters, such as Tx emissions in continuous or modulated wave and the Rx packet error rate versus channel frequency or modulation type.

2. Programming and running manufacturing (MFG) mode

The ST67W611M hardware setup wiki page describes how to program the manufacturing-mode firmware.

3. ST67W6X-RCT-TOOL

Once the MFG firmware is loaded onto the ST67W611M1 device, the ST67W6X-RCT-TOOL allows the user to control the radio settings of the module, such as:

  • The channel, output power, modulation standard, and packet settings
  • The duty cycle
  • The XO calibration value(1)
  • Enabling the power table compensation(1)

(1): Modules are already trimmed in production. However, XO compensation can be forced and power compensation can be enabled or disabled. In modulation mode, internal limitations are applied to conform with regulations.

When these settings have been configured, the RF-Phy tests can be launched.

4. Main command lines

Use a terminal emulator like Tera Term to send the UART commands through the serial port.

4.1. Serial port configuration

The UART baud rate must be set to 2 Mbps, as shown in the image below:

4.2. Common commands

Command Description
V1 Enable power compensation
V0 Disable power compensation
x32 Set frequency offset compensation factor; capcode is 32
c10 Set channel number 10
p15 Set power; target power is 15 dBm
d50 Set Tx duty cycle; duty cycle is 50% or 100%
l4096 Set payload length; length is 4096 bytes
f500 Set packet transmission frequency; frequency is 500 Hz (set to '500' for 11b; '1000' for others)
t1 Start Tx
t0 Stop Tx
r:s2 Start Rx for BW20
r:s4 Start Rx for BW40
r:p Stop Rx
r:g Get Rx stats

The following sections focus on the Wi-Fi® standard.


4.3. Standard 11b command

Preamble type Data rate
B: long preamble 0: 1 Mbps
b: short preamble 1: 2 Mbps
2: 5.5 Mbps
3: 11 Mbps

Example: set the standard 11b command to a short preamble at 1 Mbps.

b0

4.4. Standard 11g command

Preamble type Data rate
G: long 0: 6 Mbps
g: short 1: 9 Mbps
2: 12 Mbps
3: 18 Mbps
4: 24 Mbps
5: 36 Mbps
6: 48 Mbps
7: 54 Mbps

Example: set the standard 11g command to a long preamble at 54 Mbps.

G7

4.5. Standard 11n command

Preamble type Bandwidth Data rate Coding type
msg: short GI HT-GF 2: 20 MHz 0: MCS0 0: BCC
msm: short GI HT-MF 4: 40 MHz ... 1: LDPC
mlg: long GI HT-GF ...
mlm: long GI HT-MF 7: MCS7

Example: set the standard 11n command to a long-guard interval in a mixed-packet format, 20-MHz bandwidth, MCS7 modulation scheme, and BCC coding type.

mlm270

4.6. Standard 11ax command

Coding type Preamble type 0 Data rate Bandwidth
0: BCC 0: 2xHELTF + 0.8 us GI 0: MCS0 0: BW20
1: LDPC 1: 2xHELTF + 1.6 us GI ... 1: BW40
2: 4xHELTF + 3.2 us GI 9: MCS9

Example: set the standard 11ax command to a BCC coding type, 0.8-us guard interval, MCS9 modulation scheme, and 20-MHz bandwidth.

Q00090

5. Running RF tests

Connect the correct RF cable, depending on the reference design version:

  • -B: use a specific cable - ufl-like to SMA: MXHQ87WJ3000.
  • -U: use an MHF4-to-SMA cable compatible with the IPEX 20449-001E-03 connector, such as a Linx CSJ-RGFB-100-MHF4 cable.

For more details on ST67W611M1 reference designs, visit this wiki page.

Either use the ST67W6X-RCT-TOOL or send commands through the serial port (Tera Term or a Python test sequence).

5.1. Tx tests

5.1.1. Bench setup

Spectrum analyzer settings for power channel measurements:

  • RBW = 1MHz/VBW = 3MHz
  • RMS detector/power average measurement
  • Sweep time auto
  • Ext atten = 20 dB

Default settings used for test:

  • Coding type: BCC for BW20 (11n & 11ax); LDPC for BW40 (11ax)
  • HELEF/GI: 2xHELTF + 0.8us GI (for 11ax only)

5.1.2. Example Tx test sequence: standard 11ax

V1                   // Enable power compensation
c10                  // Set channel; set to channel 10
p15                  // Set power; target power is 15 dBm
d100                 // Set Tx duty cycle; duty cycle is 100%
l4096                // Set payload length; length is 4096 bytes
f500                 // Set packet transmission frequency; frequency is 500Hz
x32                  // Set frequency offset compensation factor; capcode is 32
Q00090               // Select packet mode and rate: 11ax/0.8us GI/20M BW/MCS9/BCC
t1                   // Enable Tx mode

Configure the analyzer according to the ST67W611M1 settings and execute the WLAN measurement, such as:

  • Channel power
  • Error vector magnitude (EVM)
  • Frequency/symbol error
  • Spectrum emission mask (SEM)
  • Spectral flatness
  • Spurious emissions

Note that for any configuration changes (such as the power channel or standard), the Tx has to be set OFF (no frequency or power setting during emission).

5.2. Rx tests

5.2.1. Bench setup

To avoid external perturbations, put the board into a Faraday cage, as illustrated by the image below:

The main Rx performance is the sensitivity of the receiver.

Default Rx parameters used for test (on ST67W611M1 and the generator):

  • 1x1 stream
  • Guard interval: long
  • Physical mode:
    • 11b/11g: legacy
    • 11n: mixed mode
  • Payload size:
    • 11b/11g: 1024
    • 11n: 4096

5.2.2. Example Rx test sequence

For ST67W611M1, it is not necessary to specify the packet/standard parameters.

Program the modulation parameters of the RF generator (bandwidth, standard, packet bw, FCS MAC enable, coding type, ppdu format, guard interval, payload length, and packet number).

c6                    // Set channel; set to channel 6
x32                   // Set frequency offset compensation factor; capcode is 32
r:s2                  // Start Rx & set receive bandwidth = 20 MHz
r:g                   // Gather and report the received packet count: correct packet in the field "rxok: ..."

Set RF generator output power

(For example, start a sweep from the expected sensi value -5 dBm and increase the power with 1-dB steps).

For each power step of the generator, calculate the PER:

PER = [(Packet_number – rxok) / Packet_number)] *100

The sensitivity threshold is obtained for a PER <= 10%

r:p                   // Stop RX receive mode

Change the ST67W611M1 parameters (such as the channel or standard) and execute another test.

6. LitePoint IQxel-MW

This section introduces the LitePoint part of the test flow. This equipment automates TX and RX measurements, exchanges commands with the ST67W611M1, and returns the test results to the host computer. It is well suited for repeated validation during manufacturing because it improves test repeatability and reduces manual setup.

The IQfact+ software package for the ST67W611M1 is available from LitePoint under the reference "IQfact+_ST_ST67W611".


Picture of the testbench LitePoint IQxel-MW

6.1. Hardware setup

To connect the LitePoint IQxel-MW 7G to the ST67W611M1, use the following setup:

Hardware setup for Tx and Rx tests

The schematic includes the following components:

  • The desktop contains all the tests procedures and software. it launches the tests and records the results.
  • The device under test (DUT) is isolated from external interference with a Faraday box. Depending on the test, the DUT transmits Wi-Fi signals or reports the number of received packets.
  • The LitePoint IQxel-MW is a measurement tool that reports the characteristics of the transmitted signal or generates signals to be detected by the DUT. At the end of a test, the LitePoint IQxel-MW sends the results to the desktop.

This setup ensures accurate and reliable test measurements.

6.2. Software setup

6.2.1. Web user interface

The LitePoint IQxel-MW provides a web interface to view signal characteristics. With this interface, the user can check relevant characteristics such as the spectrum, spectrum mask margins, constellation, and transmission quality. This interface allows users to verify signal detection and adjust parameters before applying them in IQfactStudio.

6.2.2. IQfactStudio

IQfactStudio user interface

IQfactStudio is a custom program provided by LitePoint to automate the test procedure for the ST67W611M1. It consists of three sections:

  • The first section is the test procedure, where the user can add multiple steps to measure EVM, margin, or emission power on different Wi-Fi standards.
  • The second section displays the test parameters, such as emission standard, test type, channel frequency, bandwidth frequency, and others.
  • The third section contains the test results after completion.

A fourth section appears during execution and contains a terminal that shows the communication between the desktop and the DUT, including error messages.

6.2.3. Contact

The LitePoint team is still available for further questions and additional support through the following link: https://www.litepoint.com/about/contact-us/