This article explains how to launch a simple preview with ISP running for a better image quality rendering on the STM32N6570-DK board.
1. Description
This example demonstrates how to stream a camera and to display a preview with ISP enabled and 2A algorithms running.
This example included in the X-Cube-ISP package uses the Camera middlleware on top of the ISP middleware.
2. Prerequisites
- Hardware
- STM32N6 discovery board
- Discovery MB1860- STM32N6 (need USBC cable)
- IMX335 camera module MB1854B
- Required tools
- X-CUBE-ISP package v2.1.0
- STM32CubeIDE (STM32CubeIDE 2.1.1)
3. Simple preview
This application streams the IMX335 sensor, runs ISP 2A algorithms and display a preview that fits the LCD in 640x480 using Camera Middleware services.
3.1. How to get application project
- Presently, a simple preview application using ISP services through Camera Middleware is available in X-CUBE-ISP package.
- Download the package then follow instructions from
Path: X-CUBE-ISP_v2.1.0/README.mdto import STM32N6_ISP_Preview_App project in STM32CubeIDE. - Then, build index and project.
3.2. Project structure
Here is the general structure of the STM32N6_ISP_Preview_App project without ISP_MW_TUNING_TOOL_SUPPORT:
Application |--> common Common directory | |--> main.c Main entry point for all applications of X-CUBE-ISP project | |--> ... |--> ISP_Preview_App Preview application directory | |--> app.c Preview application entry point, Camera Middleware callbacks | |--> ... Middleware |--> Camera_Middleware Camera middleware | |--> ISP_Library ISP middleware included in Camera Middleware | | |--> isp_algo.c IQ algorithms | | |--> isp_ae_algo.c IQ AEC algorithm | | |--> isp_awb_algo.c IQ AWB algorithm | | |--> isp_core.c Core and API | | |--> isp_services.c Internal services | |--> sensors Interfaces and drivers of supported sensors | | |--> drivers Sensor drivers | | | |--> imx335.c IMX335 sensor driver | | | |--> vd1943.c VD1943 sensor driver | | | |--> ... Other supported sensor drivers | | |--> cmw_imx335.c IMX335 sensor interface | | |--> cmw_vd1943.c IMX335 sensor interface | | |--> ... Other supported sensor sensor interfaces | |--> cmw_camera.c Core and API of Camera middleware | |--> cmw_utils.c Camera Middleware Utils functions | |--> cmw_sensor_registry.c Camera Middleware registry of available sensors Drivers Including DCMIPP, CSI and LCD HAL drivers Includes |--> project_path/Inc | |--> cmw_camera_conf.h ISP list of supported camera modules | |--> isp_param_conf.h ISP IQ configuration parameters
3.3. Code implementation
The approach here is completely different as the Camera Middleware includes the ISP_Library and directly makes the required calls to the ISP APIs. It also handles the helper functions and the DCMIPP callback functions.
3.3.1. main function
...
static uint8_t Main_DestBuffer[2][MAX_PREVIEW_BUFFER_WIDTH * MAX_PREVIEW_BUFFER_HEIGHT * BPP_RGB888];
...
void App_Run()
{
CAMERA_SensorConfTypeDef sensor_conf = {0};
uint32_t frame_pitch;
int ret;
printf("**** Initializing ISP preview application ****\r\n");
/* Initialize the DCMIPP device and the camera */
if (Camera_Config(&phDcmipp, &sensor_conf, &frame_pitch) != 0)
{
printf("ERROR: can't configure camera\r\n");
Error_Handler();
}
/* Configure the display */
Display_Config(&sensor_conf, frame_pitch);
/* Start the main pipe */
if (CMW_CAMERA_DoubleBufferStart(DCMIPP_PIPE1,
(uint8_t *) Main_DestBuffer[0],
(uint8_t *) Main_DestBuffer[1],
CMW_CAPTUREMODE_CONTINUOUS) != CMW_ERROR_NONE)
{
printf("ERROR: Failed to start CAMERA\r\n");
Error_Handler();
}
printf("Camera and ISP started\r\n");
/* Application main loop */
while (1)
{
tx_thread_sleep(1);
ret = CMW_CAMERA_Run();
assert(ret == CMW_ERROR_NONE);
}
}
- "Camera_Config": This is implemented on application side to initialize the Camera Middleware Instance (See description below).
- "CMW_CAMERA_DoubleBufferStart": Start the camera capture in continuous mode with double buffering to avoid tearing effect. ISP_Init and ISP_Start are called here (in CMW_IMX335_Start).
- "CMW_CAMERA_Run": Run the background process. ISP_BackgroundProcess is called here (in CMW_IMX335_Run).
3.3.2. Camera_Config function
/**
* @brief Configure the camera
* @param hDcmipp Pointer to the dcmipp device
* @param Instance Camera instance
* @retval 0 if success, 1 otherwise
*/
static int Camera_Config(DCMIPP_HandleTypeDef **hDcmipp, CAMERA_SensorConfTypeDef *sensor_conf, uint32_t *frame_pitch)
{
CMW_CameraInit_t initConf = {0};
int32_t ret;
initConf.width = 0; /* width and height not specified => camera full resolution is set */
initConf.height = 0; /* width and height not specified => camera full resolution is set */
initConf.fps = 30;
initConf.mirror_flip = CMW_MIRRORFLIP_NONE; /* CMW_MIRRORFLIP_NONE or CMW_MIRRORFLIP_FLIP or CMW_MIRRORFLIP_MIRROR or CMW_MIRRORFLIP_FLIP_MIRROR */
ret = CMW_CAMERA_Init(&initConf, NULL);
if (ret != CMW_ERROR_NONE)
{
printf("ERROR: Failed to Initialize camera\r\n");
return 1;
}
*hDcmipp = CMW_CAMERA_GetDCMIPPHandle();
sensor_conf->CamImgWidth = initConf.width;
sensor_conf->CamImgHeight = initConf.height;
ComputePreviewSize(sensor_conf->CamImgWidth, sensor_conf->CamImgHeight, MAX_PREVIEW_BUFFER_WIDTH,
MAX_PREVIEW_BUFFER_HEIGHT, &sensor_conf->PreviewWidth, &sensor_conf->PreviewHeight);
/* Configure the DCMIPP pipes */
DCMIPP_Pipe1Config_Preview(sensor_conf, frame_pitch);
return 0;
}
- "CMW_CAMERA_Init": It handles DCMIPP initialization, IMX335 sensor initialization, specific pipe configuration and preview display settings
- "ComputePreviewSize": Get the preview size to respect aspect ratio of the camera