STM32WB0 Bluetooth® LE Stack Modularity and Integration

1. Introduction

This wiki describes to an application developer the STM32WB0 series Bluetooth® LE stack library modularity feature and how to integrate the Bluetooth® LE stack library on a user application.


Acronym definitions
Acronym Definition
ACI Application Controller Interface
HCI Host Controller interface
LL Link Layer
N/A Not Applicable

2. Bluetooth® LE Stack v4.x overview

2.1. Release contents

The Bluetooth® LE stack v4.x is provided on the STM32_BLE middleware available on the STM32CubeWB0 FW package.

Bluetooth® LE stack v4.x library architecture


The STM32_BLE Bluetooth® LE stack v4.x architecture provides the following features with related benefits:

  • Code is modular and testable in isolation:
    • High test coverage
  • Hardware-dependent parts are provided in source form:
    • Sleep timer module external to Bluetooth® Low Energy stack (Init API and tick API to be called on user main application)
    • NVM module external to Bluetooth® Low Energy stack (Init API and tick API to be called on user main application)
    • AES, PKA, RNG modules external to Bluetooth® Low Energy stack
  • Certification targets the protocol part only:
    • It reduces the number of stack versions, since hardware-related problems are mostly isolated in other modules.
    • It reduces the number of certifications.
  • It implements a flexible and robust radio activity scheduler
    • It allows the robustness against late interrupt routines (for example, flash writes and/or interrupt disabled by the user).
  • It reduces real-time constraint (less code in interrupt handler)
    • The system gives more time to applications.

Bluetooth® Low Energy stack v4.x is a standard C library, in binary format, which provides a high-level interface to control STMicroelectronics devices Bluetooth® Low Energy functionalities. The Bluetooth® Low Energy binary library provides the following functionalities:

  • Stack APIs for
    • Bluetooth® Low Energy stack initialization
    • Bluetooth® Low Energy stack application command interface (HCI command prefixed with hci_, and vendor-specific command prefixed with aci_)
    • Bluetooth® Low Energy stack state machine handling
  • Stack event dispatcher module
    • Inform user application about Bluetooth® Low Energy stack events which have been registered and not registered
  • Interrupt handler for radio IP

In order to get access to the Bluetooth® Low Energy stack functionalities, a user application is only requested to:

  • Call the related stack APIs
  • Handle the expected events through the provided stack dispatcher module
  • Link the Bluetooth® Low Energy stack binary library to the user application, as described in following figure:
Bluetooth® LE stack v4.x reference application


2.1.1. Folder structure

The Bluetooth® LE stack delivery contains four folders:

Bluetooth® LE stack v4.x library folder structure


  • The “doc” folder contains the current document and STM32WB0_BLE_Wireless_Interface.chm which describes the Bluetooth® LE stack v4.x Application Commands Interface (ACI) and the Host Commands Interface (HCI).
  • The “include” folder contains the header files of the Bluetooth® LE stack library interface. These files contain some definitions of constants and types and the declarations of ACI and HCI functions.
  • The “config” folder contains the Bluetooth® LE stack modular configuration options file.
  • The “lib” folder contains the Bluetooth® LE stack library variants described in the following section.

2.1.2. Library variants

The Bluetooth® LE stack library is delivered in only two variants:

  • One binary image containing the Bluetooth® LE Host + Controller Stack:
    • Single binary image stm32wb0x_ble_stack.a which can be customized at compile time through Bluetooth® LE stack modularity feature
  • One binary image addressing the Bluetooth® LE Controller Only Stack:
    • stm32wb0x_ble_stack_controller_only.a which can be customized at compile time through Bluetooth® LE stack modularity feature

2.2. Bluetooth® LE stack v4.x stack library modularity

The modular configuration options allow the user to exclude some features from the available Bluetooth® Low Energy stack binary library and decrease the overall flash memory.

Bluetooth® LE stack v4.x library modular options


In particular, Bluetooth® Low Energy stack v4.x provides the capability to enable/disable, at compile time, the following Bluetooth® Low Energy stack features based on a user-specific application scenario:

  • Enable/disable controller privacy
  • Enable/disable LE secure connections
  • Enable/disable scan capability
  • Enable/disable data length extension (valid only for the device supporting the data length extension feature)
  • Enable/disable LE 2M and LE coded PHYs features
  • Enable/disable extended advertising and scanning features
  • Enable/disable L2CAP, connection-oriented data service feature (L2CAP-COS)
  • Enable/disable periodic advertising
  • Enable/disable periodic advertising with responses
  • Enable/disable constant tone extension (where applicable)
  • Enable/disable LE power control and path loss monitoring
  • Enable/disable the connection capability, configuring support to connections:
    • If the connection option is disabled, connections are not supported; the device is a broadcaster only if the scan capability option is disabled, or a broadcaster and observer only if the scan capability option is enabled.
    • If the connection option is enabled, connections are supported; the device can only act as broadcaster or peripheral if the scan capability option is disabled, or any role (broadcaster, observer, peripheral, and scan) if the scan capability option is enabled.
  • Enable/disable the connection subrating
  • Enable/disable the channel classification
  • Enable/disable the broadcast isochronous streams
  • Enable/disable the connected isochronous streams

The scan capability option is linked to the new connection option as follows:

  • Observer disabled (scan capability option disabled) or enabled (scan capability option enabled) if the connection option is disabled
  • Observer and central disabled (scan capability option disabled) or enabled (scan capability option enabled) if the connection option is enabled

2.2.1. How to select the Bluetooth® Low Energy stack modular configuration options

The following Bluetooth® Low Energy stack preprocessor configuration options defined on file app_conf.h are used to activate/disactivate each modular configuration option (1: ENABLED; 0: DISABLED):

CFG_BLE_CONTROLLER_SCAN_ENABLED
CFG_BLE_CONTROLLER_PRIVACY_ENABLED
CFG_BLE_SECURE_CONNECTIONS_ENABLED
CFG_BLE_CONTROLLER_DATA_LENGTH_EXTENSION_ENABLED
CFG_BLE_CONTROLLER_2M_CODED_PHY_ENABLED
CFG_BLE_CONTROLLER_EXT_ADV_SCAN_ENABLED
CFG_BLE_L2CAP_COS_ENABLED
CFG_BLE_CONTROLLER_PERIODIC_ADV_ENABLED
CFG_BLE_ONTROLLER_PERIODIC_ADV_WR_ENABLED
CFG_BLE_CONTROLLER_CTE_ENABLED
CFG_BLE_CONTROLLER_POWER_CONTROL_ENABLED
CFG_BLE_CONNECTION_ENABLED
CFG_BLE_CONTROLLER_CHAN_CLASS_ENABLED
CFG_BLE_CONTROLLER_BIS_ENABLED
CFG_BLE_CONNECTION_SUBRATING_ENABLED
CFG_BLE_CONTROLLER_CIS_ENABLED

Notes:

  1. The modular configurations options can be generated on app_conf.h file through the STM32CubeMX tool, STM32_BLE Middleware, by using the Configuration, Application Configuration - Modular Options tab.
  2. The file app_conf.h is generated on STM32_BLE Projects Projects\NUCLEO-WB0xyz\Applications\BLE\{BLE_Application_Name}\Core\Inc, where NUCLEO-WB0xyz can be:
    • NUCLEO-WB09KE
    • NUCLEO-WB07CC
    • NUCLEO-WB05KZ

2.3. Library dependencies

The Bluetooth® LE stack v4.x library depends on (that is, must be linked with the following libraries):

  • Middlewares\ST\STM32_BLE\cryptolib\\cryptolib.a

The cryptolib.a library provides the AES CMAC encryption functionality required by Bluetooth® Low Energy stack.

2.4. Application compilation options

These compilation options are compulsory:

  • Plain 'char' is unsigned
  • Short enum:
    • For IAR® compiler, this option is set by default
    • Keil µvision® environment with ARM® CC compiler, the following option shall be added: -fshort-enums

In Keil µvision® environment with ARM® CC compiler, the following linker options are added:

  • --diag_suppress L6312W
  • --diag_suppress L6314W
  • --diag_suppress L6329W

In CubeIDE environment with GCC compiler, the following linker options are added:

  • -z noexecstack

3. Bluetooth® LE stack user interface

In order to use the main functions of the Bluetooth® LE stack library, the user application code must include “ble_stack.h”.

3.1. Bluetooth® LE stack initialization

BLE_STACK_Init function
Functions Parameters Return Value
BleStack_Init const BLE_STACK_InitTypeDef * BLE_STACK_InitParams tBleStatus

BLE_STACK_Init: The Bluetooth® LE stack initialization routine. This function is used to define the memory and configure the Bluetooth® LE stack.
All BLE_STACK_Init' parameters are described below:

BLE_STACK_Init function's parameters
BLE_STACK_InitTypeDef parameters Definition Value
uint8_t* BLEStartRamAddress Start address of the RAM buffer required by the Bluetooth® stack. It must be 32-bit aligned.
Use TotalBufferSize to calculate the correct size.
uint32_t TotalBufferSize TotalBufferSize return value, used to check the MACRO correctness.
uint16_t NumAttrRecords Maximum number of Attributes that can be stored in the GATT database.

When a GATT characteristic is added to the database a minimum of 2 attribute records are needed: one for the characteristic declaration and one for the characteristic value. On top of this, additional records may be needed based on the characteristic properties, in particular:
- If the characteristic has the notify or indicate property set, then one additional attribute record is needed.
- If the characteristic has the broadcast property set, then one additional attribute record is needed.
- If the characteristic has the extended property set, then one additional attribute record is needed.
In summary, one characteristic may need from 2 to 5 attribute records depending on the characteristic properties.

Minimum number is 2 attributes for each characteristic
uint8_t MaxNumOfClientProcs Maximum number of concurrent Client's Procedures. It must be ≤ NumOfRadioTasks
uint8_t NumOfRadioTasks Maximum number of simultaneous radio tasks.
Radio controller supports up to 128 simultaneous radio tasks, but actual usable max value depends on the available RAM.
(NumOfRadioTasks is used in the calculation of TotalBufferSize).
It must always be set to CFG_NUM_RADIO_TASKS defined on 2.4 GHz RADIO driver.
uint8_t NumOfEATTChannels Maximum number of simultaneously EATT channels the stack should support.
  • [0 - L2CAP_NumChannels]
uint16_t NumBlockCount Number of allocated memory blocks.
uint16_t ATT_MTU Maximum supported ATT_MTU size. [23, 1020] bytes
uint32_t MaxConnEventLength Maximum duration of the connection event in system time units of 625/256 us (~2.44 us) when the device is in Peripheral role It must be ≤ 4000 (ms)
uint16_t SleepClockAccuracy Sleep clock accuracy (ppm value).
  • It should be set according to accuracy of low speed crystal (ppm):
  • If the LSE is enabled, default value is 100 ppm.
  • If LSI is enabled (LSE is not enabled) the values to be used is 500 ppm.
uint8_t NumOfAdvDataSet Maximum number of advertising data sets, valid only when Advertising Extension Feature is enabled.
uint8_t NumOfSubeventsPAwR Maximum number of Periodic Advertising with Responses subevents. [1, 128]
uint8_t MaxPAwRSubeventDataCount Maximum number of subevent data that can be queued in the controller. [1, min(15,NumOfSubeventsPAwR )]
uint8_t NumOfAuxScanSlots Maximum number of slots for scanning on the secondary advertising channel. Valid only when advertising extension feature is enabled.
uint8_t NumOfSyncSlots Maximum number of slots to be synchronized. Valid only when Periodic Advertising and Synchronizing Feature is enabled.
  • 0, if Periodic Advertising is disabled (CFG_BLE_CONTROLLER_PERIODIC_ADV_ENABLED = 0)
  • [1 - (NumOfRadioTasks-1)], if Periodic Advertising is enabled (CFG_BLE_CONTROLLER_PERIODIC_ADV_ENABLED = 1)
uint8_t FilterAcceptListSizeLog2 Two's logarithm of Filter Accept, Resolving and advertiser list size.
uint16_t L2CAP_MPS The maximum size of payload data in octets that the L2CAP layer entity can accept. [0, 1024] bytes
uint8_t L2CAP_NumChannels Maximum number of channels in LE Credit Based Flow Control mode. [0, 255] bytes
It must be ≥ NumOfEATTChannels
uint8_t CTE_MaxNumAntennaIDs Maximum number of Antenna IDs in the antenna pattern used in CTE connection oriented mode.
  • [0x02 - 0x48], if CTE feature is enabled and supported from the device (CFG_BLE_CONTROLLER_CTE_ENABLED = 1)
  • 0, if CTE feature is disabled (CFG_BLE_CONTROLLER_CTE_ENABLED = 0)
uint8_t CTE_MaxNumIQSamples Maximum number of IQ samples in the buffer used in CTE connection oriented mode.
  • [0x09-0x52], if CTE feature is enabled and supported from the device (CFG_BLE_CONTROLLER_CTE_ENABLED =1)
  • 0, if CTE feature is disabled (CFG_BLE_CONTROLLER_CTE_ENABLED = 0)
uint8_t NumOfSyncBIG Maximum number of slots for synchronizing to a Broadcast Isochronous Group. [0, 1]
uint8_t NumOfBrcBIG Maximum number of slots for broadcasting a Broadcast Isochronous Group. [0, 1]
uint8_t NumOfSyncBIS Maximum number of slots for synchronizing to a Broadcast Isochronous Stream.
  • 0, if NumOfSyncBIG= 0
  • [1-2], if NumOfSyncBIG≠ 0
uint8_t NumOfBrcBIS Maximum number of slots for broadcasting a Broadcast Isochronous Stream.
  • 0, if NumOfBrcBIG = 0
  • [1-2], if NumOfBrcBIG≠ 0
uint8_t NumOfCIG Maximum number of Connected Isochronous Groups. [0, 2]
uint8_t NumOfCIS Maximum number of Connected Isochronous Streams. [0, 2]
uint8_t ExtraLLProcedureContexts Number of extra Link Layer Control Procedure contexts [0, 128]
uint16_t isr0_fifo_size Size of the internal FIFO used for critical controller events produced by the ISR (e.g. rx data packets). > 0 (Default value = 256)
uint16_t isr1_fifo_size Size of the internal FIFO used for non-critical controller events produced by the ISR (e.g. advertising or IQ sampling reports). > 0 (Default value = 768)
uint16_t user_fifo_size Size of the internal FIFO used for controller and host events produced outside the ISR. > 0 (Default value = 1024)

Example:

BLE_STACK_InitTypeDef BLE_STACK_InitParams = {
    .BLEStartRamAddress = (uint8_t*)dyn_alloc_a,
    .TotalBufferSize = BLE_DYN_ALLOC_SIZE,
    .NumAttrRecords = CFG_BLE_NUM_GATT_ATTRIBUTES,
    .MaxNumOfClientProcs = CFG_BLE_NUM_OF_CONCURRENT_GATT_CLIENT_PROC,
    .NumOfRadioTasks = CFG_BLE_NUM_RADIO_TASKS,
    .NumOfEATTChannels = CFG_BLE_NUM_EATT_CHANNELS,
    .NumBlockCount = CFG_BLE_MBLOCKS_COUNT,
    .ATT_MTU = CFG_BLE_ATT_MTU_MAX,
    .MaxConnEventLength = CFG_BLE_CONN_EVENT_LENGTH_MAX,
    .SleepClockAccuracy = CFG_BLE_SLEEP_CLOCK_ACCURACY,
    .NumOfAdvDataSet = CFG_BLE_NUM_ADV_SETS,
    .NumOfSubeventsPAwR = CFG_BLE_NUM_PAWR_SUBEVENTS,
    .MaxPAwRSubeventDataCount = CFG_BLE_PAWR_SUBEVENT_DATA_COUNT_MAX,
    .NumOfAuxScanSlots = CFG_BLE_NUM_AUX_SCAN_SLOTS,
    .FilterAcceptListSizeLog2 = CFG_BLE_FILTER_ACCEPT_LIST_SIZE_LOG2,
    .L2CAP_MPS = CFG_BLE_COC_MPS_MAX,
    .L2CAP_NumChannels = CFG_BLE_COC_NBR_MAX,
    .NumOfSyncSlots = CFG_BLE_NUM_SYNC_SLOTS,
    .CTE_MaxNumAntennaIDs = CFG_BLE_NUM_CTE_ANTENNA_IDS_MAX,
    .CTE_MaxNumIQSamples = CFG_BLE_NUM_CTE_IQ_SAMPLES_MAX,
    .NumOfSyncBIG = CFG_BLE_NUM_SYNC_BIG_MAX,
    .NumOfBrcBIG = CFG_BLE_NUM_BRC_BIG_MAX,
    .NumOfSyncBIS = CFG_BLE_NUM_SYNC_BIS_MAX,
    .NumOfBrcBIS = CFG_BLE_NUM_BRC_BIS_MAX,
    .NumOfCIG = CFG_BLE_NUM_CIG_MAX,
    .NumOfCIS = CFG_BLE_NUM_CIS_MAX,
    .ExtraLLProcedureContexts = CFG_BLE_EXTRA_LL_PROCEDURE_CONTEXTS, 
    .isr0_fifo_size = CFG_BLE_ISR0_FIFO_SIZE,
    .isr1_fifo_size = CFG_BLE_ISR1_FIFO_SIZE,
    .user_fifo_size = CFG_BLE_USER_FIFO_SIZE
  };

  /* Bluetooth<sup>®</sup> LE stack init */
  ret = BLE_STACK_Init(&BLE_STACK_InitParams);
  if (ret != BLE_STATUS_SUCCESS) {
    APP_DBG_MSG("Error in BLE_STACK_Init() 0x%02x\r\n", ret);
    Error_Handler();
  }

3.2. Bluetooth® LE stack process

The BLEStack_Process function runs all host stack layers’ dedicated processes through the BLE_STACK_Tick(). The function is scheduled as a sequencer task within the APP_BLE_Init() function, where the VTimer_Process() and NVM_Process() are also scheduled for calling, respectively, the HAL_RADIO_TIMER_Tick() and the NVMDB_Tick() functions. HAL_RADIO_TIMER_Tick() is the radio timer module tick function used to handle the related RADIO TIMER state machine. The NVMDB_Tick() is the NVM module tick function used to handle the related NVM module state machine.

BleStack_Process function
Functions Parameters Return Value
BleStack_Process None None


UTIL_SEQ_RegTask(1U << CFG_TASK_BLE_STACK, UTIL_SEQ_RFU, BLEStack_Process);
UTIL_SEQ_RegTask(1U << CFG_TASK_VTIMER, UTIL_SEQ_RFU, VTimer_Process);
UTIL_SEQ_RegTask(1U << CFG_TASK_NVM, UTIL_SEQ_RFU, NVM_Process);
ModulesInit();


The BLEStack_Process function call BLE_STACK_Tick() function as follows:

static void BLEStack_Process(void)
{
  APP_DEBUG_SIGNAL_SET(APP_STACK_PROCESS);
  BLE_STACK_Tick();

  APP_DEBUG_SIGNAL_RESET(APP_STACK_PROCESS);
}

The API BLE_STACK_Tick() function must be called in order to process the internal Bluetooth® Low Energy stack state machines and when there are Bluetooth® Low Energy stack activities ongoing. The BLE_STACK_Tick() function executes the processing of all host stack layers and it has to be executed regularly to process incoming link layer packets and to process host layers procedures.

3.3. Bluetooth® LE stack events

The ACI/HCI asynchronous events coming from the Bluetooth® LE stack must be handled in the BLE_STACK_Event. It checks the event type (GATT event handler, proprietary non-GATT events, standard events, or unregistered events).
This function will be called by the Bluetooth® LE stack with the following parameters:

BLE_STACK_Event function
Functions Parameters Return Value
BLE_STACK_Event
  • hci_pckt *hci_pckt: packet coming from Bluetooth® LE Stack
  • uint16_t length: packet length
void


The Bluetooth® Low Energy stack library framework provides an event dispatcher module, which allows the user application to register an event handler to get notification of GATT events to be processed. The event dispatcher framework is implemented on ble_evt.[ch] files available in the Middlewares\ST\STM32_BLE\evt_handler folder. When the event dispatcher is used (recommended option), the application should register a callback for each service and each client implemented, since a GATT event is usually relevant to only one service and/or one client. When a GATT event is received, it is notified to the registered handlers. When no registered handler acknowledges positively the GATT event, it is reported to the application. A GAP event is not relevant to either a service or a client. For this reason, it is always sent to the application.

Notes:

1. The maximum number of GATT registered handlers is controlled by BLE_CFG_MAX_NBR_GATT_EVT_HANDLERS macros.

2. This handler is called from BLEStack_Process() context.

The BLEEVT_RegisterHandler API registers a handler to be called when a generic non-GATT event is received from the Bluetooth® LE core stack. A Bluetooth® profile can use this function to be notified when an event is received.

BLEEVT_RegisterHandler function
Functions Parameters Return Value
BLEEVT_RegisterHandler BLEEVT_HciPcktHandlerFunc_t EvtHandlerFunc: Service handler that is called to report a non-GATT event. void


Notes:

1. The maximum number of these registered handlers is controlled by BLE_CFG_MAX_NBR_EVT_HANDLERS macros.

2. If the handler returns BLEEVT_Ack, no other registered handlers are called.

3. This handler is called from BLEStack_Process() context.

The BLEEVT_App_Notification API callback is triggered when either:

  • A standard HCI event is received from the Bluetooth® LE core device
  • A proprietary event not positively acknowledged by the registered handler is received from the Bluetooth® LE core device

Note: This callback is triggered in the BLEStack_Process() context.


BLEEVT_App_Notification

BLEEVT_App_Notification function
Functions Parameters Return Value
BLEEVT_App_Notification
  • const hci_pckt *hci_pckt: The user event received from the Bluetooth® LE core device
void


Example:

void BLEEVT_App_Notification(const hci_pckt *hci_pckt)
{
.....
.....

  case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:
        {
          hci_le_connection_complete_event_rp0 *p_conn_complete;
          p_conn_complete = (hci_le_connection_complete_event_rp0 *) p_meta_evt->data;

          connection_complete_event(p_conn_complete->Status,
                                    p_conn_complete->Connection_Handle,
                                    p_conn_complete->Peer_Address_Type,
                                    p_conn_complete->Peer_Address,
                                    p_conn_complete->Connection_Interval,
                                    p_conn_complete->Peripheral_Latency,
                                    p_conn_complete->Supervision_Timeout);
        }
        break;
.....
.....
}
3.3.1. Commands and events interfaces

Each ACI/HCI command has its own interface, e.g. the HCI reset command can be called through the “hci_reset” interface.
The HCI commands and the ACI commands interfaces for GAP, GATT, HAL, L2CAP layers can be found in Middlewares\ST\STM32_BLE\stack\include\ble_api.h.
The HCI events and the ACI events interfaces for GAP, GATT, HAL, L2CAP layers can be found in Middlewares\ST\STM32_BLE\stack\include\ble_events.h.

4. Bluetooth® LE stack porting

The Bluetooth® LE stack uses some generic HW features, but allows the application to define them by using HW drivers or emulating some of them by SW code.
All the required porting interfaces by the Bluetooth® LE stack are defined in the bleplat.h
The following features are used and need to be implemented on the application side:

  • NVM: non-volatile memory used by the security database of the Bluetooth® LE stack
  • Sleep Timer: used by several components of the Bluetooth® LE stack
  • AES: advanced encryption standard used by the security manager layer of the Bluetooth® LE stack
  • PKA: public key accelerator used by the controller in the Bluetooth® LE stack
  • RNG: random number generation used by the controller in the Bluetooth® LE stack

4.1. Bluetooth® LE platform functions

All the BLEPLAT functions are called from the Bluetooth® LE stack process or commands. Those functions return one of the following status values:

BLEPLAT functions' returns
Status Value Description
BLEPLAT_OK 0 The function did the job and returns an OK status.
BLEPLAT_FULL -1 The function exits because the HW resource is full.
BLEPLAT_BUSY -2 The function is busy and is not available for the requested operation.
BLEPLAT_EOF -3 The function exits and notifies the HW resource (memory for example) reached the end.


All the BLEPLAT PKA functions are called from the Bluetooth® LE stack process or commands. Those functions return one of the following status values:

BLEPLAT PKA functions' returns
Status Value Description
BLEPLAT_PKA_SUCCESS 0 The function did the job and returns an OK status.
BLEPLAT_PKA_ERROR -1
BLEPLAT_PKA_ERR_BUSY -2 The function is busy and is not available for the requested operation.
BLEPLAT_PKA_ERR_PARAM -3
BLEPLAT_PKA_ERR_PROCESS -4

4.1.1. NVM functions

The NVM functions are used to store security database information (security and GATT records) in the NVM, read from the NVM, compare data with the stored data in the NVM and clear the security database or some of it.

BLEPLAT NVM functions
Functions Parameters Return Value
BLEPLAT_NvmAdd:
Store data in the NVM
  • BLEPLAT_NvmRecordTypeDef Type: The type of data to be stored can be:
    • BLEPLAT_NVM_REC_SEC: security data
    • BLEPLAT_NVM_REC_GATT: GATT data
    • BLEPLAT_NVM_REC_DEVICE_ID
  • const uint8_t *pData: The data buffer to be stored
  • uint16_t Size: The size of data to be stored
  • const uint8_t *pExtraData: If there is extra data to be stored too. If not, this parameter shall be passed with NULL value
  • uint16_t ExtraSize: The size of extra data
int: One of the return values described in the section 4.1
BLEPLAT_NvmGet:
Read data from the NVM
  • BLEPLAT_NvmSeekModeTypeDef mode: The mode of NVM reading:
    • BLEPLAT_NVM_FIRST: used to read the first record of NVM
    • BLEPLAT_NVM_NEXT: used to read the next record (after a previous call to BLEPLAT_NvmGet)
    • BLEPLAT_NVM_CURRENT: used to read the same record again (after a previous call to BLEPLAT_NvmGet)
    • BLEPLAT_NVM_ALL: used to read all records
  • BLEPLAT_NvmRecordTypeDef type: The type of data to be read can be:
    • BLEPLAT_NVM_REC_SEC: security data
    • BLEPLAT_NVM_REC_GATT: GATT data
    • BLEPLAT_NVM_REC_DEVICE_ID
  • uint16_t Offset: The offset from which the NVM starts the read an operation.
  • uint8_t *pData: The pointer to data read by the function
  • uint16_t Size: The size of data to be read
int: One of the return values described in the section 4.1
BLEPLAT_NvmCompare:
Compare passed data as parameter with data stored in the NVM
  • uint16_t Offset: The offset from which the NVM starts the comparison
  • const uint8_t *pData: The data to be compared with stored data in the NVM
  • uint16_t Size: The size of data to be compared
int:
  • if zero, the comparison is successful
  • if different from zero. the comparison is failed
BLEPLAT_NvmDiscard:
Clear a block from the NVM or the whole NVM, storing the security database (security and GATT records)
BLEPLAT_NvmSeekModeTypeDef mode: Mode of deleting data from the NVM can be:
    • BLEPLAT_NVM_FIRST: used to erase the first record of NVM
    • BLEPLAT_NVM_NEXT: used to erase the next record (after a previous call to BLEPLAT_NvmGet)
    • BLEPLAT_NVM_CURRENT: used to erase the current record
    • BLEPLAT_NVM_ALL: used to erase all records
None

4.1.2. Timer functions

The timer functions are used by the Bluetooth® LE stack to handle all procedures which are time dependent.

BLEPLAT Timer functions
Functions Parameters Return Value
BLEPLAT_StartTimer:
Start the Timer. Starts a one-shot virtual timer for the given absolute timeout value expressed in internal system time units.
  • BLEPLAT_TimerHandleTypeDef *TimerHandle: The virtual timer
  • uint64_t Time: Absolute time expressed in STU.
int:
  • 0, if the timerHandle is valid.
  • 1, if the timerHandle is not valid. It is already started. section 4.1
BLEPLAT_StopTimer:
Stop the timer
BLEPLAT_TimerHandleTypeDef *TimerHandle: The virtual timer None

4.1.3. AES functions

The AES functions are used by the Bluetooth® LE stack to encrypt a 128-bit single block or to compute CMAC which is needed by Bluetooth® LE security manager.

BLE PLAT AES functions
Functions Parameters Return Value
BLEPLAT_AesEcbEncrypt:
Encrypt a single 128-bit block with a 128-bit key
  • const uint32_t *plainTextData: table of 16 bytes that contains the key to use (Little Endian format)
  • const uint32_t *key: table of 16 bytes that contains the block to encrypt
  • uint32_t *encryptedData: table of 32 bytes that is filled by the function with the encrypted block
None

4.1.4. PKA functions

The PKA functions are used by the Bluetooth® LE stack to compute the P-256 public key and the DH key used for Bluetooth® LE secure connections.

BLEPLAT PKA functions
Functions Parameters Return Value
BLEPLAT_PkaStartP256Key:
Start P-256 public key generation
  • const uint32_t *private_key: table of 8 x 32-bit words that contains the P-256 private key (Little Endian format)
  • BLEPLAT_PkaFuncCb FuncCb: Pointer to a PKA callback function
int: One of the return values described in the section 4.1
BLEPLAT_PkaStartDhKey:
Start DH key computation
  • uint32_t *private_key: table of 8 x 32-bit words that contains the local P-256 private key (Little BLEPLAT_PkaStartDHkeyformat)
  • uint32_t *public_key: table of 32 x 32-bit words that contains the remote P-256 public key (Little Endian format)
  • BLEPLAT_PkaFuncCb FuncCb: Pointer to a PKA callback function
int: One of the return values described in the section 4.1

4.1.5. RNG functions

This function is called by the Bluetooth® LE stack to retrieve random values.

BLEPLAT RNG function
Functions Parameters Return Value
BLEPLAT_RngGet16:
Get random values a 16-bit
uint16_t16 *num: pointer to the random value returned. None
BLEPLAT_RngGet32:
Get random values a 32-bit
uint32_t *num: pointer to the random value returned. None

5. References

Bluetooth® Low Energy stack v4.x Programming Guidelines (PM0274)