Introduction to Hardware Video Encoding with STM32

1. Introduction

The VENC IP, integrated into the STM32/N6 device, provides hardware acceleration for H.264 and JPEG encoding.

This includes pre-processing for color conversion, cropping, and rotation.

Coupled with the DCMIPP IP, it makes real-time video encoding and streaming possible at a very low CPU load cost.

2. H264

2.1. H264 supported standard

2.1.1. H264 Input Formats

  • YCbCr 4:2:0 planar & semi-planar
  • YCrCb 4:2:0 semi-planar
  • YCbYCr & CbYCrY 4:2:2 interleaved
  • RGB & BRG 444,555, 565, 888

2.1.2. H264 Input Resolutions

  • Supported encoded width from 132 pixels up to 4080 pixels // width must be a multiple of 4 pixels
  • Supported encoded height from 96 pixels up to 4080 pixels // height must be even
  • Input width alignment depends on input format
    • input width should be a multiple of 16 pixels for YUV420 planar
    • input width should be a multiple o 8 pixels for YUV420 semi-planar and YUV422 interleaved inputs

In this context,input width is the width of the source image presented to the encoder, while encoded width is the width of the cropped image that is actually encoded.

2.1.3. H264 Output Standard

2.1.3.1. Codecs: H264 (MPEG4_Part10/AVC)
  • Profiles: Baseline/Main/High up to 4.1
  • Output format: byte unit stream or NAL unit stream
  • H264 / MVC :Stereo High

Information
Internally, the encoder handles images only in 4:2:0 format

Working with more than 12 bits per pixels input images brings no quality improvement.


Information
VENC is multi-instance capable

VENC can interleave frame encoding of several different streams.

This is because it does not keep the internal status for each stream, but just the reference frames located in external memory.

Each instance may run in parallel with different encoding parameters (resolution, for example).

The following pages focus on a classic use case where only one stream captured by a camera is encoded.

2.2. H264 Encoding Data Flow

2.2.1. DCMIPP

The DCMIPP (Digital Camera Memory Image Pixel Processor) has a crucial role in real-time encoding use cases.

It is connected to a camera through the CSI-2 serial interface and embeds an ISP (Image Signal Processor) block.

It provides three pipelines as output:

  • Pipe0 ("dump pipe"): Dumps raw data (not connected to ISP).
  • Pipe1 ("main pipe"): Feeds the encoder after frame processing (downsizing, color conversion, ...)
  • Pipe2 ("ancillary pipe"): Used for display (RGB only) or AI, etc...


DCMIPP/Pipe1 may output a VENC-compatible format, typically YUV422 or YUV420.

Coupled with VENC, DCMIPP can be used in two modes:

  • Frame mode

In this mode, DCMIPP captures a complete frame and stores it in external memory. When the software is signaled for frame completion, it is responsible for calling VENC and providing it with the frame location in memory.

  • Slices mode / Hardware Handshake

In this mode, DCMIPP captures a certain number of lines (typically 32 lines). When done, it directly signals VENC, which in turn encodes this set of lines. This capture/encode sequence is reiterated until the frame is fully encoded. The software is signaled when the whole frame is finished being encoded. This mode does not require storing the complete input frame. This reduces the memory footprint and allows the input frame to be placed in internal memory. In addition to this reduction in footprint, it results in optimized memory bandwidth.

  • Frame mode vs Slices Mode: Pros and Cons
Pros Cons
Frame Mode Real-time capture by the DCMIPP is decoupled from offline encoding by the VENC Extra bandwidth is required to store the frame in external memory (by the DCMIPP) and to retrieve it from the VENC.
Slices Mode Permits the transfer of the frame using only the internal memory from the DCMIPP to the VENC, thus avoiding the double bandwidth to the external memory The VENC is coupled with the real-time DCMIPP, so the VENC's pace is mandated to follow the DCMIPP's pace, smoothed only every (typically) 32 lines


Information
Either wording : 'slices mode' or 'Hardware Handshake' mode is used. in the folllowing pages.

The 'Hardware handshake' refers to the protocol between the DCMIPP and the encoder to perform encoding by slices

.

2.2.2. Encode Data Flow Example

Video Encode from Camera


Information
The Pipe2 path is givens as an example of parallel use case. Another typical use case could be AI (face recognition for example)

.

  1. Camera capture:
    • The DCMIPP pipeline supports a maximum resolution of 5 megapixels (after a decimation factor of 1, 2, 4, or 8).
    • Therefore, a maximum 40-megapixel raw sensor can be connected (5 megapixels * 8).
    • Horizontal and vertical decimation is supported
  2. Uncompressed Frame written in Memory
    • Frame format and resolution converted by DCMIPP
    • Uncompressed frame may be located in Internal or external memory depending on encoding mode (HW handshake, frame resolution,) and memory available.
    • YUV 4:2:0 is the best format for memory footprint and is the native format of the encoder
  3. Uncompressed Frame Frame Read by VENC
  4. VENC Reads Reference Frame from memory (YUV 4:2:0)
    • Note that VENC reads Chrominance (UV) data twice resulting in a average bandwidth of 16bpp
  5. VENC Writes Reference Frame to memory (YUV 4:2:0)
    • Reference Frame in external memory depending on its resolution and memory available
  6. VENC uses its internal memory (VENCRAM) for encode
  7. VENC writes compressed output stream


2.3. Code Footprints

ro code ro data rw data
50 KBytes 62 KBytes 512 Bytes
112 KBytes

2.4. VideoBuffers Footprints

The memory footprints have been monitored while running real use cases (they are measured, not calculated).

  • In Frame mode and Hardware Handshake mode
  • For 1080p, 720p and 480p
  • With a YUV 4:2:0 input frames format
  • Encoding with "Main" profile

2.4.1. Frame Mode Encode

Buffer Location Data IP 1080p 720p 480p
External RAM Raw Frame(*) DCMIPP 5.93 MBytes 2.64 MBytes 1.10 MBytes
External RAM Reference Frame +VENC buffers (**) VENC (Internal) 6.55 MBytes 2.92 MBytes 1.25MBytes
Internal SRAM H264 Stream VENC (Out) 88.22 KBytes 31.98 KBytes 17.81 KBytes
Total - - 12.57 MBytes 5.59 MBytes 2.37 MBytes

(*) Frame mode uses a 'ping-pong' buffer as the input frame.

The total size used for the input raw frame is therefore 2 x Frame Height x Frame Length x 1.5 (12 bits per pixel in YUV 4:2:0).


(**) The encoder may use one or two references frame:

Single buffer: The encoder will use only one reference buffer. This saves some memory but it will restrain the encoder by not being able to discard coded frames.

Using a single buffer should be considered if it is needed to be put in the internal memory.

Double buffer: This gives the encoder a possibility to discard a coded frame to fulfill the requirements of HRD (Hypothetical Reference Decoder). This is the default mode.

The above number is using double buffer.

2.4.2. Slices Mode Encode

The following table shows the memory footprints when encoding 32 line slices.

Buffer Location Data IP 1080p 720p 480p
External RAM Reference Frame + VENC Buffers VENC (Internal) 4.56 MBytes 2.04 MBytes 0.91 MBytes
Internal SRAM Raw Frame (Slice) DCMIPP 90.03 KBytes 60.03 KBytes 37.53 KBytes
Internal SRAM H264 Stream VENC (Out) 96.04 KBytes 33.54 KBytes 18.14 KBytes
Total - - 4.74 MBytes 2.13 MBytes 0.96 MBytes

Please note that the compressed stream bitrate may vary significantly depending on the input stream and encoding parameters. The numbers above were measured while encoding an almost static image. In any case, it remains obviously insignificant in comparison to the uncompressed buffer.

2.5. Performances

As a standalone peripheral, VENC supports 1080p30 encoding.

Nevertheless, as real-time encoding involves a complete acquisition, encoding, and data transport flow, a bottleneck related to memory bandwidth may be encountered, especially when parallel use cases run simultaneously.

To characterize realistic performances, the following use case has been tested:

  • Camera acquisition (IMX335 and OV5640)
  • H.264 encoding (Main profile)
  • RTSP transmission

The quality of the encoded stream, the frame rate, and the stability were monitored.

The test is considered successful if:

  • The real frame rate matches the expected frame rate (no frames lost)
  • The quality of the output stream is good
  • The use case is stable (overnight or 24-hour tests)

2.6. OV5640

Encoding Mode 1080p20(*) 720p30 480p30
Frame Ok Ok Ok
Slices Ok Ok Ok

2.7. IMX335

Encoding Mode 1080p20(*) 720p30 480p30
Frame Ok Ok Ok
Slices Ko (**) Ok Ok


(*) 1080p20 is the highest achievable framerate

(**) Please refer to chapter H264 Hardware Handshake encoding for an explanation of the specific issues related to encoding in 'Hardware Handshake' mode.

2.8. Bitrate Control

This chapter describes how to activate bitrate control algorithm inside H264 encoder software stack.

H264EncRateCtrl structure helps user to configure bitrate control parameters.

Rate control is considered enabled when pictureRc, pictureSkip or hrd is enabled.

The target bitrate must be set in ""bitPerSecond". The unit is in bits per second (bps). When HRD is enabled the bitrate must be within the limits set for the encoder level. The valid range is between 10000 and 40000000. Depending on the chosen H264 encoder level.

Other parameters can be found in H264 encoder API documentation: "VC8000NanoE.V50x.Video.Encoder.API-H.264-v1.01-20200323.pdf". This documentation is only available on request and with valid and active NDA.

H264EncSetRateCtrl() function is used to set the rate control parameters of the encoder. This function should be called before starting the stream. For a dynamic setting, HRD must be disabled, and the function can then be called between frames to set new rate control parameters. This, however, will reset the rate control and is recommended to do at the end of GOP.

2.9. Low Power

2.9.1. Power saving strategy

  • Switch off unused memories & peripherals
  • Enter Sleep() mode in between each frame capture/processing
    • DCMIPP is still working in sleep() mode
    • DCMIPP interrupts wakes up the device which  perform frame encoding  and push to transport before going back to sleep() mode
  • Decrease CPU/SYS clocks frequency as much as possible
  • No dynamic change of clock frequencies (could be done for optimization).

2.9.2. Power consumption

To measure realistic performances the following use case was tested:

  • Camera acquisition (IMX335 )
  • H.264 encoding (Main profile)
  • RTSP transmission

The quality of the encoded stream, the frame rate, and the stability were monitored.

The measure is considered valid if:

  • The real frame rate matches the expected frame rate (no frame lost)
  • The quality of the output stream is good
  • The use case is stable

The measurements were done using STLINK-V3 on STM32N6570-DK, reworked for power injection through external SMPS (see H264 power consumption setup).

They are related to VddCore only.

Measurements have been done on a single board and may slightly vary from one board to another.

  • CPU: 800 MHz / AXI: 400MHz
Resolution / Frame rate Frame Slices
480p30 98.37 mW 111.03 mW
720p30 111.32 mW 116.93 mW
1080p15 107.58 mW 112.45 mW
1080p20 117.99 mW N/A
  • CPU: 600 MHz / AXI: 400MHz
Resolution / Frame rate Frame Slices
480p30 74.04mW 84.41 mW
720p30 84.24 mW 89.25 mW
1080p15 80.97 mW 84.79 mW
1080p20 88.83 mW N/A
  • CPU: 25 MHz / AXI: 200MHz
Resolution / Frame rate Frame Slices
480p30 50.53 mW 54.05 mW
720p20 51.52 mW 54.22 mW
720p30 58.80 mW N/A
  • CPU: 12.5 MHz / AXI: 400MHz
Resolution / Frame rate Frame Slices
480p20 56.98 mW 65.94 mW
480p30 61.80 mW N/A
720p20 63.45 mW 68.81 mW
  • CPU: 12.5 MHz / AXI: 200MHz
Resolution / Frame rate Frame Slices
480p20 46.00 mW 50.21 mW
480p30 50.32 mW N/A
720p20 51.36 mW N/A

3. (M)JPEG

The video encoder integrated in the STM32N6 supports JPEG still image encoding.

When the encoder produces a complete JPEG image for each captured frame, and these frames are continuously transported over USB Video Class or RTP/RTSP, the resulting stream is an MJPEG stream.

The JPEG path is simpler because each encoded picture is self-contained. There are no reference frames, no group of pictures (GOP) management, and no inter-picture dependencies.

This reduces the memory footprint and bandwidth requirements of the encoding layer, allowing a smaller encoding footprint and higher frame rates.

However, this has a cost: depending on the content and quality settings, MJPEG can be several times larger than H.264.

Also, depending on the transport layer bandwidth and jitter, a higher bitrate may require larger output buffers

Note that both frame mode and hardware handshake modes are supported for JPEG encoding, as for H.264 encoding.

3.1. JPEG supported standard

3.1.1. JPEG Input Formats

  • YUV420 planar and semi-planar
  • YUV422 interleaved
  • RGB and BGR 444, 555, 565, 888 and 10:10:10

3.1.2. JPEG Input Resolutions

  • Supported encoded width from 96 pixels up to 8176 pixels // width must be a multiple of 4 pixels
  • Supported encoded height from 32 pixels up to 8176 pixels // height must be even
  • Input width must be a multiple of 16 pixels

In this context,input width is the width of the source image presented to the encoder, while encoded width is the width of the cropped image that is actually encoded.

3.1.3. JPEG Output Standard

3.1.3.1. Codecs: JPEG ITU-T T.81 / ISO/IEC 10918-1
  • Profiles:Baseline interleaved
  • JPEG/JFIF compliant stream, with JFIF 1.02 support


3.2. Quantization level : Picture Size vs Quality

The quantization level is an input parameter of the JPEG encoding API.

It determines the quality of the encoded image. A higher quantization level results in better image quality.

The size of the encoded image is also determined by the quantization level, as shown in the table below.

Q level CIF
352x288
(KBytes)
VGA
640x480
(KBytes)
MP1
1280x864
(KBytes)
MP2
1600x1232
(KBytes)
MP5
2560x1968
(KBytes)
0 4 9 26 42 97
1 6 13 34 52 115
2 7 16 42 62 134
3 9 19 47 70 150
4 10 21 54 78 166
5 12 25 62 88 186
6 13 29 70 105 229
7 17 38 92 145 326
8 24 53 158 258 595
9 42 94 561 823 1665

3.3. Footprints

Compared to H.264, the main difference is that the JPEG encoder does not need storing a reference frame, so it requires only a few kilobytes of memory.

Besides input frames and internal VENC buffers, the size required for the JPEG output buffer depends on the quantization level and application constraints.

For example, a 1080p15 stream at quantization level 9 outputs a bitrate of about 100 Mbit/s.

If the application and transport layer require 100 ms of buffering, the total size required is about 1.2 Mbytes.

3.3.1. Slices Mode Encode

The following table shows the memory footprints when encoding 32 line slices.

Data IP 1080p
VENC Buffers VENC (Internal) 10 KBytes
Raw Frame (Slice) DCMIPP 90.03 KBytes
100 KBytes

The output buffer size is not included in this table and must be added depending on the application use case.

3.3.2. Frame Mode Encode.

Data IP 1080p
VENC Buffers VENC (Internal) 10 KBytes
Raw Frame DCMIPP 5.93 MBytes
5.94 MBytes

The output buffer size is not included in this table and must be added depending on the application use case.