| Back to main page |
|---|
1. MQTT presentation
These applications demonstrate an MQTT client over Wi-Fi®, connecting to an MQTT broker to publish telemetry data and receive parameter updates or commands from the cloud.
Two MQTT demonstrations are available in the project directory:
| Project name | Description |
|---|---|
| ST67W6X_MQTT | It exercises the capabilities of the network co-processor (ST67W611M1), which embeds the MQTT client, LwIP, and Wi-Fi® stack. This demonstration is developed for the NUCLEO-U575ZI-Q host board. |
| ST67W6X_MQTT_LWIP | It exercises the capabilities of the network co-processor (ST67W611M1), which embeds the Wi-Fi® stack. The MQTT client and LwIP are offloaded and present in the host code. This demonstration is developed for the NUCLEO-H563ZI host board. |
These applications periodically publish data to an MQTT broker (this example uses EMQX, but it can be changed to a preferred MQTT broker). A subscription to the same topic is also done to be able to monitor the published data.
The MQTT uses the TCP protocol for data transmission and can be encrypted using TLS.
In the applications, the subscribed topic can be used to receive additional 'control' fields. Two actions are predefined:
- Change the LED state on the host board
- Reboot the host
To monitor data sent and received to/from the topics, an MQTT client can be installed on a PC, smartphone, or tablet. By subscribing to the configured topics, the client receives notifications each time the device publishes data to those topics.
2. Requirements
2.1. Software and system requirements
The software requirements are as follows (minimum IDE versions):
- STM32CubeIDE toolchain V2.1.0 [1].
- IAR Embedded Workbench for Arm (EWARM) toolchain V9.30.1
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.39
Programmer:
- STM32CubeProgrammer [2] to program the board with a pre-generated binary file
HyperTerminal:
- Use the application through the serial link
- Open a HyperTerminal client connected to the host ST-LINK COM port
The serial COM port must be configured as shown below:
| Baudrate | 921600 |
| Data | 8b |
| Stopbit | 1b |
| Parity | None |
| Flow control | None |
| Rx | LF |
| Tx | LF |
| Local Echo | Off |
For further details, refer to the HyperTerminal setup page.
2.2. Hardware requirements
This example runs on the NUCLEO-U575ZI-Q [3] board combined with the X-NUCLEO-67W61M1 board.
The X-NUCLEO-67W61M1 board is plugged into the NUCLEO-U575ZI-Q board through the Arduino connectors:
- The 5V, 3V3, GND through the CN6
- The SPI (CLK, MOSI, MISO), SPI_CS and USER_BUTTON signals through the CN5
- The BOOT, CHIP_EN, SPI_RDY and UART TX/RX signals through the CN9
3. ST67W6X_MQTT demonstration description
3.1. Project directory
The "ST67W6X_MQTT" and "ST67W6X_MQTT_LWIP" demonstrations are available by downloading the X-CUBE-ST67W61 Expansion Package.
Refer to the Project directory wiki page for project directory information.
3.2. Project description
3.2.1. Topology structure
The application on the host uses the network coprocessor as a Wi-Fi® station modem. It connects to a Wi-Fi® local access point (hotspot/gateway/etc.) which needs an internet connection. Once the connection is established, the host application connects to an MQTT broker to publish and subscribe to topics.
The host application uses the MEMS sensor board to generate telemetry data to be sent to the MQTT broker. It also uses an SNTP request to get the current time and date, which are added to the telemetry data.
Additionally, the host application can receive commands from the MQTT broker to change the LED state or to reboot the device.
3.2.2. Project execution
The different steps in the application initialization are described below:
| Description | Function | File | |
|---|---|---|---|
| ST67W6X_MQTT | ST67W6X_MQTT_LWIP | ||
| Initialize the system (HAL, Clocks, SPI, I2C, UART, RTC, GPIO) | main() | Core/Src/main.c | |
| Create an ST67W6XTask that starts the main application | MX_ST67W6X_Init() | ST67W6X/App/app_st67w6x.c | |
| Start all configured tasks | osKernelStart() | cmsis_os2.c | |
| Run the application entry function main_app() | ST67W6X_Task() | ST67W6X/App/app_st67w6x.c | |
| Initialize the logging utility to forward all traces on UART peripheral | W6X_Util_Init() | ST67W6X_Network_Driver/Core/w6x_sys.c | |
| Initialize the application callbacks to receive events from ST67W6X_Network_Driver | W6X_RegisterAppCb() | ST67W6X_Network_Driver/Core/w6x_sys.c | |
| Initialize the ST67W6X_Network_Driver Power up the network co-processor Display global identification |
W6X_Init() | ST67W6X_Network_Driver/Core/w6x_sys.c | |
| Initialize the ST67W6X_Network_Driver Wi-Fi® module Set the STA mode Enable the DHCP client Configure the country code Set the hostname |
W6X_WiFi_Init() | ST67W6X_Network_Driver/Core/w6x_wifi.c | |
| Initialize the ST67W6X_Network_Driver Network module | W6X_Net_Init() | - | ST67W6X_Network_Driver/Core/w6x_net.c |
| Initialize the network interface, the LwIP stack and the DHCP Client | - | MX_LWIP_Init() | LWIP/App/lwip.c |
| Initialize the ST67W6X_Network_Driver MQTT module Register pre-allocated buffer to receive subscription messages |
W6X_MQTT_Init() | - | ST67W6X_Network_Driver/Core/w6x_mqtt.c |
The different steps in the application process are described below:
| Description | Function | File | |
|---|---|---|---|
| ST67W6X_MQTT | ST67W6X_MQTT_LWIP | ||
| Connect the Wi-Fi® station device to an available access point | W6X_WiFi_Connect() | ST67W6X_Network_Driver/Core/w6x_wifi.c | |
| Enable the time synchronization through a remote SNTP server | W6X_Net_SNTP_SetConfiguration() | sntp_init() | ST67W6X_Network_Driver/Core/w6x_net.c |
| Retrieve the SNTP time to update the RTC time configuration | W6X_Net_SNTP_GetTime() | - | ST67W6X_Network_Driver/Core/w6x_net.c |
| Initialize the sensor expansion board | Sys_Sensors_Init() | X-CUBE-MEMS1/App/sys_sensors.c | |
| Configure the device for an MQTT broker | W6X_MQTT_Configure() | - | ST67W6X_Network_Driver/Core/w6x_mqtt.c |
| - | mqtt_init() | MQTT-C/src/mqtt.c | |
| Connect the device to an MQTT broker | W6X_MQTT_Connect() | - | ST67W6X_Network_Driver/Core/w6x_mqtt.c |
| - | mqtt_connect() | MQTT-C/src/mqtt.c | |
| Start a topic subscription. When a new message is received, a callback catches and parses the frame. |
W6X_MQTT_Subscribe() | - | ST67W6X_Network_Driver/Core/w6x_mqtt.c |
| - | mqtt_subscribe() | MQTT-C/src/mqtt.c | |
| Publish a new message on the selected topic. The RTC time is always set by calling HAL_RTC_GetTime() and HAL_RTC_GetDate(). If a sensor board is available, the environmental measures are added in the frame by calling Sys_Sensors_Read() |
W6X_MQTT_Publish() | - | ST67W6X_Network_Driver/Core/w6x_mqtt.c |
| - | mqtt_publish() | MQTT-C/src/mqtt.c | |
Two topic subscriptions are started:
- /devices/<MQClientID>/control
- /sensors/<MQClientID>
One topic is used for periodic publication (every 2 seconds): /sensors/<MQClientID> The device receives and displays the subscribed messages on the logging trace.
The publication message format is defined as follows:
{ "state":
{ "reported":
{
"time": "%y-%m-%d %H:%M:%S",
"rssi": %d,
...
}
}
}
The "state.reported" object hierarchy is used to help with interoperability with first tier cloud providers.
When a message from the subscribed topic is received through the APP_mqtt_cb() callback (publish_callback_1() for the ST67W6X_MQTT_LWIP), defined by W6X_RegisterAppCb() (mqtt_init() for the ST67W6X_MQTT_LWIP), the MQTT frame is pushed into a subscription queue.
An application task, Subscription_process_task(), pulls and parses each frame stored in the subscription queue using the cJSON middleware to extract all fields and values from the JSON-formatted message.
Some fields are predefined as described below:
| Field | Value type | Description |
|---|---|---|
| time | String | Current date and time. Format: "%y-%m-%d %H:%M:%S" |
| mac | String | MAC address of device. Format: "00:00:00:00:00:00" |
| rssi | Integer | Current RSSI level of the access point (in db) |
| temperature | Float | Temperature from sensor board (in degC) |
| humidity | Float | Relative humidity from sensor board (in percent) |
| pressure | Float | Pressure from sensor board (in mbar) |
| LedOn | Bool | Set the green led state available on the host board |
| Reboot | Bool | Reboot the host board |
3.3. Build and install
Refer to build and load chapter for details on how to build and download the software onto the device.
3.4. User setup
3.4.1. ST67W6X default configuration
The default system configuration can be modified in "ST67W6X/Target/w6x_config.h":
/** NCP power save mode : 0: NCP stays always active / 1: NCP goes in low power mode when idle */ #define W6X_POWER_SAVE_AUTO 0 /** NCP clock mode : 1: Internal RC oscillator, 2: External passive crystal, 3: External active crystal */ #define W6X_CLOCK_MODE 1U
The default Wi-Fi® configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:
/** Boolean to enable/disable autoconnect functionality */ #define W6X_WIFI_AUTOCONNECT 0 /** Define the region code, supported values : [CN, JP, US, EU, 00] */ #define W6X_WIFI_COUNTRY_CODE "00" /** Define if the country code will match AP's one. * 0: match AP's country code, * 1: static country code */ #define W6X_WIFI_ADAPTIVE_COUNTRY_CODE 0
The default net configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:
/** Define the DHCP configuration : 0: NO DHCP, 1: DHCP CLIENT STA, 2:DHCP SERVER AP, 3: DHCP STA+AP */ #define W6X_NET_DHCP 1U /** String defining Wi-Fi hostname */ #define W6X_NET_HOSTNAME "ST67W61_WiFi" /** Timeout in ticks when calling W6X_Net_Recv() */ #define W6X_NET_RECV_TIMEOUT 10000U /** Timeout in ticks when calling W6X_Net_Send() */ #define W6X_NET_SEND_TIMEOUT 10000U /** Default Net socket receive buffer size * @note In the NCP, the LWIP recv function is used with a static buffer with * a fixed length of 4608 (3 * 1536). The data is read in chunks of 4608 bytes * So in order to get optimal performances, the buffer on NCP side should be twice as big */ #define W6X_NET_RECV_BUFFER_SIZE 9216U
The default utilities configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:
/** Enable LittleFS */ #define LFS_ENABLE 0
The AT driver can be configured in "ST67W6X/Target/w61_driver_config.h":
/** Maximum number of detected AP during the scan. Cannot be greater than 50 */ #define W61_WIFI_MAX_DETECTED_AP 20 /** Enable/Disable Wi-Fi module logging */ #define WIFI_LOG_ENABLE 1 /** Enable/Disable Network module logging */ #define NET_LOG_ENABLE 1 /** Enable/Disable MQTT module logging */ #define MQTT_LOG_ENABLE 1 /** Maximum SPI buffer size */ #define W61_MAX_SPI_XFER 1520 /** Debugging only: Enable AT log, i.e. logs the AT commands incoming/outcoming from/to the NCP */ #define W61_AT_LOG_ENABLE 0 /** Enable/Disable System module logging */ #define SYS_LOG_ENABLE 1
Additionally, some other options can be modified in the "ST67W6X/Target" directory using different configuration files, as outlined below:
- logging_config.h: This file provides configuration for the logging component to set the log level.
- shell_config.h: This file provides configuration for the Shell component.
- w6x_config.h: This file provides configuration for the W6X APIs (used during init).
- w61_driver_config.h: This file provides configuration for the W61 configuration module.
All available defines are provided in the template directory "Middlewares/ST/ST67W6X_Network_Driver/Conf"
3.4.2. Application configuration
The Wi-Fi® configuration used in this application is defined in "Appli/App/app_config.h":
/** SSID of the local Access Point */ #define WIFI_SSID "MY_SSID" /** Password of the local Access Point */ #define WIFI_PASSWORD "MY_PASSWORD" /** Define the default factor to apply to AP DTIM interval when connected and power save mode is enabled */ #define WIFI_DTIM 1
The logging output mode can be modified in "Appli/App/app_config.h":
/** Select output log mode [0: printf / 1: UART / 2: ITM] */ #define LOG_OUTPUT_MODE 1
The host low-power mode can be modified in "Appli/App/app_config.h":
/** Low power configuration [0: disable / 1: sleep / 2: stop / 3: standby] */ #define LOW_POWER_MODE 0
The host debugger pins can be modified in "Appli/App/app_config.h":
/** * Enable/Disable MCU Debugger pins (dbg serial wires) * @note by HW serial wires are ON by default, need to put them OFF to save power */ #define DEBUGGER_ENABLED 1
The SNTP (simple network time protocol) can be modified in "Appli/App/main_app.h":
/** SNTP timezone configuration */ #define SNTP_TIMEZONE 1
The MQTT client configuration can be modified in "Appli/App/main_app.h":
/** Subscribed topic max buffer size */ #define MQTT_TOPIC_BUFFER_SIZE 100U /** Subscribed message max buffer size */ #define MQTT_MSG_BUFFER_SIZE 600U /** Host name of remote MQTT Broker * Multiple options are possible: * - broker.hivemq.com * - broker.emqx.io * - test.mosquitto.org */ #define MQTT_HOST_NAME "broker.emqx.io" /** Port of remote MQTT Broker */ #define MQTT_HOST_PORT 1883 /** Security level * 0: No security (TCP connection) * 1: SSL with Username/Password authentication * 2: SSL with Server certificate (CACertificate) * 3: SSL with Client certificate (Certificate and PrivateKey) * 4: SSL with both certificates (CACertificate, Certificate, PrivateKey) */ #define MQTT_SECURITY_LEVEL 0 /** MQTT Client ID to be identified on MQTT Broker */ #define MQTT_CLIENT_ID "mySTM32_772" /** MQTT Username to be identified on MQTT Broker. Not used in non-secure */ #define MQTT_USERNAME "user" /** MQTT Password to be identified on MQTT Broker. Not used in non-secure */ #define MQTT_USER_PASSWORD "password" /** MQTT Client Certificate. Required when the scheme is greater or equal to 3 */ #define MQTT_CERTIFICATE "client_mqtt.crt" /** MQTTClient Private key. Required when the scheme is greater or equal to 3 */ #define MQTT_KEY "client_mqtt.key" #endif /* MQTT_KEY */ /** MQTT Client CA certificate. Required when the scheme is greater or equal to 2 */ #define MQTT_CA_CERTIFICATE "ca_mqtt.crt" /** MQTT Server Name Indication (SNI) */ #define MQTT_SNI "server.local" /** Keep Alive interval using MQTT ping. Range [0, 7200]. 0 is forced to 120 */ #define MQTT_KEEP_ALIVE 120 /** Skip cleaning the MQTT session */ #define MQTT_DIS_CLEAN_SESSION 0 /** Publish QoS. 0: At most once, 1: At least once, 2: Exactly once */ #define MQTT_PUBLISH_QOS 0 /** Publish Retain flag */ #define MQTT_PUBLISH_RETAIN 0
Keep alive is the time interval used to send a PINGREQ MQTT packet to the broker and indicate that the connection must be kept open. It can be adjusted according to broker requirements.
The publish quality of service (QoS) defines the reliability guarantee level for message delivery between devices:
- At most once (QoS 0): offers "fire and forget" messaging with no acknowledgment from the receiver.
- At least once (QoS 1): ensures that messages are delivered at least once by requiring a PUBACK acknowledgment.
- Exactly once (QoS 2): guarantees that each message is delivered exactly once by using a four-step handshake (PUBLISH, PUBREC, PUBREL, PUBCOMP).
The publish retain flag offers the possibility to store on the broker the last retained message and the corresponding QoS. This ensures that a subscriber receives the most recent message even if it subscribes after the message was originally published. To delete the last stored message, the device must publish an empty message.
3.4.3. MEMS configuration
The demonstration project is configured to use the sensors values from the X-NUCLEO-IKS4A1 or X-NUCLEO-IKS01A3 expansion boards with the X-CUBE-MEMS1 expansion software package.
The sensor usage can be enabled in "X-CUBE-MEMS1\App\sys_sensors.h":
#define SENSOR_ENABLED 1
The expansion board can be selected in the STM32CubeMX > Software Packs Component Selector > STMicroelectronics.X-CUBE-MEMS. The IKS4A1 is enabled by default.
This optional configuration is used to append the currently measured temperature, humidity, and pressure values to the published MQTT messages. More details in X-CUBE-MEMS1.
3.5. Server setup
The MQTT client is a device that connects to an MQTT broker over a network.
The MQTT broker is a server that receives all messages from the clients and then routes the messages to the appropriate destination clients. It can be a service installed on a local computer in a private network or hosted by a third party in the cloud.
3.5.1. Security and certificates
The NCP utilizes littlefs to read certificates and keys from the host processor, which are then stored internally.
The following sections outline the process for loading certificates and keys onto the NCP using the MQTT demonstration.
The guide also explains how to configure the host processor and NCP to use different security schemes for MQTT over TLS.
The following part is similar to the section in MQTT Security and certificates chapter and to the section in HTTPS Client Application Security and certificates chapter.
The X-CUBE-ST67W61 expansion package provides multiple certificates and keys for testing purposes.
These keys can be found in the following directory:
Projects\ST67W6X_Scripts\LittleFS\Certificates\lfs
The client-server certificate and key pairs are named with a numerical identifier to signify their relationship (that is, ca_1.crt, client_1.crt, client_1.key, server_1.crt, server_1.key).
3.5.1.1. If the define LFS_ENABLE equals 0
To load the CA, client certificates, and keys onto the NCP, the file contents must be copied into the buffers ca_cert[], client_cert[] and client_key[]
within the Appli\App\main_app.c file.
3.5.1.2. If the define LFS_ENABLE equals 1
To load the CA, client certificates, and keys onto the NCP, the files must be placed within the lfs folder in the MQTT demonstration folder located here: Projects\NUCLEO-U575ZI-Q\Demonstrations\ST67W6X\ST67W6X_MQTT\littlefs\lfs
The certificates and keys are loaded onto the device as a littlefs.bin binary using linker input specified in the project settings.
To build this binary from the desired certificates and keys, place the files in the specified lfs folder, the build.bat (Windows) or build.sh (Linux) must be run to update the binary. This batch script is located in the directory above lfs:
Projects\NUCLEO-U575ZI-Q\Demonstrations\ST67W6X\ST67W6X_MQTT\littlefs
It may be necessary to modify the script if you wish to add files beyond those already included:
mklfs.exe -c lfs -b 4096 -p 256 -r 256 -s 0x7000 -i littlefs.bin
- The -b 4096 parameter is used to define the size of a block in the binary. This size must be equal to or greater than the size of each certificate.
- The -s 0x7000 parameter is used to define the binary file size (28 KB). It is suitable for storing six certificates. If you wish to add more, you need to increase the size in block steps (0x500 by default).
The size parameter must be aligned to the define in Projects\NUCLEO-U575ZI-Q\Demonstrations\ST67W6X\ST67W6X_MQTT\littlefs\Target\lfs_flash.c:
/** This value must be aligned with prebuild script argument */ #define LITTLEFS_SECTION_SIZE 0x7000
Once run, the binary is updated.
3.5.2. Windows MQTT broker setup
The Eclipse Mosquitto is an open-source message broker that can be installed on a local computer:
- Download and install the executable: https://mosquitto.org/files/binary/win64/mosquitto-2.0.21a-install-windows-x64.exe
- Open a command prompt (cmd.exe) and navigate to the installation folder
cd "C:\Program Files\mosquitto"
- Create/update the broker user configuration.
Create or edit the user_mosquitto.conf file, and copy the following lines:
listener 1883 allow_anonymous true
- Start the broker
mosquitto.exe -v -c user_mosquitto.conf
- Define a username/password
mosquitto_passwd.exe -c passwd st67w6x
- Then, enter a password, and provide it a second time to confirm it. For example:
12345678
- Configure the certificate files
Open the "Projects\ST67W6X_Scripts\LittleFS\Certificates\lfs" directory and copy the following files to "C:\Program Files\mosquitto":
server_1.crt server_1.key ca_1.crt
3.5.3. Linux MQTT broker setup
- Install the mosquitto broker and a client:
$ sudo apt install mosquitto mosquitto-clients
| Command | Description |
|---|---|
| systemctl status mosquitto | Check that the service is running. |
| systemctl stop mosquitto | Stop the mosquitto service. |
| systemctl start mosquitto | Start the mosquitto service. |
| systemctl restart mosquitto | Restart the mosquitto service. |
- Create/update the broker user configuration.
Create or edit the "/etc/mosquitto/conf.d/mosquitto.conf" file, and copy the following lines:
listener 1883 allow_anonymous true persistence true persistence_location /var/lib/mosquitto/ log_dest file /var/log/mosquitto/mosquitto.log include_dir /etc/mosquitto/conf.d
- Start the broker
sudo systemctl restart mosquitto
- Define a username/password
mosquitto_passwd -c /etc/mosquitto/passwd st67w6x
- Then, enter a password, and provide it a second time to confirm it. For example:
12345678
- Configure the certificate files
Open the "Projects\ST67W6X_Scripts\LittleFS\Certificates\lfs" directory and copy the following files to "/etc/mosquitto":
cp Projects/ST67W6X_Scripts/LittleFS/Certificates/lfs/server_1.crt /etc/mosquitto/server_1.crt cp Projects/ST67W6X_Scripts/LittleFS/Certificates/lfs/server_1.key /etc/mosquitto/server_1.key cp Projects/ST67W6X_Scripts/LittleFS/Certificates/lfs/ca_1.crt /etc/mosquitto/ca_1.crt
3.5.4. Local MQTT broker security setup
The following configurations are built for a local mosquitto server.
3.5.4.1. MQTT over TCP with no authentication and no encryption
- MQTT broker user configuration
listener 1883 allow_anonymous true
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "<IP Address of Broker PC>",
.HostPort = 1883,
.Scheme = 0,
.MQClientId = "mySTM32_772",
.MQUserName = "",
.MQUserPwd = "",
.Certificate = "",
.PrivateKey = "",
.CACertificate = "",
.SNI = ""
};
3.5.4.2. MQTT over TLS with username authentication
- MQTT broker user configuration
listener 8883 cafile /etc/mosquitto/ca_mqtt.crt certfile /etc/mosquitto/server_mqtt.crt keyfile /etc/mosquitto/server_mqtt.key use_identity_as_username false require_certificate false allow_anonymous false password_file /etc/mosquitto/passwd tls_version tlsv1.2
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "<IP Address of Broker PC>",
.HostPort = 8883,
.Scheme = 1,
.MQClientId = "mySTM32_772",
.MQUserName = "st67w6x",
.MQUserPwd = "12345678",
.Certificate = "",
.PrivateKey = "",
.CACertificate = "",
.SNI = "server.local"
};
3.5.4.3. MQTT over TLS with server certificate
- MQTT broker user configuration
listener 8883 cafile /etc/mosquitto/ca_mqtt.crt certfile /etc/mosquitto/server_mqtt.crt keyfile /etc/mosquitto/server_mqtt.key require_certificate false use_identity_as_username false allow_anonymous false password_file /etc/mosquitto/passwd tls_version tlsv1.2
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "<IP Address of Broker PC>",
.HostPort = 8883,
.Scheme = 2,
.MQClientId = "mySTM32_772",
.MQUserName = "st67w6x",
.MQUserPwd = "12345678",
.Certificate = "",
.PrivateKey = "",
.CACertificate = "ca_mqtt.crt",
.SNI = "server.local"
};
3.5.4.4. MQTT over TLS with client certificate
- MQTT broker user configuration
listener 8883 cafile /etc/mosquitto/ca_mqtt.crt certfile /etc/mosquitto/server_mqtt.crt keyfile /etc/mosquitto/server_mqtt.key require_certificate true use_identity_as_username false allow_anonymous false password_file /etc/mosquitto/passwd tls_version tlsv1.2
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "<IP Address of Broker PC>",
.HostPort = 8883,
.Scheme = 3,
.MQClientId = "mySTM32_772",
.MQUserName = "st67w6x",
.MQUserPwd = "12345678",
.Certificate = "client_mqtt.crt",
.PrivateKey = "client_mqtt.key",
.CACertificate = "",
.SNI = "server.local"
};
3.5.4.5. MQTT over TLS with both certificates
- MQTT broker user configuration
listener 8883 cafile /etc/mosquitto/ca_mqtt.crt certfile /etc/mosquitto/server_mqtt.crt keyfile /etc/mosquitto/server_mqtt.key require_certificate true use_identity_as_username false allow_anonymous false password_file /etc/mosquitto/passwd tls_version tlsv1.2
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "<IP Address of Broker PC>",
.HostPort = 8883,
.Scheme = 4,
.MQClientId = "mySTM32_772",
.MQUserName = "st67w6x",
.MQUserPwd = "12345678",
.Certificate = "client_mqtt.crt",
.PrivateKey = "client_mqtt.key",
.CACertificate = "ca_mqtt.crt",
.SNI = "server.local"
};
3.5.5. Remote MQTT broker security setup
The following configurations are designed for a remote MQTT broker, using HiveMQ as an example.
3.5.5.1. MQTT over TCP with no authentication and no encryption
This configuration uses the public MQTT broker over a TCP connection.
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "broker.hivemq.com",
.HostPort = 1883,
.Scheme = 0,
.MQClientId = "mySTM32_772",
.MQUserName = "",
.MQUserPwd = "",
.Certificate = "",
.PrivateKey = "",
.CACertificate = "",
.SNI = ""
};
3.5.5.2. MQTT over TLS with serverless version
This configuration uses the private MQTT Serverless broker version. This is a free version deployed on a remote cluster with limited usage (a limited subset of features is available, such as the number of devices to notify, but it is sufficient for this demonstration).
- Download the broker root CA certificate from HiveMQ (isrgrootx1.pem) and place it in the folder:
"ST67W6X_MQTT/littlefs/lfs/isrgrootx1.pem"
- Generate the littlefs.bin using the build script (.bat for Windows, .sh for Linux):
ST67W6X_MQTT/littlefs/build.bat
- In the HiveMQ web console, create a broker under a serverless plan and set up the corresponding credentials (for example, username = st67w6x, password = 12345678, with permission set to "publish & subscribe"). Refer to the official HiveMQ documentation for this step.
- MQTT client user configuration
/* MQTT Broker connection */
static W6X_MQTT_Connect_t mqtt_connect =
{
.HostName = "xxxxxxxxxxx.s1.eu.hivemq.cloud",
.HostPort = 8883,
.Scheme = 2,
.MQClientId = "mySTM32_772",
.MQUserName = "st67w6x",
.MQUserPwd = "12345678",
.Certificate = "",
.PrivateKey = "",
.CACertificate = "isrgrootx1.pem",
.SNI = "xxxxxxxxxxx.s1.eu.hivemq.cloud"
};
3.6. Creation of CSR, certificates and keys
If you use a local broker, you may need to regenerate your own certificates.
An example code in Python to generate a certificate, key and CSR (certificate signing request) for the client and the server side is available in the package location Projects\ST67W6X_Scripts\LittleFS\gen_mqtt_certificate.py.
This Python script generates a self-signed MQTT certificate and private key pair for testing purposes.
Run the gen_mqtt_certificate.py script. This creates self-signed certificates and keys in the Projects\ST67W6X_Scripts\LittleFS\Certificates\lfs folder.
The generated certificates and keys are defined as follows:
- CA Certificate: ca_<label>.crt
- Client Certificate: client_<label>.crt
- Client Private Key: client_<label>.key
- Server Certificate: server_<label>.crt
- Server Private Key: server_<label>.key
The script also generates a C header template in Projects\ST67W6X_Scripts\LittleFS\output\mqtt_certificate_template.h containing:
#define MQTT_SECURITY_LEVEL
#define MQTT_HOST_PORT (1883 for security level 0, otherwise 8883)
#define MQTT_CERTIFICATE
#define MQTT_KEY
#define MQTT_CA_CERTIFICATE
#define MQTT_SNI ("" for security levels 0 and 1)
static const char ca_certificate[]
static const char client_certificate[]
static const char client_key[]
The script generates 3 Mosquitto configuration files in Projects\ST67W6X_Scripts\LittleFS\output to be used as MQTT broker configuration depending of the security level:
- security level 0: mosquitto_0.conf
- security level 1 or 2: mosquitto_1_2.conf
- security level 3 or 4: mosquitto_3_4.conf
The script generates a Mosquitto passwd file in Projects\ST67W6X_Scripts\LittleFS\output\passwd using a pure Python implementation (PBKDF2-HMAC-SHA512).
The script generates an archive Projects\ST67W6X_Scripts\LittleFS\output\mqtt_artifacts_<label>.zip containing generated certificates/keys, Mosquitto configurations, and passwd.
Optional arguments:
| Parameter | Description | Default value |
|---|---|---|
--label <label>
|
choose a custom label for the generated files | mqtt |
--cert <type>
|
specify the type of certificate to generate (all, ca, client, or server) | all |
--nokey
|
do not renew the key files for certificates | False |
--output <certs_dir>
|
choose the output directory for the generated certificates and keys | Certificates\lfs |
--header-output <header_dir>
|
choose the output directory for the generated C header file | output |
--mqtt-username <username>
|
choose the username used for generated Mosquitto passwd and C defines | st67w6x |
--mqtt-password <password>
|
choose the password used for generated Mosquitto passwd and C defines | 12345678 |
3.7. How it works
Initialization of the ST67W6X MQTT demonstration:
- #### Welcome to ST67W6X MQTT Application ##### - # build: 13:21:52 Mar 25 2026 - --------------- Host info --------------- - Host FW Version: 1.3.0 - --------------- ST67W6X info ------------ - ST67W6X MW Version: 1.3.0 - AT Version: 1.0.0 - SDK Version: 2.0.106 - Wi-Fi MAC Version: 1.6.44 - BT Controller Version: 1.6.128 - BT Stack Version: 1.10.83 - Build Date: Mar 20 2026 09:32:19 ... ----------------------------------------- Wi-Fi init is done Net init is done MQTT init is done
Wi-Fi® scan and connection to the nearby pre-defined access point:
SCAN DONE Cb informed APP that WIFI SCAN DONE. MAC : [94:83:c4:46:c0:b3] | Channel: 9 | WPA2 | N | RSSI: -43 | SSID: GL-A1300-0b1 MAC : [50:91:e3:73:bc:03] | Channel: 2 | WPA2 | N | RSSI: -48 | SSID: TP-Link_BC03 Connecting to Local Access Point NCP is treating the connection request DHCP client start, this may take few seconds App connected Connected to following Access Point : [50:91:e3:73:bc:03] Channel: 2 | RSSI: -46 | SSID: TP-Link_BC03
Configuration of the SNTP client, initialization of the MEMS board sensors, connection to the MQTT broker and subscription of two topics:
SNTP Time: Wed May 14 15:29:16 2025 MEMS Sensors init successful MQTT Configure successful MQTT Connect successful Subscribing to topic /devices/mySTM32_772/control. Subscribing to topic /sensors/mySTM32_772.
Create and publish the MQTT message. As the topic is also subscribed, the message is received and displayed:
MQTT Publish OK MQTT Subscription Received on topic "/sensors/mySTM32_775" time: 25-05-14 15:54:58 rssi: -42 mac: 40:82:7b:00:0e:6d temperature: 26.84 pressure: 1001.62 humidity: 41.53 MQTT Publish OK MQTT Subscription Received on topic "/sensors/mySTM32_775" time: 25-05-14 15:55:00 rssi: -42 mac: 40:82:7b:00:0e:6d temperature: 26.82 pressure: 1001.58 humidity: 41.51 MQTT Publish OK MQTT Subscription Received on topic "/sensors/mySTM32_775" time: 25-05-14 15:55:02 rssi: -42 mac: 40:82:7b:00:0e:6d temperature: 26.79 pressure: 1001.61 humidity: 41.54
3.8. Memory footprint
| Module | Description |
|---|---|
| [Driver] HAL/CMSIS/BSP | STM32 CMSIS Cortex, HAL and LL, board specific package drivers |
| [Project] Core | Native STM32 core components |
| [Project] App | Main part of the application |
| [Project] Target | Configuration files for ST67W6X_Network_Driver and MEMS1 components |
| [MW] ST67W6X_Network_Driver | Core and API System, Wi-Fi®, network and MQTT components Util/Logging: Utility to process shell and trace messages onto the UART interface (can be changed by ITM) |
| [MW] FreeRTOS | FreeRTOS kernel source |
| [MW] JSON | JSON parser library |
| [MW] LittleFS | LittleFS file system |
| [Utility] lpm | Tiny low-power management |
| [Toolchain] Startup | Int_vect, init routines, init table, CSTACK and HEAP |
| [Toolchain] EWARM Libraries | Native compiler libraries |
These values depend on the chosen toolset, and they can change in future releases.
3.8.1. ROM/flash memory footprint
The picture below shows the sum of the read-only memory (flash) of the ST67W6X_MQTT and ST67W6X_MQTT_LWIP demonstrations.
The picture below shows the middleware ST67W6X_Network_Driver read-only memory (flash) used by ST67W6X_MQTT and ST67W6X_MQTT_LWIP demonstrations.
3.8.2. Read-Write (RW) memory footprint
The picture below shows only the sum of the static read/write memory (static RAM) of the ST67W6X_MQTT and ST67W6X_MQTT_LWIP demonstrations.
4. References