How to create ROT examples for STM32H5

This article gives an overview of the adaptation needed to support OEMxRoT on a H5 without HW crypto support and H5 with reduced FLASH size.

1. Adaptation for device without HW crypto

For those device:

  • Cryptography operations rely on MbedTLS middleware
  • Provisioning data in OBKeys are not encrypted

Applicable products:

Products with HW crypto Products without HW crypto Adaptations
STM32H573xx STM32H563xx NUCLEO-H563ZI example provided in STM32CubeH5 Firmware
STM32H533xx STM32H523xx Starting from NUCLEO-H533RE example, adaptations described in this page
STM32H5F5xx STM32H5E5xx Starting from STM32H5F5J-DK example, adaptations described in this page

1.1. STM32H523 device

1.1.1. OEMiRoT_Boot projects adaptations

The code adaptations are available under the compile switch STM32H533xx in NUCLEO-H533RE OEMiRoT_Boot example.

Start from NUCLEO-H533RE OEMiRoT_Boot example. Open your preferred toolchain project and change the device STM32H533RE to your STM32H523xx chipset. And update the preprocessor flag from STM32H533xx to STM32H523xx.

1.1.2. Provisioning adaptations

Disable encryption of provisioning data (in obkeys):

  • Set to 0 the value of the field <DoEncryption> in the following xml.

ROT_Provisioning\DA\Config\DA_Config.xml

ROT_Provisioning\DA\Config\DA_ConfigWithPassword.xml

ROT_Provisioning\OEMiROT\Config\OEMiRoT_Config.xml

  • Regenerate the obk files using STM32TrustedPackageCreator :

ROT_Provisioning\DA\Binary\DA_Config.obk

ROT_Provisioning\DA\Binary\DA_ConfigWithPassword.obk

ROT_Provisioning\OEMiROT\Binary\OEMiRoT_Config.obk

1.2. STM32H5E5 device

1.2.1. OEMiRoT_Boot projects adaptations

The code adaptations are available under the compile switch STM32H5E5xx in STM32H5F5J-DK OEMiRoT_Boot example.

Start from STM32H5F5J-DK OEMiRoT_Boot example. Open your preferred toolchain project and change the device STM32H5F5LJ to your STM32H5E5LJ chipset. And update the preprocessor flag from STM32H5F5xx to STM32H5E5xx.

1.2.2. Provisioning adaptations

Disable encryption of provisioning data (in obkeys):

  • Set to 0 the value of the field <DoEncryption> in the following xml.

ROT_Provisioning\DA\Config\DA_Config.xml

ROT_Provisioning\DA\Config\DA_ConfigWithPassword.xml

ROT_Provisioning\OEMiROT\Config\OEMiRoT_Config.xml

  • Regenerate the obk files using STM32TrustedPackageCreator :

ROT_Provisioning\DA\Binary\DA_Config.obk

ROT_Provisioning\DA\Binary\DA_ConfigWithPassword.obk

ROT_Provisioning\OEMiROT\Binary\OEMiRoT_Config.obk

2. Adaptation for device with reduced FLASH size

2.1. Adaptation from NUCLEO-H533RE (512KB) to H533xC (256KB)

You must uncomment DEVICE_256K_FLASH_ENABLE in NUCLEO-H533RE\Applications\ROT\OEMiROT_Boot\Inc\flash_layout.h

2.2. Adaptation from NUCLEO-H563ZI (2MB) to H563xG (1MB)

You must uncomment DEVICE_1M_FLASH_ENABLE in NUCLEO-H563ZI\Applications\ROT\OEMiROT_Boot\Inc\flash_layout.h