Bluetooth qualification workspace example with STM32WB55

This article details an example of certification using Bluetooth® Low Energy qualification workspace with STM32WB55CG.

1. STM32WB55CG reference PHY and stack QDIDs/DNs

Before going through this process, QDIDs/DNs used with STM32WB55CG module should be defined. The Bluetooth® Special Interest Group (SIG) provides a listing search [1] for finding previously qualified designs and declared products. A dedicated certification guideline wiki page [2] provides the latest QDIDs/DNs to be used for each STM32WBx product.

1.1. STM32WB55CG reference RF-PHY

According to the dedicated Certification guideline wiki page [2], DN Q306653 should be considered.


This STM32WB55CG RF-PHY was qualified with core specification 5.3 and with test case reference list (TCRL) version 2024-2.

Information
/!\ From most recent Bluetooth® certification process guideline: both RF-PHY and Controller/Host core layers shall declare same Bluetooth® Core Specification version!

Therefor STMicroelectronics recommends to customer, that must proceed with "testing required" certification path, as describe here [3] to re-certify RF-PHY layer through Bluetooth® Qualification Test Facility (BQTF) declaring Bluetooth® Core Specification version 5.4. And could combine with certified Controller/Host stack Bluetooth® Core Specification version 5.4 DN Q306500. For customer with "No testing required" path, please continue with following example.

1.2. STM32WB55CG reference stack

According to the dedicated certification guideline wiki page [2], QDID 201968 [4] should be considered.


These stacks were qualified with core specification 5.3 and using the test case reference list (TCRL) version 2023-1.

Information
If you are starting to develop your platform, STMicroelectronics recommends using the latest Bluetooth® Core Specification v6.1

2. Qualification workspace process

The Bluetooth® qualification workspace [5] is the starting point of certification journey.
Note that this page, includes additional resources to help you understand Bluetooth Qualification Process or to assist you, in case of any issue.

To start, click on "start the Bluetooth Qualification Process".


Each subchapter of this article describes a different step of the qualification process on the Bluetooth® website.

2.1. Product details

In this step, product details should be entered as illustrated in the following example.



Once the product details are entered, the customer can, if required, add an additional product. To move forward, "No, I do not" must be selected, as shown below.


2.2. Specify the design

Since the customer is reusing QDIDs/DNs, "Yes, I do" is selected and both DN's associated with STM32WB55CG are entered, as shown below.



Once this is done, the following step must be completed



The customer can now proceed to layer selection and select “Save and go to the layer selection”.

2.3. Layer Selection

In this example, the customer is considering certifying a complete product with proprietary profile and should proceed as follows:


Information
If using traditional profiles, refer our dedicated Certification guideline wiki page [2] to get available DNs)


The customer can now proceed to ICS selection and select “Save and go to ICS selection”


The customer can proceed to ICS selection and select “Save and go to ICS selection”.

2.4. ICS selection

Customer can now check any inconsistencies by clicking the 'Consistency Check' button.
Since QPRD v4 [6], tool will automatically ignore invalid Implementation Conformance Statement (ICS) entries when the corresponding ICS does not exist, eliminating the need for a test coverage waiver (TCW).


As no inconsistencies are observed, customer can proceed to the next step by selecting “save and go to Test plan and documentation”.

2.5. Test Plan and Documentation

In this example, no test plan should be generated for the new design thanks to the pre-qualified DNs associated to STM32WB55CG.
In the next step, the customer selects “Upload test declaration and test reports” and uploads their own certified RF-PHY test report executed from certified test house. As explained in dedicated Certification guideline wiki page [2].



The customer can now complete the process with qualification fee payment.

2.6. Product Qualification Fee

In this step, product qualification fee needs to be addressed.



The customer can now complete the process with submission page.

2.7. Submission

The customer receives a summary of the requirements status based on the provided product declarations or reports.



Your qualification journey with STM32WB55CG is now completed !

3. References