ST67W611M1 Wi-Fi® – HTTPS Client Project

Back to main page

1. HTTPS Client presentation

This application provides an example of the HTTPS Client feature over Wi-Fi®.

It provides a starting point for an HTTPS client solution with basic GET requests to retrieve the weather from different major capitals around the globe.

The application starts in STA mode, connecting to its predefined access point (AP), which must have access to the Internet.
Once the station is connected, it displays the current temperature of the place whose coordinates are preconfigured in the program (by default set around Montreal).

Then, the command-line interface (CLI) mode starts, enabling users to use a new command to request weather data from a predefined list of cities via a weather API.

Warning
In LWIP off-load architecture (also known as Architecture T01), the use of the HTTPS protocol is limited because of the SSL socket implementation on the ST67W611M1 module.

The SSL socket has specific internal buffer configurations. The maximum size (in bytes) of plaintext fragments is reduced to 6*1024 bytes (6144 bytes). This might result in failure when the server does not acknowledge this change. SSL extension Maximum Fragment Length (MFL) can inform the server about this limitation if it is supported by the server.

For users who need an HTTPS client architecture without these T01 module-side restrictions, a T02 approach can be used instead, with the network stack and TLS handled on the STM32 host side. The ST67W6X_FOTA_LWIP[1] application provides a starting point for HTTPS client based on T02 architecture through host-side LwIP and MbedTLS.

2. Requirements

2.1. Software and system requirements

Note
Each project uses a specific ST67W611M1 binary, ST67W6X_HTTPS_Client requires st67w611m_mission_t01_v2.x.y.bin

More information is available in ST67W611M1 Hardware setup wiki page.

The software requirements are as follows (minimum IDE versions):

  • STM32CubeIDE toolchain V2.1.0 [2].
  • IAR Embedded Workbench for Arm (EWARM) toolchain V9.30.1
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.39

Programmer:

  • STM32CubeProgrammer [3] to program the board with a pre-generated binary file

HyperTerminal:

  • Use the application through the serial link
  • Open a HyperTerminal client connected to the host ST-LINK COM port

The serial COM port must be configured as shown below:

Baudrate 921600
Data 8b
Stopbit 1b
Parity None
Flow control None
Rx LF
Tx LF
Local Echo Off

For further details, refer to the HyperTerminal setup page.

2.2. Hardware requirements

This example runs on the NUCLEO-U575ZI-Q [4] board combined with the X-NUCLEO-67W61M1 board.

The X-NUCLEO-67W61M1 board is connected to the NUCLEO-U575ZI-Q board via the Arduino® connectors:

  • The 5V, 3V3, GND through the CN6
  • The SPI (CLK, MOSI, MISO), SPI_CS and USER_BUTTON signals through the CN5
  • The BOOT, CHIP_EN, SPI_RDY and UART TX/RX signals through the CN9

3. ST67W6X_HTTPS_Client application description

3.1. Project directory

The "ST67W6X_HTTPS_Client" application is available by downloading the X-CUBE-ST67W61 Expansion Package.

Refer to the Project directory wiki page for more information on the project directory.

3.2. Project description

3.2.1. Topology structure

The ST67W6X_HTTPS_Client project uses the station topology:

STA topology

The HyperTerminal is used to print the result of the weather request and change the location of the weather prediction.

3.2.2. Project initialization

The different steps in the application initialization are described below:

HTTPS client application initialization

The common initialization steps shared by all applications are highlighted in light blue. The remaining steps are specific to the HTTPS Client application.

3.3. Build and install

Refer to the build and load chapter for detailed instructions on how to build and download the software onto the device.

3.4. User setup

3.4.1. ST67W6X default configuration

The default system configuration can be modified in "ST67W6X/Target/w6x_config.h":

/** NCP power save mode : 0: NCP stays always active / 1: NCP goes in low power mode when idle */
#define W6X_POWER_SAVE_AUTO                     1

/** NCP clock mode : 1: Internal RC oscillator, 2: External passive crystal, 3: External active crystal */
#define W6X_CLOCK_MODE                          1

The default Wi-Fi® configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Define the region code, supported values : [CN, JP, US, EU, 00] */
#define W6X_WIFI_COUNTRY_CODE                   "00"

/** Define if the country code will match AP's one.
  * 0: match AP's country code,
  * 1: static country code */
#define W6X_WIFI_ADAPTIVE_COUNTRY_CODE          0

The default Net configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Define the DHCP configuration : 0: NO DHCP, 1: DHCP CLIENT STA, 2:DHCP SERVER AP, 3: DHCP STA+AP */
#define W6X_NET_DHCP                            1

/** String defining Wi-Fi hostname */
#define W6X_NET_HOSTNAME                        "ST67W61_WiFi"

/** Timeout in ticks when calling W6X_Net_Recv() */
#define W6X_NET_RECV_TIMEOUT                    10000

/** Timeout in ticks when calling W6X_Net_Send() */
#define W6X_NET_SEND_TIMEOUT                    10000

The default HTTP configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** HTTP Client thread stack size */
#define W6X_HTTP_CLIENT_THREAD_STACK_SIZE       1536

/** HTTP Client thread priority */
#define W6X_HTTP_CLIENT_THREAD_PRIO             30

/** Timeout value in millisecond for receiving data via TCP socket used by the HTTP client.
  * This value is set to compensate for when the NCP get stuck for a long time (1 second or more)
  * when retrieving data from an HTTP server for example */
#define W6X_HTTP_CLIENT_TCP_SOCK_RECV_TIMEOUT   1000

/** Size of the TCP socket used by the HTTP client, recommended to be at least 0x2000 when fetching lots of data.
  * 0x2000 is the value used in the SPI host project for OTA update, which retrieves around 1 mega bytes of data. */
#define W6X_HTTP_CLIENT_TCP_SOCKET_SIZE         9216

The default utilities configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Enable LittleFS */
#define LFS_ENABLE                              0

The Shell can be configured in the "ST67W6X/Target/shell_config.h" file:

/** Enable the shell component */
#define SHELL_ENABLE                            1

/** Default shell commands list level (0: Minimal, 1: Full) */
#define SHELL_CMD_LEVEL                         0

/** Shell command maximum size */
#define SHELL_CMD_SIZE                          256

/** Shell using color */
#define SHELL_USING_COLOR                       1

/** Print an additional status message at the end of the command execution */
#define SHELL_PRINT_STATUS                      0

/** Shell receive buffer size */
#define SHELL_FREERTOS_RX_BUFF_SIZE             256

The AT driver can be configured in "ST67W6X/Target/w61_driver_config.h":

/** Maximum number of detected AP during the scan. Cannot be greater than 50 */
#define W61_WIFI_MAX_DETECTED_AP                20

/** Enable/Disable Wi-Fi module logging */
#define WIFI_LOG_ENABLE                         1

/** Enable/Disable Network module logging */
#define NET_LOG_ENABLE                          1

/** Maximum SPI buffer size */
#define W61_MAX_SPI_XFER                        1520

/** Debugging only: Enable AT log, i.e. logs the AT commands incoming/outcoming from/to the NCP */
#define W61_AT_LOG_ENABLE                       0

/** Enable/Disable System module logging */
#define SYS_LOG_ENABLE                          1

Additionally, some other options can be modified in the "ST67W6X/Target" directory using different configuration files, as outlined below:

  • logging_config.h: This file provides configuration for the logging component to set the log level.
  • shell_config.h: This file provides configuration for the Shell component.
  • w6x_config.h: This file provides configuration for the W6X APIs (used during init).
  • w61_driver_config.h: This file provides configuration for the W61 configuration module.

All available defines are provided in the template directory "Middlewares/ST/ST67W6X_Network_Driver/Conf"

3.4.2. Application configuration

The Wi-Fi® configuration used in this application is defined in "Appli/App/app_config.h":

/** SSID of the local Access Point */
#define WIFI_SSID                   "MY_SSID"

/** Password of the local Access Point */
#define WIFI_PASSWORD               "MY_PASSWORD"

/** Define the default factor to apply to AP DTIM interval when connected and power save mode is enabled */
#define WIFI_DTIM                   1

The logging output mode can be modified in "Appli/App/app_config.h":

/** Select output log mode [0: printf / 1: UART / 2: ITM] */
#define LOG_OUTPUT_MODE             1

The host low-power mode can be modified in "Appli/App/app_config.h":

/** Low power configuration [0: disable / 1: sleep / 2: stop / 3: standby] */
#define LOW_POWER_MODE              0

The host debugger pins can be modified in "Appli/App/app_config.h":

/**
* Enable/Disable MCU Debugger pins (dbg serial wires)
* @note by HW serial wires are ON by default, need to put them OFF to save power
*/
#define DEBUGGER_ENABLED            1

3.5. How it works

3.5.1. Overview

Once the HTTPS Client application starts, the station must connect to the registered AP, which must provide access to the Internet.

First, the application retrieves weather conditions for the upcoming week for the hardcoded location in the application. No user action is required at this stage. Once completed, the application displays a log similar to the following:

Weather forecast for the region you selected:
Today:
	Overcast sky,
	Temperature between  8.2°C and  25.9°C,
	Wind blows up to 19.4km/h mainly at 150° (SE),
	0mm of rain within a span of 0h
Tomorrow:
	Overcast sky,
	Temperature between  12.2°C and  26.2°C,
	Wind blows up to 19.1km/h mainly at 166° (S),
	0mm of rain within a span of 0h
In 2 days:
	Light drizzle,
	Temperature between  13.7°C and  23.4°C,
	Wind blows up to 18.6km/h mainly at 183° (S),
	0mm of rain within a span of 5h
In 3 days:
	Moderate rain showers,
	Temperature between  15.0°C and  24.2°C,
	Wind blows up to 15.9km/h mainly at 188° (S),
	30mm of rain within a span of 13h
In 4 days:
	Dense drizzle,
	Temperature between  13.5°C and  20.6°C,
	Wind blows up to 20.7km/h mainly at 200° (S),
	1mm of rain within a span of 7h
In 5 days:
	Light drizzle,
	Temperature between  9.9°C and  13.7°C,
	Wind blows up to 15.3km/h mainly at 245° (SW),
	2mm of rain within a span of 6h
In 6 days:
	Overcast sky,
	Temperature between  7.8°C and  10.1°C,
	Wind blows up to 18.4km/h mainly at 351° (N),
	0mm of rain within a span of 0h

Then the CLI starts, and the user can use a "weather" command to get weather conditions for the upcoming week for a registered city:

w61/>weather Paris
Weather forecast for Paris:
Today:
	Fog,
	Temperature between  11.5°C and  22.1°C,
	Wind blows up to 10.4km/h mainly at 31° (NE),
	0mm of rain within a span of 0h
Tomorrow:
	Partly cloudy sky,
	Temperature between  12.3°C and  25.7°C,
	Wind blows up to 17.4km/h mainly at 16° (N),
	0mm of rain within a span of 0h
In 2 days:
	Overcast sky,
	Temperature between  9.3°C and  19.2°C,
	Wind blows up to 16.8km/h mainly at 13° (N),
	0mm of rain within a span of 0h
In 3 days:
	Partly cloudy sky,
	Temperature between  9.7°C and  21.2°C,
	Wind blows up to 15.3km/h mainly at 19° (N),
	0mm of rain within a span of 0h
In 4 days:
	Overcast sky,
	Temperature between  8.7°C and  21.3°C,
	Wind blows up to 13.8km/h mainly at 22° (N),
	0mm of rain within a span of 0h
In 5 days:
	Partly cloudy sky,
	Temperature between  10.3°C and  21.8°C,
	Wind blows up to 12.3km/h mainly at 18° (N),
	0mm of rain within a span of 0h
In 6 days:
	Partly cloudy sky,
	Temperature between  9.7°C and  21.5°C,
	Wind blows up to 12.6km/h mainly at 14° (N),
	0mm of rain within a span of 0h

If the given city is not registered, the application prints the supported list.

3.5.2. HTTPS requests

Once the application has started, it connects to the access point.

Then, the application initiates DNS resolution to obtain the IP address of the HTTPS server. This IP address, along with the port (443 for HTTPS) and other HTTPS configuration details, is stored for use by the middleware:

  • Certificate: The CA certificate authenticates the server during the connection (refer to Security and certificates).
  • Server name: The unresolved address needed during the SSL connection.
  • URI: The path to the resource to GET, built using the coordinates of the location for which the weather is requested.
  • Method: GET is used to interact with the weather API.

The middleware creates an SSL socket (since the port is set to 443 in the application) and connects to the server.

Next, it sends a simple HTTP GET request to the server using the appropriate URI to obtain the temperature for a specific area.

Following this, it begins receiving data: first the HTTP header, then the actual data, which is given to the application by the middleware in chunks of 4 KB.

Since the expected data is smaller than 4 KB, it can be processed in a single call in the callback registered by the application (HTTPS_recv_cb).

These steps are repeated each time the weather command is called, with an additional one: the city's coordinates are determined using a static array in the application.

3.5.3. Security and certificates

The NCP utilizes littlefs to read certificates and keys from the host processor, which are then stored internally.

The following sections outline the process for loading certificates and keys onto the NCP using the HTTPS client demonstration.
The guide also shows the process for configuring the host processor and NCP to use different security schemes for HTTP over TLS.

The following part is similar to the section in MQTT Security and certificates chapter and the section in HTTPS Client Application Security and certificates chapter.

The X-CUBE-ST67W61 expansion package provides multiple certificates and keys for testing.
These keys can be found in the directory: Projects\ST67W6X_Scripts\LittleFS\Certificates\lfs

ST67W6X Scripts certificates directory

The client-server certificate and key pairs are named with a numerical identifier to signify their relationship (i.e., ca_1.crt, client_1.crt, client_1.key, server_1.crt, server_1.key).

Note
The certificate file r12.pem used for the URL api.open-meteo.com is available on the website: https://letsencrypt.org/certificates/

The file used is that of the subordinate (intermediate) Let's Encrypt R12 certification authorities in PEM format: https://letsencrypt.org/certs/2024/r12.pem

Warning
The Let's Encrypt R12 certificate can be revoked before its expiration date. If the application fails to connect to the server, please check other certificates on the Let's Encrypt website.
3.5.3.1. If the define LFS_ENABLE equals 0

To load the weather certificate onto the NCP, the file content must be copied into the weather_cert[] buffer in Appli\App\https_client.c.

Note
preserve the trailing `\r\n` line endings
3.5.3.2. If the define LFS_ENABLE equals 1

To load the weather certificate onto the NCP, the file must be placed in the lfs folder in the HTTPS client demonstration folder located here: Projects\NUCLEO-U575ZI-Q\Applications\ST67W6X\ST67W6X_HTTPS_Client\littlefs\lfs

The certificate is loaded onto the device as a littlefs.bin binary using linker input specified in the project settings.
To build this binary from the desired certificate, once it is placed in the lfs folder specified above, run build.bat (Windows) or build.sh (Linux) to update the binary. This batch script is located in the directory above lfs: Projects\NUCLEO-U575ZI-Q\Applications\ST67W6X\ST67W6X_HTTPS_Client\littlefs

It may be necessary to modify the script if you wish to add more files than those already present:

mklfs.exe -c lfs -b 4096 -p 256 -r 256 -s 0x7000 -i littlefs.bin
  • The -b 4096 parameter is used to define the size of a block in the binary. This size must be equal to or greater than the size of each certificate.
  • The -s 0x7000 parameter is used to define the binary file size (28 KB). It is suitable for storing 6 certificates. If you wish to add more, you need to increase the size in block steps (0x500 by default).

The size parameter must be aligned to the define in Projects\NUCLEO-U575ZI-Q\Applications\ST67W6X\ST67W6X_HTTPS_Client\littlefs\Target\lfs_flash.c:

/** This value must be aligned with prebuild script argument */
#define LITTLEFS_SECTION_SIZE 0x7000

Once run, the binary will be updated.

3.6. Memory footprint

Module Description
[Driver] HAL/CMSIS/BSP STM32 CMSIS Cortex, HAL and LL, Board Specific Package drivers
[Project] Core Native STM32 core components
[Project] App Main part of the application
[Project] Target Configuration files for ST67W6X_Network_Driver component
[MW] ST67W6X_Network_Driver Core and API System, Wi-Fi®, Bluetooth® LE, Network, HTTP and MQTT components
Util/Shell: Utility to manage the API through the serial interface
Util/Logging: Utility to process shell and trace messages onto the UART interface (can be changed by ITM)
Util/Performance: iperf, memory allocation report, task usage utilities
[MW] FreeRTOS FreeRTOS kernel source
[MW] LittleFS LittleFS file system
[Utility] lpm Tiny low-power management
[Toolchain] Startup Int_vect, init routines, init table, CSTACK and HEAP
[Toolchain] EWARM Libraries Native compiler libraries

These values depend on the chosen toolset, and they can change in future releases.

3.6.1. ROM/flash memory footprint

The picture below shows the total read-only memory (flash) used by the HTTPS Client application.

ST67W6X_HTTPS_Client Read Only memory footprint.

The picture below shows the middleware ST67W6X_Network_Driver read-only memory (flash) used by the HTTPS Client application.

ST67W6X_Network_Driver Read Only memory footprint used by ST67W6X_HTTPS_Client application.

3.6.2. Read-write (RW) memory footprint

Information
The FreeRTOS Heap is not part of the chart below.
The dynamic memory allocation adds 200'000 bytes (value set for the TOTAL_HEAP_SIZE FreeRTOS parameter).

The ST67W6X_HTTPS_Client project uses only 28 KB of the heap. Refer to Dynamic memory overview wiki page.

The picture below shows only the sum of the static read/write memory (static RAM) of the HTTPS Client application.

ST67W6X_HTTPS_Client Read Write memory footprint

4. References