This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.| Back to main page |
|---|
1. Introduction
The ST67W611M1 module can be configured in low power as can be seen in the datasheet. Deep-sleep mode is available.
A hardware wake-up signal needs to be sent to leave the Deep-sleep mode.
2. Wake-up pins hardware implementation
Besides its role in the SPI protocol (see the SPI related page), SPI_CS (24) pin is used to convey the wake-up signal to the module. Connect this pin to the host. The host sends the wake-up command over a signal that uses VDDIO logic levels. Refer to the software documentation for more details.