In a context of symmetric or asymmetric cryptography, protection of secret keys is essential. For this purpose, ST proposes a solution so that the keys remain secret at any time and usable only on a specific device. On STM32, two elements are required to do so:
- The first one is a hardware coupling and chaining bridge (CCB) to isolate the key manipulation inside hardware cryptographic IPs.
- The second one is a Root Security Services extension (RSSe) library allowing the user firmware to use the secret key while never giving access to the secret key itself. In the document, the library is referenced as “RSSe KW” (RSSe for Key Wrap) and the output is referenced as “wrapped key”.
A detailed description of RSSe KW is provided in AN6278
List of applicable products:
| Type | Products |
|---|---|
| Microcontroller | STM32G564xx |
1. RSSe KW for DUA
The provisioning of unique keys may be required for some use cases as initial attestation, for example. This provisioning is a crucial step and may be very costly to guaranty the unicity and confidentiality of the keys. STMicroelectronics addresses this challenge by provisioning, in secure facilities, each applicable STM32 with unique key pairs called Device Unique Authentication keys (DUA). These keys are ECC (Elliptic Curve Cryptographic) keys of 256 bits. The public part is freely accessible through a certificate signed by an STMicroelectronics Certificate Authority (CA) while the wrapped private part is accessible only through the RSSe KW.
2. RSSe KW principles overview
RSSe KW is a library implemented in STM32 microcontrollers that get wrapped DUA keys in trusted facilities. The main goal of the RSSe KW is to provide wrapped keys usable only on one specific device. The RSSe KW prevents the sensitive keys from:
- Being accessed by any firmware or debugging access.
- Being used by another device (including STM32).
3. DUA wrapped key usage contexts
The output of the RSSe KW contains the selected DUA key wrapped for a specific context along with elements needed to use it. On STM32G5 devices, the "specific context" depends on:
- The security state (secure or nonsecure).
- The privilege state (privileged or unprivileged).
- The key usage: signature or scalar multiplication computation (for ECC keys).
- The HDP level.
- The Epoch counter selection.
All these elements can be chosen when launching the key wrap command.
The list of allowed contexts is:
| Key wrapped | Security state | Privilege state | Key usage | HDP level | Epoch counter selection |
|---|---|---|---|---|---|
| DUA License Usage key | Secure | Privilege | Signature | HDPL2 | Epoch forced to zero |
| DUA License Usage key | Secure | Privilege | Scalar multiplication | HDPL2 | Epoch forced to zero |
| DUA License Usage key | Secure | Privilege | Signature | HDPL3 | Epoch forced to zero |
| DUA License Usage key | Secure | Privilege | Scalar multiplication | HDPL3 | Epoch forced to zero |
| DUA User key | Secure | Privilege | Signature | HDPL2 | Epoch forced to zero |
| DUA User key | Secure | Privilege | Scalar multiplication | HDPL2 | Epoch forced to zero |
| DUA User key | Secure | Privilege | Signature | HDPL3 | Epoch forced to zero |
| DUA User key | Secure | Privilege | Scalar multiplication | HDPL3 | Epoch forced to zero |
4. RSSe KW interface
With the use of Cube Programmer, the user can get the wrapped key with only one command. The output container is stored into a binary file chosen by the user
If a custom tool is used, the RSSe KW must first be installed in STM32 RAM memory before receiving the KW command as described in AN6278