This page contains application examples, document references, and tips related to the STM32 Bluetooth® Low Energy protocol.
1. Bluetooth® Low Energy overview
1.1. What is Bluetooth® Low Energy (BLE)?
Bluetooth® Low Energy is a low-power, short range, wireless personal area network technology designed and marketed by the Bluetooth® Special Interest Group (Bluetooth® SIG[1]) to allow devices to communicate with each other.
The keys features are:
- Reducing battery consumption, as the amount of transmitted data is low.
- Creating simultaneous connections, as data packets are short.
- Developing standardized applications, specified by the Bluetooth® SIG.
- Developing Mesh network applications.
- Developing proprietary applications, with flexible services and the creation of dedicated features.
Most of the smartphones and tablets built since 2012 support Bluetooth® Low Energy (BLE).
The STM32WB series[2], STM32WB0 series[3] and the STM32WBA series[4] are the ideal MCUs families for developing connected accessories that control sensors and transmit information to central devices.
Further information on technology specifications is available on the STM32WBx BLE programming manual[5] and the STM32WB0 BLE programming manual[6] .
2. Bluetooth® Low Energy wiki: Breakdown of pages
For users that are familiar with the Bluetooth® Low Energy wiki pages, find below the direct links to dedicated articles. For beginners, you can start by reading the following chapter first.
- Introduction to Bluetooth® LE with STM32 (this current page)
- STM32WBA series
- Bluetooth® LE hardware setup How to configure the board and run the application
- Bluetooth® LE Software setup - STM32CubeWBA Bluetooth® LE software development information
- Several Bluetooth® SIG specified applications
- Several ST proprietary Bluetooth® LE applications
- Bluetooth® LE audio applications
- STM32WBA software architecture
- STM32WBA STM32CubeMX Bluetooth® LE application creation & configuration
- STM32WB0 series
- Bluetooth® LE hardware setup How to configure the board and run the application
- Bluetooth® LE software setup - STM32CubeWB0 Bluetooth® LE software development information
- Several Bluetooth® SIG specified applications
- Several ST proprietary Bluetooth® LE applications
- STM32WB0 software architecture
- STM32WB0 STM32CubeMX Bluetooth® LE application creation & configuration
- STM32WB series
- Bluetooth® LE Hardware setup How to configure the board and run the application
- Bluetooth® LE Software setup - STM32CubeWB Bluetooth® LE software development information
- Several Bluetooth® SIG specified applications
- Several ST proprietary Bluetooth® LE applications
- STM32WB STM32CubeMX Bluetooth® LE application creation & configuration
- STM32WB Bluetooth® LE Sniffer
- STM32 Bluetooth® LE sniffer setup How to configure the hardware and software to run the STM32WB Bluetooth® LE sniffer application
- STM32WBA series
3. Easy bring up with the STM32WBA series and Bluetooth® Low Energy
From a hardware point of view, STMicroelectronics offers various boards to set up the Bluetooth® LE connectivity solution on STM32 MCUs. The device architecture leverages state-of-the art STM32 ultra-low-power process node. Different offers are available:
- STM32WBA5 line, with up to 100 MHz of CPU, 1 Mbyte of flash memory, 128 Kbytes of RAM
- STM32WBA6 line, with up to 100 MHz of CPU, 2 Mbytes of flash memory, 512 Kbytes of RAM
Evaluation boards are the following:
- NUCLEO-WBA55CG board with STM32WBA55CG UQFN48' package
- STM32WBA55G-DK1 discovery kit with module STM32WBA5MMG LGA76' package
- B-WBA5M-WPAN connectivity expansion board with module STM32WBA5MMG LGA76' package
- NUCLEO-WBA65RI board with STM32WBA65RI VFQFPN68' package
- STM32WBA65RI-DK1 discovery Kit with STM32WBA65RIV7 VFQFPN68' package
On the software side, the STM32CubeWBA MCU Package[7] provides a software solution to allow customers to quickly and easily develop their own firmware using:
- several Bluetooth® SIG specified applications
- several ST proprietary Bluetooth® LE applications
For more information on how to use and develop Bluetooth® LE applications, refer to the Bluetooth® LE Software setup - STM32CubeWBA page.
3.1. STM32WBA software application notes and user manuals
- AN5929 - STM32Cube MCU Package examples for STM32WBA series
- AN5928 - How to build a short range wireless application with STM32WBA MCUs
- STM32WBA BLE Wireless Interface
3.2. STM32WBA hardware guidance
- STM32WBA product selector
- RM0493 - STM32WBA52 reference manual
- UM3103 - STM32WBA Nucleo-64 board
- DS14127 - STM32WBA5xxx Data Sheet
- DS14736 - STM32WBA6xxx Data Sheet
4. Easy bring up with STM32WB0 Series and Bluetooth® LE
From a hardware point of view, STMicroelectronics offers various boards to set up the Bluetooth® LE connectivity solution on STM32 MCUs.
The device architecture leverage state-of-the art Bluetooth® LE and ultra-low-power. It is available up to 512kB Flash and 64KB of SRAM.
Evaluation boards are the following:
- NUCLEO-WB05KZ board with STM32WB05
- NUCLEO-WB07CC board with STM32WB07
- NUCLEO-WB09KE board with STM32WB09
On the software side, the STM32CubeWB0 MCU Package[8] provides a software solution to allow customers to quickly and easily develop their own firmware using:
- several Bluetooth® SIG specified applications
- several ST proprietary Bluetooth® LE applications
For more information on how to use and develop Bluetooth® LE applications, refer to the Bluetooth® LE software setup - STM32CubeWB0 page.
4.1. STM32WB0 software application notes and user manuals
- AN5976 - STM32Cube MCU Package examples for STM32WB0 series
- AN5977 - How to build a Bluetooth® Low Energy application with STM32WB0 MCUs
- AN6142 - STM32WB0 Bluetooth® Low Energy (BLE) wireless interface
4.2. STM32WB0 hardware guidance
- UM3343 - STM32WB05 Nucleo-64 board user manual
- UM3345 - STM32WB09 Nucleo-64 board user manual
- UM3344 - STM32WB07 Nucleo-64 board user manual
5. Easy bring up with the STM32WB series and Bluetooth® Low Energy
From a hardware point of view, STMicroelectronics offers various boards to set up the Bluetooth® LE connectivity solution on STM32 MCUs.
The device architecture leverages state-of-the art STM32 ultra-low-power process node, and is available from 256 KB up to 1 MB of flash memory, and up to 256 KB of SRAM.
Various packages are available: UQFN48, VQFN68, LGA86, WLCLSP100, and UFBGA129.
The first evaluation board is the P-NUCLEO-WB55 pack, which includes one USB dongle and one Nucleo-64 board with the STM32WB55 MCU.
NUCLEO-WB15CC is the newest entry-level development board for Bluetooth 5.2 applications running on the STM32WB15CC microcontroller. It offers 329 KB of flash memory, 48 KB of RAM, and the necessary peripherals to suit engineers working on simple applications.
STMicroelectronics has expanded the STM32WB portfolio of dual-core multi-protocol microcontrollers (MCUs) by introducing the first STM32WB5MMG module provided on the STM32WB5MM-DK Discovery kit.
The module enriches the STM32WB ecosystem and offers customers an easy way to add this BLE feature for faster time-to-market for the product introduction.
For more information on how to bring up the hardware to run simple Bluetooth® LE application, check the Bluetooth® LE hardware setup page.
On the software side, the STM32CubeWB MCU Package[9] provides a software solution to allow customers to quickly and easily develop their own firmware using:
- several Bluetooth® SIG specified applications
- several ST proprietary Bluetooth® LE applications
- STM32CubeMX Bluetooth® LE application creation & configuration
For more information on how to use and develop Bluetooth® LE applications, refer to the Bluetooth® LE Software setup - STM32CubeWB page.
5.1. STM32WB software application notes and user manuals
5.2. STM32WB hardware guidance
6. Quick access to STM32WBA online resources
6.1. STM32WBA Bluetooth® LE MOOC (massive online courses)
MOOC - STM32WBA workshop Simplify your wireless design journey with ST, from MCU selection to RF certification.
7. Quick access to STM32WB online resources
7.1. STM32WB Bluetooth® LE videos
STM32WB Getting Started Series
1st 32-bit Wireless module presentation
7.2. STM32WB Bluetooth® LE MOOC (massive online courses)
STM32WB Firmware Update Over the Air (FUOTA)
Basic information about software update STM32WB MCU line using different tools and techniques, including over the air methods
STM32 Bluetooth® LE MESH Introduction
How to build Bluetooth Mesh network with STM32WB using the STM32WB55 Nucleo pack and its software package
STM32 Bluetooth® LE Security
Learn basic principles concerning the BLE security concepts with STM32WB
8. Specific tools
- STM32CubeMonitor-RF - Software tool to test the RF performance of STM32-based hardware devices
- STM32CubeMX - STM32Cube initialization code generator
- STM32CubeProgrammer - Software programmer for all STM32
- STM32PowerShield - Power and analyze current consumption
9. References
10. Terms and definitions
| Term | Definition |
|---|---|
| ACI | Application control Interface |
| ATT | Attribute protocol |
| BLE | Bluetooth® Low Energy |
| DK | Development kit |
| GAP | Generic access profile |
| GATT | Generic attribute profile |
| HCI | Host control interface |
| L2CAP | Logical link control adaptation layer protocol |
| MCU | Microcontroller unit |
| PDU | Protocol data unit |
| RF | Radio frequency |
| RSSI | Receive signal strength indicator |
| SIG | Special Interest Group |
| UUID | Universally unique identifier |
| WPAN | Wireless personal area network |
Pages in category "Introduction to Bluetooth® LE with STM32"
The following 11 pages are in this category, out of 11 total.
4
- STM32StepByStep:STM32WB1M Discovery Kit Out Of Box Demonstration
- STM32StepByStep:STM32WBA5M Discovery Kit Out Of Box Demonstration
- STM32StepByStep:STM32WBA6M Discovery Kit Out Of Box Demonstration
- STM32StepByStep:STM32WBA55 Discovery Kit Out Of Box Demonstration
- STM32StepByStep:Nucleo-WBA65RI Out Of Box Demonstration
- STM32StepByStep:STM32WBA65I Discovery Kit Out Of Box Demonstration