1. HTTP Server Presentation

This application provides an example of an HTTP server over Wi-Fi®, hosted by a device configured as a soft access point (soft-AP).

It provides a starting point for an HTTP server solution with basic GET requests to allow the client to interact with the server.

The application starts in soft-AP mode, with a set SSID and password for a WPA2 connection and then shows its IP address.
Once the device is connected, open a preferred web browser, and enter the IP address of the server/soft-AP.
The client sends a request to the server which returns the main HTML page. This page includes the different buttons to interact with the LEDs on the board and a status indicator of the user button on the host board.

2. Requirements

2.1. Software and system requirements

The software required are the following (minimum IDEs version):

  • STM32CubeIDE toolchain V1.18.1 [1].
  • IAR Embedded Workbench for ARM (EWARM) toolchain V9.30.1
  • RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.39

Programmer:

  • STM32CubeProgrammer [2] to program the board with pre-generated binary file

HyperTerminal:

  • Use the application through the serial link
  • Open a HyperTerminal client connected to the Host ST-LINK COM port

The Serial COM port must be configured as below:

For more details, refer to the HyperTerminal setup page.

2.2. Hardware requirements

This example runs on the NUCLEO-U575ZI-Q [3] board combined with the X-NUCLEO-67W61M1 board.

The X-NUCLEO-67W61M1 board is connected to the NUCLEO-U575ZI-Q board via the Arduino®connectors:

  • The 5V, 3V3, GND through the CN6
  • The SPI (CLK, MOSI, MISO), SPI_CS and USER_BUTTON signals through the CN5
  • The BOOT, CHIP_EN, SPI_RDY and UART TX/RX signals through the CN9

The USER_BUTTON refers to the button mounted on the X-NUCLEO-67W61M1. Indeed, the user button on the STM32 Nucleo board is not used as external interrupt mode due to conflict with other EXTI pin requirement. The button must be defined with the user label USER_BUTTON and EXTI falling mode.

This example requires to have a red LED defined with the user label LED_RED, and a green LED defined with the user label LED_GREEN on the host board.

3. ST67W6X_HTTP_Server application description

3.1. Project Directory

The "ST67W6X_HTTP_Server" application is available by downloading the X-CUBE-ST67W61 Package.

Refer to the Project directory wiki page for more information on the project directory.

3.2. Project Description

3.2.1. Structure - Topology

The ST67W6X_HTTP_Server project uses the soft-AP topology:

soft AP topology

The HyperTerminal is used to collect connection information about the soft-AP, including the SSID and its IP address.

3.2.2. Project initialization

The different steps of the application initialization are described below:

httpserver application initialization

The common initialization steps shared by all applications are highlighted in light blue. The remaining steps are specific to the HTTP server application.

3.3. Build and install

Refer to the build and install chapter for detailed instructions on how to build and download the software onto the device.

3.4. User setup

3.4.1. ST67W6X default configuration

The default system configuration can be modified in "ST67W6X/Target/w6x_config.h":

/** NCP will go by default in low power mode when NCP is in idle mode */
#define W6X_POWER_SAVE_AUTO                     1

/** NCP clock mode : 1: Internal RC oscillator, 2: External passive crystal, 3: External active crystal */
#define W6X_CLOCK_MODE                          1

The default Wi-Fi® configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Define the DHCP configuration : 0: NO DHCP, 1: DHCP CLIENT STA, 2:DHCP SERVER AP, 3: DHCP STA+AP */
#define W6X_WIFI_DHCP                           3

/** Define the max number of stations that can connect to the Soft-AP */
#define W6X_WIFI_SAP_MAX_CONNECTED_STATIONS     4

/** String defining Soft-AP subnet to use.
  *  Last digit of IP address automatically set to 1 */
#define W6X_WIFI_SAP_IP_SUBNET                  {192, 168, 8}

/** String defining Soft-AP subnet to use in case of conflict with the AP the STA is connected to.
  *  Last digit of IP address automatically set to 1 */
#define W6X_WIFI_SAP_IP_SUBNET_BACKUP           {192, 168, 9}

/** Define if the DNS addresses are set manually or automatically */
#define W6X_WIFI_DNS_MANUAL                     0

/** String defining DNS IP 1 address to use
  * @note: This address will be used only if W6X_WIFI_DNS_MANUAL equals 1 */
#define W6X_WIFI_DNS_IP_1                       {208, 67, 222, 222}

/** String defining DNS IP 2 address to use
  * @note: This address will be used only if W6X_WIFI_DNS_MANUAL equals 1 */
#define W6X_WIFI_DNS_IP_2                       {8, 8, 8, 8}

/** String defining DNS IP 3 address to use
  * @note: This address will be used only if W6X_WIFI_DNS_MANUAL equals 1 */
#define W6X_WIFI_DNS_IP_3                       {0, 0, 0, 0}

/** Define the region code, supported values : [CN, JP, US, EU, 00] */
#define W6X_WIFI_COUNTRY_CODE                   "00"

/** Define if the country code will match AP's one.
  * 0: match AP's country code,
  * 1: static country code */
#define W6X_WIFI_ADAPTIVE_COUNTRY_CODE          0

/** String defining Wi-Fi hostname */
#define W6X_WIFI_HOSTNAME                       "ST67W61_WiFi"

The default net configuration can be modified in the "ST67W6X/Target/w6x_config.h" file:

/** Timeout in ticks when calling W6X_Net_Recv() */
#define W6X_NET_RECV_TIMEOUT                    10000

/** Timeout in ticks when calling W6X_Net_Send() */
#define W6X_NET_SEND_TIMEOUT                    10000

/** Default Net socket receive buffer size
  * @note In the NCP, the LWIP recv function is used with a static buffer with
  * a fixed length of 4608 (3 * 1536). The data is read in chunks of 4608 bytes
  * So in order to get optimal performances, the buffer on NCP side should be twice as big */
#define W6X_NET_RECV_BUFFER_SIZE                4608

The AT driver can be configured in "ST67W6X\Target\w61_driver_config.h":

/** Maximum number of detected AP during the scan. Cannot be greater than 50 */
#define W61_WIFI_MAX_DETECTED_AP                50

/** Debugging only: Enable AT log, i.e. logs the AT commands incoming/outcoming from/to the NCP */
#define W61_AT_LOG_ENABLE                       0

Additionally, some other options can be modified in the "ST67W6X/Target" directory with different configuration files, as outlined below:

  • logging_config.h: This file provides configuration for the logging component, enabling the setting of the log level.
  • shell_config.h: This file provides configuration for Shell component.
  • w6x_config.h: This file provides configuration for the W6X APIs (used during init).
  • w61_driver_config.h: This file provides configuration for the W61 configuration module.

All available defines are available in template directory "Middlewares/ST/ST67W6X_Network_Driver/Conf"

3.4.2. Application configuration

The Wi-Fi soft-AP configuration used in this application is defined in "App_HTTP_Server/App/app_config.h":

/* Soft-AP connection parameters */
#define WIFI_SAP_SSID               "ST67W6X_AP"

#define WIFI_SAP_PASSWORD           "12345678"

#define WIFI_SAP_CHANNEL            1

#define WIFI_SAP_SECURITY           W6X_WIFI_AP_SECURITY_WPA2_PSK

#define WIFI_SAP_MAX_CONNECTIONS    4

The logging output mode can be modified in "App_WiFi_Commissioning/App/app_config.h":

/** Select output log mode [0: printf / 1: UART / 2: ITM] */
#define LOG_OUTPUT_MODE             1

The host low power mode can be modified in "App_WiFi_Commissioning/App/app_config.h":

/** Low power configuration [0: disable / 1: sleep / 2: stop / 3: standby] */
#define LOW_POWER_MODE              1

The host debugger pins can be modified in "App_WiFi_Commissioning/App/app_config.h":

/**
* Enable/Disable MCU Debugger pins (dbg serial wires)
* @note by HW serial wires are ON by default, need to put them OFF to save power
*/
#define DEBUGGER_ENABLED            1

3.5. How it works

3.5.1. Overview

Once the HTTP Server application is started, the server is up and waits for incoming connections.
First, the station must connect to the soft-AP. By default, the soft-AP SSID is ST67W6X_AP, and the password is 12345678. To connect, use this QR-code:

QR code to connect HTTP server soft-AP

Use a device with an embedded web browser to connect to the server using the IP address provided in the logs.
Multiple clients can be connected to the server (up to two clients at the same time). The topology of the system is as following:

topology_AP_STA

On the main page, two buttons are available to control and display the status of the Blue and Green LEDs on the host board. These buttons generate a 'GET' request to the server, which toggles the corresponding LED.
There is another section which displays the status of the user button on the board (button pressed aka ON, button released aka OFF).

httpserver_main_page

3.5.2. HTTP requests flow

3.5.2.1. Initial HTTP requests

Once the application has started, it creates a new socket (that acts as server socket), binds it to the IP address of the soft-AP, and listens for incoming connections. In a while loop, when a new connection to the server socket is received, the server creates a new socket to manage the new connection within a dedicated thread, while the server socket continues to listen for incoming connections. In this thread, the request received is parsed and processed to send the appropriate response and/or execute the actions implied by the request.

GET requests Client-Server
3.5.2.2. User actions

When pressing on the LED buttons, it generates a GET request "GET /LedGreen" or "GET /LedBlue" .
The server parses the request, toggles the corresponding LED, and sends the response to the client, indicating that both the connection and the child socket should be closed.

In this use case, the button information originates from the server and is sent to the client, as the button is located on the host board. This setup contrasts with the typical HTTP protocol flow, where requests are initiated by the client and directed to the server.
To address this issue, the client automatically generates a request at startup through the HTML page ( "GET /pins_status" in the diagram below), which remains until the server notices a state change on the user button pin.
At that point, the server responds to the pending request with the button pin state.

To notify multiple clients connected to the server, a dedicated thread is created on the server side at startup to check when there is a state change on the button pin, ( "PUSH USER BUTTON" ), and on the LEDs pin ( "GET /LedGreen" ).
This thread notifies all the threads handling the request for the pin status: "GET /pins_status" . The server can then respond to all the clients.

This method puts the server in control of the connection with the client, facilitating the sending of asynchronous responses.
Below is the request diagram illustrating the interaction between the server and the client:

GET requests Client-Server and pin status requests

3.5.3. File conversion

The device must be capable of handling various elements such as pages, images, and icons to send them effectively. Without a file system on our devices, these files must be converted to ASCII format for storage on the host device and transmission to the client. To achieve this, a Python script executed during pre-build performs the conversion ("Html/html_to_h.py").

It takes as input the list of the different files needed by the application, located in "Html/conf.txt". The Python script processes these files, converting them to ASCII and storing the results in pre-formatted HTTP responses, ready for transmission to the client. All the responses are stored in the file "App_HTTP_Server/App/html_pages.h", which manages the HTML pages, images and icons.

This Python script is common to both ST67W6X_Wi-Fi Commissioning Application and ST67W6X_HTTP_Server applications.

To add a new file to the conversion process, add a new specific header with the response name and a new entry in the file dictionary.

html_desc_dict = {
    'index_httpserver.html': [index_httpserver_header, index_httpserver_middle],
    '404.html': [error_404_header, error_404_middle],
    'favicon.svg': [favicon_header, svg_middle],
    'ST_logo_2020_white_no_tagline_rgb.svg': [st_logo_header, svg_middle]
}

This dictionary aims to link the correct header and HTML's file's type field (text/html, image/svg here named xxx_middle) to build valid responses.

This generation tool facilitates the development by using HTML files directly, bypassing the need for manual conversion and insertion of outputs into the code.

3.6. Memory footprint

Module Description
[Driver] HAL/CMSIS/BSP STM32 CMSIS Cortex, HAL and LL, Board Specific Package drivers
[Project] Core Native STM32 core components
[Project] App Main part of the application
[Project] Target Configuration files for ST67W6X_Network_Driver component
[MW] ST67W6X_Network_Driver Core and API System, Wi-Fi® and Network components
Util/Logging: Utility to process shell and trace messages onto the UART interface (can be changed by ITM)
[MW] FreeRTOS FreeRTOS kernel source
[Utility] lpm Tiny low-power Management
[Toolchain] Startup Int_vect, init routines, init table, CSTACK and HEAP
[Toolchain] EWARM Libraries Native compiler libraries

These values depend on the chosen toolset, and they can change in next releases.

3.6.1. ROM/Flash Memory footprint

The picture below shows the total read-only memory (flash) used by the HTTP Server application.

ST67W6X_HTTP_Server Read Only memory footprint.

The picture below shows the middleware ST67W6X_Network_Driver read-only memory (flash) used by Echo application.

ST67W6X_Network_Driver Read Only memory footprint used by ST67W6X_HTTP_Server application.

3.6.2. Read-write (RW) Memory footprint

The picture below shows only the sum of the static read/write memory (static RAM) of the HTTP Server application.

ST67W6X_HTTP_Server Read Write memory footprint

4. References