Difference between revisions of "AI:FP-AI-FACEREC1 getting started"

[unchecked revision] [quality revision]
m (Escoda Michael moved page FP-AI-FACEREC1 getting started to AI:FP-AI-FACEREC1 getting started: Previously without namspace)
m
 
Warning.png The face recognition binary is available on demand. Please contact the local STMicroelectronics support for more information about this application or send a request to edge.ai@st.com

This article explains how to get started on the Face Reco face recognition application running on the STM32 microcontroller. The face recognition application is capable of recognizing a user's face among those of enrolled users.

This article provides an overview of the following topics:

  • Overview of the required hardware setup
  • Overview of the software architecture
  • Description of the Face Reco application running on STM32

1 Hardware setup[edit]

The Face Reco application is running on a hardware setup made up of an STM32 microcontroller board connected to a camera module board.

1.1 STM32 board: STM32H747 Discovery Kit[edit]

The STM32H747I-DISCO is a complete demonstration and development platform for STMicroelectronics STM32H747XIH6 microcontroller, designed to simplify user application development. The STM32H747XIH6 device is based on the high-performance Arm® Cortex®-M7 and Cortex®-M4 32-bit RISC cores. The Cortex®-M7 core operates at up to 480 MHz and the Cortex®-M4 core at up to 240 MHz.

The STM32H747XIH6 device incorporates high-speed embedded memories with a dual-bank Flash memory of 2 Mbytes and of 1 Mbyte of RAM.

The other key specifications of the board are:

  • On-board STLINK-V3E debugger/programmer
  • USB OTG HS
  • 4” capacitive touch LCD display module with MIPI® DSI interface
  • 2 x 512-Mbit Quad-SPI NOR Flash memory
  • 256-Mbit SDRAM
  • 8-bit camera connector
  • microSD™ card
STM32H747I-DISCO board

1.2 Camera board[edit]

In the context of the Face Reco application, the firmware supports the two following camera sensors:

  • The OV5640 sensor
  • The OV9655 sensor

The recommended camera setup is the B-CAMS-OMV bundle for STM32 boards. Module boards are supported.

The B-CAMS-OMV bundle is made up of:

  • One camera module adapter board (MB1683)
  • One STMicroelectronics camera module (MB1379), based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
  • One flexible flat cable (FFC)

The picture below shows the B-CAMS-OMV without FFC:

B-CAM-OMV camera board

1.3 STM32H747I-DISCO connection to camera boards[edit]

The picture below shows how to connect the camera board to the STM32H747I-DISCO board using a flat flex cable:

Connection between  STM32H747I-DISCO and camera board
Warning.png Make sure that the STM32H747I-DISCO board is powered off (unplugged) to avoid short circuit when inserting the flat flex cable.

2 Software architecture[edit]

The figure below depicts the software architecture of the face recognition application:

Software architecture for the Face Reco application

Here is below a brief description of the middleware components:

2.1 STM32_AI_Runtime[edit]

This is an STM32 optimized AI library generated by the X-CUBE-AI tool when generating the C neural network model.

2.2 STM32_Image[edit]

This is a library of functions for image preprocessing, such as rescaling or pixel format conversion.

2.3 STM32_Face_Detect[edit]

Library containing functions for face detection purpose.

2.4 STM32_Face_Reco[edit]

Library containing functions for face recognition purpose.

3 Description of Face Reco application[edit]

Info.png In the current version of the Face Reco application: a single face can be detected and identified from the camera capture frame.

The figure below shows the different frame processing stages involved in the face recognition application:

Data pipe for the Face Reco application

3.1 Camera capture[edit]

The camera frame capture has the following characteristics:

  • Resolution is set to QVGA (320 x 240)
  • Pixel color format is set to RGB565

3.2 Frame Preprocessing[edit]

The main preprocessing stage involved in the Face Reco application is the pixel color format conversion so to convert the RGB565 captured frame into a RGB888 frame.

3.3 Face Detection[edit]

The Face Detection block is in charge of finding the faces present in the input frame (QVGA, RGB888). In the current version of the application, the maximum number of faces that can be found is set to one. The output of this block is a frame of resolution 96 x 96 that contains the face found in the input captured frame.

3.4 Face Recognition[edit]

The Face Recognition block is in charge of extracting features from the face and computing a signature (embedding vector) corresponding to the input face.

3.5 Face Identification[edit]

The Face Identification block is in charge of computing the distance between:

  • The vector produced by the Face Recognition block, and
  • Each of the vectors stored in memory (and corresponding to the enrolled faces)

The output Face Identification block generates the two following outputs:

  • a User Face ID corresponding to the minimum distance
  • a similarity score

4 Running the application[edit]

The application has two main operating modes:

  • The "nominal" mode

It is the default operating mode during which the application is attempting to match the face contained in the input frame with a specific User Face ID.

  • The "enrollment" mode

Prior to being able to link a face with a User Face ID, the system must have the User face ID recorded into its database. For that purpose, a user must enroll himself to have his face features (in the form of a feature vector) recorded into the memory.

Note that the current version of the Face Reco application does not support the retention of the enrolled users. In other words, all the enrollment information are lost upon reset.

Practically, here is how it works:

4.1 Nominal mode[edit]

Upon reset, the system is running in the so-called nominal mode.

As soon as a face is detected within the camera captured frame, a rectangle box is drawn around it.

If the system is not able to match the detected face with one of the enrolled faces (either because the user face is not yet enrolled or because the Face Identification similarity score is lower than the default recognition threshold), the "No match" message is displayed on the right banner of the LCD screen and the rectangle box is drawn in red.

If the system is able to match the detected face with one of the enrolled faces, the rectangle box is drawn in green and a thumbnail (representing the user's enrolled face matching the detected face) is displayed on the right banner of the LCD screen along with the following information:

  • The User Face ID
  • The similarity score expressed in percentage (%).

When in nominal mode a FPS (Frame Per Second) information is displayed at the top of the right banner. This FPS corresponds to the number of frames that could be processed by the system in one second. As a result, the FPS is directly linked to the following timings:

  • Duration of the Face Detection execution
  • Duration of the Face Recognition execution

The camera frame acquisition is performed in parallel of the Face Detection and Face Recognition algorithm executions.

Screenshot of the Face Reco application

4.2 Enrollment mode[edit]

In order to enroll his face, the user must perform a long press on the blue joystick [SEL] button present on the board. There exist two options for triggering the enrollment:

  • Either the enrollment is triggered immediately and automatically following up a long press on the joystick [SEL] button (= default behavior upon reset)
  • Or the enrollment is triggered after a 3 seconds countdown following up a long press on the joystick [SEL] button (refer to section Configuration menu for details on how to enable this mode)

In both cases, once the enrollment is completed the "ENROLLMENT COMPLETED RELEASE JOYSTICK" message is displayed and a thumbnail corresponding to the enrolled face is displayed on the right banner of the LCD screen along with the User Face ID.

Up to 100 users can be enrolled in the system.

In this version of the application, the enrollment information is stored in volatile memory. As a consequence they are lost when resetting the system.

4.3 Camera orientation[edit]

By default the OV5640 camera sensor is configured in such a way that the original image is generated without being flipped or mirrored. The original image appears on the display without being flipped or mirrored when the relative position of the B-CAMS-OMV bundle versus the STM32H747I-DISCO board is as below:

Position of camera vs STM32 board for original display.

If the relative position of the B-CAMS-OMV bundle versus the STM32H747I-DISCO board is different, there is the possibility to flip, mirror or flip & mirror the image captured by the OV5640 sensor. Refer to the section Configuration menu for details on how to modify the camera orientation settings.

4.4 Testing conditions[edit]

The user must keep in mind that the following parameters impact the accuracy of the recognition:

  • Ambiance light and illumination
  • Distance between the camera and the user (best results are achieved at distance <1.5 m)
  • Enrollment phase: it is important to perform enrollment in good conditions (i.e. good illumination and without moving so to avoid blurring)

Adjusting the camera contrast by pressing the joystick [LEFT] and [RIGHT] buttons is a way to improve the accuracy of the recognition. For an optimized recognition, good illumination condition is important.

4.5 Configuration menu[edit]

A configuration menu is available through a long press on the blue Wakeup button:

Config menu
  • "Display debug info" sub menu enables to visualize debug information such as:
    • Execution timing
    • Recognition threshold value
    • Number of enrolled user
  • "Enroll mode" sub menu enables to change the enrollment trigger mode:
    • Countdown
    • Immediate
  • "Change Face Reco Threshold" sub menu enables to change the value of the recognition threshold:
    • The recognition threshold corresponds to the similarity score above which the input face is successfully mapped to one of the enrolled faces.
    • The default recognition threshold is set to 0.70 and its value can be updated by steps of 0.05.
    • TAR (True Acceptance Rate) and FAR (False Acceptance Rate) are the metrics that have been used to compute the default value for the recognition threshold.
    • The True Acceptance Rate represents the degree at which the system can correctly match the biometric information from the same person.
    • The "False Acceptance Rate" is the probability of cases for which the system fallaciously authorizes an unauthorized person.
    • A recognition threshold of 0.70 corresponds to a FAR of ~1% when plotting the TAR=f(FAR) graph using a dedicated (non-public) test database.
  • "Change Camera Orientation" sub menu enables to change the flip and mirror settings of the camera :
    • None: original captured image
    • Flip: flips the captured image
    • Mirror: mirrors the captured image
    • Mirror and Flip: mirrors and flips the captured image

4.6 Programming Flashing the firmware binary in flash[edit]

The STM32CubeProgrammer (STM32CubeProg) tool can be used to flash the binary into the target memory.

Here is below the procedure to follow:

  • Connect to the target via ST-LINK
  • Select the Erasing & programming tab on the left to access the Erasing & programming view shown in the picture below
  • Browse for the binary of the application
  • Program the target
STM32CubeProgrammer screenshot


{{Warning | The face recognition binary is available on demand. Please contact the local STMicroelectronics support for more information about this application or send a request to [mailto:edge.ai@st.com edge.ai@st.com]}}

This article explains how to get started on the Face Reco face recognition application running on the STM32 microcontroller.
The face recognition application is capable of recognizing a user's face among those of enrolled users.

This article provides an overview of the following topics:
* Overview of the required hardware setup
* Overview of the software architecture
* Description of the Face Reco application running on STM32

== Hardware setup ==
The Face Reco application is running on a hardware setup made up of an STM32 microcontroller board connected to a camera module board.

=== STM32 board: STM32H747 Discovery Kit ===
The [https://www.st.com/en/product/stm32h747i-disco STM32H747I-DISCO]  is a complete demonstration and development platform for STMicroelectronics [https://www.st.com/en/product/stm32h747xi STM32H747XIH6] microcontroller, designed to simplify user application development.  The [https://www.st.com/en/product/stm32h747xi STM32H747XIH6] device is based on the high-performance Arm<sup>®</sup> Cortex<sup>®</sup>-M7 and Cortex<sup>®</sup>-M4 32-bit RISC cores. The Cortex<sup>®</sup>-M7 core operates at up to 480 MHz and the Cortex<sup>®</sup>-M4 core at up to 240 MHz.

The [https://www.st.com/en/product/stm32h747xi STM32H747XIH6] device incorporates high-speed embedded memories with a dual-bank Flash memory of 2 Mbytes and of 1 Mbyte of RAM.

The other key specifications of the board are: 

* On-board STLINK-V3E debugger/programmer 
* USB OTG HS
* 4” capacitive touch LCD display module with MIPI<sup>®</sup> DSI interface
* 2 x 512-Mbit Quad-SPI NOR Flash memory
* 256-Mbit SDRAM
* 8-bit camera connector
* microSD™ card
<div class="res-img">

[[File:STM32H747 DISCO.png|center| STM32H747I-DISCO board]]</div>


=== Camera board===

In the context of the Face Reco application, the firmware supports the two following camera sensors:
* The OV5640 sensor 
* The OV9655 sensor 

The recommended camera setup is the [https://www.st.com/en/product/b-cams-omv B-CAMS-OMV] bundle for STM32 boards. Module boards are supported.

The [https://www.st.com/en/product/b-cams-omv B-CAMS-OMV] bundle is made up of:
* One camera module adapter board (MB1683)
* One STMicroelectronics camera module (MB1379), based on the OV5640 image sensor offering a 5-Mpixel resolution with 8-bit color
* One flexible flat cable (FFC)

The picture below shows the [https://www.st.com/en/product/b-cams-omv B-CAMS-OMV] without FFC:<div class="res-img">

[[File:B-CAM-OMV.png|center|B-CAM-OMV camera board]]</div>

=== STM32H747I-DISCO connection to camera boards ===

The picture below shows how to connect the camera board to the [https://www.st.com/en/product/stm32h747i-disco STM32H747I-DISCO] board using a flat flex cable:<div class="res-img">

[[File:CameraBoard Connection.png|center| Connection between  STM32H747I-DISCO and camera board]]</div>


{{ Warning | Make sure that the STM32H747I-DISCO board is powered off (unplugged) to avoid short circuit when inserting the flat flex cable. }}

== Software architecture ==

The figure below depicts the software architecture of the face recognition application:<div class="res-img">

[[File:Soft archi.png|center| Software architecture for the Face Reco application]]</div>


Here is below a brief description of the middleware components:

=== STM32_AI_Runtime===

This is an STM32 optimized AI library generated by the [https://www.st.com/en/product/x-cube-ai X-CUBE-AI] tool when generating the C neural network model.

=== STM32_Image===

This is a library of functions for image preprocessing, such as rescaling or pixel format conversion.

=== STM32_Face_Detect===

Library containing functions for face detection purpose.

=== STM32_Face_Reco===

Library containing functions for face recognition purpose.

== Description of Face Reco application ==

{{Info | In the current version of the Face Reco application: a single face can be detected and identified from the camera capture frame.}}

The figure below shows the different frame processing stages involved in the face recognition application:
<div class="res-img">

[[File:FaceReco Dataflow.png|center| Data pipe for the Face Reco application]]</div>


=== Camera capture===

The camera frame capture has the following characteristics:
* Resolution is set to QVGA (320 x 240)
* Pixel color format is set to RGB565

=== Frame Preprocessing===

The main preprocessing stage involved in the Face Reco application is the pixel color format conversion so to convert the RGB565 captured frame into a RGB888 frame.

=== Face Detection===

The Face Detection block is in charge of finding the faces present in the input frame (QVGA, RGB888).
In the current version of the application, the maximum number of faces that can be found is set to one.
The output of this block is a frame of resolution 96 x 96 that contains the face found in the input captured frame.

=== Face Recognition===

The Face Recognition block is in charge of extracting features from the face and computing a signature (embedding vector) corresponding to the input face.

===Face Identification===

The Face Identification block is in charge of computing the distance between:
* The vector produced by the Face Recognition block, and
* Each of the vectors stored in memory (and corresponding to the enrolled faces)

The output Face Identification block generates the two following outputs:
* a ''User Face ID'' corresponding to the minimum distance
* a similarity score

== Running the application ==

The application has two main operating modes:

* The "nominal" mode
It is the default operating mode during which the application is attempting to match the face contained in the input frame with a specific ''User Face ID''.

* The "enrollment" mode
Prior to being able to link a face with a ''User Face ID'', the system must have the ''User face ID'' recorded into its database.
For that purpose, a user must enroll himself to have his face features (in the form of a feature vector) recorded into the memory.

Note that the current version of the Face Reco application does not support the retention of the enrolled users. In other words, all the enrollment information are lost upon reset.

Practically, here is how it works:

===Nominal mode=== 

Upon reset, the system is running in the so-called ''nominal'' mode.

As soon as a face is detected within the camera captured frame, a rectangle box is drawn around it.

If the system is not able to match the detected face with one of the enrolled faces (either because the user face is not yet enrolled or because the Face Identification similarity score is lower than the default recognition threshold), the "No match" message is displayed on the right banner of the LCD screen and the rectangle box is drawn in red.

If the system is able to match the detected face with one of the enrolled faces, the rectangle box is drawn in green and a thumbnail (representing the user's enrolled face matching the detected face) is displayed on the right banner of the LCD screen along with the following information:
* The ''User Face ID''
* The similarity score expressed in percentage (%).

When in nominal mode a FPS (Frame Per Second) information is displayed at the top of the right banner.
This FPS corresponds to the number of frames that could be processed by the system in one second.
As a result, the FPS is directly linked to the following timings:
* Duration of the Face Detection execution
* Duration of the Face Recognition execution

The camera frame acquisition is performed in parallel of the Face Detection and Face Recognition algorithm executions.
<div class="res-img">

[[File:screenshot facereco.png|center| Screenshot of the Face Reco application]]</div>


===Enrollment mode=== 

In order to enroll his face, the user must perform a long press on the blue joystick [SEL] button present on the board.
There exist two options for triggering the enrollment:
* Either the enrollment is triggered immediately and automatically following up a long press on the joystick [SEL] button (= default behavior upon reset)
* Or the enrollment is triggered after a 3 seconds countdown following up a long press on the joystick [SEL] button (refer to section [[Face_Recognition:_quick_start_guide#Configuration menu | Configuration menu]] for details on how to enable this mode)

In both cases, once the enrollment is completed the "ENROLLMENT COMPLETED RELEASE JOYSTICK" message is displayed and a thumbnail corresponding to the enrolled face is displayed on the right banner of the LCD screen along with the ''User Face ID''.

Up to 100 users can be enrolled in the system.

In this version of the application, the enrollment information is stored in volatile memory. As a consequence they are lost when resetting the system.

===Camera orientation=== 

By default the OV5640  camera sensor is configured in such a way that the original image is generated without being flipped or mirrored.
The original image appears on the display without being flipped or mirrored when the relative position of the [https://www.st.com/en/product/b-cams-omv B-CAMS-OMV] bundle versus the [https://www.st.com/en/product/stm32h747i-disco STM32H747I-DISCO] board is as below:

[[File:Cam Orientation-None.png|center|middle|650px|Position of camera vs STM32 board for original display.]]

If the relative position of the  [https://www.st.com/en/product/b-cams-omv B-CAMS-OMV] bundle versus the  [https://www.st.com/en/product/stm32h747i-disco STM32H747I-DISCO] board is different, there is the possibility to flip, mirror or flip & mirror the image captured by the OV5640 sensor.
Refer to the section [[Face_Recognition:_quick_start_guide#Configuration menu | Configuration menu]] for details on how to modify the camera orientation settings.

===Testing conditions=== 

The user must keep in mind that the following parameters impact the accuracy of the recognition:
* Ambiance light and illumination
* Distance between the camera and the user (best results are achieved at distance <1.5 m)
* Enrollment phase: it is important to perform enrollment in good conditions (i.e. good illumination and without moving so to avoid blurring)

Adjusting the camera contrast by pressing the joystick [LEFT] and [RIGHT] buttons is a way to improve the accuracy of the recognition. For an optimized recognition, good illumination condition is important.

===Configuration menu=== 

A configuration menu is available through a long press on the blue Wakeup button:
<div class="res-img">
[[File:screenshot config menu.png|center| Config menu]]</div>


* "''Display debug info''" sub menu enables to visualize debug information such as:
** Execution timing
** Recognition threshold value
** Number of enrolled user

* "''Enroll mode''" sub menu enables to change the enrollment trigger mode:
** Countdown
** Immediate

* "''Change Face Reco Threshold''" sub menu enables to change the value of the recognition threshold:
** The recognition threshold corresponds to the similarity score above which the input face is successfully mapped to one of the enrolled faces.
** The default recognition threshold is set to 0.70 and its value can be updated by steps of 0.05.
** TAR (''True Acceptance Rate'') and FAR (''False Acceptance Rate'') are the metrics that have been used to compute the default value for the recognition threshold.  
** The ''True Acceptance Rate'' represents the degree at which the system can correctly match the biometric information from the same person. 
** The "False Acceptance Rate" is the probability of cases for which the system fallaciously authorizes an unauthorized person.
** A recognition threshold of 0.70 corresponds to a FAR of ~1% when plotting the TAR=f(FAR) graph using a dedicated (non-public) test database.

* "''Change Camera Orientation''" sub menu enables to change the flip and mirror settings of the camera :
**None: original captured image
**Flip: flips the captured image
**Mirror: mirrors the captured image
** Mirror and Flip: mirrors and flips the captured image

===Flashing the firmware binary=== 
{{ReviewsComments|-- [[User:Gerald Baeza|Gerald Baeza]] ([[User talk:Gerald Baeza|talk]]) 10:28, 11 March 2021 (CET)<br />Be careful because "flashing" means "clignotement". "Flash programming" or "Programming the firmware binary in flash=== " should be prefered to avoid ambiguity with english speakers}}The STM32CubeProgrammer ([https://www.st.com/en/product/stm32cubeprog STM32CubeProg]) tool can be used to flash the binary into the target memory.

Here is below the procedure to follow:
* Connect to the target via ST-LINK 
* Select the ''Erasing & programming'' tab on the left to access the ''Erasing & programming'' view shown in the picture below
* Browse for the binary of the application
* Program the target
<div class="res-img">

[[File:STM32CubeProgrammer.png|center| STM32CubeProgrammer screenshot]]</div>

<noinclude>

[[Category:Artifical Intelligence|01]]
{{PublicationRequestId | 18222 | 2020-12-11 }}	</noinclude>
Line 224: Line 224:
 
** Mirror and Flip: mirrors and flips the captured image
 
** Mirror and Flip: mirrors and flips the captured image
   
===Flashing the firmware binary===  
+
===Programming the firmware binary in flash===  
{{ReviewsComments|-- [[User:Gerald Baeza|Gerald Baeza]] ([[User talk:Gerald Baeza|talk]]) 10:28, 11 March 2021 (CET)<br />Be careful because "flashing" means "clignotement". "Flash programming" or "Programming the firmware binary in flash" should be prefered to avoid ambiguity with english speakers}}
 
 
The STM32CubeProgrammer ([https://www.st.com/en/product/stm32cubeprog STM32CubeProg]) tool can be used to flash the binary into the target memory.
 
The STM32CubeProgrammer ([https://www.st.com/en/product/stm32cubeprog STM32CubeProg]) tool can be used to flash the binary into the target memory.