X-CUBE-ST67W61 Architecture

back to main page

1. General description

1.1. Introduction

X-CUBE-ST67W61 is a set of software components implementing host applications driving a Wi-Fi and Bluetooth® LE coprocessor (ST67W611M). The coprocessor is controlled through an AT command over an SPI interface.

The figure below depicts the architecture of the solution.

ST67W611M architecture view

1.2. ST67W611M features

The ST67W611M features the following:

  • 2.4 GHz RF transceiver
  • Integrated RF balun, PA/LNA
  • External PA/LNA support
  • Wi-Fi 6 (IEEE 802.11 b/g/n/ax)
  • Wi-Fi/Bluetooth coexistence
  • Wi-Fi security WPS/WEP/WPA/WPA2/WPA3
  • Wi-Fi 20/40 MHz bandwidth, 1T1R, up to 229.4 Mbps
  • IEEE 802.11e QoS WMM (Wi-Fi multi-media)
  • IEEE 802.11w PMF (Protected Management Frames)
  • STA, SoftAP, STA + SoftAP
  • LDPC, STBC, beamformee, DL/UL OFDMA, MU-MIMO, Target Wake Time (TWT), Spatial Reuse
  • (SR), Dual Carrier Modulation (DCM), Extended Range (ER)
  • A-MPDU, A-MSDU, immediate block ACK, fragmentation, and defragmentation
  • Rx diversity
  • Bluetooth 5.3 (BLE)

1.3. Overview

1.3.1. SW top view

ST67W61 Host software architecture

The X-CUBE-ST67W61 is composed of a set of applications, ST67W6X_Network_Driver middleware, and ST67W61 drivers. In particular, it:

  • Exposes the generic API to applications offering:
    • System and OTA services
    • Bluetooth® LE services
    • Wi‑Fi® API services
    • Net module is aligned on BSD socket (blocking socket)
    • MQTT and HTTP services
  • Encompasses ST67W61 AT driver which:
    • Exposes basic AT command API
    • Parses SPI recv message to detect boundaries of AT messages.
    • Detects out of band message (nonsolicited messages, asynchronous event) and executes associated callback
  • Requires SPI sync module:
    • For sending and receiving messages to/from SPI link
    • Does not have a callback mechanism to be informed that some data are ready to be read; the dedicated Rx thread at higher level handles the received data and messages

Eight applications are delivered as part of the X-CUBE-ST67W61:

Additionally, one demonstration is provided:

1.3.2. FreeRTOS implementation view

ST67W61 middleware driver: FreeRTOS view


Spi_iface runs within a FreeRTOS thread which wakes up any time a DMA from SPI Rx or SPI Tx is triggered. The Spi_iface embeds two buffer queues which contain data to be sent to the ST67W611M NCP and data to be received from the ST67W611M NCP. The Spi_iface module implements the frame protocol between the host and the ST67W611M NCP. This frame protocol features a synchronization word, sequence number, length, the buffer, and a crc32 protecting the frame.

The scope of the AT driver is to format the AT messages on the Tx path (host to ST67W611M coprocessor) and parse the AT messages on the Rx path (ST67W611M coprocessor to host). Its sits on top of the Spi_iface.

The AT driver is constituted of two units:

  • One AT command unit handles the AT commands and responses. After sending a command through ATsend, the caller waits until the response is available on ATrecv.
  • Another unit retrieves the message, parses, and dispatches it to the upper layer. AT driver runs a thread (ATD_RxPooling_task) to extract received data. This thread parses the received data to find AT message separators. The extracted message is stored in a local buffer ATD_RecvBuf. The message is analyzed to detect if it is an asynchronous event (unsolicited), a synchronous response, or data-payload.
    • Synchronous responses are pushed in the ATD_Resp_Queue. Such a queue serves to sync the ATD_RxPooling_task with the application tasks. The response is then extracted from the ATD_Resp_Queue when the ATrecv is executed by the task that has sent the command. Actually, after sending a command through ATsend such tasks call ATrecv which waits until the response is available in the ATD_Resp_Queue, unless the timeout expires.
    • Asynchronous (unsolicited) event messages are pushed in dedicated ATD_Evt_Queue. The AT driver runs a second thread (ATD_EventsPooling_task) which pulls the messages from ATD_Evt_Queue; depending on the event “type” (Wi-Fi, Bluetooth® LE, Net, etc.) dedicated functions (AT_xx_Event) are executed to fully decode the event (pointer to the ATD_Evt_xMessageBuffer is passed as a parameter) and it sends the extracted parameters to the upper layer through callbacks.
    • Data-payload also arrives from SPI through ATD_RecvBuf. It has a specific treatment: it is copied to buffers allocated directly by the application which provides the pointer where ATD_RxPooling_task has to copy the data-payload. The application has also the responsibility to consume it in due time, for this, different strategies can be adopted.

Services APIs are the application APIs provided to the customers to build their application. The services APIs feature:

  • System services manage the central system functions of the network control processor (NCP). Key functionalities include:
    • Power management: Controls power modes, sleep states, and energy-saving features
    • System information: Provides access to system status, diagnostics, and hardware information
  • Over-the-Air (OTA) updates manage firmware updates and system upgrades remotely.
  • Bluetooth® LE services manage Bluetooth connections and data exchange. Key functionalities include:
    • Connection management: Establishes and maintains Bluetooth® LE connections with other devices
    • Data transmission: Sends data packets over Bluetooth® LE connections
    • Notifications: Receives and processes Bluetooth® LE notifications from connected devices
    • Security: Establishes secure Bluetooth® LE connections
  • Wi-Fi services handle Wi-Fi network control and management. Key functionalities include:
    • Network scanning: Searches for available Wi-Fi networks
    • Connection management: Connects to and disconnects from Wi-Fi networks
    • Signal strength monitoring: Monitors and reports the strength of Wi-Fi signals
  • Net services manage the TCP/IP stack and routes data across the network. Key functionalities include:
    • TCP/IP stack management: Handles the core TCP/IP protocols for data communication
    • Data routing: Routes TCP/IP data packets to and from the network
    • Network configuration: Manages IP addresses, subnets, and other network settings
  • MQTT (message queuing telemetry transport) services:
    • Publish/subscribe: Manages MQTT topics and message exchanges
    • Broker communication: Connects to and communicates with MQTT brokers
  • HTTP (HyperText transfer protocol) services:
    • Request handling: Manages HTTP HEAD, GET, POST, and PUT requests
    • Response processing: Processes and interprets HTTP responses from servers

Further details and technical specifications are provided in section Services API of the documentation.

1.3.3. General requirement

  • All applications are based on the embedded system RTOS FreeRTOS.
  • Each protocol module API has a CLI command (See CLI/Shell).
  • Each module uses the logging mechanism from FreeRTOS (see Logging).
  • The application must be easily portable across different STM32s.
  • No secure channel (for example, safelink) is implemented.

1.4. Framework

1.4.1. FreeRTOS

The projects and the middleware are based on the FreeRTOS.

For ThreadX porting, ThreadX to FreeRtos port is available. You can refer to threadx/utility/rtos_compatibility_layers/FreeRTOS

Please Note that stack Size in ThreadX is defined in Bytes while the stack size in FreeRtos is in words.

1.4.2. CLI from shell

The shell features:

  • Autocompletion
  • Command history (down/up key)
  • Right/left key
  • Backspace functionality
  • Help and command-specific help
  • Decentralized command implementation
  • Colorized CLI

1.4.3. Logging

The logging component provides 4 logging macros listed in increasing order of verbosity:

  • LogError()
  • LogWarn()
  • LogInfo()
  • LogDebug()

The logging component features:

  • Differed logging: Message is built within the calling function and sent to a log queue. The log queue is consumed by an output task. This limits the real-time impact of logging.
  • Standard log levels: See FreeRtos website [1]
  • Add metadata to the log message such as timestamp, filename and line number, task name. Metadata inclusion is configurable.
  • Memory consumption scales with needs (dynamic allocation of log buffer). Maximum size is configurable.
  • Thread safe
  • Output hardware choice is left to the application writer.

For example, LogError() is only called when there is an error, so it is the least verbose, whereas LogDebug() is called more frequently to provide debug level information.

The application can output the logs on:

  • UART hardware (same or other UART than CLI)
  • ITM (dedicated ARM debug port on SWO)

1.4.4. FreeRTOS low power application

  • The low power host supports FreeRTOS™ tickless idle mode to allow the STM32 to enter low power mode anytime FreeRTOS is idle. LPTIM1 is used as a low power timer while the system is in low power mode to maintain the time. Minimum low power mode is configurable in app_conf.h
  • The ST67W611M1 power save depends on the connection of the ST67W611M1:
    • When unconnected, the power save mode is activated by setting W6X_SetPowerMode to 1. This sets the ST67W611M1 in standby low power mode after each command sent to the ST67W611M1 .
    • If the ST67W611M1 device is connected to an access point, the device does not enter in standby power-save mode unless DTIM (using W6X_WiFi_SetDTIM) is activated.
    • If the ST67W611M1 device is connected to a Wi-Fi®-6 access point, the individual TWT power save can be entered. W6X_SetPowerMode and W6X_WiFi_SetDTIM must be set to 0 before configuring TWT (TWT W6X_WiFi_SetupTWT) and starting TWT (W6X_WiFi_SetTWT).

1.4.5. FOTA support

There are two types of FOTA available:

  • The FOTA application that updates the NUCLEO-U575ZI-Q and the ST67W611M1 using a FOTA header descriptor in JSON format
  • The FOTA application that only updates the ST67W611M1, that does not use a FOTA header descriptor

When the FOTA option is enabled, a low-priority task is initiated and waits for an event to start the FOTA update process (timer, button push, or CLI command for example). Then it fetches all the necessary resources to proceed with the update.

For the NUCLEO-U575ZI-Q FOTA variant, the header descriptor contains information such as the versions of the binaries and values for a binary integrity check. The NUCLEO-U575ZI-Q binary is stored in flash and if the integrity verification passes, it boots on the binary stored in flash on next reboot.

For the ST67W611M1 update, during download of the binary, the data is transferred to the ST67W611M1. When the transfer is done, the ST67W611M1 performs the necessary check and reboots on the new binary.

Pythons scripts are provided to help with FOTA header descriptor generation and run server hosting files needed by the FOTA in a local environment.

2. Services API

2.1. System services

2.1.1. System API functions

The system module proposes an API set of functions needed to control the chip. Below is a list of the available main functions:

Function Description
W6X_Init Initialize the LL part of the W6X core.
W6X_DeInit De-Initialize the LL part of the W6X core.
W6X_RegisterAppCb Register Upper Layer callbacks.
W6X_GetCbHandler Get the W6X Callback handler.
W6X_GetModuleInfo Get the W6X module info.
W6X_ModuleInfoDisplay Display the module information.
W6X_SetPowerMode Configure Power mode.
W6X_GetPowerMode Get Power mode.
W6X_FS_WriteFile Write a file to the NCP file system.
W6X_FS_ReadFile Read a file from the NCP file system.
W6X_FS_DeleteFile Delete a file from the NCP file system.
W6X_FS_GetSizeFile Get the size of a file in the NCP file system.
W6X_FS_ListFiles List files in the file system (NCP and Host if LFS is enabled)
W6X_RestoreDefaultConfig Restore module default configuration.
W6X_ExeATCommand Send an AT command to the NCP

2.2. FOTA services

The FOTA module manages ST67W611M1 firmware updates remotely.

2.2.1. FOTA APIs functions

The FOTA (firmware update Over-The-Air) module proposes an API set of functions needed to update the ST67W611M1. Below is a list of the available main functions:

Function Description
W6X_OTA_Starts Starts the ST67W611M1 OTA process.
W6X_OTA_Finish Finish the ST67W611M1 OTA process which reboots the module to apply the new firmware.
W6X_OTA_Send Send the firmware binary to the module.

2.3. Wi-Fi services

2.3.1. Wi-Fi APIs functions

The Wi-Fi module proposes an API set of functions needed to control the chip. Below is a list of the available main functions:

Function Description
W6X_WiFi_Init Init the Wi-Fi module.
W6X_WiFi_DeInit De-Init the Wi-Fi module.
W6X_WiFi_StartSta Set the module in station mode.
W6X_WiFi_Scan List a defined number of available access points.
W6X_WiFi_PrintScan Print the scan results.
W6X_WiFi_Connect Join an Access Point.
W6X_WiFi_GetStaMode Get the Wi-Fi station mode.
W6X_WiFi_SetStaMode Set the Wi-Fi station mode.
W6X_WiFi_GetAutoConnect Retrieve autoconnect state.
W6X_WiFi_SetHostname This function set the Wi-Fi STA host name.
W6X_WiFi_GetHostname This function retrieves the Wi-Fi STA host name.
W6X_WiFi_GetStaIpAddress This function retrieves the Wi-Fi interface's IP address.
W6X_WiFi_GetStaMacAddress This function retrieves the Wi-Fi station MAC address.
W6X_WiFi_SetStaIpAddress This function set the Wi-Fi interface's IP address.
W6X_WiFi_GetDnsAddress This function retrieves the Wi-Fi DNS addresses.
W6X_WiFi_SetDnsAddress This function set the Wi-Fi DNS addresses.
W6X_WiFi_GetStaState This function retrieves the Wi-Fi station state.
W6X_WiFi_GetCountryCode This function retrieves the country code configuration.
W6X_WiFi_SetCountryCode This function set the country code configuration.
W6X_WiFi_Disconnect Disconnect from a Wi-Fi Network.
W6X_WiFi_StartAp Configure a Soft-AP.
W6X_WiFi_StopAp Stop the Soft-AP.
W6X_WiFi_GetApConfig Get the Soft-AP configuration.
W6X_WiFi_ListConnectedSta List the connected stations.
W6X_WiFi_DisconnectSta Disconnect station from the Soft-AP.
W6X_WiFi_GetApMode Get the Wi-Fi Soft-AP mode.
W6X_WiFi_SetApMode Set the Wi-Fi Soft-AP mode.
W6X_WiFi_GetApIpAddress Get the Soft-AP IP addresses.
W6X_WiFi_GetDhcp Get the DHCP configuration.
W6X_WiFi_SetDhcp Set the DHCP configuration.
W6X_WiFi_GetApMacAddress This function retrieves the Wi-Fi Soft-AP MAC address.
W6X_WiFi_StateToStr Convert the Wi-Fi state to a string.
W6X_WiFi_SecurityToStr Convert the Wi-Fi security type to a string.
W6X_WiFi_ReasonToStr Convert the Wi-Fi error reason to a string.
W6X_WiFi_SetDTIM Set Low Power Wi-Fi DTIM (Delivery Traffic Indication Message)
W6X_WiFi_GetDTIM Get Low Power Wi-Fi DTIM (Delivery Traffic Indication Message)
W6X_WiFi_SetupTWT Setup Target Wake Time (TWT) for the Wi-Fi station.
W6X_WiFi_SetTWT Set Target Wake Time (TWT) for the Wi-Fi station.
W6X_WiFi_TeardownTWT Teardown Target Wake Time (TWT) for the Wi-Fi station.

2.3.2. Wi-Fi events

The following events are sent back to the application layer:

Event Description
STA events
W6X_WIFI_EVT_CONNECTED_ID Event received when the station is connected to an access point.
W6X_WIFI_EVT_DISCONNECTED_ID Event received when the station is disconnected to an access point.
W6X_WIFI_EVT_GOT_IP_ID Event received when the station receives an IP address after a successful connection to an access point.
W6X_WIFI_EVT_CONNECTING_ID Event received when the station is in the connection process to an access point.
W6X_WIFI_EVT_REASON_ID Event received when the device encouters an issue in the connection process or at disconnection.
soft-AP events
W6X_WIFI_EVT_STA_CONNECTED_ID Event received when a station is connected to the soft-AP.
W6X_WIFI_EVT_STA_DISCONNECTED_ID Event received when a station is disconnected from the soft-AP.
W6X_WIFI_EVT_DIST_STA_IP_ID Event received when a station, connected to the soft-AP, receives an IP address.

2.3.3. Wi-Fi FSM

Shown below is the Wi-Fi FSM for the station mode only that describes the different states of the system.

Wi-Fi Station FSM

The second chart below shows the behavior of the system when the station and the soft access point modes are enabled (station mode is active by default and cannot be deactivated).

When both interfaces are enabled, some verifications must be done to ensure they are operating on the same channel and do not use the same subnet IP address to avoid unexpected behaviors.

Wi-Fi STA + soft-AP behavior chart.

The system behavior is the same if the soft-AP is on, the station is not connected, and it tries to connect to an AP. The same sequence is performed to verify channel and subnet compatibility.

When the soft-AP is stopped, all connected stations are disconnected from the soft-AP.


2.4. Net services

The net module implements all the API functions related to the internet protocol.  It supports the BSD socket API and some specific services that are commonly used, like ping or SNTP services.

Up to five sockets can be managed in parallel.

2.4.1. NET APIs functions

The NET module proposes an API set of functions needed to control TCP/IP stack features. Below is a list of the available main functions:

Function Description
W6X_Net_Init Init the Net module.
W6X_Net_DeInit De-Init the Net module.
W6X_Net_Ping Ping an IP address in the network.
W6X_Net_GetHostAddress Get IP address from URL using DNS.
W6X_Net_GetTime Query date string from SNTP, the used format is asctime style time.
W6X_Net_GetSNTPConfiguration Get current SNTP status, timezone and servers.
W6X_Net_SetSNTPConfiguration Set SNTP status, timezone and servers.
W6X_Net_GetSNTPInterval Get SNTP Synchronization interval.
W6X_Net_SetSNTPInterval Set SNTP Synchronization interval.
W6X_Net_GetConnectionStatus Get information for an opened socket.
W6X_Net_Socket Get a socket instance is available.
W6X_Net_Close Close a socket instance and release the associated resources.
W6X_Net_Shutdown Shut down a server socket instance.
W6X_Net_Bind Bind a socket instance to a specific address.
W6X_Net_Connect Connect a socket instance to a specific address.
W6X_Net_Listen Listen for incoming connections on a socket.
W6X_Net_Accept Accept an incoming connection on a socket.
W6X_Net_Send Send data on a socket.
W6X_Net_Recv Receive data from a socket.
W6X_Net_Getsockopt Get a socket option.
W6X_Net_Setsockopt Set a socket option.
W6X_Net_Sendto Send data on a socket to a specific address.
W6X_Net_Recvfrom Receive data from a socket from a specific address.
W6X_Net_Tls_Credential_Add Add the credential to the TLS context.
W6X_Net_Tls_Credential_Delete Delete the credential from the TLS context.
W6X_Net_Inet_ntop Convert an IP address from uint32_t format to text.
W6X_Net_Inet_pton Convert an IP address from text format to uint32_t.

2.4.2. NET events

The following net events are sent back to the application layer:

Event Description
W6X_NET_EVT_SOCK_DATA_ID Event sent when data is received on a socket

2.4.3. NET FSM

The following figure shows the FSM for both TCP client and server socket.

There are six possible states:

  • RESET: Default state
  • ALLOCATED: An available socket has been reserved.
  • CONNECTED: Connection is established; socket is ready to exchange data. It can be either a client or a server (for incoming connections).
  • BIND: Socket is set to server mode and port and protocol are set, but the server is not running yet.
  • LISTENING: Server is running, ready to accept incoming connections.
  • CLOSING: Temporary state, when close or shutdown operations are being performed, after that, state is set to RESET again.
TCP sockets FSM

Since UDP is a connectionless protocol, UDP sockets use a slightly different state machine. State 'CONNECTED' is used here after the first call to 'sendto()' to signal that incoming data can be expected since communication with a server has been initiated:

UDP sockets FSM

2.5. Bluetooth® LE services

2.5.1. Bluetooth® LE APIs functions

The Bluetooth® LE module proposes an API set of functions needed to control the chip. Below is a list of the available main functions:

Function Description
W6X_Ble_Init Initialize Bluetooth® LE Server/Client.
W6X_Ble_DeInit De-Initialize Bluetooth® LE Server/Client.
W6X_Ble_GetInitMode Get Bluetooth® LE initialization mode.
W6X_Ble_SetBdAddress Set Bluetooth® LE BD Address.
W6X_Ble_GetBDAddress Retrieve the Bluetooth® LE BD address.
W6X_Ble_SetDeviceName Set Bluetooth® LE device Name.
W6X_Ble_GetDeviceName Retrieve the Bluetooth® LE device name.
W6X_Ble_SetTxPower Bluetooth® LE Set TX Power.
W6X_Ble_GetTxPower Bluetooth® LE Get TX Power.
W6X_Ble_SetAdvData Set Bluetooth® LE Advertising Data.
W6X_Ble_SetAdvParam Set Bluetooth® LE Advertising Parameters.
W6X_Ble_GetAdvParam Get Bluetooth® LE Advertising Parameters.
W6X_Ble_AdvStart Bluetooth® LE Server Start Advertising.
W6X_Ble_AdvStop Bluetooth® LE Server Stop Advertising.
W6X_Ble_SetScanRespData Set Bluetooth® LE scan response Data.
W6X_Ble_SetScanParam Set the Bluetooth® LE scan parameters.
W6X_Ble_GetScanParam Get the Scan parameters.
W6X_Ble_StartScan Start Bluetooth® LE Device scan.
W6X_Ble_StopScan Stop Bluetooth® LE Device scan.
W6X_Ble_Print_Scan Print Bluetooth® LE scan results.
W6X_Ble_SetConnParam Set Bluetooth® LE Connection Parameters.
W6X_Ble_GetConnParam Get the connection parameters.
W6X_Ble_Connect Create connection to a remote device.
W6X_Ble_Disconnect Disconnect from a Bluetooth® LE remote device.
W6X_Ble_GetConn Get the connection information.
W6X_Ble_ExchangeMTU Exchange Bluetooth® LE MTU length.
W6X_Ble_SetDataLength Set the Bluetooth® LE Data length.
W6X_Ble_CreateService Create Bluetooth® LE Service.
W6X_Ble_DeleteService Delete Bluetooth® LE Service.
W6X_Ble_CreateCharacteristic Create Bluetooth® LE Characteristic.
W6X_Ble_GetServicesAndCharacteristics List Bluetooth® LE Services and their Characteristics.
W6X_Ble_RegisterCharacteristics Register Bluetooth® LE characteristics.
W6X_Ble_RemoteServiceDiscovery Discover Bluetooth® LE services of remote device.
W6X_Ble_RemoteCharDiscovery Discover Bluetooth® LE Characteristics of a service remote device.
W6X_Ble_ServerSendNotification Notify the Characteristic Value from the Server to a Client.
W6X_Ble_ServerSendIndication Indicate the Characteristic Value from the Server to a Client.
W6X_Ble_ServerSetReadData Set the data when Client read characteristic from the Server.
W6X_Ble_ClientWriteData Write data to a Server characteristic.
W6X_Ble_ClientReadData Read data from a Server characteristic.
W6X_Ble_ClientSubscribeChar Subscribe to notifications or indications from a Server characteristic.
W6X_Ble_ClientUnsubscribeChar Unsubscribe to notifications or indications from a Server characteristic.
W6X_Ble_SetSecurityParam Set Bluetooth® LE security parameters.
W6X_Ble_GetSecurityParam Get Bluetooth® LE security parameters.
W6X_Ble_SecurityStart Start Bluetooth® LE security.
W6X_Ble_SecurityPassKeyConfirm Bluetooth® LE security pass key confirm.
W6X_Ble_SecurityPairingConfirm Bluetooth® LE pairing confirm.
W6X_Ble_SecuritySetPassKey Bluetooth® LE set passkey.
W6X_Ble_SecurityPairingCancel Bluetooth® LE pairing cancel.
W6X_Ble_SecurityUnpair Bluetooth® LE unpair.
W6X_Ble_SecurityGetBondedDeviceList Bluetooth® LE get paired device list.

2.5.2. Bluetooth® LE events

The following Bluetooth® LE events are sent back to the application layer:

Event Description
W6X_BLE_EVT_CONNECTED_ID Bluetooth® LE connection established.
W6X_BLE_EVT_DISCONNECTED_ID Bluetooth® LE connection ends.
W6X_BLE_EVT_CONNECTION_PARAM_ID Bluetooth® LE connection parameters update.
W6X_BLE_EVT_READ_ID Read operation from Bluetooth® LE remote device.
W6X_BLE_EVT_WRITE_ID Write operation from Bluetooth® LE remote device.
W6X_BLE_EVT_SERVICE_FOUND_ID Bluetooth® LE service discovered on remote device.
W6X_BLE_EVT_CHAR_FOUND_ID Bluetooth® LE characteristic discovered on remote device.
W6X_BLE_EVT_INDICATION_STATUS_ENABLED_ID Bluetooth® LE indication enabled.
W6X_BLE_EVT_INDICATION_STATUS_DISABLED_ID Bluetooth® LE indication disabled.
W6X_BLE_EVT_NOTIFICATION_STATUS_ENABLED_ID Bluetooth® LE notification enabled.
W6X_BLE_EVT_NOTIFICATION_STATUS_DISABLED_ID Bluetooth® LE notification disabled.
W6X_BLE_EVT_INDICATION_ACK_ID Bluetooth® LE Indication acknowledged.
W6X_BLE_EVT_INDICATION_NACK_ID Bluetooth® LE Indication unacknowledged.
W6X_BLE_EVT_NOTIFICATION_DATA_ID Bluetooth® LE service receives notification/indication data.
W6X_BLE_EVT_MTU_SIZE_ID Bluetooth® LE MTU size update.
W6X_BLE_EVT_PAIRING_FAILED_ID Bluetooth® LE pairing failed.
W6X_BLE_EVT_PAIRING_COMPLETED_ID Bluetooth® LE pairing completed.
W6X_BLE_EVT_PAIRING_CONFIRM_ID Bluetooth® LE pairing confirm notification.
W6X_BLE_EVT_PASSKEY_ENTRY_ID Bluetooth® LE pairing passkey entry notification.
W6X_BLE_EVT_PASSKEY_DISPLAY_ID Bluetooth® LE pairing passkey display notification.
W6X_BLE_EVT_PASSKEY_CONFIRM_ID Bluetooth® LE pairing passkey confirm notification.

2.6. HTTP Services

The HTTP module offers HTTP requests and processes and interprets HTTP responses from servers.

It supports both HTTP and HTTPS with HEAD, GET, PUT and POST methods.

For POST and PUT requests, the following content types can be used:

  • Text/plain : Regular text without any formatting
  • Application/x-www-form-urlencoded : Data is given as key value pairs (key1=value1&key2=value2...)
  • Application/json : JSON format
  • Application/xml : XML format
  • Application/octet-stream : Binary data

2.6.1. HTTP APIs function

The HTTP module proposes an API function to create HTTP client requests.

Function Description
W6X_HTTP_Client_Request HTTP Client request based on BSD socket.

2.7. MQTT services

2.7.1. MQTT APIs functions

The MQTT module proposes an API set of functions needed to control the chip. Below is a list of the available main functions:

Function Description
W6X_MQTT_Init Init the MQTT module.
W6X_MQTT_DeInit De-Init the MQTT module.
W6X_MQTT_SetRecvDataPtr Set/change the pointer where to copy the Recv Data.
W6X_MQTT_Configure MQTT Set user configuration.
W6X_MQTT_Connect MQTT Connect to broker.
W6X_MQTT_GetConnectionStatus MQTT Get connection status.
W6X_MQTT_Disconnect MQTT Disconnect from broker.
W6X_MQTT_Subscribe MQTT Subscribe to a topic.
W6X_MQTT_GetSubscribedTopics MQTT Get subscribed topics.
W6X_MQTT_Unsubscribe MQTT Unsubscribe from a topic.
W6X_MQTT_Publish MQTT Publish a message to a topic.
W6X_MQTT_StateToStr Convert the MQTT state to a string.

2.7.2. MQTT events

The following MQTT events are sent back to the application layer:

Event Description
W6X_MQTT_EVT_CONNECTED_ID Event received when the MQTT client is connected to the broker.
W6X_MQTT_EVT_DISCONNECTED_ID Event received when the MQTT client is disconnected from the broker.
W6X_MQTT_EVT_SUBSCRIPTION_RECEIVED_ID Event received when the MQTT client receives data from a topic it subscribed to.

3. References