How to perform people counting using FP-AI-VISION1 and STM32H747XI

Revision as of 20:06, 13 October 2023 by Registered User

Some recent STM32H747I-DISCO kits are shipping with MB1166-A09 LCD daughterboards. This daughterboard uses an updated LCD controller, NT35510. This article describes how to run FP-AI-VISION1 projects kits with the updated LCD daughterboard, with a focus on incorporating the updated LCD driver into existing projects.

Prerequisites: 1. STM32H747I-DISCO with LCD daughterboard "MB1166-A09" Note: This guide is not suitable for MB1166-A08 and MB1166-A10 LCD revisions. Follow the instructions given in FP-AI-VISION1 / TODO for these revisions. 2. Computer with STM32CubeIDE installed (v1.13.1 or higher)


Steps: 1. Download and unzip NT35510 drivers from this zip file. Alternatively, up-to-date drivers can be downloaded directly from the [STM32CubeH7 GitHub repo](https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Drivers/BSP/Components/nt35510). 2. Copy the entire nt35510 directory to ```..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\``` 3. Copy ```stm32h747i_discovery_lcd.c``` and ```stm32h747i_discovery_lcd.h``` , and paste them into ```..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\``` 4. Use a text editor to open ```..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h```. On line 34, make the following changes: ```C /* LCD controllers defines */

  1. define USE_LCD_CTRL_NT35510 1U
  2. define USE_LCD_CTRL_OTM8009A 0U
  3. define USE_LCD_CTRL_ADV7533 0U

```

5. TODO: Drag/drop nt355510 to components directory in CubeIDE 6. Compile and flash

No categories assignedEdit