Revision as of 07:32, 11 May 2021 by Registered User


1. Principle of SVPWM

Space vector modulation index is limited to (√3)/2 but there is way to extend this limit with the over-modulation. This technique is required when the modulation index (the length of the reference space vector Us) exceeds the edges of the hexagon


1.1. Linear mode

STM32 MC Overmodulation slide9 1.png

In the linear area, V'cmd can keep both the amplitude and angle of Vcmd, then V'cmd=T'1*V1+T'2*V2 with T'1=T1 and T'2=T2

1.2. The detail OVM mode 1

STM32 MC Overmodulation slide10 1.png
STM32 MC Overmodulation slide10 2.png


1.3. The detail OVM mode 2

STM32 MC Overmodulation slide11 1.png
STM32 MC Overmodulation slide11 2.png


STM32 MC Overmodulation slide12 1.png
STM32 MC Overmodulation slide12 2.png


STM32 MC Overmodulation slide13 1.png
STM32 MC Overmodulation slide13 2.png


STM32 MC Overmodulation slide14 1.png
STM32 MC Overmodulation slide14 2.png


STM32 MC Overmodulation slide15.png


STM32 MC Overmodulation slide16.png


1.4. Example: F4 three shunt with Shinano motor at 4000rpm

STM32 MC Overmodulation slide17.jpg