This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Coming soon |
Click here for BLE overview
1. How To...
1.1. Introduction
This wiki page is a guideline describing how to perform the main activities with .
1.2. How to find the needed delivered binary
1.3. How to set up the Teraterm parameters
- Terminal
- [New line]
- [Receive]: Auto
- [Transmit]: CR
- [Local echo] selected
- [New line]
- Serial
- [Baud rate]: 115200
- [Data]: 8 bit
- [Parity]: none
- [Stop]: 1 bit
- [Flow control]: none
- [Transmit delay]: 10 ms each
1.4. How to configure the modem radio band
- Open a Tera Term serial terminal and set the right parameters
- Start the firmware and select Modem power on option in the boot menu
- Type the modem command to get help of the modem configuration.
1.5. How to build and install delivered applications
Refer to this page to see how to build and install example application using IAR IDE or Cube IDE: Build & Install BLE example application on STM32WB platforms
1.6. How to change default behavior of the application
1.7. How to implement your own application
The easiest way to implement your application is to adapt