This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
Coming soon |
Click here for BLE overview
1. Introduction
The STM32CubeWB MCU Package provides software components running on the STM32WB Series MCU.
The STM32WB combines a a well-know ARM Cortex-M4 for the application, plus, a 2.4 GHz radio subsystem and a ARM Cortex-M0+ core for the wireless stack processor, which can be considered in most cases as "black box"
File:STM32WB SW archi.png
STM32WB_Sotware_Architecture_Dual_Core
For all examples provided with package, the following integrated development environments are supported:
- STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
- IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
- Keil® Microcontroller Development Kit (MDK-ARM)
2. STM32WB BLE Software architecture
3. BT SIG Profile application
- Heart Rate Sensor
- ...
4. Proprietary Application
- P2P server
- https://wiki.st.com/stm32mcu/wiki/STM32WB_-_BLE_AT_Server
- https://wiki.st.com/stm32mcu/wiki/STM32WB_-_Bluetooth%C2%AE_LE_Fast_FUOTA
5. BLE Mesh
- https://wiki.st.com/stm32mcu/wiki/Sensor_Server_Measurement_on_Sensor_Client_Request
- https://wiki.st.com/stm32mcu/wiki/Vendor_Model_Demonstration