Zigbee certification process for STM32WB and STM32WBA

1. Introduction

Zigbee® is widely used in smart homes, commercial, and industrial applications. To ensure interoperability between Zigbee devices, the CSA has established a certification process that involves rigorous testing.
Depending on the scope of the certification, two types of certifications are defined:

  • Platform Certification
    • Zigbee PRO Compliant Platform (FFD/RFD)
  • End Product Certification
    • Zigbee 3.0 Certified Product (FFD/RFD)
    • Zigbee Smart Energy Product (FFD/RFD)

Zigbee Certified End Product must be built on a Zigbee PRO Compliant Platform.

2. Zigbee Certification Process

To obtain a Zigbee certification, companies must join the Zigbee Alliance and follow a general set of steps:

  • Select the type of certification to pursue, such as Zigbee Platform Certification or End Product Certification.
  • Ensuring that the product meets the necessary hardware, software, and functional requirements.
  • If the company wishes, they can also conduct an in-house pre-certification to identify and address any issues before submitting the product for testing.
  • Once the product is ready, the company must select an authorized test house and submit the product for testing. The list of authorized testing providers could be found here.
  • If the product fails any of the tests, the company must address the issues and resubmit the product for testing.
  • Once the product passes all the tests, the company will receive the appropriate certification, such as the Zigbee Certified logo.

3. Zigbee Platform Certification

  • Zigbee Platform Certification is a process that certifies the compliance of a specific hardware or software platform with the CSA standards and requirements for interoperability with other Zigbee devices. The certification process involves rigorous testing of the product's hardware, software, and functionality to ensure that it can communicate effectively with other Zigbee devices and operate within a Zigbee network. This certification is typically obtained by manufacturers of chips and software stacks.
  • The test house requires completed versions of PICS documents. The PICS is a checklist (Yes/No) table of supported functions by the platform. From this documents, test house can drive the test cases during certification.

    Among the table elements, feature set support shows if an item is mandatory (M), optional (O), or prohibited (X) based on whether another item reflects the DUT’s behavior. All mandatory PICS items must be supported.

PICS sample
  • Depending on device type, FFD or RFD, dedicated tests set will be applied.
  • Green Power Proxy tests (GPP) are run as part of Zigbee Platform Certification to ensure that the platform or device can support GPP functionality and can communicate with low-power devices using GPP.
  • 802.15.4 MAC & PHY certification has to be performed before running Zigbee PRO Compliant Platform certification tests.

3.1. Setting up ST test harness for Zigbee Pro Compliant Platform testing

By conducting in-house testing using a test harness, companies can simulate the testing environment and identify any potential issues that may arise during formal certification testing. This can help saving time and money.

Test specification defines the list of test cases to be run, detailing methods to be used, expected outcomes, and observables.

The following items are needed to set up the test harness:

  • Device Under Test (DUT): refers to the product or device that is being tested.
  • Golden Unit (GU): is used as a reference platform. It is certified by the CSA and considered to be the standard.
  • Sniffer to capture and analyze communication over the air.
  • Powered USB Hub.
Test Harness

It is necessary to meet the following hardware/software requirements to get the STM32WB certification:

Hardware requirements:

  • DUT: STM32WB
  • GU: Exegin Q55

Software used:

  • DUT:
    • For M0: stm32wbxxxFFD.bin or stm32wbxxxRFD.bin depending on the test/role
    • For M4: in-house developed application
  • GU: Exegin firmware
STM32WB test bench for Zigbee Pre-Certification

It is necessary to meet the following hardware/software requirements to get the STM32WBA certification:

Hardware requirements:

  • DUT: STM32WBA
  • GU: Exegin bbg90-atmel

Software used:

  • DUT: Zigbee-FFDxxx.bin or Zigbee-RFDxxx.bin depending on the test/role, with a Zigbee command line interface application.
  • GU: Exegin firmware
STM32WBA test bench for Zigbee Pre-Certification

3.2. Certification status

  • STM32WB is Zigbee PRO R22 Compliant Platform certified, and is referenced on Connectivity Standards Alliance website.
  • STM32WBA is Zigbee PRO R23 Compliant Platform certified, and is referenced on Connectivity Standards Alliance website.
  • STM32WBA is Zigbee PRO R22 Compliant Platform certified, and is referenced on Connectivity Standards Alliance website.

4. End Product Certification

End Product Certification is a process that certifies the compliance of a final product or device that incorporates Zigbee technology with the CSA standards and requirements. This certification is typically obtained by manufacturers of consumer/commercial products that use Zigbee technology, such as smart home devices or lighting systems.

Zigbee Platform Certification process

4.1. Zigbee 3.0 Certification

This certification intends to check Zigbee End Product interoperability & application middleware (ZCL cluster library/BDB).

Depending on device type (FFD/RFD), dedicated BDB tests set applies.

Zigbee Green Proxy cluster (GPP) is mandatory to get Zigbee 3.0 certificate in FFD device case.

Zigbee PRO Compliant platform certification has to be obtained before running Zigbee 3.0 certification tests. The list of the compliant platforms can be found on the CSA web page and can be filtered by company, device type, and program type.
STM32WB has been Zigbee 3.0 certified for FFD and RFD: CSA site.

CSA End Products STM32WB certified

4.2. Zigbee Smart Energy Certification

Zigbee Smart Energy (SE) certification is typically performed on real end products that are intended for use in energy management applications, such as gas meters, power meters, in-home displays, and other related devices.

The Zigbee SE certification is dependent on the version of the Zigbee Smart Energy standard that the device adheres to. Each version of the standard may have different requirements and features that need to be tested and certified. Zigbee PRO Compliant platform certification must be performed before running Zigbee SE certification tests to ensure the device is Zigbee PRO compliant.

Zigbee SE Certification process


For Smart Energy, our platforms WB and WBA are following the Zigbee Smart Energy 1.4a standard. SE 1.4a is based on an R22 flavour of the stack.

To run those tests, we can use different golden units including Green BeagleBone from Exegin or STM32WB boards from ST.

For Smart Energy, STM32WB was selected as golden unit for Smart Energy (We need to put the reference here ... )

Internally, ST is checking the compliancy of the clusters and of the BDB to the specification through its internal lab.

5. Official CSA Certification tools

ZigBee testing through time

5.1. Zigbee Unified Test Harness (ZUTH)

It is the official CSA test tool for certification testing. It is used for formal testing by Alliance Authorized Test Laboratories (ATLs) and is also available to all Alliance members for pre-certification testing.

ZUTH is a flexible testing tool for Zigbee that can be used in both Command Line Interface (CLI) and Graphical User Interface (GUI) modes. It allows users to execute individual or multiple test cases, create log files, and create custom test cases using Python. The tool is compatible with Windows® 10, Mac®, and Linux® operating systems.
For instance, ZUTH is mainly targeting cluster validation.

6. Certification by Similarity Program

The CSA offers a certification by similarity Program that allows a Zigbee product that is derived from a certified Zigbee product to keep the certification without having to go through the entire certification process again. The aim of this program is to reduce certification costs and minimize the time and the effort.
In general, the program allows for changes that are considered minor and do not significantly impact the conformance of the product to Zigbee standards. These changes may include modifications to the product's design, components, or materials, as long as they do not affect Zigbee or radio functionality.
If the original certified product on which the certification by similarity is based is older than three years, then the product may not be eligible for the program, and complete testing is required.

7. Certification Transfer Program

Customers who want to sell a certified product but do not want to go through the entire certification process themselves can participate in the Certification Transfer Program. Customers are allowed to re-certify the product under its company name. Once a product has been approved for certification by the Connectivity Standards Alliance, the product can display the Certified logo for that standard under the name of the Adopter company.
Eligible products for this Transfer program must:

  • be an End Product.
  • be previously certified by the Alliance.
  • belong to a participant or promoter member company.

8. Acronyms and definitions

Term Definition
ATL Authorized Test Lab
BDB Base Device Behavior
CLI Command Line Interface
DUT Device Under Test
FFD Full Feature Device
RFD Reduced Feature Device
PICS Protocol Implementation Conformance Statement
ZCL ZigBee Cluster Library

9. References