1. Serial communication profile
Serial communication applications are proprietary applications that are used to exchange the data entered on the UART of each board.
SerialCom applications are named BLE_SerialCom_Central and BLE_SerialCom_Peripheral: One board is configured as central using BLE_SerialCom_Central. The other board is configured as peripheral using BLE_SerialCom_Peripheral.
Both boards support data transfer by sending the L2CAP data through a COC (Connection Oriented Channel) link.
- Open VT100 terminals on both client and server sides.
- Connect to ST-LINK via the COM port @115200 bauds/s, 8 data bits, with no parity and 1 stop bit:
- Configure the terminal with local echo settings:
- No service is added.
Once a Bluetooth® LE link is established, a Connection Oriented Channel (COC) is established.
Data are exchanged through the COC link.
The SerialCom projects provided within the STM32CubeWB0 MCU Package[1] are described below:
Example of COC link establishment between a SerialCom central (STM32WB0 or Smartphone) & a SerialCom peripheral (STM32WB0) |
---|
Example of COC exchanged data between a SerialCom peripheral (STM32WB0) & a SerialCom central (STM32WB0 or smartphone) |
---|
1.1. On board buttons configuration
Button configuration for Bluetooth® Low Energy SerialCom applications on STM32WB0 nucleo boards | ||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
2. Requirements
2.1. Software and hardware requirements
For software and hardware requirements, refer to the STM32WB0 Build BLE project wiki page.
2.2. Collector applications compatibility
The STM32CubeWB0 SerialCom peripheral application is compatible with the following collector:
3. STM32WB0 SerialCom peripheral description
3.1. Project directory
The "BLE_SerialCom_Peripheral" application is available by downloading the STM32CubeWB0 MCU Package[1].
Refer to the How to Build a Bluetooth® LE project wiki page for information on the project directory.
3.2. Project description
3.2.1. Structure
The software project structure and its most important parts are described below.
3.2.2. Application initialization
The application initialization steps are described below:
3.2.3. GAP and GATT initialization and interaction
The Bluetooth® LE SerialCom peripheral application initialization is done within app_ble.c:
- Start the Bluetooth® Low Energy stack:
- Initialize the device as peripheral.
- Configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
- Call the services controller initialization BLEEVT_Init() - ble_evt.c.
- Manage the GAP event - BLEEVT_App_Notification().
- HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE provides information on the connection interval, the slave latency, and the supervision timeout.
- HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE provides information on the new connection.
- HCI_DISCONNECTION_COMPLETE_EVT_CODE communicates with the application in the event of a link disconnection, and provides details about the reason.
The Event management is done by the Bluetoooth® Low Energy Event Dispatcher, ble_evt.c:
- Initialize the number of the registered handler - BLEEVT_Init()
- Manage events - BLE_STACK_Event()- from the Bluetooth® Low Energy Host Stack, and redirect them to the gap event handler - BLEEVT_App_Notification()
The application level of the SerialCom peripheral is done using coc_peripheral_app.c:
- Initialize the application context.
- Manage the COC link establishment.
- Initialize Rx UART to process data from the terminal.
3.3. How to use the Bluetooth® Low Energy SerialCom Peripheral application
Once the BLE SerialCom Peripheral application is installed on the STM32WB0 platform, use the BLE SerialCom Central application on STM32WB0 platform or on a smartphone.
- Open a VT100 terminal on the central and peripheral sides via the ST-Link Com port, @115200 bauds, 8 data bits, no parity and 1 stop bit:
- Press B1 on the central to scan, connect and establish the COC link. When the link is ready, the CONNECTION READY message is displayed.
- Enter data on UART, on the peripheral or central side. Check that the peer device receives data correctly.
Pressing B2 while not connected allows to clear the security database. Pressing B2 while connected allows to send peripheral security request.
There are two different modes to send messages from an STM32WB0: Send button or Real time.
On the terminal, when you type data using a keyboard (on either central or peripheral): when LF or CR is encountered, or data buffer is full (20 bytes), data is sent to the peer in L2CAP SDUs (Service Data Units).
3.4. UART debug trace
The debug log via UART interface ensures the application project is traced.
To enable the traces within the project, enable them within app_conf.h as described below:
/**
* Enable or Disable traces in application
*/
#define CFG_DEBUG_APP_TRACE (1)
SerialCom Peripheral - Initialization phase | Connected phase |
---|---|
==>> Start BLE_Init function Success: aci_hal_set_tx_power_level command Success: aci_gatt_srv_profile_init command Success: aci_gap_init command Static Random Bluetooth Address: f1:7e:3e:db:2d:97 Success: Gap_profile_set_dev_name - Device Name Success: Gap_profile_set_appearance - Appearance Success: aci_gap_set_io_capability command Success: aci_gap_set_security_requirements command Success: aci_gap_configure_filter_accept_and_resolving_list command ==>> End BLE_Init function ==>> aci_gap_set_advertising_configuration - Success ==>> aci_gap_set_advertising_data - Success ==>> Success: Start Fast Advertising |
>>== hci_le_connection_complete_event - Connection handle: 0x0801 - Connection established with @:ea:a4:97:ab:53:79 - Connection Interval: 50.00 ms - Connection latency: 0 - Supervision Timeout: 5000 ms BLE_SVC_L2CAP_Conn_Update(), Successfully >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 45.00 ms - Connection latency: 0 - Supervision Timeout: 10000 ms |
4. STM32WB0 SerialCom central example description
4.1. Project directory
The "BLE_SerialCom_Central" application is available by downloading the STM32CubeWB0 MCU Package[1]
Refer to the How to Build a Bluetooth® LE project wiki page for project directory information.
4.2. Project description
4.2.1. Structure
The software project structure and its most important parts are described below:
4.2.2. Application initialization
The different steps of the application initialization are described below:
4.2.3. GAP and GATT initialization and interaction
The Bluetooth LE SerialCom central application initialization is done within app_ble.c
- Start the Bluetooth® LE stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init()
- Call the services controller initialization BLEEVT_Init() - ble_evt.c.
- Manage the GAP event - BLEEVT_App_Notification() - ble_evt.c
- HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE - provides information of the connection interval, slave latency, supervision timeout
- HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - provides new information about the connection
- HCI_DISCONNECTION_COMPLETE_EVT_CODE - informs the application about the link disconnection, and the reason
Event management is done by the Bluetoooth® Low Energy Event Dispatcher, ble_evt.c
- Initialize the number of registered handler - BLEEVT_Init()
- Manage events - BLE_STACK_Event() - from the Bluetooth® Low Energy Host Stack and redirect them to the gap event handler - BLEEVT_App_Notification()
The application level of the SerialCom central is done with gatt_client_app.c:
- Initialize Gatt Client Application
- Manage COC link establishment
- Initialize Rx UART to process data from terminal
4.3. How to use the Bluetooth® Low Energy SerialCom central application
Once the BLE SerialCom Central application is installed on the STM32WB0 platform, use BLE SerialCom Peripheral application on other STM32WB0.
- Open a VT100 terminal on central and peripheral sides via the ST-Link Com Port (Connection is displayed as ST Link), @115200 bauds, 8 data bits, no parity and 1 stop bit:
- Press B1 on the central side to scan, connect and establish COC. Once the link is ready, the CONNECTION READY message is displayed.
- Enter data on the central or the peripheral side, and check that data are correctly received on peer device.
In terminal, when you type data using keyboard (on either Central or Peripheral): when LF or CR is encountered or data buffer is full (20 bytes), data are sent to the peer in L2CAP SDUs (Service Data Units).
Pressing B2 while not connected allows to clear the security database. Pressing B2 while connected allows to send pairing request.
Pressing B3 while connected allows to send connection update.
4.4. UART debug trace
Traces are enabled within the project, in app_conf.h, as described below:
/**
* Enable or Disable traces in application
*/
#define CFG_DEBUG_APP_TRACE (1)
SerialCom Central - Initialization phase | Press B1. The connected phase starts. |
---|---|
==>> Start BLE_Init function Success: aci_hal_set_tx_power_level command Success: aci_gatt_srv_profile_init command Success: aci_gap_init command Static Random Bluetooth Address: ea:a4:97:ab:53:79 Success: Gap_profile_set_dev_name - Device Name Success: Gap_profile_set_appearance - Appearance Success: aci_gap_set_io_capability command Success: aci_gap_set_security_requirements command Success: aci_gap_configure_filter_accept_and_resolving_list command ==>> End BLE_Init function -- CENTRAL INITIALIZED |
** START GENERAL DISCOVERY (SCAN) ** --- ST MANUFACTURER data BlueSTv2 Serial Port Server, db addr 0xF1:7E:3E:DB:2D:97 >>== ACI_GAP_PROC_COMPLETE_VSEVT_CODE -- GAP_GENERAL_DISCOVERY_PROC completed Create connection to Serial Port Server ==>> aci_gap_set_scan_configuration - Success ==>> aci_gap_set_connection_configuration Success , result: 0x00 wait for event HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE HCI_LE_META_EVT: 0x14 >>== hci_le_connection_complete_event - Connection handle: 0x0801 - Connection established with @:f1:7e:3e:db:2d:97 - Connection Interval: 50.00 ms - Connection latency: 0 - Supervision Timeout: 5000 ms >>== ACI_GAP_PROC_COMPLETE_VSEVT_CODE GATT services discovery Success: aci_l2cap_connection_parameter_update_resp command Success: aci_hal_set_radio_activity_mask command Fail : aci_l2cap_connection_parameter_update_resp command ACI_ATT_READ_BY_GROUP_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0801 1/2 short UUID=0x1801, handle [0x0001 - 0x000A], GENERIC_ATTRIBUTE_SERVICE_UUID found 2/2 short UUID=0x1800, handle [0x000B - 0x000F], GAP_SERVICE_UUID found HCI_VENDOR_EVT: 0x0C0A HCI_VENDOR_EVT: 0x0C11 HCI_VENDOR_EVT: 0x0C10 PROC_GATT_CTL_DISC_ALL_PRIMARY_SERVICES services discovered Successfully DISCOVER_ALL_CHARS ConnHdl=0x0801 ALLServiceHandle[0x0001 - 0x000F] ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0801 ConnHdl=0x0801, number of value pair = 3 1/3 short UUID=0x2A05, Properties=0x0020, CharHandle [0x0002 - 0x0003], GATT SERVICE_CHANGED_CHARACTERISTIC_UUID charac found 2/3 short UUID=0x2B29, Properties=0x000A, CharHandle [0x0005 - 0x0006] 3/3 short UUID=0x2B2A, Properties=0x0002, CharHandle [0x0007 - 0x0008] HCI_VENDOR_EVT: 0x0C06 >>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE - Connection Interval: 45.00 ms - Connection latency: 0 - Supervision Timeout: 10000 ms ==>> Start Connection Oriented Channel Success: aci_l2cap_cos_connection_req command ACI_ATT_READ_BY_TYPE_RESP_VSEVT_CODE - ConnHdl=0x0801 ConnHdl=0x0801, number of value pair = 3 1/3 short UUID=0x2B3A, Properties=0x0002, CharHandle [0x0009 - 0x000A] 2/3 short UUID=0x2A00, Properties=0x0002, CharHandle [0x000C - 0x000D], GAP DEVICE_NAME charac found 3/3 short UUID=0x2A01, Properties=0x0002, CharHandle [0x000E - 0x000F], GAP APPEARANCE charac found HCI_VENDOR_EVT: 0x0C06 >>== ACI_L2CAP_COS_CONNECTION_RESP_VSEVT_CODE Channel_Type: 0 Peer_MTU: 64 Peer_MPS: 64 Initial_Credits:1 Result: 0x00 CID_Count: 1 ==>> Connection Oriented Channel established MTU exchanged size = 247 Success: set data length command HCI_VENDOR_EVT: 0x0C03 HCI_VENDOR_EVT: 0x0C11 HCI_VENDOR_EVT: 0x0C10 All characteristics discovered Successfully DISCOVER_ALL_CHAR_DESCS [0x0001 - 0x000F] ACI_ATT_FIND_INFO_RESP_VSEVT_CODE - ConnHdl=0x0801 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0002 UUID=0x2A05, handle=0x0003, found GATT SERVICE_CHANGED_CHARACTERISTIC_UUID Descriptor UUID=0x2902, handle=0x0002-0x0003-0x0004, Service Changed found reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0005 UUID=0x2B29, handle=0x0006 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0007 UUID=0x2B2A, handle=0x0008 reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x0009 UUID=0x2B3A, handle=0x000A PRIMARY_SERVICE_UUID=0x2800 handle=0x000B reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x000C UUID=0x2A00, handle=0x000D, found GAP DEVICE_NAME_UUID reset - UUID & handle - CHARACTERISTIC_UUID=0x2803 CharStartHandle=0x000E UUID=0x2A01, handle=0x000F, found GAP APPEARANCE_UUID HCI_VENDOR_EVT: 0x0C04 HCI_VENDOR_EVT: 0x0C10 All characteristic descriptors discovered Successfully HCI_VENDOR_EVT: 0x0C11 HCI_VENDOR_EVT: 0x0C10 ServiceChangedCharDescHdl =0x0004 All notifications enabled Successfully |
5. STM32WB0 SerialCom peripheral with ST BLE Toolbox smartphone app
Required: phone with Android 10 or newer.
ST BLE ToolBox is a user-friendly application which interacts with and debugs ST Bluetooth®LE devices.
On the ST BLE Toolbox, when clicking on a device corresponding to an ST board with a firmware ID SerialCom Peripheral (0x87), a "COC" button appears (next to the "Connect" button).
After accepting the pairing with the device (which is mandatory), a special page for COC appears. This means the L2CAP socket has been created and you can now receive and send data via the L2CAP channel.
Messages sent by the board will immediately appear in the chat.
Two different modes can be used to send messages from the phone: Send button and Real time.
- With the Send button mode, you can type your message in the text field at the bottom of the chat, then sending this message by clicking on the "Send" button.
- With the Real time mode, each character that you write is immediately sent.
You can erase all messages by clicking on "Clear".
Data format:
When sending the message "hello", what is actually sent is 0x 05 00 68 65 6C 6C 6F.
- 0x 05 00 is the length of the message in little endian (05 00 in little endian => 00 05 => 5 => number of letters of "hello").
- 0x 68 65 6C 6C 6F is "hello" in ascii ("h" = 0x68, "e" = 0x65, "l" = 0x6C, "o" = 0x6F).
6. References