OEMiRoT for STM32H7R

This article gives an overview of the OEMiRoT solution integrated in STM32H7R.

The chapter About hardware highlights the main differences with STM32H7S with an impact on the secure boot solutions. Except these differences this article is very similar to OEMiRoT OEMuRoT for STM32H7S

List of applicable products:

Type Products
Microcontroller STM32H7R7A8, STM32H7R7I8, STM32H7R7L8, STM32H7R7N8 STM32H7R7Z8, STM32H7R3A8, STM32H7R3I8, STM32H7R3L8, STM32H7R3L8U, STM32H7R3N8, STM32H7R3R8, STM32H7R3V8, STM32H7R3Z8


1. OEMiRoT presentation

1.1. Overview

OEMiRoT stands for OEM immutable (unchangeable) Root of Trust and acts as a first boot stage. OEMiRoT is an example based on the MCUboot open-source software (refer to MCUboot) provided with STM32CubeH7RS. OEMiRoT offers two services:

  • The Secure Boot (root of trust service) is an immutable code, which is always executed after a system reset. It checks static protections (options bytes), activates runtime protections, and then verifies the authenticity and integrity of the user application code before every execution.
  • The Secure Firmware Update application is an immutable code that detects any new firmware image candidate. It checks the version (version downgrade prevention), authenticity, and integrity of the new firmware condidate before installing it after decryption.

1.2. About hardware

  • Unlike the STM32H7S, the STM32H7R does not support hardware cryptography, such as SAES, PKA and MCE.
    • STM32H7R OEMiRoT solution relies on software cryptography: Mbed™ library.
    • As there is no MCE, the application which is installed in external flash memory or external RAM is not encrypted.
  • STiRoT is not supported on STM32H7R (the Option Byte IROT_SELECT is irrelevant on STM32H7R). Therefore the two boot stages bootpath (STiROT + OEMuRoT) is not possible on STM32H7R.

Note: for more details about difference between the STM32H7S and the STM32H7R, see STM32H7RS Reference manual

1.3. Protection measures and security strategy

Cryptography ensures integrity, authentication, and confidentiality. However, the use of cryptography alone is not enough: a set of measures and system-level strategies are needed for protecting critical operations, sensitive data (such as a secret key), and the execution flow in order to improve security robustness. On the STM32H7R, the security strategy is based on:

  • Product life cycle: product state CLOSED or LOCKED must be selected in order to ensure that the JTAG debugger cannot access the device, except to execute the DA process (more details in Debug Authentication for STM32H7RS wiki article).
  • Boot configuration: On the STM32H7R, the system always boots on the user flash memory. The IROT_SELECT option byte is still set to OEMiRoT for compliance with STMH7S configuration. However, on STM32H7R, this configuration is ignored.
  • Antitamper protection: the antitamper protection is used to protect sensitive data from being physically tampered with. The antitamper protection is activated at the start of OEMiRoT_Boot project and remains active during OEMiRoT_Appli execution. In case there is any tamper detection, sensitive data and the caches are immediately erased, and a reboot is forced. Both external active tamper pins and internal tamper events are used.
  • MPU: The Memory Protection Unit (MPU) is a memory protection mechanism that allows specific access rights to be defined for any memory-mapped resources of the device: flash memory, SRAM, and peripheral registers. The MPU is configured to limit the execution surface to the code section of OEMiRoT_Boot project during its execution, then extended to the application code section after verifying its integrity and its authenticity. This protection is dynamically managed at runtime.
  • HDP: the HDP area is configured to cover the whole OEMiRoT_Boot project code area in order to prevent any execution out of the OEMiRoT_Boot. When jumping into the application, the temporal isolation (HDP level) is increased from HDPL1 to HDPL3 preventing any access to the OEMiRoT_Boot project code.
  • OBkeys: HDPL1 OBkeys are a protected and isolated areas used to store secrets such as encryption and authentication cryptographic keys. These areas are no longer accessible when switching from HDPL1 to HDPL2 or to HDPL3.
  • WRP: Write protection is used to ensure the OEMiRoT_Boot code immutability as requested by the state-of-the-art standards in the secure boot implementation. In the OEMiRoT_Boot project, the system has been configured to make the OEMiRoT_Boot code as immutable.
  • RAM ECC: RAM Elliptic Curve Cryptography (ECC) is a mechanism to prevent memory corruption. A reset is generated in case of RAM ECC detection.

See also STM32H7RS Reference manual for more description on each feature.

1.4. OEMiRoT activation

On the STM32H7R, the OEMiRoT activation is done by:

  • Configuring secrets: authentication and encryption keys used by OEMiRoT.
  • Building OEMiRoT_Boot binary in the configuration OEMiRoT.

All these operations are part of the provisioning process.

There is only one use case:

  • One boot stage, OEMiRoT: OEMiRoT_Boot project binary is built into the OEMiRoT configuration. OEMiRoT directly manages the user application binary.

See also Secure Boot and Secure Firmware Update for STM32H7RS article.

1.4.1. One boot stage: OEMiRoT

OEMiRoT is generated by compiling the OEMiRoT_Boot project with the OEMUROT_ENABLE switch de-activated.

At reset, the OEMiRoT which is located in the user flash memory, is executed in temporal isolation 1 (HDPL1). After a successful verification of the authenticity and the integrity of the user application code image, the OEMiRoT executes the user application in HDPL3. In case a verification failure is detected, a reset is triggered except if OEMIROT_DEV_MODE compilation switch is activated during OEMiRoT_Boot project generation. In this case the execution enters into an infinite loop.

The following figure illustrates the secure boot and the secure update process by showing all the steps required to boot the user application code image located in the installation slot of the external flash memory:

  1. In the CLOSED or LOCKED product state, the RSS is the first software executed. The RSS jumps into the OEMiRoT.
  2. The OEMiRoT checks if a new user application is stored in the download slot. If any, the OEMiRoT decrypts it then controls its integrity, its authenticity and the antirollback version. If successful, the image is decrypted and copied in the user application installation slot.
  3. The OEMiRoT controls the integrity and the authenticity of the user application image from the installation slot located in the external flash memory. If successful, the OEMiRoT executes it from external flash memory or from external/internal RAM memories. In case of RAM memory execution (load and run use case), an additional copy is made before its execution. Refer to the Features list for more details on OEMiRoT execution modes.

Security H7R OEMiRoT bootstage.png

Notes:

  1. To ensure the security of the device, the MPU is configured to allow only the user application code area to be executed when the OEMiRoT jumps into the user application, minimizing the risk of unauthorized code execution. The user application must reconfigure the MPU to fit with its security needs.
  2. There is no external RAM on Nucleo-H7S3L8 board.

1.4.2. Swap upgrade strategy

The swap upgrade strategy is configured when generating OEMiRoT, the scratch buffer is used:

  • during installation, to swap download and installation slots.
  • at reset, the images are swapped back if the new user application is not confirmed.

Security H7R OEMiRoT swap.png

In the swap upgrade strategy, the antirollback version is saved at reset if the user application is confirmed. However, in overwrite mode, it is saved at the end of the installation process. Refer to OEMiRoT start-up sequence for more details.

2. Features list

The main features of the OEMiRoT are:

  • Software cryptography operations with Mbed™ library:
  1. ECDSA-P256 asymmetric cryptography for image authentication.
  2. SHA256 cryptography for image integrity check.
  3. AES-CTR-128 cryptography for image encryption with a symmetric key encrypted in ECIES-P256 provided in the image itself. Refer to Image generation for more details.
  • Accelerated boot thanks to SHA256 image reference management. The image verification mainly consists of verifying the SHA256 of the image (integrity check), and then verifying the signature of this SHA256 (authentication check). If successful, the SHA256 is stored as reference for the next boot. At the next boot, the signature verification is skipped if the SHA256 of the image matches the reference stored in the OBKeys. This feature brings performance optimization (under the MCUBOOT_USE_HASH_REF compilation switch).
  • Antirollback version check based on image version stored in the OBkeys.
  • Image installation resistant to asynchronous power down and reset.
  • Integration of the full entropy True Random Number Generator (TRNG) source (RNG hardware peripheral) for random delays generation.
  • Configurable firmware image upgrade strategy for primary and secondary slots mode:
  1. Overwrite strategy, for which the image in the secondary slot overwrites the image in the primary slot.
  2. Swap strategy, for which the image in primary and secondary slots are swapped. After the swap, the new image in the primary slot must be confirmed by the user application. Otherwise, at the next boot, the images are swapped back.
Note: A reset must be generated by the user application after confirmation to update the confirmation flag inside the image in the installation slot. The "read while write" feature is not managed for the external flash memory.
  • Memory configuration:
  1. Download slot in external flash memory. The image is encrypted in AES-CTR-128 with a symmetric key. This key is encrypted in ECIES-P256 with MCUBootkey.
  2. Installation slot in external flash memory.
  3. Execution slot from internal RAM or external RAM memories (load and run configuration).
  • Load and run execution mode capability is configured with OEMIROT_LOAD_AND_RUN defined. In addition to the standard execution mode which is in place, the user application can be executed:
  1. from external RAM memory
  2. from internal RAM memory. In this configuration, the size of the application is limited to 128 Kbytes. During the application load process into the internal RAM, the OEMiRoT/OEMuRoT data, OEMuRoT code (depends on the bootpath selected) and the application code are mapped in RAM at the same time.
  • Integration of hardware security peripherals and mechanisms in order to implement a root of trust. Product life cycle, MPU, WRP, HDP, and TAMPER are combined to protect the product. When connected on the HW board, external tamper can be activated with the OEMIROT_TAMPER_ENABLE define.
  • Image generation with the STM32TrustedPackageCreator tool delivered within STM32CubeProgrammer.

Features configurability:

Feature OEMiRoT Configuration switch

Boot project generation

OEMiRoT generation

OEMUROT_ENABLE

Image upgrade strategy

  • Overwrite only mode
  • Swap mode
MCUBOOT_OVERWRITE_ONLY

Flash memory configuration

  • External flash memory for download and installation slots
  • Execution slot definition depending on load and run configuration
MCUBOOT_OVERWRITE_ONLY

Load and run execution modes configuration

  • No: execution from external flash memory
  • Execution from external RAM memory
  • Execution from internal RAM memory
OEMIROT_LOAD_AND_RUN

Antitamper

  • None
  • Internal tampers only
  • Internal and external tampers
OEMIROT_TAMPER_ENABLE

Project phase (Application development phase )

  • Development mode
  • Production mode
OEMIROT_DEV_MODE

3. Memory layout

The STM32CubeH7RS OEMiRoT relies on a memory layout defining several regions:

  • SCRATCH region: region used by OEMiRoT_Boot to store the image data temporarily during the image swap process (not used in overwrite-only mode).
  • OEMiRoT_Boot code region: region to program the OEMiRoT_Boot code binary that manages the "Secure Boot" and "Secure Firmware Update” functions.
  • OEMiRoT_Boot volatile data: region used to locate the internal variables and call the stack, during OEMiRoT_Boot code execution.
  • Application installation (primary) slot region: region to program the image of an “active” firmware after installation.
  • Application download (secondary) slot region: region to program the image of a “new” firmware, candidate for installation.
  • Application execution slot region when the load and run feature is activated.
  • Image confirmation flag and RAM ECC handle.


Memories layout is as follow:

Security H7S OEMiRoT layout.png


Default values are:

Symbol Execute in place Load and run in external RAM Load and run in internal RAM
FLASH_AREA_0_OFFSET 0x00000000 0x00000000 0x00000000
FLASH_AREA_0_SIZE 0x00200000 0x00200000 0x00020000
FLASH_AREA_2_OFFSET 0x00200000 0x00200000 0x00020000
FLASH_AREA_2_SIZE 0x00200000 0x00200000 0x00020000
PRIMARY_RUN_PARTITION_START NA 0x90000000 0x24040000
FLASH_AREA_SCRATCH_OFFSET 0x00400000 0x00400000 0x00040000
FLASH_AREA_SCRATCH_SIZE 0x00010000 0x00010000 0x00010000
FLASH_AREA_BL2_OFFSET 0x00000000 0x00000000 0x00000000
FLASH_AREA_BL2_SIZE 0x00010000 0x00010000 0x00010000
BL2_DATA_START 0x20000000 0x20000000 0x20000000
BL2_DATA_SIZE 0x00020000 0x00020000 0x00020000
RAMECC_HANDLE_START 0x30007FA0 0x30007FA0 0x30007FA0
RAMECC_HANDLE_SIZE 0x40 0x40 0x40
CONF_FLAG_SIZE 0x20 0x20 0x20

If the definition of the FLASH_AREA_0 or FLASH_AREA_2 is modified, whether it is the offset or the size, the MPU regions configuration must be updated taking into account the constraints on Cortex®-M7 MPU (refer to ARM documentation for more details):

  • region start address is a multiple of the region size
  • each region can be divided in 8 sub-regions

4. Provisioning process

4.1. OEMiRoT provisioning process

The product provisioning to activate and configure the OEMiRoT is done following the three steps below:

  1. Configuration of the OEMiRoT. This is when the cryptographic keys for authentication and encryption are defined.
  2. Generation of the firmware image.
  3. Programming of the OBkeys, the option bytes, the application image in the device.

Security H7S OEMiRoT provisioning.png

Note: After adaptating the existing OEMiRoT example (Refer to STM32H7S RoT example adaptation), a set of scripts will be present in ROT_Provisioning/OEMiRoT folder.

4.2. OEMiRoT configuration file

OEMiRoT configuration file (OEMiRoT_Config.obk) is generated using STM32TrustedPackageCreator with a template file listing all the different parameters (OEMiRoT_Config.xml) as input. The obk file is saved in HDPL1 OBkeys.

The list of the configuration parameters is as follows:

Parameter Description Additional constraints
Encryption key Key used to encrypt the firmware image When this key is regenerated, the firmware image must be processed with the TPC “Image Gen” tab (OEMiRoT_Code_Image.xml)
Authentication key Key used to authenticate the firmware image When this key is regenerated, the firmware image must be processed with the TPC “Image Gen” tab (OEMiRoT_Code_Image.xml)

5. Image generation

OEMiRoT manages an image based on the MCUBoot format including:

  • a header,
  • the encrypted firmware binary,
  • some metadata information (TLV format: Tags Length Value) which allows the control of the image (SHA256, ECDSA-P256 signature…), and
  • a magic value to trigger the installation at the end of the slot.

Further information about the MCUBoot open-source software is available at MCUboot.

A PC tool, called STM32TrustedPackageCreator, is provided to generate the firmware code image. This image is encrypted and signed using the keys configured in OBkeys configuration file (OEMiRoT_Config.xml). The OEMiRoT_Code_Image.xml contains all the parameters driving the image generation such as:

  • The authentication and encryption keys. Keys value inherited from OEMiRoT_Config.xml.
  • The version. OEMiRoT_Code_Image.xml can be edited with STM32TrustedPackageCreator in order to modify the version.

The following figure shows the firmware image generation:

Security H7S OEMiRoT image.png

6. Appendix

6.1. OEMiRoT start-up sequence

Security H7S OEMiRoT startup.png

Note: When no valid firmware image is installed, a continuous reset loop is triggered. Debug authentication process must be executed to force the download of a new image. Refer to Debug Authentication for STM32H7RS article.

Performance measured in "production mode (OEMIROT_DEV_MODE not defined)" @ 380 MHz:

Configuration Typical user application boot time
64 Kbytes 127 Kbytes 512 Kbytes 1 Mbyte 2 Mbytes
Execution from external flash 51 ms 63 ms 137 ms 236 ms 433 ms
Execution from external RAM memory 120 ms 195 ms 660 ms 1279 ms 2509 ms
Execution from internal RAM memory 114 ms 193 ms NA NA NA

Notes:

  • As there is no MCE on STM32H7R, the installed firmware image is not encrypted. The boot time of a user application executed from the external flash is then reduced when compared to a STM32H7S one.
  • In the case of an execution from RAM (external or internal), the additional verifications based on software cryptography increase the boot time. The boot time is then greater than the STM32H7S one.

6.2. Application development phase

During the development phase, it is recommended to compile OEMiRoT_Boot project with the DEV_MODE defined and to select the OPEN state during provisioning process:

  • When DEV_MODE is defined:
  • logs are displayed in tera term during the OEMiRoT_Boot project execution.
  • an infinite reset loop is executed instead of a single reset in Error_Handler() function.
  • tamper event is cleared at startup when required. No need to power off/on the board to clear this event.
  • OPEN product state can be selected during the provisioning process.
  • When the OPEN product state is selected during provisioning process, a specific script (obkey_provisioning_open.bat) is called in order to execute additional actions usually done in the PROVISIONING product state:
  • provision the AHKs (see STM32H7RS Reference manual for more description) used to encrypt OBkeys and to encrypt images with the MCE peripheral.
  • initialize the OEMiRoT data area in the OBkeys containing the version of the firmware installed as well as its SHA256 used when MCUBOOT_USE_HASH_REF is activated. Refer to the Features list for more details on MCUBOOT_USE_HASH_REF.

In CLOSED or LOCKED product state, the DA process should be run to be able to connect the debugger through JTAG. At the end of the development phase, the DEV_MODE must be disabled and the product CLOSED or LOCKED state must be selected during provisioning process. Refer to Debug Authentication for STM32H7RS article.

6.3. OEMiRoT_Config.obk file format

Offset Size Type Description
0 1 uint8 sdp command header : destination OBKey index
1 1 uint8 sdp command header : destination OBKey HDP level
2 2 uint16 sdp command header : reserved
4 4 uint32 sdp command header : data size
8 4 uint32 sdp command header : encryption always disabled for STM32H7R (0)
12 32 array SHA256 of the following data content (from offset 44 to 235)
44 91 array ECDSA-P256 authentication public key
135 70 array ECDSA-P256 encryption private key
205 31 array Reserved

6.4. OEMiRoT_Code_image xml file format

Parameter Updatable Description
Authentication key Automatic Private key inherited from OEMiROT_Config.xml file.
Encryption key Automatic Public key inherited from OEMiROT_Config.xml file.
Endianness No Little endian.
Padding No Add an installation magic value at the end of the image to trigger image installation. Padding with 0xFF when required.
Firmware area size Automatic Firmware slot size information. This value is updated during the postbuild of the OEMiRoT_Boot project compilation based on the slot configuration from flash_layout.h
Header Size No 0x400 bytes
Padding Header No Padding the header with 0xFF to complete the 0x400 bytes.
Dependency with data image No The dependency is disabled by setting the <enable> property to 0.
Write Option Automatic Image upgrade strategy: Overwrite, Swap. This value is updated during the postbuild of the OEMiRoT_Boot project compilation based on the MCUBOOT_OVERWRITE_ONLY definition from flash_layout.h.
Version Yes x.y.z firmware image version.
Security Counter No Security counter value automatically generated based on version information.
Align No The size of the encrypted binary generated is a multiple of 16 bytes.
Firmware download area offset Automatic Used to generate .hex binary file format including the destination address. This value is updated during the postbuild of the OEMiRoT_Boot project compilation based on slot configuration from flash_layout.h.
Firmware binary input file Automatic Location of the firmware binary file. This parameter is updated during the provisioning process based on information from env.bat file.
Image output file Yes Location of the encrypted image which is generated. If changed, provisioning scripts must be updated accordingly.

6.5. System clock frequency

The system clock is set to 380 MHz to be functional with all hardware configurations (ECC_ON_SRAM enabled, no internal regulator) and with the full range of temperature (Tj up to 125 degrees).

If the constraints related to power and temperature are met, and if the RAMECC security feature is disabled (boot_hal_cfg.h, ob_flash_programming.bat (.sh)), it is possible to increase the system clock up to 600MHz.

The system clock configuration and the power configuration shall then be updated in OEMiROT_Boot project. The power configuration shall be applied before any XSPI configuration.