This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Overview
The OpenThread border router (OTBR) is crucial in Matter to enable the communication between IP-based networks. It acts as a bridge between the Thread network and the outside world.
The STM32MP1 OTBR works with the NUCLEO-WB55RG radio coprocessor (RCP), which is connected to the STM32MP157F-DK2 Discovery kit (wiki for STM32MP15 Discovery kits) through a serial connection using an FTDI.
2. Boards needed
- as OpenThread border router:
- as Thread® RCP firmware, NUCLEO-WB55RG ST radio coprocessor (RCP):
3. Package content
A Linux® PC running under Ubuntu® 18.04 or 20.04 must be used. The developer can follow this link.
The Linux package can be found in Github.