This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Overview
This prototype application provides an example of use of the Matter bridge and the NUCLEO-H753ZI-Q board with Ethernet connectivity.
This application provides a dynamic endpoint with device commissioning and cluster control. The application adds the non-Matter device as an endpoint on a bridge acting as Matter device.
In the example below, 8 light devices supporting one on-off cluster have been added as endpoints.
System presentation |
---|
2. Boards Needed
- The bridge runs on:
3. Package content
You can download the necessary files on Github