This article details an example of certification using Bluetooth® Low Energy qualification workspace with STM32WB55CG.
1. STM32WB55CG reference PHY and stack QDIDs/DNs
Before going through this process, QDIDs/DNs used with STM32WB55CG module should be defined. The Bluetooth® Special Interest Group (SIG) provides a listing search [1] for finding previously qualified designs and declared products. A dedicated certification guideline wiki page [2] provides the latest QDIDs/DNs to be used for each STM32WBx product.
1.1. STM32WB55CG reference RF-PHY
According to the dedicated Certification guideline wiki page [2], DN Q308129 [3] should be considered.
This STM32WB55CG RF-PHY was qualified with core specification 5.2 and using the test case reference list (TCRL) version 2024-2.
1.2. STM32WB55CG reference stack
According to the dedicated certification guideline wiki page [2], DN Q332452 [4] should be considered.
These stacks were qualified with core specification 5.4 and using the test case reference list (TCRL) version 2024-2.
2. Qualification workspace process
The Bluetooth® qualification workspace [5] is the starting point of certification journey.
Note that this page, includes additional resources to help you understand Bluetooth Qualification Process or to assist you, in case of any issue.
To start, click on "start the Bluetooth Qualification Process".
Each subchapter of this article describes a different step of the qualification process on the Bluetooth® website.
2.1. Product details
In this step, product details should be entered as illustrated in the following example.
Once the product details are entered, the customer can, if required, add an additional product. To move forward, "No, I do not" must be selected, as shown below.
2.2. Specify the design
Since the customer is reusing QDIDs/DNs, "Yes, I do" is selected and both DN's associated with STM32WB55CG are entered, as shown below.
Once this is done, the following step must be completed
The customer can now proceed to layer selection and select “Save and go to the layer selection”.
2.3. Layer Selection
In this example, the customer is considering certifying a complete product with proprietary profile and should proceed as follows:
To avoid inconsistencies in the future, "UHCI" in "Core Host Layers" should be added as shown below.
The customer can proceed to ICS selection and select “Save and go to ICS selection”.
2.4. ICS selection
To avoid inconsistencies in the future, follow these steps:
- Select "UHCI" and check 0/54 as shown below
- Select "IOP" and check 2/2 as shown below
- Select "Core" and uncheck 1/54 as shown below
Then, the customer can confirm if there are no inconsistencies by clicking on the "Consistency Check" button.
If all inconsistencies are resolved, proceed to the next step by selecting “Save and go to Test plan and documentation” located at the bottom of the page.
2.5. Test Plan and Documentation
In this example, no test plan should be generated for the new design thanks to the pre-qualified DNs associated to STM32WB55CG.
In the next step, the customer selects “Upload test declaration and test reports” and uploads their own certified RF-PHY test report executed from certified test house. As explained in dedicated Certification guideline wiki page [2].
The customer can now complete the process with qualification fee payment.
2.6. Product Qualification Fee
In this step, product qualification fee needs to be addressed.
The customer can now complete the process with submission page.
2.7. Submission
The customer receives a summary of the requirements status based on the provided product declarations or reports.
Your qualification journey with STM32WB55CG is now completed !
3. References