Revision as of 11:02, 29 March 2024 by Registered User
This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. RDP level management
The STM32U0 silicon device life cycle is based on the RDP mechanism implemented for the FLASH interface,
as specified in the STM32U0 reference manual RM0503[1] (Section: 3.5.1).
RDP protection level |
Debug |
Comments
|
Level 0: device open |
Allowed |
The boot address can be either the user flash memory, bootloader in system memory, or embedded SRAM, depending on the boot mode configuration.
Any security configuration including OEM1 and OEM2 keys can be provisioned in the flash memory user option bytes.
|
Level 1: device memories protected |
Limited |
The boot address can be either the user flash memory, bootloader in system memory, or embedded SRAM, depending on the boot mode configuration.
Debug access to the user flash memory, embedded SRAM, and backup registers is not allowed.
Any security configuration including OEM1 and OEM2 keys can be provisioned in the flash memory user option bytes.
|
Level 2: device closed |
None |
The boot address must target the user flash memory. The flash memory user option bytes are read-only, so RDP level 2 cannot be changed, unless the OEM2 unlocking key is activated.
}
The figure below illustrates the level transitions:
Changing the read protection level:
- From level 0 to level 1: write any other values than 0xCC or 0xAA in the RDP register.
- From level 0 or 1 to level 2: write 0xCC in the RDP register.
- From level 2 to level 1: inject the OEM2KEY value through the debug interface during reset. This operation is relevant only if the OEM2 password lock activation was executed previously.
- From level 1 to level 0:
- If the OEM1 password lock activation was done: inject the OEM1KEY value through the debug interface during reset.
- If the OEM1 password lock activation was not done: write 0xAA in the RDP register.
Warning
|
As specified in RM0503[1]Section:3.5.6, the debug capabilities of the device are stopped if BOOT_LOCK is set in association with RDP level 1.
A debug reactivation must be mandatorily inserted in the boot sequence to reactivate the debug capabilities and make possible the regression level 1 to level 0.
Please refer to the example code in system_stm32u0xx.c from STM32U0 firmware package OEMiSB:
/* Software addition added to keep Debug enabled after Boot_Lock activation and RDP=1 */
#ifdef ENABLE_DBG_SWEN
if (((FLASH->SECR & FLASH_SECR_BOOT_LOCK) == FLASH_SECR_BOOT_LOCK) \
&& (((FLASH->OPTR & FLASH_OPTR_RDP) != 0xCCU) \
&& ((FLASH->OPTR & FLASH_OPTR_RDP) != 0xAAU)))
{
FLASH->ACR |= FLASH_ACR_DBG_SWEN; /* Debug access software enabled to avoid the chip
to be locked when RDP=1 and Boot_Lock=1 */
}
#endif /* ENABLE_DBG_SWEN */
|
2. RDP Password Regression
Regression allows reopening the product, by returning to RDP level 0.
A full flash user memory mass erase is applied prior to the reopening.
The devices support both permanent RDP level 2 or password-based RDP level 2 regression to level 1.
This level 2 to level 1 regression does not erase the application code, and it does not change the RDP level 1 protections in place.
The provisioning of two 128-bit passwords controls independently the unlocking of:
- RDP level 2 to RDP level 1 regression password configured when OEM2LOCK=1
- RDP level 1 to level 0 regression password configured when OEM1LOCK=1
The table below describes the possible combinations of mutual passwords usage:
OEM2LOCK |
OEM1LOCK
|
|
0 |
1
|
0 |
RDP 1 to 0 always granted RDP 2 to 1 never granted |
RDP 1 to 0 needs OEM1KEY unlock sequence RDP 2 to 1 never granted
|
1 |
RDP 1 to 0 always granted RDP 2 to 1 needs OEM2KEY unlock sequence |
RDP 1 to 0 needs OEM1KEY unlock sequence RDP 2 to 1 needs OEM2KEY unlock sequence
|
3. References
|