Revision as of 14:19, 31 May 2023 by Registered User
Under construction.png Coming soon

1. What is new product state

The product lifecycle is used to control the product security configuration. It allows the activation of the platform security mechanisms. A new lifecycle is introduced to the latest microcontrollers, based on a new state machine with an updated set of rules.

1.1. New product lifecycle

A new product lifecycle is being introduced to the STM32H5 family, to bring added flexibility to product manufacturing and maintenance.
The new product lifecycle includes the following phases:
- Development phase, offering full debug capabilities to the developer.
- Provisioning phase, the main asset areas are protected (no longer accessible)
- Final phase, the product is in the field.
- Maintenance phase, including field return management.
During the product life, the solution must guarantee that the ROT (Root Of Trust) and user assets are never disclosed.
This must be true for all four phases stated above.
The new product lifecycle lists all the product states:
Product Lifecycle (Simplified +Trust Zone)
Info white.png Information
When TrustZone® (TZ) is not proposed, the TZ-Closed does not exist.
Info white.png Information
This simplified version does not show the debug authentication part (regressions and debug reopening). The complete version is available in the dedicated debug authentication section.
Warning white.png Warning
The debug authentication configuration (DA-config) must be provisioned in provisioning state.

1.2. Up to three parties

In the development and provisioning phases, the product lifecycle allows up to three parties to develop the same product.
Different third parties means that for development and provisioning, the product can be set to protect (isolate) the different parties. This means three different responsibilities, and potentially three different keys (Firmware & data key pairs for install and update).
ST lifecycle allows the installation of up to three main parts on the product. They rely on three different parties
The figure below represents the product states to cover this three party model.
The three parties identified with their own colors: orange for immutable code, blue for updatable code running in TrustZone®, then grey for the non secure application(s).
To summarize:
- iROT-Provisioned is used once the iROT is provisioned (code and data).
- TZ-Closed is used once the iROT and security (TrustZone®) are provisioned.
- Closed or locked is used as soon as the full device is provisioned.
Up to 3 parties

1.3. Device provisioning

The device provisioning is completed in one or several steps.
This depends on the manufacturing constraints, and on the number of parties to provision:
• Initial provisioning
• Initial setup of the product, that determines who controls the ROT
• Could be only the [iROT] : in this case the product is set in iROT-Provisioned
• Could be [iROT+TZ-application] : in this case the product is set in TZ-Closed
• Could be [iROT+TrustZone®+none-secure application]
• Updates
• When several third parties are considered
• the Initial Provisioning is not complete,
• then the installed firmware oversees new firmware & keys to install

1.3.1. ST lifecycle development and provisioning considering up to three parties

The below figure represents the considered distribution models to considering up to three parties.
In short
- 1 party: All firmware owned by one entity.
- 2 parties: All secure part owned by one part, then non-secure application owned by a second part. This means 2 different responsibilities, and potentially key pairs (to manage install and updates).
- 3 parties: iROT, secure and non-secure applications owned by three different parties. This means three different responsibilities, and potentially key pairs (to manage install and updates).
Distribution models

1.3.2. ST lifecycle initial provisioning (from Open or Provisioning)

The device can be provisioned in one or several steps. This depends on its usage, on the manufacturing constraints, and on the number of third parties to provision. Overall, we are considering the inital provisioning as starting from a blank device. We recommend to make Provisioning for final product in Provisioning product state. While in development, all the lifecycle can use Open product state.
The below figure represents the initial provisioning considering the different distribution models.
  • Initial setup of the product, that will determine who is controlling its ROT
  • Could be only the [iROT]: in that case the product will be set in iROT-Provisioned
  • Could be [iROT+TrustZone®]: in that case the product will be set in TZ-Closed
  • Could be [iROT+TrustZone®+Non-Secure]
Initial Provisioning
It is recommended to use SFI (Secure Firmware Install) solution for initial provisioning in untrusted manufacturing.
It is also recommended to protect all key provisioning, even if the manufacturing is trusted.

1.3.3. ST lifecycle lo complete the initial provisioning

When several third parties are considered, the initial provisioning can cover only a part of the installation.
The end of the provisioning can be done based on firmware(s) which are already installed (at initial provisioning)
- Secure Firmware Update / Secure Key Provisioning
- In one step: both secure and non-secure installed on same time or in 2 steps: Secure is installed then non-secure in a second step.
To Complete Initial Provisioning

1.4. ST lifecycle / Product states

1.4.1. ST lifecycle / Product states = Open

The Open state corresponds to the default state of product when delivered.
This state is ideal to use while under development, as the debug is fully available.
In this state, the BOOT path configuration can be done thanks to TZEN and UBE Option Bytes, and most of features can be used as HDPL, TrustZone®, …
Product state = Open

1.4.2. ST lifecycle / Product states = Provisioning

The Provisioning state allows to provision the device, taking care of the assets protection.
We recommend to manage the product provisioning in this state, in order to take benefit of:
- the assets protection ==> in this state, the Debug is limited to HDPL3-NonSecure.
- When SAES available, encryption of the assets using a valid DHUK (to encrypt the OBKeys or other information). Effectively, the RHUK is not differentiated in Open state, whereas it is unique per product in all other states.
- Bootloader and JTAG/SWD availability for HDPL3-NS
Product state = Provisioning

1.4.3. ST lifecycle / Product states = iROT-Provisioned

The iROT-Provisioned state corresponds to an intermediate state of the product
The iROT code and data are provisioned.
From this state, the next level can be updated with Firmware Update mechanism.
Product state = iROT-Provisioned

1.4.4. ST lifecycle / Product states = TrustZone®-Closed

The TZ-Closed state corresponds to an intermediate state of the product. All the secure is installed, the non-secure application can be developped, or loaded later.
The iROT + uROT (optional) + Secure-OS code and data are provisioned.
From this state the non-secure application can be updated, thanks to Firmware Update mechanism, or directly programmed through flash loader (embedded in IDE).
Product state = TZ-Closed

1.4.5. ST lifecycle / Product states = Closed/Locked

The Closed state corresponds to the final state of the product. All debug accesses are closed, and only accessible through Debug Authentication.
From Closed state, the Debug Authentication can be used to launch partial or Full regressions, or to open the Debug.
The Locked state corresponds to the final state of the product. All debug accesses are Locked.
Warning white.png Warning
This state is final, the Debug Authentication is NOT usable.
Product state = Closed / Locked

1.5. ST lifecycle / Debug Authentication

The Debug Authentication feature allows to control the product lifecycle when it is in the field (maintenance).
The Debug Authentication feature can also be used during product configuration, to manage partial/full regressions or to activate intrusive debug. This is represented by green arrows in the below figure.

Security ProductLifecyle-TZEN1-Full.png

For more details, refer to: Debug authentication wiki article

2. References