Connectivity:Getting started with STM32CubeWiSE-RadioExplorer: Difference between revisions


Latest revision as of 14:18, 8 April 2025

1. Introduction

STM32CubeWiSE-RadioExplorer is a graphical user interface to interact with the STM32WL3x microcontroller and evaluate its radio capabilities. Using this tool, it is possible to program both the MRSUBG and the LPAWUR radio IPs of the device. The tool provides an easy-to-use interface in which it is possible to select and tweak all the system and radio parameters, read and write SoC and radio registers, and execute transmission and reception tests.

2. System requirements

2.1. Computer requirements

The STM32CubeWiSE-RadioExplorer application has the following minimum requirements:

  • PC with Intel® or AMD® processor running the Microsoft® Windows 10 operating system
  • At least 2 Gbytes of RAM
  • USB ports
  • Adobe Acrobat Reader 6.0

2.2. Supported devices

A NUCLEO-WL3x, for instance the NUCLEO-WL33CCx including a STM32WL33CC mini-board (MB1801D) and a NUCLEO-64 and an antenna

Note that a USB Type-C connector is used for:

  • Power supply
  • USB virtual COM port
  • STLink programmer and debugger

2.3. Supported firmware

Use the "Command Line Interface" software from the STM32Cube_FW_Vx.x.x package.

The CLI can be modified, recompiled with STM32CubeIDE, Keil, and IAR. This makes it possible to adapt the CLI firmware to any customized designs.

3. First launch of the STM32CubeWiSE-RadioExplorer

If this is the first time using NUCLEO-WL33CCx evaluation boards, it is recommended to check the Connectivity:NUCLEO-WL33CC : Out Of Box Demonstration wiki page to find more information and details on the procedure.

3.1. Step 1 Connect the evaluation kit

Connect the NUCLEO-WL33C1 to the USB port of the computer.

A USB type-C to USB type-A cable is recommended for this purpose.

3.2. Step 2 Build the CLI firmware

The CLI binary may not be available in the Cube package. For instance, it is not available in STM32Cube_FW_V1.0.0, so it needs to be compiled:

  • Unzip STM32CUBE_FW_WL3_V1.1.0.zip
  • Go to: STM32Cube_FW_WL3_V1.1.0\Projects\NUCLEO-WL33CC\Demonstrations\Command_Line_Interface\CLI
  • Choose one of the three IDEs:  
    • STM32CubeIDE, IAR, or Keil
  • Compile the project and download to the board

3.3. Step 3 Flash the device

Flashing the device can be done directly from the IDE used for compilation of the CLI binary.

Alternatively, the STM32CubeProgramer tool can be used.

3.4. Step 4 Start and connect the GUI

4Launch the STM32CubeWiSE-RadioExplorer.exe executable frm the WiSE_RadioExplorer folder and connect the board:

Launch the STM32CubeWiSE-RadioExplorer.exe and connect the device

By default, the baud rate is set to 115200 bps (using USART in the CLI firmware).

4. STM32CubeWiSE-RadioExplorer panels description

4.1. System settings

Configuration of the system settings:

STM32CubeWiSE-RadioExplorer system settings


The TX path option also depends on the hardware configuration, there are three possible RF implementations:

  • Tx-pin : Provides the lowest TX current up to +16 dBm – with limitation of minimum Vbat (+14/+16dBm)
  • TxHP-pin : Optimized solution to transmit up to +16 dBm without minimum Vbat limitation
  • Tx + TxHP pins : Transmits up to +20 dBm

In system settings tab, select TX, TX_HP or TX + TX_HP for TX path configuration, as shown below:

STM32CubeWiSE-RadioExplorer Tx path configuration

4.2. Radio settings

The main radio settings are available inside the Radio settings panel, they can be fine tuned using direct registers accesses

STM32CubeWiSE-RadioExplorer radio settings

4.3. Data coding

Below is the description of the coding capabilities that can be enabled/disabled using this panel:

STM32CubeWiSE-RadioExplorer data coding

4.4. Basic packet format configuration

The basic packet format is flexible enough to implement most of the custom packet formats. Below is the description of the available settings:

STM32CubeWiSE-RadioExplorer basic packet configuration

4.5. 802.15.4 packet format configuration

The STMWL3x contains an automatic packet handler for IEEE802.15.4 type of frames:

STM32CubeWiSE-RadioExplorer 802.15.4 packet format configuration

4.6. Registers setting

The STM32WL3x can be configured at the register level using this panel:

STM32CubeWiSE-RadioExplorer registers settings

The registers settings can be stored in a *.json file:

STM32CubeWiSE-RadioExplorer store registers

5. Radio tests

5.1. Continuous transmission test, XTAL frequency offset estimation, and power consumption in RX state

The radio test panel is used to center the base frequency of the device, to perform output power measurement, and to verify the power consumption when the radio is in RX state:

Connectivity Radio test.png

For more information on power consumption measurement setup, refer to the Connectivity:NUCLEO-WL33CC Hardware setup wiki webpage.

5.2. Communication test (using two instances of the STM32CubeWiSE-RadioExplorer)

Using two instances of the STM32CubeWiSE-RadioExplorer, it is possible to check the correct communication between two devices. For this purpose, make sure the radio configuration is similar between the two devices, and also verify that the frequency alignment is correct.

STM32CubeWiSE-RadioExplorer packet test

On the receiver's side the Status column indicates whether the reception is successful, or if there are any errors decoding the incoming frame.

It is also possible to use either "RX packet test" or "TX packet test" panels to perform interoperability tests with legacy devices. For this, set the radio & packet settings and send or receive directly from STM32CubeWiSE-RadioExplorer without any software development.