Registered User mNo edit summary |
Registered User mNo edit summary |
||
Line 501: | Line 501: | ||
<noinclude> | <noinclude> | ||
{{PublicationRequestId | 26425| 11/03/2023|}} | {{PublicationRequestId | 26425| 11/03/2023|}} | ||
[[Category: | [[Category:BLE_software_project_for_STM32WBA|05]] | ||
</noinclude> | </noinclude> |
Revision as of 10:26, 24 July 2023
1. Heart Rate Profile
Heart Rate Profile (HRP) [1] is a generic attribute profile (GATT) based low-energy profile defined by the Bluetooth® Special Interest Group[2]
The HRP, widely used in fitness applications, defines the communication process between a GATT-server of a Heart Rate Sensor device, such as a wrist band, and a GATT-client Collector device, such as a smartphone or tablet.
- The Heart Rate Sensor:
- Measures the heart rate and exposes it via the Heart Rate Service[3].
- Contains the Device Information Service that includes information, for example, about the manufacturer of the device.
- Is the GATT server.
- The Heart Rate Collector:
- Accesses the information exposed by the heart rate sensor. It can display it to the end user, or store it on a nonvolatile memory for later analysis.
- Is the GATT client.
The description of the Heart Rate Sensor project provided within the STM32CubeWBA MCU Package[4] is the subject of this article.
The table below describes the structure of Heart Rate Sensor services:
Bluetooth® Low Energy Heart Rate Service specification | |||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
The Heart Rate Profile is a combination of a Heart Rate Collector and a Heart Rate Sensor. The goal is to connect and exchange data in different applications.
The GAP - Generic Access Profile defines and manages advertising and connection.
The GATT - generic attribute profile defines and manages in/out data exchange.
1.1. Advertising Data
At startup, the Heart Rate Sensor application starts a fast advertising(80ms/100ms).
Data advertised are composed as follow:
Heart Rate Advertising packet | ||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
The manufacturer data are encoded following STMicroelectronics BlueST-SDK v2 as described below:
STMicroelectronics Manufacturer Advertising data | |||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Advertising is switched to Low Power advertising (1s/2.5s) after 60s.
1.2. On board buttons configuration
Button configuration for Bluetooth® Low Energy HeartRate Application on Nucleo-WBA52CG boards | ||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
2. Requirements
2.1. Software and system requirements
The following list contains the required software as well as the required minimum IDE version:
- IAR Embedded Workbench for ARM (EWARM) toolchain V9.20.1, plus a patch available in WBA Firmware Package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.2.zip
- RealView Microcontroller Development Kit (MDK-ARM) toolchain V5.37, plus a patch available in WBA Firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.0.0.zip
- STM32CubeIDE toolchain V1.12.0 [5].
The following programmer software is required to flash the board with an already generated binary:
- STM32CubeProgrammer[6]
2.2. Hardware requirements
The board NUCLEO-WBA52CG[7] is required to install the application.
2.3. Collector applications compatible
The STM32CubeWBA Heart Rate Sensor project is compatible with the following collectors:
3. STM32WB Heart Rate Sensor example description
3.1. Project directory
The "BLE_HeartRate" application is available by downloading the STM32CubeWBA MCU Package[4].
Refer to How to Build a Bluetooth® Low Energy project Wiki page for project directory information.
3.2. Project description
3.2.1. Structure
Below, a software project structure with the most important parts:
3.2.2. Application initialization
The different steps of the application initialization are described below:
3.2.3. GAP and GATT initialization and interaction
and The Bluetooth® Low Energy Heart Rate Sensor application initialization is done within app_ble.c
- Initialize the Bluetooth® Low Energy stack - initialize the device as peripheral - configure and start advertising: ADV parameters, local name, UUID - APP_BLE_init().
- Call the services controller initialization SVCCTL_Init() - svc_ctl.c.
- Manage the GAP event - SVCCTL_App_Notification().
- HCI_LE_CONNECTION_COMPLETE - provides information of the connection interval, slave latency, supervision timeout.
- HCI_LE_CONNECTION_UPDATE_COMPLETE- provides the new information of the connection.
- HCI_DISCONNECTION_COMPLETE - informs the application about the link disconnection and the reason.
The Services management is done by the service controller, svc_ctl.c
- Initialize the number of registered handlers - SVCCTL_Init().
- Manage events - SVCCTL_UserEvtRx()- from the Bluetooth® Low Energy Host Stack and redirect them to the gap event handler - SVCCTL_App_Notification.
The application level of the Heart Rate Sensor is done with hrs_app.c:
- Initialization of the services:
- Heart Rate Service - HRS_Init() - hrs.c
- Initialization of the context of the application
- Measurement value flags support
- Body sensor location - HRS_BODY_SENSOR_LOCATION_HAND
- Receive notification from the Heart Rate Service - HRS_Notification()
- When Heart rate measurement characteristics are enabled by the remote, simulate every 1 s the Heart Rate Measure (HRS_APP_Measurement) and increase the energy expended to transfer to the remote device (collector) - HRS_UpdateValue().
The Heart Rate Service hrs.c manages the specification of the service:
- Service Init - HRS_Init()
- Registers Heart Rate Event Handle to Service Controller - SVCCTL_RegisterSvcHandler(HRS_EventHandler).
- Initializes Service UUID – add Heart Rate service as Primary services.
- Initializes Heart rate measurement characteristic.
- Initializes Body Sensor location characteristic.
- Manages the GATT event from the Bluetooth® Low Energy Stack - HRS_EventHandler().
- ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
- Reception of a Write Command: HR Control Point Characteristic Value
- Sending of an aci_gatt_write_response() with an OK or KO status
- Notification to the application to Reset Energy Expended - HRS_Notification(HRS_RESET_ENERGY_EXPENDED_EVT)
- Reception of a Write Command: HR Control Point Characteristic Value
- ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
- Reception of an attribute modification - HR Measurement Characteristics Description Value : ENABLE or DISABLE Notification
- Notify application of the Measurement Notification - HRS_Notification(HRS_NOTIFICATION_ENABLED/DISABLED)
- Reception of an attribute modification - HR Measurement Characteristics Description Value : ENABLE or DISABLE Notification
- ACI_GATT_WRITE_PERMIT_REQ_VSEVT_CODE
3.3. How to use the Bluetooth® Low Energy Heart Rate application
Once the Bluetooth® Low Energy Heart Rate application is installed on the STM32WBA platform, launch the ST BLE Sensor or ST BLE Toolbox smartphone application. Then, scan and connect the device called HR_XX (where XX is replaced by the last byte of the BD address) to the application.
Once the Bluetooth® Low Energy connection is established and the notification enabled by the smartphone:
- Heart Rate measurement is provided remotely every 1 second thanks to the timer server and the task manager.
The Bluetooth® Low Energy Heart Rate application supports the pairing procedure.
- Pressing B2 while not connected allows to clear the security database.
- Pressing B2 while connected allows to request pairing.
With the Nucleo-WBA52CG board, it is also possible to change the RF PHY modulation.
- Pressing B1 while connected allows to switch between 2 Mbit/s and 1 Mbit/s PHY.
The Bluetooth® Low Energy Heart Rate application allows other actions on button:
- Pressing B1 while not connected allows to restart the fast advertising.
- Pressing B3 while connected allows to update the connection interval.
3.4. Low-power optimization
The project is delivered with the full system low-power enabled:
- no debug trace
- no debugger
It is possible to enable/disable the low-power feature within app_conf.h.
/******************************************************************************
* Low Power
*
* When CFG_FULL_LOW_POWER is set to 1, the system is configured in full
* low power mode. It means that all what can have an impact on the consumptions
* are powered down.(For instance LED, Access to Debugger, Etc.)
*
* When CFG_FULL_LOW_POWER is set to 0, the low power mode is not activated
*
******************************************************************************/
#define CFG_FULL_LOW_POWER (1)
3.5. UART debug trace
Thanks to the debug log via UART interface , it is possible to trace the application project.
To enable the traces within the project, enable them within app_conf.h as described below:
/**
* Enable or Disable traces in application
*/
#define CFG_DEBUG_APP_TRACE (0)
A debugger can also be supported by enabling it within app_conf.h as described below:
/**
* User interaction
* When CFG_LED_SUPPORTED is set, LEDS are activated if requested
* When CFG_BUTTON_SUPPORTED is set, the push button are activated if requested
* When CFG_DBG_SUPPORTED is set, the debugger is activated
*/
[...]
#define CFG_DBG_SUPPORTED (1)
Heart Rate Sensor - Initialization phase | Connected Phase |
---|---|
==>> Start Ble_Hci_Gap_Gatt_Init function
Success: hci_reset command
Success: aci_hal_write_config_data command -
CONFIG_DATA_PUBADDR_OFFSET
Public Bluetooth Address: 00:80:e1:2a:7c:ea
Success: aci_hal_write_config_data command -
CONFIG_DATA_IR_OFFSET
Success: aci_hal_write_config_data command -
CONFIG_DATA_ER_OFFSET
Success: aci_hal_set_tx_power_level command
Success: aci_gatt_init command
Success: aci_gap_init command
Success: aci_gatt_update_char_value - Device Name
Success: aci_gatt_update_char_value - Appearance
Success: hci_le_set_default_phy command
Success: aci_gap_set_io_capability command
Success: aci_gap_set_authentication_requirement command
Success: aci_gap_configure_whitelist command
==>> End Ble_Hci_Gap_Gatt_Init function
Services and Characteristics creation
Success: aci_gatt_add_service command: HRS
Success: aci_gatt_add_char command : HRME
Success: aci_gatt_add_char command : BSL
Success: aci_gatt_add_char command : HRCP
Success: aci_gatt_update_char_value BSL command
Success: aci_gatt_add_service command: DIS
Success: aci_gatt_add_char command : MANS
Success: aci_gatt_add_char command : MNBS
Success: aci_gatt_add_char command : SNS
Success: aci_gatt_add_char command : HRS
Success: aci_gatt_add_char command : FRS
Success: aci_gatt_update_char_value MANS command
Success: aci_gatt_update_char_value MNBS command
Success: aci_gatt_update_char_value SNS command
Success: aci_gatt_update_char_value HRS command
Success: aci_gatt_update_char_value FRS command
End of Services and Characteristics creation
==>> aci_gap_set_discoverable - Success
==>> Success: Start Advertising
|
>>== HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE -
Connection handle: 0x0001
- Connection established with @:62:f1:e7:ab:a6:18
- Connection Interval: 48.75 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
- Connection Interval: 7.50 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
>>== HCI_LE_CONNECTION_UPDATE_COMPLETE_SUBEVT_CODE
- Connection Interval: 48.75 ms
- Connection latency: 0
- Supervision Timeout: 5000 ms
ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE
HRS_NOTIFICATION_ENABLED
|
4. Heart Rate Collector - smartphone application
4.1. ST BLE Toolbox application
Once the Bluetooth® Low Energy Heart Rate application is installed on the STM32WBA platform, launch the STBLEToolbox smartphone application. The application starts scanning and enables seeing advertisement data, or to connect to the device. Once the device is connected, bpm and kcal measurements are displayed in real time.
5. References