Security:Introduction to Cryptography: Difference between revisions

Registered User
mNo edit summary
Registered User
mNo edit summary
 
(3 intermediate revisions by the same user not shown)
Line 69: Line 69:


<noinclude>
<noinclude>
[[Category:Cryptography|00]]
[[Category:Cryptographic_library|20]]
[[Category:Cryptographic_library|20]]
{{PublicationRequestId|19777| 4/28/2021| ?}}
{{PublicationRequestId|19777| 4/28/2021| ?}}
</noinclude>
</noinclude>

Latest revision as of 15:09, 22 June 2023

Cryptography is a fundamental block for implementing information security. It deals with algorithms that process data in order to grant certain properties, depending on the application needs:

  1. Data integrity services address the unauthorized or accidental modification of data. This includes data insertion, deletion, and modification. To ensure data integrity, a system must be able to detect unauthorized data modification. The goal is for the receiver of the data to verify that the data has not been altered.
  2. Confidentiality services restrict access to the content of sensitive data to only those individuals who are authorized to view the data. Confidentiality measures prevent the unauthorized disclosure of information to unauthorized individuals or processes.
  3. Identification and authentication services establish the validity of a transmission, the message, and its originator. The goal is for the receiver of the data to determine its origin.
  4. Non-repudiation services prevent an individual from denying that previous actions have been performed. The goal is to ensure that the recipient of the data is assured of the sender’s identity.

These services can be used by one of the following cryptography branches.

1. Encryption

Encryption is a branch of cryptography science. It converts clear data (also known as raw data), called plaintext, to unreadable data, called cipher text, using key(s), called cipher key(s), to perform cryptographic operations. The cipher text can only be decrypted into meaningful (clear text) form by using a secret key.

Cipher block diagrams

Symmetric cipher

This is a cipher that uses a single key for encryption and decryption. The key is shared between both entities (that which encrypts the plaintext and the one that decrypts the cipher text).

The ciphertext security relies mainly on the secrecy of the key, which must be securely shared between two entities.

Asymmetric cipher

Cipher that uses two keys, a public key for encryption and a private key for decryption. These keys are generally generated by putting a large random number into a complex mathematical algorithm to generate a key pair.

The ciphertext security relies mainly on the parameters of the mathematical algorithm (curve order, modulus length and so on) since the private key is never shared and remains an owner entity.

2. Hash

A cryptographic Hash function is a type of one-way function with additional properties that can be used for integrity checking. This deterministic algorithm takes an input data block of arbitrary size and returns a fixed-size bit string, called digest. Hash functions are built in such a way that it is computationally infeasible to:

  • find the data value given the “digest” of an unknown data
  • find two messages that hash to the same digest.
Hash operation block diagram

3. Message authentication code

A MAC (message authentication code) requires two inputs: a message and a secret key known only by the originator of the message and its intended recipient(s). This allows the recipient(s) of the message to verify its integrity and ensure that the message’s sender has the shared secret key. If a sender doesn’t know the secret key, the hash value would then be different, allowing the recipient to understand that the message was not from the original sender.

Authentication operation block diagram

4. Digital signature

Digital signature is a mechanism by which a message is authenticated, that is, proving that a message comes from a given sender in a similar manner to a signature on a paper document. This is based on asymmetric cryptography; the private key is used to sign the message, while only the public key is required to verify signatures. Therefore only the owner of the private key can compute signatures, while anyone can verify them.

Digital sign operation block diagram

5. Random number generator

RNG (random number generator). The secure aspect of cryptography algorithms is based on the impossibility of guessing the key or the additional, one-time usage data used, for example, to sign a message. Therefore, keys and additional data must be random. To perform this generation an RNG algorithm can be used; it receives an entropy string as an input that must be generated by a source of true randomness (for example a true random number generator peripheral) and produces a cryptographically strong random output of much larger size.

RNG operation block diagram

6. Cryptographic branch usage

Each of the above branches of the cryptography standard needs to be used according to the application level requirement.

Summary of cryptography branch applications
Application Data integrity Confidentiality Identification and authentication Non-repudiation
Symmetric key encryption NO YES NO NO
Secure Hash Functions YES NO NO NO
MAC YES NO YES NO
Digital signatures YES NO YES YES