Introduction to Cellular LTE CatM / NBIoT

Revision as of 13:40, 14 February 2022 by Registered User

This article contains application examples, document references, tips, and so on related to STM32 Cellular.

1. What are Cellular LTE CatM and NBIoT?


Technologies


LTE CatM and Narrowband Internet of Things (NBIoT) are low-power wide-area network (LPWAN) radio technology standards developed by 3GPP to enable a wide range of cellular devices and services.
NBIoT focuses specifically on indoor coverage, low cost, long battery life, and high connection density.
The advantage of LTE CatM over NBIoT is its higher data rate, mobility, and voice over the network. However it requires more bandwidth and is more costly.

Check also GSMA's NBIoT / LTE CatM world wide coverage information[1].

2. Wiki MCU / Cellular : pages breakdown

Find here the direct links to access dedicated articles. For beginners, it is recommended to start by reading next chapter first.

3. Getting started with STM32 and Cellular LTE Cat M and NBIoT


From a hardware point of view, STMicroelectronics offers various ways to set up cellular connectivity solutions on STM32 MCUs. For STM32 boards that support the STMod+ connector, STMod+ modem boards can be directly connected to the STM32 board. For STM32 boards that do not have an STMod+ connector, an ARDUINO® / STMod+ adapter (X-NUCLEO-STMODA1) can be inserted between the STM32 board and the modem board.
To obtain a complete setup, packs are available that contain the STM32 board together with the modem board. Otherwise the STM32 board and the modem board can be ordered separately. For more information check the hardware setup article.
Note that for each version of the Cellular middleware software there is a set of supported hardware. See also the details in the hardware setup article.

On the software side, X-CUBE-CELLULAR (X-CUBE Expansion Package) provides a software solution to allow customers to quickly and easily develop their own firmware:

  • Based on ThreadX (fromV7.x onwards) and FreeRTOS (From V1.0.0 onwards)
  • Users can choose to use either the IP stack in the modem or in the STM32 (LwIP or NetX Duo)
  • Command line through Virtual COM UART over USB ST-LINK to configure the cellular connectivity parameters (technology selection, bands, APN, and others), and the connection to the cloud IoT platform
  • Easy to support a new modem.

Several applications are provided as examples.

For more information check the X-CUBE-CELLULAR Wiki article.

New hardware setups and new software features in X-CUBE-CELLULAR are to be provided to customers over time.

4. How to...

This part is a guideline that describes how to perform the main activities with X-CUBE-CELLULAR. All the information is merged in the Cellular How To Wiki article

5. FAQ

All the frequently-asked questions are listed in the dedicated Cellular F.A.Q Wiki article.

6. Video related to Cellular LTE CatM and NBIoT

pc videol.png

Zigbee 3.0 mesh to cloud over cat-M with BLE 5.0 user control (MWC/EW 2020)

pc videol.png

ST at CES 2019 - LTE IoT Starter Kits

pc videol.png

STM32 Cellular to Cloud Discovery Packs: 2G/3G and Espruino JS, LTE IoT! Embedded World 2018

pc videol.png

Getting started with STMicroelectronics cellular IoT discovery kit

pc videol.png

How to program FP-SNS-DATALOG1 firmware on STWIN using STM32CubeProgrammer

7. Specific tools

Those tools can be used in users projects but are not mandatory.

  • STMicroelectronics’ STM32 Power Shield to power and analyze current consumption[2]
  • Network simulator for both LTE CatM & NBIoT[3]


8. Terms and definitions

Term Definition
API Application programming interface / Access point identifier
APN Access point name
BSD Berkeley software distribution
BSP Board support package
CID Context ID (context identifier of a cellular connection)
CLI Command-line interface
COM Cellular communication
DC Data Cache
HAL Hardware abstraction layer
IDE Integrated development environment
IF Interface
IoT Internet of things (refer to [4])
IPC Inter-processor channel
LED Light-emitting diode
NAT Network address translation
NFMC Network-friendly management configuration (refer to [4])
MNO Mobile network operator
MVNO Mobile virtual network operator
PDN Packet data network
PDP Packet data protocol
PPP Point-to-point protocol
PPPoSIF PPP over serial IF
PS Packet switching
RAM Random-access memory
RSSI Received-signal strength indication
RTC Real-time clock
TCP Transmission control protocol
UDP User datagram protocol
URC Unsolicited result code

9. Important note regarding the safety

Caution requirements about the RF exposition must be fulfilled by the end-user as defined by the regulatory standards.
Warning: Use the hardware only with the antenna connected. With no antenna connected, there is a risk of damage to the modem.

10. References