Migration from previous Cryptographic Library version

Revision as of 15:47, 6 May 2021 by Registered User (→‎New algorithms)

This page explains the differences between the previous Cryptographic Library version V3.x.x and the current one V4.x.x.

1. What's new in the V4.x.x version

Cryptographic Library V4.x.x, in addition to new algorithms, brings more simplicity and more performances (both speed and size)

1.1. New algorithms

Here are the new algorithms available:

Hash
SHA3, SHAKE, SM3
MAC
KMAC
Cipher
SM4
ECC
SM2, ECDH on Curve448, EdDSA on edwards448 curve
RSA
PKCS#1 v2.2, CRT, Bellcore Attack protection
DRBG
CTR_DRBG-AES256

1.2. Simplicity

Here is an example on simpler interface brought by the Cryptographic Library V4.x.x in performing ECDSA verification:

V3.x.x V4.0.0
int32_t rv;
EC_stt EC_st;
membuf_stt Crypto_Buffer;
ECpoint_stt *PubKey = NULL;
ECDSAsignature_stt *sign = NULL;
uint8_t membuf[MAX_MEMBUF_SIZE];
ECDSAverifyCtx_stt verctx;

uint8_t pub_x[] = {…}, pub_y[] = {…};
uint8_t sign_r[] = {…}, sign_s[] = {…}, digest[] = {…};

Crypto_Buf.pmBuf = membuf;
Crypto_Buf.mUsed = 0;
Crypto_Buf.mSize = sizeof(membuf);

// ToDo: manually fill EC_st with curve parameters!!!

/* Init the EC main struct */
rv = ECCinitEC(&EC_st, &Crypto_Buf);

/* Init the public key */
ECCinitPoint(&PubKey, &EC_st, &Crypto_Buf);
ECCsetPointCoordinate(PubKey,
                      E_ECC_POINT_COORDINATE_X,
                      pub_x,
                      sizeof(pub_x));
ECCsetPointCoordinate(PubKey,
                      E_ECC_POINT_COORDINATE_Y,
                      pub_y,
                      sizeof(pub_y));

/* Init the signature */
ECDSAinitSign(&sign, &EC_st, &Crypto_Buf);
ECDSAsetSignature(sign,
                  E_ECDSA_SIGNATURE_R_VALUE,
                  sign_r, sizeof(sign_r));
ECDSAsetSignature(sign,
                  E_ECDSA_SIGNATURE_S_VALUE,
                  sign_s, sizeof(sign_s));

/* Verification */
verif_ctx.pmEC = &EC_st;
verif_ctx.pmPubKey = PubKey;
rv = ECDSAverify(digest, sizeof(digest),
                 sign, &verif_ctx, &Crypto_Buf);
cmox_ecc_retval_t rv;
cmox_ecc_handle_t Ecc_Ctx;
uint8_t membuf[MAX_MEMBUF_SIZE];
uint32_t fault_check = CMOX_ECC_AUTH_FAIL;

uint8_t pubkey[] = {…}, digest[] = {…}, signature[] = {…};

/* Construct a ECC context */
cmox_ecc_construct(&Ecc_Ctx,
                  CMOX_ECC256_MATH_FUNCS,
                  membuf, sizeof(membuf));

/* Verify directly the signature passing
   all the needed parameters */
rv = cmox_ecdsa_verify(&Ecc_Ctx,
                       CMOX_ECC_CURVE_SECP256R1,
                       pubkey, pubkey(Public_Key),
                       digest, sizeof(digest),
                       signature, sizeof(signature),
                       &fault_check);


1.3. Performances

Here is a comparative view of the best performances achievable on a STM32G4 using both the Cryptographic Library V3.x.x and V4.x.x versions.

Use cases V3.1.3 Cycles V4.0.0 Cycles Improvements V3.1.3 Code Size V4.0.0 Code size Improvements
AES CBC 64 Bytes encryption 11189 8660 22.6% 8218 4592 44.1%
AES CBC 64 Bytes decryption 12000 10098 15.8% 8218 4592 44.1%
SHA256 16 bytes Digest 9630 6137 36.2% 2204 2144 2.7%
ECDSA SECP256R1 Signature 20298504 2957360 85.4% 21616 14610 32.41%
ECDSA SECP256R1 Verification 26891792 6575536 75.55% 21616 15110 30.10%

2. Deprecated algorithms

Some algorithms available in the V3.x.x are no more supported, cause they have been deprecated for security reason.

Algorithm Comment
MD5 More details on MD5 vulnerabilities are available here rfc6151
ARC4 More details on RC4/ARC4 vulnerabilities are available here rfc7465
DES Withdrawn by NIST on May 19, 2005:FIPS46-3
T-DES Withdrawn by NIST on September 26, 2018:NIST-SP800-20
Info white.png Information
NOTE: SHA1 algorithm, even if it is also considered as deprecated, is still available in the Cryptographic Library cause it comes with other SHA implementations.

3. V3.x.x to V4.x.x migration information and links

In the Cryptographic Library middleware legacy_v3 folder, we provide migration helpers.

This files are provided to help you migrate your software designed upon V3.x.x APIs onto the V4.x.x APIs.

3.1. Switch your project from V3.x.x to V4.x.x

  • Remove the old V3.x.x library from your project, including the path to the V3.x.x library header folder.
  • Update your project to include the V4.x.x as describe in Creating a project
  • Add to your project settings the path to the legacy_v3/include folder
  • Add to your project settings the sources to the legacy_v3/src files coresponding to the algorithms you are using
  • Rebuild all your project, it should work as before


3.2. Migrate your project from V3.x.x to V4.x.x

You can now rewrite your application progressively to use the V4.x.x APIs and then fully benefit of all the V4.x.x improvments.


Warning white.png Warning
Please notice: It is not recommended to use this helpers in your final product, as they are ONLY helpers for migration; and will not allow taking benefit of all the best of the Cryptographic Library