This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The STM32 Sniffer for Bluetooth® LE allows you to learn, analyze and debug Bluetooth® LE communications.
You will be able to listen to advertising packets or follow communications between a device and the device it is communicating with. In case devices start pairing, it may even be possible to decrypt the packets.
System presentation |
---|
The sniffer firmware is compatible with two development boards :
Compatible development boards |
---|
The following articles will help you to setup and use the sniffer.
1. Installing the STM32 Sniffer
2. Using the STM32 Sniffer
3. Troubleshooting