STM32 Sniffer for BLE Setup guide

1. Introduction

The STM32 Sniffer for Bluetooth® Low Energy is composed of two main parts:

  • The software part running on the computer: analyzes and displays packets.
  • The firmwares part running on the STM32WB, STM32WB09 MCUs: intercepts over the air packets.

There are two sniffer firmwares targeting the following devices:

  • STM32WB55
  • STM32WB09


STM32WB55 System Architecture
System Architecture

Download the necessary STM32WB55 files on the STM32 hotspot.

STM32WB09 System Architecture
System Architecture

Download the necessary STM32WB09 files on the STM32 hotspot.

2. Minimum requirements

The following software and hardware parts are needed.

2.1. Hardware

At least one of these STM32WB55 development boards is needed:

The following STM32WB09 development boards is needed:

2.2. Software

Operating system:

  • Windows 10 or 11

Wireshark:

  • Version 4.0.3 or later
  • During the setup, accept the installation of Ncap.

Python:

  • Version 3.11.2 or later
  • Add Python to your path (you can select “Add Python to environment variable.” during setup).

PySerial:

  • Version 3.5 or later
  • Make sure that PySerial is installed on the correct version of Python if you have multiple installations. Use pip3 for example to force install on Python3.

libscrc python library is required from st_ble_sniffer_stm32wb09.py:


3. Programming the board

3.1. STM32WB55 steps

There are two files to flash:

  • The sniffer application: stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex
  • The sniffer Bluetooth® LE wireless stack: stm32wb55_ble_sniffer_cm0_stack.bin

1. Install STM32CubeProgrammer

2. Update the wireless stack:

  • Use the stm32wb55_ble_sniffer_cm0_stack.bin file at the start address: 0x080CE000.
  • Follow the part 3.2 of the tutorial to learn how to update the wireless stack.

3. Flash the application firmware:

  • Use the stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex file.
  • Follow the part 3.3 of the tutorial to learn how to flash the application firmware.

3.2. STM32WB09 steps

There is one file to flash:

  • The sniffer application: STM32WB09_BLE_Sniffer.hex

1. Install STM32CubeProgrammer

2. Update the sniffer application firmware:

  • Use the STM32WB09_BLE_Sniffer.hex or STM32WB09_BLE_Sniffer.bin file at the start address: 0x10040000
  • Follow the part 4.4 of the tutorial to learn how to flash the application firmware.

4. Installing Wireshark plugins

Launch Wireshark:

Click on the Help menu.
Click on About Wireshark to open a new window.
Select the Folders tab.
Double click on the Personal Extcap path and Personal Lua Plugins to open the corresponding locations in the file explorer.
Finding the Wireshark plugins directories

4.1. Installing the plugins

4.2. STM32WB55 steps

  • Copy the st_ble_sniffer_dissector.lua file into your Wireshark Personal Lua Plugins folder.
  • Copy the st_ble_sniffer.py and st_ble_sniffer.bat files into your Wireshark Personal Extcap path folder.

Your folders should look like this:

Plugins folders
  • Open a command prompt in your Personal Extcap path folder.
  • Run: st_ble_sniffer.bat --extcap-interfaces

You should have an output similar to this:

Verifying that the extcap plugin runs
  • Make sure that the board with the sniffer firmware is plugged, and that no other programs use the com port such as the serial terminal.
  • In Wireshark, refresh the capture interfaces list:
Click on the Capture menu.
Click on Refresh Interfaces.
Verifying extcap plugin can run in Wireshark

You should now see the STM32WB sniffer interface like this:

Verifying that extcap plugin runs in Wireshark

4.3. STM32WB09 steps

Repeat the same steps as STM32WB55 ones, using the following files:

  • st_ble_sniffer_dissector_wb09.lua
  • st_ble_sniffer_wb09.py
  • st_ble_sniffer_wb09.bat

It is important to create a Python virtual environment inside your personal extcap folder by launching the following commands in a Windows terminal

1.  Create virtual environment:

    > python -m venv venv

2.  Activate virtual environment:

    > venv\Scripts\activate

3.  Install required python libraries:

    > pip install -r requirements.txt

You should now be able to see the STM32WB09 sniffer interface in Wireshark.

4.4. Installing the profile

In Wireshark:

Click on the Help menu.
Click on About Wireshark to open a new window.
Select the Folders tab.
Double click on Personal configuration to open the corresponding location in the file explorer.
Finding the Wireshark profiles directory


Copy the ST_BLE_Sniffer_profile folder (for STM32WB55) or ST_BLE_Sniffer_profile_stm32wb09 folder (for STM32WB09) into your Wireshark Personal configuration/profiles folder.

Your folder should look like this:

Verifying that extcap plugin runs in Wireshark

5. Configuring Wireshark

5.1. Enabling the sniffer profile

In Wireshark:

Click on the Edit menu.
Click on Configuration Profiles... to open a new window.
Select the ST_BLE_Sniffer_profile for STM32WB55 or ST_BLE_Sniffer_profile_stm32wb09 for STM32WB09.
Click on OK.
Enabling the profile

5.2. Enabling the interface toolbar

Open Wireshark:

Click on the View menu.
Click on Interface Toolbars.
Enable the STM32WB interface for STM32WB55 or STM32WB09 interface for STM32WB09.
Enabling the interface toolbar

These toolbars should be visible:

STM32WB55 Interface toolbar
STM32WB09 Interface toolbar

5.3. Testing

Double click on the STM32WB or STM32WB09 sniffer interface to launch the capture.

Verifying that extcap plugin runs in Wireshark


If advertising packets are visible like in the graphic below, it means that the installation of the STM32 Sniffer for Bluetooth® Low Energy is successful.

Verifying the installation

Refer to theuser guide to learn more about how to use the sniffer.



No categories assignedEdit