Coming soon |
This page contains information such as, application examples, document references, and tips related to STM32 Bluetooth® Low Energy protocol.
1. LoRaWAN® overview
1.1. What is LoRaWAN® ?
This section provides a general overview of LoRaWAN® , particularly focusing on the LoRaWAN® end device. LoRaWAN® is a type of wireless telecommunication network designed to allow long-range communication at a very low bit rate and enabling long-life battery-operated sensors and actuators. LoRaWAN® defines the communication and security protocol ensuring interoperability with the LoRaWAN® network. Table 3 shows the LoRaWAN® class usage definition.
Class name | Intended usage |
---|---|
A - All |
|
B - Beacon |
|
C - Continuous |
|
1.2. LoRaWAN® Network architecture
The LoRaWAN® network is structured in a star of stars topology, where the end devices are connected via a single LoRaWAN® link to one gateway.
Note: While the physical layer of LoRa® is proprietary, the rest of the protocol stack (LoRaWAN® ) is kept open and its development is carried out by the LoRa Alliance® .
The STM32WL series[1] is the ideal MCU family for developing Long Range sub-gigahertz application such sensors and transmit information to central devices.
2. Wiki Bluetooth® LE: pages breakdown
For users aware of this wiki Bluetooth® LE, see below the direct links to dedicated articles. For beginners, start reading the next chapter first.
- Bluetooth® LE overview (this current page)
- STM32WB Series
- Bluetooth® LE Hardware setup (Information regarding the configuration of the board to run the application)
- Bluetooth® LE Software setup - STM32CubeWB (Information about the Bluetooth® LE software development)
- Several Bluetooth® SIG specified applications
- Several ST proprietary Bluetooth® LE applications
- STM32WB BLE STM32CubeMX Bluetooth® LE application creation & configuration
- STM32WB Series
3. Getting started with STM32WL Series and LoRaWAN®
The device architecture leverage state-of-the art STM32 ultra-low-power process node and is available from 64KB up to 256KB of Flash memory and up to 256 KB of SRAM.
Various packages are available: UQFN48, BGA73.
The evaluation board is the NUCLEO-WL55JC integrating stm32wlxx, ST link, LEDs, Buttons and a Arduino connector.
The Nucleo exists in 2 frequency bands:
Nucleo Reference | Description |
---|---|
NUCLEO-WL55JC1 | High Band |
NUCLEO-WL55JC2 | LowBand |
On the software side, the STM32CubeWL MCU Package[2] provides a software solution to allow customers to quickly and easily develop their own firmware thanks to:
- several LoRaWan® certified applications
- several Radio Application
THe STM32CubeWL Software Package can also be found on Github here
4. STM32WB learning center
4.1. STM32WL LoRaWAN®
4.2. STM32WB Bluetooth® LE MOOC (massive online courses)
STM32WB workshop
Information about STM32WB MCU line, with its hardware and software tools introduction and multiple hands-on session. The course provides an introduction to BLE theory and its implementation within STM32WB stack.
STM32WB Firmware Update Over the Air (FUOTA)
Basic information about software update STM32WB MCU line using different tools and techniques, including over the air methods
STM32 Bluetooth® LE MESH Introduction
How to build Bluetooth Mesh network with STM32WB using STM32WB55 Nucleo pack and its software package
5. STM32WL software application notes and user manuals
6. STM32WL hardware guidance
7. Specific tools
- STM32CubeMonitor - Software tool to test the RF performance of STM32-based hardware devices
- STM32CubeMX - STM32Cube initialization code generator
- STM32CubeProgrammer - Software Programmer for all STM32
- STM32PowerShield - Power and Analyze current consumption
8. References
9. Terms and definitions
Term | Definition |
---|---|
LoRaWAN | Long Range Wireless Area Network |
Example | Example |
Example | Example |
Example | Example |