STM32WB Bluetooth® LE Hardware Setup

Revision as of 17:14, 25 January 2022 by Registered User (→‎Boards and ST-LINK USB cable connections)
Under construction.png Coming soon

Click here for Bluetooth® LE overview

1. STM32WB Dual Core

The STM32WB combines a well-known ARM Cortex-M4 for the application, plus, a 2.4 GHz radio subsystem and a ARM Cortex-M0+ processor running the Firmware Upgrade Service (FUS) and the Wireless Stack .


STM32WB Dual Core
Connectivity STM32WB SW archi.png


All the code running on ARM Cortex-M0+ (CPU2) is delivered as encrypted binary and it is necessary to upgrade the wireless stack before developing a project on the application side.

  • Black box for customer perspective

All the code running on ARM Cortex-M4 (CPU1) is delivered as source code.
The STM32WB will be pre-loaded with so-called Root Security System (FUS) firmware necessary to authenticate the selected Wireless stack (binary encrypted format) loaded by the customer on st.com.

STM32WB memory mapping
Connectivity STM32WB memory mapping.png



Cortex-M0+ security protects upper parts of Flash and SRAM2 memories. Size of each areas are automatically set during wireless stack install or update.

  • Secure Flash Start Address (SFSA) is the lower boundary of protected Flash memory. It is aligned on 4KBytes(WB5x) or 2KBytes(WB1x) granularity.
  • For STM32WB5x and STM32WB3x Families:
    • Secure Backup Ram Start Address (SBRSA) and Secure Non-Backup Ram Start Address (SNBRSA) are respective lower address of protected parts of SRAM2a and SRAM2b memories. Size can be set with a granularity of 1KBytes.
    • backup SRAM2a can be used to store data when system is in Standby Mode
  • For STM32WB1x Families:
    • Secure Backup Ram Start Address (SBRSA_A) and Secure Backup Ram Start Address (SBRSA_B) are respective lower address of protected parts of SRAM2a and SRAM2b memories. Size can be set with a granularity of 1KBytes.
    • Both can be used to store data when system is in Standby Mode, in addition to the SRAM1.

However settings of these option bytes are under the responsibility of FUS. They are set during a first install or an update of the wireless stack. They cannot be modified by the user.



This wiki article contains information to help users how to use STM32Cubeprogrammer[1] to upgrade the secure area of the STM32WB.

2. Hardware Platform Configuration

2.1. P-NUCLEO-WB55[2] and STM32WB5MM-DK Discovery kit[3]

2.1.1. Boards and ST-LINK USB cable connections

Nucleo Discovery Kit
Connectivity Nucleo-connection.jpg
Connectivity DK-connection.jpg


The USB cable from the PC is used to power and interact with the STM32.

  • P-NUCLEO-WB55 : Jumper JP1 to USB STL and USB ST-LINK to be used
  • STM32WB5MM-DK Discovery kit : Jumper JP2 to 1-2 and USB ST-LINK to be used




3. FUS and Wireless Stack Update

Firmware Upgrade Service (FUS) and Bluetooth® Low Energy Stack can be updated using STM32CubeProgrammer software[1]
Regarding FUS, more information can be found on the dedicated Firmware Upgrade Services wiki article or within the Firmware Upgrade Service for STM32WB series Application Note[4].

3.1. How to Update the FUS

FUS (firmware upgrade services) is a firmware running on STM32WB Cortex®-M0+ and offering following features:

  1. Install, upgrade or delete STM32WB Cortex®-M0+ wireless stack
  2. FUS self-upgrade
  3. Customer authentication key management
  4. User key management
  5. Communication with Cortex®-M4 (user code or bootloader)


Below are described the different steps to update the FUS of P-NUCLEO-WB55 and STM32WB5MM-DK Discovery platforms.
Connect your platform using STM32Cubeprogrammer[1].

CubeProgrammer: connection
Connectivity Dk1.png

3.1.1. Start FUS

When connected, go to Firmware Upgrade Services interface, and start the actual FUS, clicking on the associated button.

CubeProgrammer: start FUS
Connectivity 3-bis.png


Warning white.png Warning
If an error occurs while starting the FUS. Reconnect the board and restart the FUS.


Once the FUS is correctly started, the following logs should be visible on the CubeProgrammer logs interface.

CubeProgrammer: FUS started logs
Connectivity 4.png

3.1.2. Read FUS

Once the FUS is started read its value by clicking the button "Read FUS infos"


CubeProgrammer: read FUS
Connectivity 5-bis.png

3.1.3. Update Firmware Upgrade Service binary

The latest version of the FUS can be found in STM32CubeWB MCU Package[5].

Check the Releases Notes to know what is the latest FUS version and the FUS Start Address.

FUS information
Connectivity 7-bis.png


If the FUS version of your platform is different than the version specified in Release Notes, proceed to FUS update by following the below steps:

- If the platform FUS version is 0.5.3, use the binary dedicated:
STM32Cube_FW_WB_V[...]\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw_for_fus_0_5_3.bin
.

CubeProgrammer: FUS 0.5.3
Connectivity 6.png


- If the platform FUS version is different from 0.5.3, then use the other binary: STM32Cube_FW_WB_V[...]\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw.bin
.

Complete the file path with the right file and add start address (see release notes). Click on Firmware Upgrade.

CubeProgrammer: update FUS
Connectivity 7-trd.png


A popup occurs to confirm the correct upgrade.

3.1.4. Check new FUS version

Check the new FUS version by clicking on Read FUS info button.

CubeProgrammer: read new FUS
Connectivity 9.png

3.2. How to update the Bluetooth® LE Wireless Stack

The Bluetooth® LE Stack can be updated on the same way as the FUS.

Firstly, check the start address of the stack in the Release Notes.

Stack start address
Connectivity 11-bis.png


Select the type of stack to be loaded in STM32CubeWB package[5].
For P-NUCLEO-WB55 and STM32WB5MM-DK Discovery platforms, the Bluetooth® LE stack recommended is: STM32Cube_FW_WB_V[...]\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_BLE_Stack_full_fw.bin.

Check First Install checkbox if it is the first time you install the stack on your platform.

CubeProgrammer: stack installation
Connectivity 11.png

3.3. How to check Bluetooth LE Application is up and running

To ensure FUS and Bluetooth® LE stack are fully functional, it is necessary to load an application on the ARM Cortex-M4. The STM32CubeWB package[5] provides different applications

Example project binaries are provided in STM32CubeWB package[5]

  • for P-NUCLEO-WB55 board:
    • STM32Cube_FW_WB_V[...]\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\[...].
  • for STM32WB5MM-DK board:
    • STM32Cube_FW_WB_V[...]\Projects\STM32WB5MM-DK\Applications\BLE\[...].


Below steps explain how to install and launch BLE_p2pServer project on board.
Go to Erasing & programming interface.
Select the path to the application binary, for example:
STM32Cube_FW_WB_V[...]\Projects\[...]\Applications\BLE\BLE_p2pServer\Binary\BLE_p2pServer_reference.hex.
Then, click on Start Programming button.

CubeProgrammer: install application
Connectivity p2p-install1.png


Once the application correctly flashed on the platform, open a terminal as described with the Debug Interface Chapter and reset the platform.


Once the board is connected and the terminal window setup, press the reset button of the board. The following messages are printed to the virtual COM window when the firmware starts successfully: At this point the FUS and Bluetooth® LE Stack are correctly installed on your platforms, BLE_p2pServer application prints the following messages to the virtual COM window when the firmware starts successfully:

  • FUS and Bluetooth® LE stack version are displayed on terminal log:
application startup logs
Connectivity FUS version logs.png

3.4. Debug Log via UART Interface

The P-NUCLEO-WB55 and STM32WB5MM-DK platforms embed the ST-LINK/V2 in-circuit debugger and programmer for STM32 microcontrollers. The single-wire interface module (SWIM) and JTAG/serial wire debugging (SWD) interfaces are used to communicate with the STM32WB microcontroller. It supports as well the STM32 Virtual COM Port Driver to be able to communication between a PC and the application processor via a serial interface.

Use any convenient software terminal to open the serial communication port of the PC to check the messages from the board. Select your Serial port and setup your connection as follow (example done with Tera Term software).

Set a new serial connection to the ST platform:

Tera Term setup (1/2)
Connectivity tera-term-1-2.png

Setup your serial connection as below:

Tera Term setup (2/2)
Connectivity tera-term-3-4.png

4. Related Video

Further information can be found on the following videos:

pc videol.png

Getting Started: Stack loading

pc videol.png

Getting Started: STM32WB USB Dongle

pc videol.png

Stack and FUS Update over USB bootloader

5. Going Further

6. References