1. General information
The ST Motor Profiler software tool provides you with an easy and friendly way to find profiled information for a user custom motor and save it as user motor.
The ST Motor Profiler runs on PC system, using Windows® OS, and requires an USB type A connector.
Please, refer to the STM32 MC SDK release note to get all information about the ST Motor Profiler usage possibilities.
The ST Motor Profiler software tool can be used to identify the main PMSM characteristics, which are further transferred to the ST MC Workbench.
2. Launch the ST Motor Profiler
Launch the “ST Motor Profiler” software tool by clicking either its icon (Cf. Figure 1) or either running directly from the installation folder.
The user can run “ST Motor Profiler” software tool also from the dedicated link button from the ST Motor Control Workbench GUI (Cf. Figure 2).
Then, the ST Motor Profiler starts-up a GUI window as shown in Figure 3.
3. Configure your hardware setup
Click on the “Select Boards” button to display the list of supported boards (Cf. Figure 3), then choose your ST application board setup. Please, note that the ST Motor Profiler software tool can be used only with the ST hardware setup listed there. Figure 4 presents an example from this list.
Just click on the ST hardware setup to select it, thus configure the ST Motor Profiler software tool.
As an example, the Figure 4 shows the P-NUCLEO-IHM001 selection.
Then, complete the parameter fields with your motor information:
- the number of pole pairs inside your motor (mandatory field);
- the Max Speed of your motor (optional field);
By default, the ST Motor Profiler software tool looks for the maximum allowed speed matching the motor and the hardware setup used.
- the Max Current admissible by your motor (optional field);
By default, it is the maximum peak current deliverable by your hardware setup.
- the nominal DC Bus Voltage used by your hardware setup (optional field);
By default, it is the power supply stage as either the bus voltage for low voltage applications (DC voltage), or either the √2VACrms for high voltage application (AC voltage).
- the magnetic build-in type (mandatory field);
By default, it is the SM-PMSM with is selected.
- the Ld/Lq ratio (mandatory field) only in case of I-PMSM build-in (Cf. Figure 6).
Figure 5 provides example values for the BR2804-1700KV-1 motor provided with the P-NUCLEO-IHM001 hardware setup.
4. Connect to your hardware setup
When the ST Motor Profiler is configured, click on the “Connect” button (Cf. red area in Figure 7).
Then, depending on your hardware setup history, a status window appears as shown in Figure 8. In case of problem, a troubleshot message window will pop-up (Cf. Table 1) to support your recovery action.
When successfully connected to your hardware setup, the “Start Profile” button shall appear as surrounded in Figure 9.
5. Profile your motor
Click on the “Start Profile” button as surrounded in Figure 9 to profile the motor.
First the Electrical parameters are identified, then the Mechanical ones. In case of Over-Current fault detection, the profiling is restarted with a reduced current. When profiling is successfully completed, all the motor measurements are shown in green or orange colors (Cf. Figure 10) depending on the relative accuracy. When red color is used, please check your hardware setup and restart the motor profiling sequence.
6. Save your profiled motor
Click on the “Save…” button (Cf. Figure 10) to store the motor measurements for a later usage with the ST MC Workbench software tool.
The Figure 11 shows the saving window in that case, then you may provide the motor information:
- Naming of your profiled motor;
Provides with details about your profiled motor.
7. Play with your motor
Click on the “Play” button (Cf. Figure 10) to spin your just profiled motor.
The Figure 12 shows the spin control window. Preset the maximum acceleration and click on the “Start” button to activate your motor control. Then, select your “Speed [RPM]” with the cursor.
The Figure 13 presents how to stop properly playing with your motor.
8. End the ST Motor Profiler
Click on the “Disconnect” button (Cf. Figure 10) to stop properly the ST Motor Profiler software tool, then close the window using the upper right cross icon.
If you have forget to save your motor parameters, then select the “No” button (Cf. Figure 14), click on the “Connect” button (Cf. Figure 7) and save your motor parameters. However, clicking on the “Yes” button will lost your unsaved motor parameters and close the ST Motor Profiler software tool.