This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This category groups together all articles related to the Motor control
![]() |
Category under construction |
1. Proposition 1
Let's start with an overview of our STM32 Motor control ecosystem overview and of the X-CUBE-MCSDK, our main STM32 Software package:
The goal of this wiki site is to centralize as much information as possible, either through dedicated pages, or redirecting you to the most interesting ST information source on the web.
You can have a look on the STM32 MC SDK Getting Started:
There is a dedicated area for the most frequently asked questions:
and articles such as:
and as the articles describing the new features of the latest version of STM32 MC SDK:
- Single Shunt Phase Shift (new in V5.Y)
- Discontinuous PWM (new in V5.Y)
- AC Induction Motor (new in V5.Y)
- Overmodulation (new in V5.Y)
2. Proposition 2
Let's start with the STM32 Motor Control ecosystem.
2.1. Motor Control introduction
2.2. Learn more on STM32 Motor Control
Pages in category "Welcome to the STM32 Motor Control (STM32 MC) Knowledge Database"
The following 15 pages are in this category, out of 15 total.
6
S
- STM32MotorControl:SDK AC induction motor
- STM32MotorControl:SDK discontinuous PWM
- STM32MotorControl:SDK Overmodulation
- STM32MotorControl:Single Shunt Phase Shift
- STM32MotorControl:STM32 MC Motor Pilot - Start-up guide
- STM32MotorControl:STM32 MC Motor Profiler - Start-up guide
- STM32MotorControl:STM32 MC Suite