STM32WBA Bluetooth® LE Hardware Setup

Revision as of 17:19, 6 May 2024 by Registered User (→‎How to connect external debuggers)

Click here for Bluetooth® LE overview

1. STM32WBA Nucleo-64 board

NUCLEO-WBA55CG[1] is a Bluetooth® Low Energy wireless and ultra-low-power board embedding a powerful and ultra-low-power radio compliant with the Bluetooth® Low Energy SIG specification v5.3.

  • Called the Ultra-low-power wireless STM32WBA55CG[2] microcontroller based on the Arm® Cortex®‑M33 core, featuring 1 Mbyte of flash memory and 128 Kbytes of SRAM in a UFQFPN48 package

The NUCLEO-WBA55CG is composed of:

  • MCU RF board (MB1863):
    • 2.4 GHz RF transceiver supporting Bluetooth® specification v5.3
    • Arm® Cortex® M33 CPU with TrustZone®, MPU, DSP, and FPU
    • Integrated PCB antenna
  • Mezzanine Board (MB1801)
    • Three user LEDs
    • Three user and one reset push button
    • Board connectors:
      • ARDUINO® Uno V3 expansion connector
      • ST morpho headers for full access to all STM32 I/Os
      • Flexible power-supply options: ST-LINK USB VBUS or external sources
      • On-board STLINK-V3MODS debugger/programmer with USB re-enumeration capability: mass storage, virtual COM port, and debug port


NUCLEO-WBA55CG platform illustration
Nucleo-WBA5


2. Hardware platform configuration

2.1. Debug log via UART interface

The NUCLEO-WBA55CG [1] embeds the ST-LINK/V3 in-circuit debugger and programmer for STM32 microcontrollers.
STM32WBA microcontroller supports the STM32 virtual COM port driver for communication with a PC using a serial interface.

Use any convenient software terminal to open the serial communication port of the PC to check the messages from the board. Select the serial port and set up the connection as follows (example done with Tera Term software).

Set a new serial connection to the ST platform:

Tera Term setup (1/2)
Connectivity tera-term-1-2.png

Setup the serial connection as below:

Tera Term setup (2/2)
Connectivity tera-term-3-4.png

2.2. How to connect external debuggers

This paragraph explains how to connect an external debugger to the NUCLEO-WBA55CG[1] platform. This could be either an ST-LINK or a J-LINK debugger. To disconnect the embedded ST-LINK, set SW1 to position 3.
For a connection with ST-LINK:

  • On the miniboard, check if CN3 is fitted with an STDC14 connector. Add one if not.
  • Place 47 Ohm resistors (type 0402) for R2-R9 (i.e. 8 components).
  • Remove jumpers JP1 and JP2
  • Connect the ST-LINK output OUT to connector JP2.2
  • Connect ST-LINK GND to CN13.1
  • Connect a ribbon between ST-LINK DEBUG and CN3.
ST-link debugger connected to a NUCLEO-WBA55CG[1] board
Connectivity:Connectivity - Nucleo with STLINK.png

For a connection with J-LINK:

  • On the miniboard, check if CN3 is fitted with an STDC14 connector. Add one if not.
  • Place 47 Ohm resistors (type 0402) for R2-R9 (i.e. 8 components).
  • Plug the JLINK 10-pin patch adapter into the J-LINK
  • Connect a ribbon between this adapter and JP1 on the WBA5x miniboard
Correspondence of pins from CN3 footprint to STDC14 or MIPI10 connector
Connectivity:Connectivity - STDC14 and MIPI10 pin correspondance.png
J-Link debugger connected to NUCLEO-WBA55CG[1] board
Connectivity:Connectivity - Nucleo with J-LINK.png
The Segger patch adapter needs to be inserted between the J-Link and the NUCLEO-WBA55CG[1]
Connectivity:Connectivity - Segger patch adapter.png

3. Going further

4. References