This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. STM32WB - BLE P2P Server and Arduino
This is a description on how to create the proprietary application P2P Server thanks to the Arduino IDE.
Chapter 7.4 of the following application note describes the P2P Server application specification:
- AN5289-Building wireless applications with STM32WB Series microcontrollers[1]
1.1. Arduino configuration for P-NUCLEO-WB55
- Add the support of STM32 MCU in Arduino IDE[2]:
- Include STM32duinoBLE library:
- STM32duinoBLE[5]
- From the "Tools > Manage Libraries..." menu, select the STM32duinoBLE library:
- STM32duinoBLE[5]
STM32duinoBLE library |
---|
- Configuring IDE:
- Connect the Nucleo-64 WB55 board to the computer USB port.
- Launch the Arduino software.
- Select the Nucleo-64 WB55 board in two steps:
- From the "Tools > Board" menu, select the STM32 boards groups: Nucleo-64
- Then from the "Tools > Board part number" menu, select the P-NUCLEO WB55RG.
Arduino Nucleo-64 WB55 configuration |
---|
1.2. BLE stack configuration for P-NUCLEO-WB55
BLE stack configuration for P-NUCLEO-WB55:
- For release v1.12.0 and previous use full stack (stm32wb5x_BLE_Stack_full_fw.bin)
- For release v1.13.0 and next use HCI layer stack (stm32wb5x_BLE_HCILayer_fw.bin) and do the following modification in stm32BLEDuino library:
- In HCISharedMemTransport.cpp file comment the following lines:
HCISharedMemTransport.cpp modification |
---|
1.3. Sketch STM32WB_P2P_Server.ino
The following Arduino's Sketch demonstrates the P2P Server application including debug traces on the UART hyperterminal.
- Compile and upload STM32WB_P2P_Server.ino
/**
******************************************************************************
* @file STM32WB_P2P_Server.ino
* @author WBL BLE Application Team
* @brief Arduino STM32WB P2P Server Application (Custom STM)
******************************************************************************
* @attention
* This example creates a P2P server Application
* P2P service - 0000FE40-cc7a-482a-984a-7f2ed5b3e58f
* Led control Characteristic - 0000FE41-8e22-4541-9d4c-21edae82ed19 (Read|WritewithoutResponse)
* Byte 0 - Board Selection
* Byte 1 - LED Status (1 : ON; 0 : OFF)
* Button control Characteristic - 0000FE42-8e22-4541-9d4c-21edae82ed19 (Notify)
* Byte 0 - Board Selection
* Byte 1 - LED Status (1 : ON; 0 : OFF)
* To be supported by Smart Phone application ST BLE Sensor, the advertsing data shall contain the AD Element Manufacturer as following:
* Manufacturer_data:
* 0x01, // SKD version
* 0x83, // CFG_DEV_ID_P2P_SERVER1
* 0x00, // GROUP A Feature
* 0x00, // GROUP A Feature
* 0x00, // GROUP B Feature
* 0x00, // GROUP B Feature
* };
*
* The two characteristics are used :
* -- to control (Write) the LED1 of Nucleo64-WB55 board LED
* -- or to Notify the remote device by pushing SW1 f Nucleo68-WB55 board.
*
* The circuit:
* - Nucleo68-WB55
* You can use a generic BLE central app, like ST BLE sensor or ST BLE Toolbox, to interact with the services and characteristics.
* created in this sketch.
*
* This example code is in the public domain.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include <STM32duinoBLE.h>
/* Private typedef -----------------------------------------------------------*/
typedef struct __attribute__((packed)) {
byte boardSelection;
byte ledStatus;
} P2P_STM32WB_led_t;
P2P_STM32WB_led_t ledControl;
typedef struct __attribute__((packed)) {
byte boardSelection;
byte ButtonStatus;
} P2P_STM32WB_button_t;
P2P_STM32WB_button_t buttonInfo;
/* Private variables ---------------------------------------------------------*/
const int buttonPin = PC4; // set buttonPin to digital pin PC4
const int ledPin = LED_BUILTIN; // set ledPin to on-board LED
const int buttonPushed = 1;
const int boardWB_1 = 1;
int buttonPushCounter = 0; // counter for the number of button presses
int buttonState = 0; // current state of the button
int lastButtonState = 1; // previous state of the button
/* Private variables ---------------------------------------------------------*/
/* UUID for P2P Service-------------------------------------------------------*/
BLEService P2PService("0000FE40-cc7a-482a-984a-7f2ed5b3e58f");
/* create switch characteristic and allow remote device to read and write -----*/
BLECharacteristic ledCharacteristic("0000FE41-8e22-4541-9d4c-21edae82ed19", BLERead | BLEWriteWithoutResponse,sizeof(ledControl),true);
/* create button characteristic and allow remote device to get notifications --*/
BLECharacteristic buttonCharacteristic("0000FE42-8e22-4541-9d4c-21edae82ed19", BLENotify,sizeof(buttonInfo),true);
/* Manufacturer Advertising Data element structure ----------------------------*/
static const uint8_t manufacturer_data[6] = {
0x01, // BlueST Protocol - SDK Version
0x83, // Device ID - STM32WB P2P Server
0x00, // GROUP A Feature
0x00, // GROUP A Feature
0x00, // GROUP B Feature
0x00, // GROUP B Feature
};
HCISharedMemTransportClass HCISharedMemTransport;
BLELocalDevice BLEObj(&HCISharedMemTransport);
BLELocalDevice& BLE = BLEObj;
/**
* @brief Connection Event Handler
* @param BLE Central Device
* @retval None
*/
void blePeripheralConnectHandler(BLEDevice central) {
// central connected event handler
Serial.print("==> Connection established with central: ");
Serial.print(central.address());
if (BLE.connected()) {
Serial.print(" -- RSSI = ");
Serial.println(BLE.rssi());
}
}
/**
* @brief Disconnection Event Handler
* @param BLE Central Device
* @retval None
*/
void blePeripheralDisconnectHandler(BLEDevice central) {
// central disconnected event handler
Serial.print("==> Disconnection event with central: ");
Serial.println(central.address());
}
/**
* @brief Event Handler when Characteristic Written
* @param BLE Central Device
* @param Characteritic
* @retval None
*/
void LedCharacteristicWritten(BLEDevice central, BLECharacteristic characteristic) {
byte data[sizeof(ledControl)];
// central wrote new value to characteristic, update LED
if (ledCharacteristic.written()) {
Serial.println("==>Led Characteritics written:");
Serial.print("Data Received: ");
ledCharacteristic.readValue(data, sizeof(ledControl));
Serial.print(ledCharacteristic.valueLength());
Serial.print(" ");
Serial.print("bytes -- ");
for (int i = 0; i < sizeof(ledControl); i++) {
Serial.print("0x");
Serial.print(data[i], HEX);
Serial.print(" ");
}
Serial.println();
ledControl.boardSelection=data[0];
ledControl.ledStatus=data[1];
Serial.print("Board Selected:");
Serial.println(ledControl.boardSelection);
Serial.print("Value:");
Serial.println(ledControl.ledStatus);
if(ledControl.ledStatus){
Serial.println("==>LED1 ON");
digitalWrite(ledPin, HIGH);
}
if(!ledControl.ledStatus){
Serial.println("==>LED1 OFF");
digitalWrite(ledPin, LOW);
}
}
}
/**
* @brief Arduino main Setup
* @param None
* @retval None
*/
void setup() {
Serial.begin(115200);
while (!Serial);
pinMode(ledPin, OUTPUT); // use the LED as an output
pinMode(buttonPin, INPUT_PULLUP); // use button pin as an input
//Project P2P server
Serial.println("======================================");
Serial.println("== STM32WB - P2P Server Application ==");
Serial.println("======================================");
// begin initialization
if (!BLE.begin()) {
Serial.println("==>starting BLE failed!");
while (1);
}
//Set the device name in the built in device name characteristic.
BLE.setDeviceName("STM32WB-Arduino");
//set the local name peripheral advertises
Serial.println("==> Advertising Name - P2P_Server");
BLE.setLocalName("P2P_Server");
//Set the manufacturer data value used when advertising.
BLE.setManufacturerData(manufacturer_data, sizeof(manufacturer_data));
//Set the advertising interval in units of 0.625 ms.
//Defaults to 100ms (160 * 0.625 ms) if not provided.
BLE.setAdvertisingInterval(160); // 160 * 0.625 ms
// set the UUID for the service this peripheral advertises:
//BLE.setAdvertisedService(P2PService);
// add the characteristics to the service
P2PService.addCharacteristic(ledCharacteristic);
P2PService.addCharacteristic(buttonCharacteristic);
// assign event handlers for characteristic
ledCharacteristic.setEventHandler(BLEWritten, LedCharacteristicWritten);
// add the service
BLE.addService(P2PService);
//configure data to Notify when SW1 pushed
buttonInfo.boardSelection = boardWB_1;
buttonInfo.ButtonStatus=buttonPushed;
// start advertising
BLE.advertise();
String address = BLE.address();
Serial.print("==>Local address is: ");
Serial.println(address);
Serial.println("==>Advertising Started, waiting for connections...");
// assign event handlers for connected, disconnected to peripheral
BLE.setEventHandler(BLEConnected, blePeripheralConnectHandler);
BLE.setEventHandler(BLEDisconnected, blePeripheralDisconnectHandler);
}
/**
* @brief Arduino Loop
* @param None
* @retval None
*/
void loop() {
// poll for BLE events
BLE.poll();
// read the SW1 Button input pin:
buttonState = digitalRead(buttonPin);
// compare the buttonState to its previous state
if (buttonState != lastButtonState) {
// if the state has changed, increment the counter
if (buttonState == LOW) {
// if the current state is HIGH then the button went from off to on:
buttonPushCounter++;
//Serial.println("on");
Serial.print("==> Number of time button is pushes: ");
Serial.println(buttonPushCounter);
//check if connection is established by Central device
if(BLE.central()){
//check if Notification is enabled
if (buttonCharacteristic.subscribed()) {
Serial.println("buttonCharacteristic is subscribed:");
Serial.println("==>Notification of Button Pushed is sent");
buttonCharacteristic.writeValue((byte*) &buttonInfo, sizeof(buttonInfo));
} else {
Serial.println("buttonCharacteristic is NOT subscribed:");
Serial.println("==>Notification is NOT sent");
}
}
} else {
// if the current state is LOW then the button went from on to off:
//Serial.println("off");
}
// Delay a little bit to avoid bouncing
delay(50);
}
// save the current state as the last state, for next time through the loop
lastButtonState = buttonState;
}
/************************************ STMicroelectronics *****END OF FILE****/
1.4. Debug traces
At startup, the HyperTerminal displays the following traces
Startup Debug Trace |
---|
2. Smart Phone application - ST BLE Sensor
- Download ST BLE Sensor or ST BLE ToolBox application on the smartphone.
- Scan and connect to P2P_Server
- Toggle SmartPhone LED or push SW1 button of the Nucleo-64 WB55 board.
ST BLE Sensor Scan | ST BLE Sensor Connect |
---|---|
- Debug trace displays all the sequences at the application level
Arduino Nucleo-64 WB55 traces |
---|
3. References