In this tutorial, we will use AI and a Time Of Flight to create a Rock Paper Scissors game.
The goal is to demonstrate how to use NanoEdge AI Studio and Arduino IDE to be able to create any project you can think of using AI.
NanoEdge AI Studio is a tool developed by STMicroelectronics especially designed for embedded profiles to help them acquire an AI library to embed in their project, only using their data.
Through a simple and step by step process, we will collect data related to your use case, use the tool to get the best model with little effort.
NanoEdge AI Studio libraries are compatible with any Cortex M and since version 4.4, the tool is able to compile library ready to import directly in Arduino IDE.
1. Goals
- Create a Rock Paper Scissors game using TOF data and AI from scratch.
- Learn how to use NanoEdge AI Studio to easily integrate AI in any future projects through this example.
2. Hardware & Software Needed
Hardware:
- An Arduino GIGA R1 board
- An Arduino GiGA display shield
- A ST time of flight X-nucleo-53L5A1
- A Micro USB cable to connect the Arduino board to your desktop machine
Software:
- To program your board, you can use the Arduino Web Editor or install the Arduino IDE. We’ll give you more details on how to set these up in the following sections.
- To create and get the AI model for the Rock Paper Scissors sign recognition, you need NanoEdge AI Studio v4.4 or above.
Note: For windows user, we recommend using Arduino IDE v1.8.19. Do not use the Microsoft store version.
2.1. Hardware setup:
Just a word concerning the setup montage. You need to plug the display screen on top of the GIGA R1 board and the TOF expansion board under the board like this:
Important:
We need to modify the I2C communication pins between the TOF and the Arduino board to avoid conflict with the display screen: Plug a jumper wire from the SDA1 pin to the 20SDA pin Plug another wire from the SCL1 pin to the 21SCL pin
3. NanoEdge AI Studio
For any part linked with NanoEdge AI Studio, you can take a look at the documentation for more information: https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Studio
3.1. Install:
First, we need to install NanoEdge AI Studio.
Download link: https://stm32ai.st.com/download-nanoedgeai/
then:
- After filling the form, an email with the license to use the studio is sent.
- Wait for the end of the download and launch the .exe to start the install.
- Once installed, enter the license and that it!
In case of troubles, here are useful links:
- https://wiki.st.com/stm32mcu/wiki/AI:NanoEdge_AI_Studio#Running_NanoEdge_AI_Studio_for_the_first_time
- https://community.st.com/t5/stm32-mcus/nanoedge-ai-studio-install-activation-troubleshooting/ta-p/624832
3.2. Create a project:
In Nanoedge AI Studio, four kinds of project are available, each one serving a different purpose:
- Anomaly detection (AD): to detect a nominal behavior and an abnormal one. Can be retrained directly on board
- 1 class classification (1c): Create a model to detect also a nominal behavior and an abnormal one but with only nominal data. (in case you cannot collect abnormal example)
- N class classification (Nc): Create a model to classify data in multiple classes that you define
- Extrapolation (Ex): Regression in short. To predict a value instead of a class from the input data (a speed or temperature for example)
In our case, we want to create an AI able to recognize three signs (scissor, paper and rock) so we click on N class classification >Create new project
In the project settings:
- Enter a project name
- Define a RAM and FLASH limit if you need
- Click SELECT TARGET, then go to the ARDUINO BOARD tab and select the GIGA R1 WiFi
- In sensor type, put GENERIC and 1 as the number of axis
Then click SAVE AND NEXT
Note: we are working with the TOF matrix of 64 values (8x8), but each measure are taking independently. That the reason why we use 1 axis.
3.3. Data collection:
In the Signal part of NanoEdge AI Studio, we need to import 4 datasets:
- Nothing: When we are not playing
- Paper
- Scissor
- Rock
The TOF can collect data in a matrix of size 8x8, so every signals in our dataset if of size 64. We then need to collect data to create 4 datasets containing various example of one sign each.
Arduino code for data collection:
To collect data, create a new project in Arduino IDE and copy the following code:
#include <Wire.h>
#include <SparkFun_VL53L5CX_Library.h> //http://librarymanager/All#SparkFun_VL53L5CX
SparkFun_VL53L5CX myImager;
VL53L5CX_ResultsData measurementData; // Result data class structure, 1356 bytes of RAM
int imageResolution = 0; //Used to pretty print output
float neai_buffer[64];
void setup() {
Serial.begin(115200);
delay(100);
Wire.begin(); //This resets to 100kHz I2C
Wire.setClock(400000); //Sensor has max I2C freq of 400kHz
if (myImager.begin() == false)
{
Serial.println(F("Sensor not found - check your wiring. Freezing"));
while (1);
}
myImager.setResolution(8*8); //Enable all 64 pads
myImager.setRangingFrequency(15); //Ranging frequency = 15Hz
imageResolution = myImager.getResolution(); //Query sensor for current resolution - either 4x4 or 8x8
myImager.startRanging();
}
void loop() {
if (myImager.isDataReady() == true)
{
if (myImager.getRangingData(&measurementData)) //Read distance data into array
{
for(int i = 0 ; i < imageResolution ; i++) {
neai_buffer[i] = (float)measurementData.distance_mm[i];
}
for(int i = 0 ; i < imageResolution ; i++) {
Serial.print(measurementData.distance_mm[i]);
Serial.print(" ");
}
Serial.println();
}
}
}
We need to add 2 libraries in the project:
- Wire.h for I2C communication: click on Sketch > Include Library > Wire
- SparkFun_VL53L5CX_Library: to use the TOF: Sketch > Include Library > Manage Library > SparkFun_VL53L5CX_Library and click install
Once ready, click on the verify sign to compile the code and then to the right arrow to flash the code on the board. Make sure that the board is connected to the pc beforehand.
Make sure that the right COM port is selected. Click on Tools > Port to select it. If the board is plugged, you should see its name displayed.
Back in NanoEdge:
In the step SIGNALS:
- Click on ADD SIGNAL
- Click on FROM SERIAL
- Make sure to select the right COM port
- Leave the Baudrate as it is
- Click on maximum number of lines and enter 500
- Click START/STOP to log data
- Once finished click CONTINUE and then IMPORT
VERY IMPORTANT:
Do not log data as if playing Rock Paper Scissors multiple times, log a sign continuously at different positions below the captor (up, down, left, right etc). For example, do the scissor sign and move below the captor while collecting the 500 signal without ever leaving the captor sight.
We really need to only have data corresponding to the class only. If you simulate playing to log data, you will have data corresponding to no signs (because you are not in the captor sight) and then data corresponding to the class.
Make also sure not to be to close to the TOF as it will not be able to see anything but a big object covering the whole matrix.
3.4. Finding the best model
Go to the BENCHMARK step.
In this step, NanoEdge AI Studio will look for the best pretraitment of your data, model and parameters for this model in order to find the best combination for your usecase.
Once done, you will be able at the end of the project to compile the combination found as an AI Library to import in Arduino IDE.
- Click NEW BECHMARK
- Select the four classes collected previously
- Click START
The studio display few metrics:
- Balanced accuracy which is the weighted mean of good classification per classes
- RAM and FLASH needs
- Score: this metrics takes in account the performance and size of the model found
The time required for the benchmark is heavily correlated to the size of buffer used and their quantity. The benchmark will improve fast at the beginning at tends to slow down to find the most optimized library at the end. So you can stop the benchmark when you are satisfied of the results (above 95% is a good reference).
Validate the model found:
The validation and emulator steps are made to make sure that the library found is indeed the best. To achieve that, it is recommended to test the few best libraries with new data and make sure that the one selected is the best.
Note: To collect new dataset for the validation, you can go back to the step signal, import new dataset via serial and download them to use them in validation:
- Go to the Validation step
- Select 1 to 10 libraries
- Click NEW EXPERIMENT
- Import new dataset for the 4 classes
- click START
You also have the emulator to push tests further if needed on one library and also to test it live using serial for a quick demo for example:
3.5. Getting the Arduino library
To obtain the AI library containing the model and the function to add it in you Arduino code:
- Go to Compilation
- Important: leave the Float abi uncheck for the GIGA R1 WIFI.
- Click COMPILE LIBRARY
The output is a .zip file that we will directly import in Arduino IDE later.
4. Arduino IDE
4.1. Library setup
After getting the zip containing the AI library from NanoEdge AI Studio, Create a new project by clicking File > New.
To make this project, we need few libraries to make it work.
Click on Sketch > Include Library > Wire to include the Wire.h library for I2C communication (it is installed by default)
To add a standard libraries click on Sketch > Include Library > Manage Library and install the following libraries:
- ArduinoGraphics: for display on the screen.
- SparkFun_VL53L5CX_Library: to use the TOF.
To add the NanoEdge AI Studio library:
- Extract the .zip provided by NanoEdge AI Studio After compilation.
- In Arduino IDE click on Sketch > Include Library > Add .ZIP Library…
- Find the previously extrated content and import the .zip file in the Arduino folder.
We also need to add incbin.h:
- You can find incbin.h here: https://github.com/graphitemaster/incbin/blob/main/incbin.h
- Copy and paste it inside the folder containing the .ino file of the project.
Lastly, we need to select the GIGA R1 WIFI as our board:
- Click Tools > Board: “your actual board” > Boards Manager…
- Search and Install Arduino Mbed OS Giga Boards
- Then go back to Tools > Board: “your actual board” > Arduino Mbed OS Giga Boards >Arduino Giga R1
Note: Arduino_H7_Video.h is automatically added when selecting the board, you don't need to add it manually.
4.2. Code:
The following code takes care of 3 main parts:
- Collect data from the TOF
- Use the NanoEdge AI Library every time we collect data from the TOF to detect what sign is being played
- Load and display images corresponding to the sign detect by NanoEdge AI Studio
here is the code:
#include "Arduino_H7_Video.h"
#include "ArduinoGraphics.h"
#include "incbin.h"
#include <Wire.h>
#include <SparkFun_VL53L5CX_Library.h> //http://librarymanager/All#SparkFun_VL53L5CX
#include "NanoEdgeAI.h"
#include "knowledge.h"
// Online image converter: https://lvgl.io/tools/imageconverter (Output format: Binary RGB565)
//#define DATALOG
#define SCREEN_WIDTH 800
#define SCREEN_HEIGHT 480
#define SIGN_WIDTH 150
#define SIGN_HEIGHT 200
#define LEFT_SIGN_X 115
#define RIGHT_SIGN_X 530
#define SIGN_Y 200
#define INCBIN_PREFIX
INCBIN(backgnd, "YOUR_PATH/backgnd.bin");
INCBIN(rock, "YOUR_PATH/rock.bin");
INCBIN(paper, "YOUR_PATH/paper.bin");
INCBIN(scissors, "YOUR_PATH/scissors.bin");
void signs_wheel(void);
void signs_result(uint16_t neaiclass);
uint16_t mostFrequent(uint16_t arr[], int n);
Arduino_H7_Video Display(SCREEN_WIDTH, SCREEN_HEIGHT, GigaDisplayShield);
Image img_backgnd(ENCODING_RGB16, (uint8_t *) backgndData, SCREEN_WIDTH, SCREEN_HEIGHT);
Image img_rock(ENCODING_RGB16, (uint8_t *) rockData, SIGN_WIDTH, SIGN_HEIGHT);
Image img_paper(ENCODING_RGB16, (uint8_t *) paperData, SIGN_WIDTH, SIGN_HEIGHT);
Image img_scissors(ENCODING_RGB16, (uint8_t *) scissorsData, SIGN_WIDTH, SIGN_HEIGHT);
Image img_classes[CLASS_NUMBER - 1] = {img_paper, img_rock, img_scissors};
SparkFun_VL53L5CX myImager;
VL53L5CX_ResultsData measurementData; // Result data class structure, 1356 bytes of RAM
int imageResolution = 0; //Used to pretty print output
int imageWidth = 0; //Used to pretty print output
float neai_buffer[DATA_INPUT_USER];
float output_buffer[CLASS_NUMBER]; // Buffer of class probabilities
uint16_t neai_class = 0;
uint16_t previous_neai_class = 0;
int class_index = 0;
uint16_t neai_class_array[10] = {0};
void setup() {
randomSeed(analogRead(0));
Display.begin();
neai_classification_init(knowledge);
Serial.begin(115200);
delay(100);
Wire.begin(); //This resets to 100kHz I2C
Wire.setClock(400000); //Sensor has max I2C freq of 400kHz
if (myImager.begin() == false)
{
Serial.println(F("Sensor not found - check your wiring. Freezing"));
while (1);
}
myImager.setResolution(8*8); //Enable all 64 pads
myImager.setRangingFrequency(15); //Ranging frequency = 15Hz
imageResolution = myImager.getResolution(); //Query sensor for current resolution - either 4x4 or 8x8
imageWidth = sqrt(imageResolution); //Calculate printing width
myImager.startRanging();
Display.beginDraw();
Display.image(img_backgnd, (Display.width() - img_backgnd.width())/2, (Display.height() - img_backgnd.height())/2);
Display.endDraw();
delay(500);
}
void loop() {
if (myImager.isDataReady() == true)
{
if (myImager.getRangingData(&measurementData)) //Read distance data into array
{
for(int i = 0 ; i < DATA_INPUT_USER ; i++) {
neai_buffer[i] = (float)measurementData.distance_mm[i];
}
#ifdef DATALOG
for(int i = 0 ; i < DATA_INPUT_USER ; i++) {
Serial.print(measurementData.distance_mm[i]);
Serial.print(" ");
}
Serial.println();
#else
neai_classification(neai_buffer, output_buffer, &neai_class);
if(class_index < 10) {
neai_class_array[class_index] = neai_class;
Serial.print(F("class_index "));
Serial.print(class_index);
Serial.print(F(" = class"));
Serial.println(neai_class);
class_index++;
} else {
neai_class = mostFrequent(neai_class_array, 10);
Serial.print(F("Most frequent class = "));
Serial.println(neai_class);
class_index = 0;
if (neai_class == 4 && previous_neai_class != 4) // EMPTY
{
previous_neai_class = neai_class;
Display.beginDraw();
Display.image(img_backgnd, (Display.width() - img_backgnd.width())/2, (Display.height() - img_backgnd.height())/2);
Display.endDraw();
Serial.println(F("Empty class detected!"));
}
else if (neai_class == 1 && previous_neai_class != 1) // PAPER
{
previous_neai_class = neai_class;
Serial.println(F("Paper class detected!"));
signs_wheel();
signs_result(neai_class);
}
else if (neai_class == 3 && previous_neai_class != 3) // SCISSORS
{
previous_neai_class = neai_class;
Serial.println(F("SCISSORS class detected!"));
signs_wheel();
signs_result(neai_class);
}
else if (neai_class == 2 && previous_neai_class != 2) // ROCK
{
previous_neai_class = neai_class;
Serial.println(F("Rock class detected!"));
signs_wheel();
signs_result(neai_class);
}
}
#endif
}
}
}
void signs_wheel(void)
{
for(int i = 0 ; i < 10 ; i++) {
Display.beginDraw();
Display.image(img_backgnd, (Display.width() - img_backgnd.width())/2, (Display.height() - img_backgnd.height())/2);
Display.image(img_SCISSORS, LEFT_SIGN_X, SIGN_Y);
if(i % (CLASS_NUMBER - 1) == 0) {
Display.image(img_rock, RIGHT_SIGN_X, SIGN_Y);
} else if(i % (CLASS_NUMBER - 1) == 1) {
Display.image(img_paper, RIGHT_SIGN_X, SIGN_Y);
} else {
Display.image(img_SCISSORS, RIGHT_SIGN_X, SIGN_Y);
}
Display.endDraw();
}
}
void signs_result(uint16_t neaiclass)
{
Display.beginDraw();
Display.image(img_backgnd, (Display.width() - img_backgnd.width())/2, (Display.height() - img_backgnd.height())/2);
int random_img = random(0, CLASS_NUMBER - 1);
if(random_img == neaiclass - 1) {
Display.fill(255, 127, 127);
Display.rect(LEFT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
Display.rect(RIGHT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
} else if(random_img == (neaiclass == 1) ? 2 : (neaiclass == 2) ? 0 : 1) {
Display.fill(255, 0, 0);
Display.rect(LEFT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
Display.fill(0, 255, 0);
Display.rect(RIGHT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
} else {
Display.fill(0, 255, 0);
Display.rect(LEFT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
Display.fill(255, 0, 0);
Display.rect(RIGHT_SIGN_X - 10, SIGN_Y - 10, SIGN_WIDTH + 20, SIGN_HEIGHT + 20);
}
Display.image(img_classes[neaiclass - 1], LEFT_SIGN_X, SIGN_Y);
Display.image(img_classes[random_img], RIGHT_SIGN_X, SIGN_Y);
Display.endDraw();
delay(1000);
}
uint16_t mostFrequent(uint16_t arr[], int n)
{
int count = 1, tempCount;
uint16_t temp = 0,i = 0,j = 0;
//Get first element
uint16_t popular = arr[0];
for (i = 0; i < (n- 1); i++)
{
temp = arr[i];
tempCount = 0;
for (j = 1; j < n; j++)
{
if (temp == arr[j])
tempCount++;
}
if (tempCount > count)
{
popular = temp;
count = tempCount;
}
}
return popular;
}
Before being able to flash the code, we need to do a few things.
4.3. Screen display:
We display on the screen a background and the signs to play SHIFUMI (scissor, paper and rock). You can download these images:
We also need to convert them to bin files using this website:
- Online image converter - BMP, JPG or PNG to C array or binary | LVGL
- Select the images
- Change the output format to Binary RGB565
- Click convert
Get all the binary images and copy them in the project folder. You can create a folder named images for example and put them in it.
In the code, update the image path. You may need to add the full path of the images
NanoEdge:
Conserning the use of NanoEdge AI Library, it is really simple: We use the function neai_classification_init(knowledge) in the setup() to load the model with the knowledge acquired during the benchmark We use the function neai_classification(neai_buffer, output_buffer, &neai_class) to make the detection. This function takes as input 3 variable that we created as well:
- float neai_buffer[64]: the input data for the detection, which are the TOF data
- float output_buffer[CLASS_NUMBER]: An output array of size 4 containing the probability for the input signal to be part of each class
- uint16_t neai_class = 0: the variable we use to get the class detected. It correspond to the class with the highest probability.
That’s it!
5. Demo Setup:
If you want to reproduce this demo setup, here are the resources used:
3 support plates:
- Support.svg
- 4x Brackets 20.stl: https://www.printables.com/model/113989-corner-bracket-optimized-for-3d-printing/files
- M3 nylon 12mm screws and M3 nylon nuts