1. SFI
1.1. Features
The secure firmware install (SFI) solution provides security when programming devices in a non-trusted facility owned by a contract manufacturer (CM).
SFI addresses the two main issues at a non-trusted facility:
- OEM application confidentiality against CM during STM32 programming.
- Avoid CM overproduction of OEM devices.
1.2. Principles
There are two steps:
- The application creation flow
- The application installation flow
The next two sections detail the flows.
1.2.1. The application creation flow
The OEM uses the STM32 Trusted Package Creator software to:
- Create and manage his secret encryption key (the firmware key as indicated in the figure below).
- Encrypt its application and option bytes configuration with the firmware key. It is the SFI OEM application image (the encrypted file in the figure below).
- Program the firmware key within an HSM before locking it. Before that step, the firmware key cannot be read or extracted clearly from the HSM. Only STM32 can handle the firmware key from the HSM.
1.2.2. The application installation flow
The CM uses the STM32CubeProgrammer (or any other SFI-recommended partner programming tools) to securely program STM32 MCUs in untrusted environments.
- The STM32 securely extracts the firmware key from the HSM. HSM verifies the firmware key extraction request number.
- The STM32 securely decrypts and programs the OEM application within the internal flash memory.
- The OEM application is never disclosed outside the STM32. The SFI process guarantees the OEM application confidentiality against the CM.
2. SFI for STM32H5 with the secure manager
This procedure must be followed if the OEM installs an application developed using the secure manager. In this case, there are several additional components (OEM secrets, secure manager, and modules) to prepare, to test, and to install.
Here is the list of applicable products:
Type | Products |
---|---|
Microcontroller | STM32H573xx |
The preparation and installation flow is described below:
SFI HSM license and SFI Global License can be used.
Refer to the following page for an example on getting started with SFI on STM32H573xx microcontrollers with the secure manager:
How to start SFI on STM32H5 with the secure manager.
3. SFI for STM32H5 without the secure manager
This procedure must be followed when the OEM installs an application developed without the use of the secure manager.
Here is the list of applicable products:
Type | Products |
---|---|
Microcontroller | STM32H573xx, STM32H563xx, STM32H533xx, STM32H523xx |
The preparation and installation flow is described below:
Only the SFI HSM license can be used (the SFI global license cannot be used).
In this case, the SFI procedure on the STM32H5 series is similar to the SFI procedure applied on other platforms.
Follow SFI step-by-step on STM32 boards to run the SFI procedure on the STM32H5 without the secure manager.