1. Introduction
This article gives an overview about Debug Authentication applied to STM32H7RS MCUs.
A detailed description of Debug Authentication is provided in AN6008
If you want to learn more about Debug Authentication specific usage for each STM32H7RS device and you want to practice, refer to Debug Authentication STM32H7RS How to Introduction
List of applicable products:
Type | Products |
---|---|
Microcontroller | STM32H7Rxx, STM32H7Sxx |
2. Debut Authentication Services
The debug authentication allows to securely:
- Re-open the debug access
- Perform full regression to product states OPEN
- Force download
The debug authentication services are usable:
- During development
- For field return analysis
Here is an overview of the debug authentication setup :
Two Authentication methods are available :
- use a password. Only a full regression to the OPEN state is possible.
- use a certificate chain. Regression and debug opening are possible.
When using certificates, the authorized actions are defined through masks.
Refer to AN6008 for more details about Debug Authentication certificates, actions and masks usage.
The Debug Authentication protocol uses the JTAG dedicated access point (ap0) to communicate with the chip.
The protocol is defined by Arm®: ARM PSA ADAC V1.0. (Authenticated Debug Access Control PSA ADAC V1.0. (Authenticated Debug Access Control)
Refer to AN6008 for more details on the Debug Authentication protocol.
3. Debug Authentication provisioning
The debug authentication provisioning consists in storing the password hash or hash of the key related to the root certificate inside the chip.
These data are stored in OBKey on STM32H7RS series devices.
Refer to AN6008 for more details on the Debug Authentication provisioning.