STM32CubeWBA: Trace management

Revision as of 17:00, 19 February 2024 by Registered User (→‎Introduction)


Under construction.png Coming soon
Info white.png Information
This page is not yet finished but will be soon.


1. Introduction

The log module is a module that provides a logging mechanism for embedded systems. It allows developers to print logs with different verbose levels and regions, making it easier to debug and troubleshoot issues in the system.

The module is highly customizable and can be configured to meet the specific user needs.

2. Concepts

The Advanced Trace is split into two layers:

Advanced Trace services
API that regroups all the services available for traces.
Trace Interface
Interface between the HW and the Advance Trace services layer.

2.1. Advanced Trace services

The advanced trace proposes some interesting features to users for Trace debugging or logging:

Trace FIFO management
The advanced trace module manages a circular FIFO - Size is customizable - to store all the application data before their push on the media. The module guarantees the data integrity and parallel access to the trace services.
  • Unchunk mode:
The “unchunk” mode is an optional mode which could be enabled inside the utilities’ configuration header. The goal of this mode is to guarantee that a frame is not split inside two transfers.
  • Timestamp management:
The timestamp management allows the user to add a timestamp buffer ahead of the frame to output.
However, user shall follow two steps:
  • User shall create a callback function that returns a time stamp buffer and its buffer size.
  • Use the adequate functions that allow timestamp management.
This mode can be activated within the utilities’ configuration header.
  • Verbose level and region management:
The Verbose Level and the Region are two different levels to determine whether a frame can be sent or not. If one of these two condition fails, the frame is discarded.
The Verbose Level
The user can define his own current verbose level. The default setup is 0 meaning only value frame with verbose level equal to zero are sent through the Advanced Trace. If the application verbose level is lower or equal to the current verbose level, the frame is sent else discarded.
The Region
The user can define his own region mask. The default setup is 0 meaning only application frame with region equal to zero are sent through the Advanced Trace. If the application region value is equal to zero or if value is aligned with the mask region, the frame is sent else discarded.
  • Overrun management:
This feature aims to indicate when frame has been discarded due to a FIFO full. The switch enabled is not enough to make it functional, the user shall provide a callback function which returns an overrun frame and the size of this frame.
This feature can be activated within the utilities’ configuration header.

2.2. Trace interface

The trace interface handles the HW interface. The only requirements for the HW are to provide characteristics such as:

  • Shall be able to send data (8-bit data).
  • Shall be able to receive data.

This hardware layer has been built to match with the UART but there is others’ HW IPs compatibles with these requirements: USB, I2C, SPI, etc. The choice shall be managed by the application designer according to the available resources and the application requirements.

3. Interface

3.1. Functions

Log_Module_Init
Description
Initializes the log module with the given configuration.
Syntax
void Log_Module_Init(Log_Module_t log_configuration);
Parameters
[in] log_configuration
Type: Log_Module_t
Description: The configuration of the log module.
Return Value
None
Log_Module_DeInit
Description
Deinitializes the log module.
Syntax
void Log_Module_DeInit(void);
Parameters
None
Return Value
None
Log_Module_Set_Verbose_Level
Description
Sets the verbose level of the log.
Syntax
void Log_Module_Set_Verbose_Level(Log_Verbose_Level_t new_verbose_level);
Parameters
[in] new_verbose_level
Type: Log_Verbose_Level_t
Description: The new verbose level to be set.
Return Value
None
Log_Module_Set_Region
Description
Replaces the current region mask to use and sets only the given region.
Syntax
void Log_Module_Set_Region(Log_Region_t new_region);
Parameters
[in] new_region
Type: Log_Region_t
Description: The new region to use.
Return Value
None
Log_Module_Add_Region
Description
Adds the given region to the current region mask.
Syntax
void Log_Module_Add_Region(Log_Region_t new_region);
Parameters
[in] new_region
Type: Log_Region_t
Description: The new region to use, alongside the others.
Return Value
None
Log_Module_Enable_All_Regions
Description
Enables all the regions.
Syntax
void Log_Module_Enable_All_Regions(void);
Parameters
None
Return Value
None
Log_Module_Set_Color
Description
Sets/Replaces the color for a region.
Syntax
void Log_Module_Set_Color(Log_Region_t eRegion, Log_Color_t eNewColor);
Parameters
[in] eRegion
Type: Log_Region_t
Description: The region where to apply the color.
[in] eNewColor
Type: Log_Color_t
Description: The color to apply to the selected region.
Return Value
None
Log_Module_RegisterTimeStampFunction
Description
Registers a callback function to insert the 'TimeStamp' to the log.
Syntax
void Log_Module_RegisterTimeStampFunction(CallBack_TimeStamp * pCallbackFunc);
Parameters
[in] pCallbackFunc
Type: CallBack_TimeStamp *
Description: Callback function to insert Time Stamp.
Return Value
None
Log_Module_Print
Description
Prints a log with the given verbose level and region.
Syntax
void Log_Module_Print(Log_Verbose_Level_t eVerboseLevel, Log_Region_t eRegion, const char * pText, ...);
Parameters
[in] eVerboseLevel
Type: Log_Verbose_Level_t
Description: The level of verbose for this log.
[in] eRegion
Type: Log_Region_t
Description: The region where the log is issued.
[in] pText
Type: const char *
Description: Pointer to the text to be printed.
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
Log_Module_PrintWithArg
Description
Prints a log with already an arg list.
Syntax
void Log_Module_PrintWithArg(Log_Verbose_Level_t eVerboseLevel, Log_Region_t eRegion, const char * pText, va_list args);
Parameters
[in] eVerboseLevel
Type: Log_Verbose_Level_t
Description: The level of verbose for this log.
[in] eRegion
Type: Log_Region_t
Description: The region where the log is issued.
[in] pText
Type: const char *
Description: Pointer to the text to be printed.
[in] args
Type: va_list
Description: Arguments list.
Return Value
None

3.2. Macros

LOG_INFO_BLE
Description
Macro to print an info log for the BLE region.
Syntax
LOG_INFO_BLE(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_ERROR_BLE
Description
Macro to print an error log for the BLE region.
Syntax
LOG_ERROR_BLE(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_WARNING_BLE
Description
Macro to print a warning log for the BLE region.
Syntax
LOG_WARNING_BLE(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_DEBUG_BLE
Description
Macro to print a debug log for the BLE region.
Syntax
LOG_DEBUG_BLE(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_INFO_SYSTEM
Description
Macro to print an info log for the System region.
Syntax
LOG_INFO_SYSTEM(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_ERROR_SYSTEM
Description
Macro to print an error log for the System region.
Syntax
LOG_ERROR_SYSTEM(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_WARNING_SYSTEM
Description
Macro to print a warning log for the System region.
Syntax
LOG_WARNING_SYSTEM(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_DEBUG_SYSTEM
Description
Macro to print a debug log for the System region.
Syntax
LOG_DEBUG_SYSTEM(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_INFO_APP
Description
Macro to print an info log for the App region.
Syntax
LOG_INFO_APP(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_ERROR_APP
Description
Macro to print an error log for the App region.
Syntax
LOG_ERROR_APP(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_WARNING_APP
Description
Macro to print a warning log for the App region.
Syntax
LOG_WARNING_APP(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None
LOG_DEBUG_APP
Description
Macro to print a debug log for the App region.
Syntax
LOG_DEBUG_APP(...);
Parameters
[in] ...
Type: ...
Description: Any other parameters to be printed with the text.
Return Value
None

4. How to

TBD.