Coming soon |
1. Telephony & Media Audio Profile
1.1. Introduction
The Telephony and Media Audio Profile is a BLE Audio profile specified by the Bluetooth SIG. It's categorized as a "use-case profile", meaning that it's a high-layer profile designed for a specific use case. The complete specification can be found on the Bluetooth SIG website[1].
The TMAP addresses the use-cases of Telephony and Media over BLE Audio. This covers Broadcast audio, where audio data is “broadcasted” from a Broadcast Source to an unlimited number of Broadcast Sinks, using Broadcast Isochronous Streams. It also covers the Unicast audio, where audio is streamed between two connected devices, allowing bidirectional streams and more efficient acknowledgement. For more details about Unicast and Broadcast features, see the wiki page "Introduction to Bluetooth LE Audio"[2].
1.2. Roles
The TMAP introduces 6 different roles:
- Call Gateway: Based on the BAP Unicast Client, it concerns devices connected to networks used for telephony or VoIP applications. Example of devices implementing this role are smartphones, laptops, tablets, and PCs.
- Call Terminal: Based on the BAP Unicast Server, it concerns devices rendering audio for telephony and VoIP applications. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
- Unicast Media Sender: Based on the BAP Unicast Client, it concerns devices able to send media audio content using Unicast. Example of devices implementing this role are smartphones, laptops, media players, TV, tablets, and PCs.
- Unicast Media Receiver: Based on the BAP Unicast Server, it concerns devices rendering audio for media streams using Unicast. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
- Broadcast Media Sender: Based on the BAP Unicast Client, it concerns devices able to send media audio content using Broadcast. Example of devices implementing this role are smartphones, laptops, media players, TV, tablets, and PCs.
- Broadcast Media Receiver: Based on the BAP Unicast Server, it concerns devices rendering audio for media streams using Broadcast. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
The requirements for the 6 roles are the following:
TMAP Role | CAP Roles | BAP Roles | GAP Roles | VCP Roles |
---|---|---|---|---|
Call Gateway | Initiator & Commander | Unicast Client | Central | Volume Controller |
Call Terminal | Acceptor | Unicast Server | Observer & Peripheral | Volume Renderer |
Unicast Media Sender | Initiator & Commander | Unicast Client | Central | Volume Controller |
Unicast Media Receiver | Acceptor | Unicast Server | Peripheral | Volume Controller |
Broadcast Media Sender | Initiator | Broadcast Source | Broadcaster | |
Broadcast Media Receiver | Acceptor | Broadcast Sink & Scan Delegator | Observer & Peripheral | Volume Controller |
1.3. TMAP Announcement
A device implementing a TMAP role shall put a bitfield of the TMAP roles supported it in the advertising data.
1.4. Telephony And Media Audio Service (TMAS)
A device implementing a TMAP role (except for BMS role) shall implement the GATT Server role with one instance of Telephony and Media Service (TMAS). This service permits a remote TMA Client to retrieve the roles of the device upon connection.
2. Telephony and Media Audio Profile Application APIs
The following section lists and describes APIs typically Used in a TMAP Application.
2.1. TMAP APIs
The following APIs are available for the TMAP:
TMAP_Init | Initialize the Telephony and Media Audio Profile with the selected role(s) |
TMAP_Linkup | Link Up the TMAP Client with remote TMAP Server. |
TMAP_DB_IsPresent | Indicate if a TMAP Database is saved in NVM |
TMAP_BuildAdvPacket | Build Advertising Packet for TMAP Peripheral |
TMAP_ReadRemoteTMAPRole | Read the remote TMAP Role Value |
2.1.1. TMAP Initialization
1. First initialize the Use-case Device Management module:
USECASE_DEV_MGMT_Init();
2. Then, initialize the TMAP with a TMAP_Config_t structure containing the desired role(s), the maximum number of links and a pointer to a RAM section that will contain the TMAP data:
static uint32_t aTMAPMemBuffer[DIVC(TMAP_DYN_ALLOC_SIZE,4)];
TMAP_Config_t tmap_config;
tmap_config.Role = Role;
tmap_config.MaxNumBleLinks = CFG_BLE_NUM_LINK;
tmap_config.pStartRamAddr = (uint8_t *)&aTMAPMemBuffer;
tmap_config.RamSize = TMAP_DYN_ALLOC_SIZE;
TMAP_Init(&tmap_config);
3. When implementing the CT or the UMR roles, mandatory Published Audio Capabilities (PAC) must be registered using the following APIs:
CAP_RegisterSnkPACRecord(&aSnkPACRecord,&aSnkPACRecordHandle);
CAP_RegisterSrcPACRecord(&aSrcPACRecord,&aSrcPACRecordHandle);
2.1.2. Linkup remote TMAP Server
To perform Linkup on a remote TMAP Server, use the dedicated API. If a database is already present, use the Restore mode.
/* Check if TMAP link is present in NVM from a previous connection*/
if (TMAP_DB_IsPresent(p_conn->Peer_Address_Type,p_conn->Peer_Address) == 0)
{
TMAP_Linkup(ConnHandle, TMAP_LINKUP_MODE_COMPLETE);
}
else
{
TMAP_Linkup(pNotification->ConnHandle,TMAP_LINKUP_MODE_RESTORE);
}
During the Linkup process, the TMAP_REM_ROLE_VALUE_EVT and TMAP_LINKUP_COMPLETE_EVT events will be generated:
void TMAP_Notification(TMAP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case TMAP_LINKUP_COMPLETE_EVT:
{
break;
}
case TMAP_REM_ROLE_VALUE_EVT:
{
uint16_t *tmap_role = (uint16_t *) pNotification->pInfo;
break;
}
}
}
2.2. Audio Stream Management APIs
The following APIs are used by TMAP Applications to manage audio streams:
API | BAP Role(s) | Description |
---|---|---|
CAP_Unicast_AudioStart | Unicast Client | Configure and Start a Broadcast Source with the given parameters. |
CAP_Unicast_AudioStop | Unicast Client | Stop a Broadcast Source and go to Configured or Idle State. |
CAP_Broadcast_AudioStart | Broadcast Source | Configure and Start a Broadcast Source with the given parameters. |
CAP_Broadcast_AudioStop | Broadcast Source | Stop a Broadcast Source and go to Configured or Idle State. |
CAP_SetSnkAudioLocations | Unicast Server / Scan Delegator | Set/Update the supported Sink Audio Locations. |
CAP_SetSrcAudioLocations | Unicast Server / Scan Delegator | Set/Update the supported Source Audio Locations. |
CAP_RegisterSnkPACRecord | Unicast Server / Scan Delegator | Register Published Audio Capabilities Record for Audio Sink role. |
CAP_RegisterSrcPACRecord | Unicast Server / Scan Delegator | Register Published Audio Capabilities Record for Audio Source role. |
CAP_SetSupportedAudioContexts | Unicast Server / Scan Delegator | Set/Update supported audio context for reception and transmission. |
CAP_SetAvailableAudioContexts | Unicast Server / Scan Delegator | Set/Update available audio context for reception and transmission. |
CAP_RegisterAudioChannels | Unicast Server / Scan Delegator | Register Sink/Source Audio Channels (and associated Audio Stream Endpoint) supported by Unicast Server. |
For more details about the Audio Stream management procedures, see the Architecture and Integration wiki page[3].
2.3. Volume Control Management APIs
The following APIs are used by TMAP Applications to manage Volume Control:
API | VCP Role(s) | Description |
---|---|---|
VCP_RENDER_SetAbsVolume | Volume Renderer | Set the Absolute Volume of the local volume renderer |
VCP_RENDER_SetMuteState | Volume Renderer | Set the Mute value of the local volume renderer. |
CAP_VolumeController_StartSetVolumeProcedure | Volume Controller | Start procedure to change the volume level on all the Acceptors of the Coordinated Set acting in the VCP Volume Renderer role. |
CAP_VolumeController_StartSetVolumeMuteStateProcedure | Volume Controller | Start the procedure to change the (Volume) mute state on all the Acceptors of the Coordinated Set acting in the VCP Volume Renderer role. |
For more details about the Audio Stream management procedures, see the Architecture and Integration wiki page[4].
2.4. Media Control Management APIs
The following APIs are used by TMAP Applications to manage Media Control:
API | MCP Role(s) | Description |
---|---|---|
MCP_SERVER_SetTrackTitle | MCP Server | Set the title of the current track. |
MCP_SERVER_SetTrackDuration | MCP Server | Set the length of the current track. |
MCP_SERVER_SetTrackPosition | MCP Server | Set the current track position of the current track. |
MCP_SERVER_NotifyTrackChanged | MCP Server | Notify the remote MCP Client that the track has changed. |
MCP_CLIENT_MoveNextTrack | MCP Client | Request the remote MCP Server to move to the next track. |
MCP_CLIENT_MovePreviousTrack | MCP Client | Request the remote MCP Server to move to the previous track. |
MCP_CLIENT_PlayTrack | MCP Client | Request the remote MCP Server to start playing the current track. |
MCP_CLIENT_PauseTrack | MCP Client | Request the remote MCP Server to pause the playing current track. |
MCP_CLIENT_ConfigureTrackTitleNotification | MCP Client | Configure the Track Title update Notification. |
For more details about the Media Control management procedures, see the Architecture and Integration wiki page[5].
2.5. Call Control Management APIs
The following APIs are used by TMAP Applications to manage Call Control:
API | CCP Role(s) | Description |
---|---|---|
CCP_SERVER_SetActiveCall | CCP Server | Set the current track position of the current track. |
CCP_SERVER_TerminateCall | CCP Server | Notify the remote MCP Client that the track has changed. |
CCP_CLIENT_AnswerIncomingCall | CCP Client | Set the title of the current track. |
CCP_CLIENT_TerminateCall | CCP Client | Set the length of the current track. |
For more details about the Media Control management procedures, see the Architecture and Integration wiki page[5].
3. TMAP Demonstrator using STM32WBA
The STM32WBA Cube firmware allows to easily build and deploy TMAP Unicast Server and TMAP Unicast Client applications.
3.1. Project architecture
The figure below represents the Firmware Architecture of the TMAP Unicast Server/Client example projects inside STM32CubeWBA MCU Package.
3.2. Demo using 2 STM32WBA
3.2.1. Hardware required
This demonstrator requires the following hardware:
- 2x STM32WBA55G-DK1 boards
- 1x Headphones/Headset with a 3.5mm jack cable, optionally with a microphone in which case the jack will be 4-pin.
Additionally, as an audio source on the Unicast Client side, one of the following can be used:
- 1x Music sources with a 3.5mm jack output (Laptop or Smartphone with a jack output). If the music source is powered using a power supply, use a Ground Loop isolator device or run the laptop on battery to avoid Ground Loop issues
- 1x Headset with microphone
3.2.2. Setup
3.2.3. Operate Demonstrator
The two projects integrate a menu permitting to operate the demonstrator.
1. To establish the connection between the two STM32WBAs, press the right direction on the joystick of the Unicast Server to start advertising, then do the same on the Unicast Server to start scanning. Select your device in the list and press the right direction to initiate connection.
2. Once the Linkup done on each side, access the menu using the right direction of the joystick
- To start or stop an audio stream, navigate to the “Audio Stream” sub-menu on the Unicast Client target and select the desired item list
- To operate the Unicast Client’s volume, navigate to the “Local Volume” on the Unicast Client target
- To operate the Unicast Server’s volume, navigate to the “Remote Volume” sub-menu on the Unicast Client target, or navigate to the “Volume” sub-menu on the Unicast Server target
The following configurations are used in the Unicast Client's project:
Configuration | BAP Audio Configuration | Legend | Codec Configuration |
---|---|---|---|
Media | 4 | ------->> | 48_4 |
Telephony | 3 | <-------> | 32_2 |
3.3. Demo using a STM32WBA and a compatible Smartphone
The Unicast Client role can be managed by a Smartphone compatible with LE Audio. This allows to fully use the Media Control and Call Control brought by the Media Control Profile (MCP) and Call Control Profile (CCP).
3.3.1. Hardware required
- 1x STM32WBA55G-DK1 boards
- 1x Headphones/Headset with a 3.5mm jack cable, optionally with a microphone in which case the jack will be 4-pin.
- 1x Smartphone compatible with LE Audio
The following smartphones are listed as compatible with LE Audio
Brand | Model | Features | ST Compatible |
---|---|---|---|
Pixel 7/7Pro | Unicast | Yes | |
Pixel 8/8Pro | Unicast | Yes | |
Samsung | Galaxy S23 | Unicast | No |
Samsung | Galaxy S24 | Unicast | No |
Sony | Xperia V 1/5 | Unicast & Broadcast | Yes (Broadcast), No (Unicast) |
3.3.2. Setup
3.3.3. Smartphone Configuration
3.3.3.1. Google Pixel Configuration & Pairing
In order to first activate the experimental BLE Audio feature on Google Pixel smartphones, go to the Developer Options menu and
- Uncheck "Disable Bluetooth LE Audio
- Check "Disable Bluetooth LE Audio hardware offload
The first time you connect to a BLE Audio device, you have to enable the LE Audio parameter in the device parameters.
3.3.4. Operate Demonstrator
1. To establish the connection between the STM32WBA and the Smartphone, press the right direction on the joystick of the STM32WBA Unicast Server to start advertising. Connect to the STM32WBA using the smartphone and unable LE Audio on the peripheral.
2. Use any media application (Spotify, YouTube, …) and start playing to establish a unidirectional audio stream between the two devices
3. Initiate or receive and accept a call on the smartphone using the cellular network or with a VoIP application to establish a bidirectional audio stream between the two devices.
The Unicast Server application can use the Volume Control Profile (VCP), the Media Control Profile (MCP) and Call Control profile (CCP) to interact with the smartphone.
- Navigate to the “Volume Control” sub-menu, using the right direction of the joystick, to control the output volume of the Unicast Server. The smartphone should be notified of this volume change
- Navigate to the “Media Control” sub-menu to control the media currently played on the smartphone. The current track title and media state is retrieved and displayed on the screen of the Unicast Server. Use the up, right and down directions of the joystick to go to next track, pause/play, or go to previous track.
- Navigate to the “Call Control” sub-menu to control the calls received on the smartphone. The call state is displayed on the screen of the Unicast Server. Use the Up and Down directions of the joystick to answer or hang up a call.
4. References
- ↑ Telephony & Media Audio Profile Bluetooth Specification Page
- ↑ Introduction to Bluetooth LE Audio
- ↑ Bluetooth LE Audio - STM32WBA Architecture and Integration - Audio Stream Transition Procedures
- ↑ Bluetooth LE Audio - STM32WBA Architecture and Integration - Volume Control Procedures
- ↑ 5.0 5.1 Bluetooth LE Audio - STM32WBA Architecture and Integration - Content Control