Coming soon |
1. Telephony & Media Audio Profile
1.1. Introduction
The Telephony and Media Audio Profile is a BLE Audio profile specified by the Bluetooth SIG. It's categorized as a "use-case profile", meaning that it's a high-layer profile designed for a specific use case. The complete specification can be found on the Bluetooth SIG website[1]. Location of PBP inside BLE Audio Profiles architecture
The TMAP addresses the use-cases of Telephony and Media over BLE Audio. This covers Broadcast audio, where audio data is “broadcasted” from a Broadcast Source to an unlimited number of Broadcast Sinks, using Broadcast Isochronous Streams. It also covers the Unicast audio, where audio is streamed between two connected devices, allowing bidirectional streams and more efficient acknowledgement. For more details about Unicast and Broadcast features, see the wiki page "Introduction to Bluetooth LE Audio"[2].
1.2. Roles
The TMAP introduces 6 different roles:
- Call Gateway: Based on the BAP Unicast Client, it concerns devices connected to networks used for telephony or VoIP applications. Example of devices implementing this role are smartphones, laptops, tablets, and PCs.
- Call Terminal: Based on the BAP Unicast Server, it concerns devices rendering audio for telephony and VoIP applications. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
- Unicast Media Sender: Based on the BAP Unicast Client, it concerns devices able to send media audio content using Unicast. Example of devices implementing this role are smartphones, laptops, media players, TV, tablets, and PCs.
- Unicast Media Receiver: Based on the BAP Unicast Server, it concerns devices rendering audio for media streams using Unicast. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
- Broadcast Media Sender: Based on the BAP Unicast Client, it concerns devices able to send media audio content using Broadcast. Example of devices implementing this role are smartphones, laptops, media players, TV, tablets, and PCs.
- Broadcast Media Receiver: Based on the BAP Unicast Server, it concerns devices rendering audio for media streams using Broadcast. Examples of devices implementing this role are earbuds, headphones, headsets, and speakers.
The requirements for the 6 roles are the following:
TMAP Role | CAP Roles | BAP Roles | GAP Roles | VCP Roles |
---|---|---|---|---|
Call Gateway | Initiator & Commander | Unicast Client | Central | Volume Controller |
Call Terminal | Acceptor | Unicast Server | Observer & Peripheral | Volume Renderer |
Unicast Media Sender | Initiator & Commander | Unicast Client | Central | Volume Controller |
Unicast Media Receiver | Acceptor | Unicast Server | Peripheral | Volume Controller |
Broadcast Media Sender | Initiator | Broadcast Source | Broadcaster | |
Broadcast Media Receiver | Acceptor | Broadcast Sink & Scan Delegator | Observer & Peripheral | Volume Controller |
1.3. TMAP Announcement
A device implementing a TMAP role shall put a bitfield of the TMAP roles supported it in the advertising data.
1.4. Telephony And Media Audio Service (TMAS)
A device implementing a TMAP role (except for BMS role) shall implement the GATT Server role with one instance of Telephony and Media Service (TMAS). This service permits a remote TMA Client to retrieve the roles of the device upon connection.
2. Public Broadcast Profile APIs
The following section lists and describes the Public Broadcast Source and Sink APIs.
2.1. Public Broadcast Source APIs
The following APIs are available for the Public Broadcast Source role:
PBP_Init | Initialize the Public Broadcast Profile with the selected role(s) |
PBP_PBS_BroadcastAudioStart | Perform a Broadcast Audio Start procedure using PBP requirements to start a Public Broadcast Source. |
PBP_PBS_BroadcastAudioStop | Perform the Broadcast Audio Stop procedure to stop a Public Broadcast Source |
PBP_PBS_BroadcastAudioUpdate | Perform the Broadcast Audio Update Procedure to update a Public Broadcast Source's metadata |
CAP_Broadcast_ReadSupportedControllerDelay | Reat the supported controller delay range function of the number of BIS |
CAP_Broadcast_SetupAudioDataPath | Setup the data path of the chosen BISs |
2.1.1. Public Broadcast Source Initialization
1. In order to initialize and establish a Public Broadcast Source, it's first necessary to initialize the GATT and GAP layers using the appropriated roles
aci_gatt_init();
/* Broadcaster GAP role is required */
aci_gap_init(GAP_BROADCASTER_ROLE, PRIVACY, DEV_NAME_CHAR_HANDLE,
&service_handle, &dev_name_char_handler, &appearance_char_handle );
2. The audio stack should also be initialized
tBleStatus ret;
BleAudioInit_t BleAudioInit;
/* Initialize the Audio IP*/
BleAudioInit.NumOfLinks = CFG_BLE_NUM_LINK;
BleAudioInit.bleStartRamAddress = (uint8_t*)aAudioInitBuffer;
BleAudioInit.total_buffer_size = BLE_AUDIO_DYN_ALLOC_SIZE;
ret = BLE_AUDIO_STACK_Init(&BleAudioInit);
3. Then the Common Audio Profile (CAP) should be initialized using the CAP Initiator and BAP Broadcast Source roles. Other profiles and roles are not required for a Public Broadcast Source.
CAP_Config_t PBPAPP_CAP_Config = {0};
BAP_Config_t PBPAPP_BAP_Config = {0};
CCP_Config_t PBPAPP_CCP_Config = {0};
MCP_Config_t PBPAPP_MCP_Config = {0};
VCP_Config_t PBPAPP_VCP_Config = {0};
MICP_Config_t PBPAPP_MICP_Config = {0};
CSIP_Config_t PBPAPP_CSIP_Config = {0};
/* Configure CAP */
PBPAPP_CAP_Config.Role = CAP_ROLE_INITIATOR;
PBPAPP_CAP_Config.MaxNumLinks = CFG_BLE_NUM_LINK;
PBPAPP_CAP_Config.pStartRamAddr = (uint8_t *)&aCAPMemBuffer;
PBPAPP_CAP_Config.RamSize = CAP_DYN_ALLOC_SIZE;
/* Configure BAP */
PBPAPP_BAP_Config.Role = BAP_ROLE_BROADCAST_SOURCE;
PBPAPP_BAP_Config.MaxNumBleLinks = CFG_BLE_NUM_LINK;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumCIG = 0;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumCISPerCIG = 0;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumBIG = MAX_NUM_BIG;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumBISPerBIG = MAX_NUM_BIS_PER_BIG;
PBPAPP_BAP_Config.ISOChnlConfig.pStartRamAddr = 0;
PBPAPP_BAP_Config.ISOChnlConfig.RamSize = 0u;
/* Initialize the Common Audio Profile*/
ret = CAP_Init(&PBPAPP_CAP_Config,
&PBPAPP_BAP_Config,
&PBPAPP_VCP_Config,
&PBPAPP_MICP_Config,
&PBPAPP_CCP_Config,
&PBPAPP_MCP_Config,
&PBPAPP_CSIP_Config);
4. The Public Broadcast Profile can finally be initalized using the Public Broadcast Source role
PBP_Init(PBP_ROLE_PUBLIC_BROADCAST_SOURCE);
2.1.2. Start a Public Broadcast Source
Public Broadcast Source State Machine:
1. To start a public Broadcast Source, use the PBP_PBS_BroadcastAudioStart
PBP_PBS_BroadcastAudioStart(&pbp_audio_start_params);
2. During the Public Broadcast Source start procecure, the CAP_CODEC_CONFIGURED_EVT event will be called in the CAP Callback when the sampling frequency is configured. Use the sampling frequency to initialize the Audio Clocks.
static void CAP_App_Notification(CAP_Notification_Evt_t *pNotification)
{
switch (pNotification->EvtOpcode)
{
case CAP_CODEC_CONFIGURED_EVT:
{
/* Init Audio Clock with configured Sampling Frequency */
Sampling_Freq_t *freq = (Sampling_Freq_t *)pNotification->pInfo;
AudioClock_Init(*freq);
}
break;
}
}
3. The PBP_PBS_BROADCAST_AUDIOSTARTED_EVT event will be generated upon BIG creation. Use this event to setup the data path and the audio peripherals. The PBP_BROADCAST_AUDIO_UP_EVT event will then be generated to indicate that the audio path is up.
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_PBS_BROADCAST_AUDIOSTARTED_EVT:
{
/* Register Start Rx callback */
CODEC_RegisterTriggerClbk(1,0,&start_audio_source);
/* Initialize Audio peripherals */
MX_AudioInit(role,
sampling_freq,
frame_duration,
0,
(uint8_t *) aPlayBuff,
(AudioDriverConfig) PBPAPP_Context.audio_driver_config);
/* Read Controller Delay */
CAP_Broadcast_ReadSupportedControllerDelay(NUM_BIS, DATA_PATH_INPUT,
a_codec_id,
&controller_delay_min,
&controller_delay_max);
/* Setup Audio Data Path */
CAP_Broadcast_SetupAudioDataPath(NUM_BIS, bis_conn_handle, direction,
codec_id, controller_delay,
DATA_PATH_CIRCULAR_BUF,
datapath_param_len, &datapath_param);
break;
}
case PBP_BROADCAST_AUDIO_UP_EVT:
{
/* Audio is UP */
break;
}
}
}
2.1.3. Stop a Public Broadcast Source
1. To stop a public Broadcast Source, use the PBP_PBS_BroadcastAudioStop
/* Use 1 as release parameter to stop the related Extended and Periodic Advertising, 0 to keep them */
PBP_PBS_BroadcastAudioStop(BIG_HANDLE, 1);
2. The Audio Data Path will automatically be removed and the event PBP_BROADCAST_AUDIO_DOWN_EVT will be called
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_BROADCAST_AUDIO_DOWN_EVT:
{
/* Audio is DOWN */
/* Deinit Audio peripherals*/
MX_AudioDeInit();
break;
}
}
}
2.2. Public Broadcast Sink APIs
The following APIs are available for the Public Broadcast Sink role:
PBP_Init | Initialize the Public Broadcast Profile with the selected role(s) |
PBP_PBK_StartAdvReportParsing | Start the parsing of Extended Advertising Reports to look for PBP UUIDs and generate PBP_PBK_BROADCAST_SOURCE_ADV_REPORT_EVT events |
PBP_PBK_StopAdvReportParsing | Stops the parsing of Extended Advertising Reports |
PBP_PBK_StartPASync | Synchronize to the periodic advertising train of the given Public Broadcast Source to discover more details about the related audio stream |
PBP_PBK_StartBIGSync | Synchronize to a BIG and start receiving audio data from it |
PBP_PBK_StopPASync | Stop the synchronization to a periodic advertising train |
PBP_PBK_StopBIGSync | Terminate the synchronization to a BIG |
CAP_Broadcast_ReadSupportedControllerDelay | Reat the supported controller delay range function of the number of BIS |
CAP_Broadcast_SetupAudioDataPath | Setup the data path of the chosen BISs |
2.2.1. Public Broadcast Sink Initialization
1. In order to initialize and establish a Public Broadcast Source, it's first necessary to initialize the GATT and GAP layers using the appropriated roles
aci_gatt_init();
/* Observer and Peripheral GAP roles are required */
aci_gap_init(GAP_OBSERVER_ROLE | GAP_PERIPHERAL_ROLE, PRIVACY, DEV_NAME_CHAR_HANDLE,
&service_handle, &dev_name_char_handler, &appearance_char_handle );
2. The audio stack should also be initialized
tBleStatus ret;
BleAudioInit_t BleAudioInit;
/* Initialize the Audio IP*/
BleAudioInit.NumOfLinks = CFG_BLE_NUM_LINK;
BleAudioInit.bleStartRamAddress = (uint8_t*)aAudioInitBuffer;
BleAudioInit.total_buffer_size = BLE_AUDIO_DYN_ALLOC_SIZE;
ret = BLE_AUDIO_STACK_Init(&BleAudioInit);
3. Then the Common Audio Profile (CAP) should be initialized using the CAP Acceptor, BAP Broadcast Sink and BAP Scan Delegator roles. Other profiles and roles are not required for a Public Broadcast Sink.
CAP_Config_t PBPAPP_CAP_Config = {0};
BAP_Config_t PBPAPP_BAP_Config = {0};
CCP_Config_t PBPAPP_CCP_Config = {0};
MCP_Config_t PBPAPP_MCP_Config = {0};
VCP_Config_t PBPAPP_VCP_Config = {0};
MICP_Config_t PBPAPP_MICP_Config = {0};
CSIP_Config_t PBPAPP_CSIP_Config = {0};
/* Configure CAP */
PBPAPP_CAP_Config.Role = CAP_ROLE_ACCEPTOR;
PBPAPP_CAP_Config.MaxNumLinks = CFG_BLE_NUM_LINK;
PBPAPP_CAP_Config.pStartRamAddr = (uint8_t *)&aCAPMemBuffer;
PBPAPP_CAP_Config.RamSize = CAP_DYN_ALLOC_SIZE;
/* Configure BAP */
PBPAPP_BAP_Config.Role = BAP_ROLE_BROADCAST_SINK | BAP_ROLE_SCAN_DELEGATOR;
PBPAPP_BAP_Config.MaxNumBleLinks = CFG_BLE_NUM_LINK;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumCIG = 0;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumCISPerCIG = 0;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumBIG = MAX_NUM_BIG;
PBPAPP_BAP_Config.ISOChnlConfig.MaxNumBISPerBIG = MAX_NUM_BIS_PER_BIG;
PBPAPP_BAP_Config.ISOChnlConfig.pStartRamAddr = 0;
PBPAPP_BAP_Config.ISOChnlConfig.RamSize = 0u;
/* Initialize the Common Audio Profile*/
ret = CAP_Init(&PBPAPP_CAP_Config,
&PBPAPP_BAP_Config,
&PBPAPP_VCP_Config,
&PBPAPP_MICP_Config,
&PBPAPP_CCP_Config,
&PBPAPP_MCP_Config,
&PBPAPP_CSIP_Config);
4. The Public Broadcast Profile can finally be initalized using the Public Broadcast Sink role
PBP_Init(PBP_ROLE_PUBLIC_BROADCAST_SINK);
2.2.2. Synchronize a Public Broadcast Sink
The synchronization process of a Public Broadcast Sink can be summarized like this:
1. The Public Broadcast Sink should first enable the Extended Advertising event parsing and start a scan using the ACI Start Observation procedure
uint8_t ret;
ret = PBP_PBK_StartAdvReportParsing();
if (ret == BLE_STATUS_SUCCESS)
{
/* Starts an Observation procedure */
ret = aci_gap_start_observation_proc(SCAN_INTERVAL,
SCAN_WINDOW,
0x00, /* LE_Scan_Type */
0x00, /* Address type: Public */
0x00, /* Filter duplicates: No */
0x00 ); /* Filter policy: Accept all */
}
2. Upon scanning a Public Broadcast Source, the PBP_PBK_BROADCAST_SOURCE_ADV_REPORT_EVT will be generated with the details of the Public Broadcast Source. Start Syncing to the Periodic Advertising train
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_PBK_BROADCAST_SOURCE_ADV_REPORT_EVT:
{
PBP_Broadcast_Source_Adv_Report_Data_t *data = (PBP_Broadcast_Source_Adv_Report_Data_t*) pNotification->pInfo;
PBP_PBK_StartPASync(data->pBAPReport->AdvSID,
data->pBAPReport->pAdvAddress,
data->pBAPReport->AdvAddressType,
PA_EVENT_SKIP,
PA_SYNC_TIMEOUT);
break;
}
}
}
3. When the Periodic Advertising Synchronization is established, the PBP_PBK_PA_SYNC_ESTABLISHED_EVT is generated, followed by PBP_PBK_BASE_REPORT_EVT containing the Broadcast Source Configuration information contained in the Periodic Advertising Data and the PBP_PBK_BIGINFO_REPORT_EVT containing the details of the BIG of the Broadcast Source. Parse the Broadcast Source configuration to initialize audio clocks and initiate BIG synchronization.
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_PBK_PA_SYNC_ESTABLISHED_EVT:
{
/* Periodic Advertising Synchronization is established */
break;
}
case PBP_PBK_BASE_REPORT_EVT:
{
BAP_BASE_Report_Data_t *base_data = (BAP_BASE_Report_Data_t*) pNotification->pInfo;
/* Retrieve BASE Data */
/* [...] */
uint32_t freq = LTV_GetConfiguredSamplingFrequency(PBPAPP_Context.base_subgroups[0].pCodecSpecificConf,
PBPAPP_Context.base_subgroups[0].CodecSpecificConfLength);
/* Init Audio Clock with Broadcast Source frequency */
AudioClock_Init(freq);
break;
}
case PBP_PBK_BIGINFO_REPORT_EVT:
{
BAP_BIGInfo_Report_Data_t *data = (BAP_BIGInfo_Report_Data_t *) pNotification->pInfo;
uint8_t bis_index[2u] = {0x01, 0x02};
/* Start BIG Synchronization */
status = PBP_PBK_StartBIGSync(BIG_HANDLE,
data->SyncHandle,
&(bis_index[0]),
data->NumBIS,
&(PBPAPP_Context.base_group),
0u,
BAP_BROADCAST_ENCRYPTION,
aPBPAPP_BroadcastCode,
BIG_MSE,
BIG_SYNC_TIMEOUT);
break;
}
}
}
4. Upon synchronization to the BIG, PBP_PBK_BIG_SYNC_ESTABLISHED_EVT will be generated. Stop the scan procedure and setup the data path to generate the PBP_BROADCAST_AUDIO_UP_EVT when the data path is up.
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_PBK_BIG_SYNC_ESTABLISHED_EVT:
{
/* BIG Sync is established */
/* Stop Advertising Report parsing and Observation procedure */
PBP_PBK_StopAdvReportParsing();
aci_gap_terminate_gap_proc(GAP_OBSERVATION_PROC);
/* Read Controller Delay */
CAP_Broadcast_ReadSupportedControllerDelay(NUM_BIS, DATA_PATH_OUTPUT,
a_codec_id,
&controller_delay_min,
&controller_delay_max);
/* Setup Audio Data Path */
CAP_Broadcast_SetupAudioDataPath(NUM_BIS, bis_conn_handle, direction,
codec_id, controller_delay,
DATA_PATH_CIRCULAR_BUF,
datapath_param_len, &datapath_param);
break;
}
case PBP_BROADCAST_AUDIO_UP_EVT:
{
/* Audio data path is up */
break;
}
}
}
2.2.3. Stop Public Broadcast Sink Synchronization
1. To stop the synchronization to a Public Broadcast Source from a Public Broadcast Sink, terminate the BIG and the Periodic Advertising synchronization.
PBP_PBK_StopPASync(PBPAPP_Context.PASyncHandle);
PBP_PBK_StopBIGSync(BIG_HANDLE);
2. The PBP_BROADCAST_AUDIO_DOWN_EVT will be generated. Deinitialize the Audio Peripherals.
void PBP_Notification(PBP_Notification_Evt_t *pNotification)
{
switch(pNotification->EvtOpcode)
{
case PBP_BROADCAST_AUDIO_DOWN_EVT:
{
/* Audio data path is down, deinit Audio Peripherals */
MX_AudioDeInit();
break;
}
}
}
3. PBP Demonstrator using STM32WBA
The STM32WBA Cube firmware allows to easily build and deploy Public Broadcast Sources and Public Broadcast Sinks applications.
3.1. Hardware required
The PBP demonstrator requires the following hardware:
- 3x STM32WBA55G-DK1 Boards
- 2x Music Source with a 3.5mm jack output (Laptop or Smartphone with a jack output). If a laptop is used as a source, use a Ground Loop isolator device or run the laptop on battery to avoid Ground issue
- 1x Music renderer with 3.5mm jack input (Headphones or Speakers)
3.2. Setup
The setup is as following:
PBP Demonstrator Setup |
---|
3.3. Project architecture
The figure below represents the Firmware Architecture of the Public Broadcast Profile example projects inside STM32CubeWBA MCU Package.
STM32WBA PBP Firmware Architecture |
---|
3.4. PBP Source configuration
Following is a summary of the main changes possible on the PBP_Source project
PBP_Source project configuration |
---|
Setting | File | Description |
---|---|---|
BROADCAST_SOURCE_BAP_CONFIG | pbp_app.c | Configuration index in BroadcastQoSConf array. 0 corresponds to 8_2_1 configuration, 1 to 8_2_2, … Commonly used values are 3 (16_2_1 config), 5 (24_2_1 config), and 13 (48_4_1 config). For more details about the configurations, refer to the Introduction to Bluetooth LE Audio wiki page. |
BROADCAST_SOURCE_FRAME_BLOCK_PER_SDU | pbp_app.c | Number of concatenated codec frames sent at the same time. May be 1 or 2. Setting it to 2 reduces the number of events needed to send the packets which can improve reliability but increase the latency. |
BROADCAST_SOURCE_NUM_BIS | pbp_app.c | Number of BIS used for the Broadcast Source. May be 1 or 2. Setting it to 1 reduces the number of events needed to send the packets which can improve reliability but a value of 2 reduces the strain on Sink devices synchronizing to mono audio. |
BROADCAST_SOURCE_CHANNEL_ALLOC_1 | pbp_app.c | Audio Channel Allocation of BIS #1. Bitfield of Audio Location values. Commonly used values are 0x01 for "Front Left" location or 0x03 for "Front Left + Front Right" location. |
BROADCAST_SOURCE_CHANNEL_ALLOC_2 | pbp_app.c | Audio Channel Allocation of BIS #2. Bitfield of Audio Location values. Commonly used value is 0x02 for "Front Right". Ignored if "BROADCAST_SOURCE_NUM_BIS" is 1. |
BROADCAST_CONTROLLER_DELAY | pbp_app.c | Controller delay value. Refer to "STM32WBA LC3 codec and audio data path" wiki page[3] |
BAP_BROADCAST_MAX_TRANSPORT_LATENCY | pbp_app.c | Maximum Transport Latency value. Refer to "STM32WBA LC3 codec and audio data path" wiki page[3] |
BAP_BROADCAST_ENCRYPTION | pbp_app.c | 1 to enable broadcast encryption, 0 to disable it |
BIG_HANDLE | pbp_app.c | Handle of the BIG used for the Broadcast |
STREAMING_AUDIO_CONTEXT | pbp_app.c | Audio Context Type of the Broadcast Source. Common values are AUDIO_CONTEXT_MEDIA (0x0004) and AUDIO_CONTEXT_CONVERSATIONAL (0x0002). Refer to Assigned Numbers section 6.12.3 for more details[4] |
APPEARANCE | pbp_app.c | Appearance value of the Broadcast. Describe the physical appearance of the device. Refer to Assigned Number section 2.6 for more details[4] |
BROADCAST_NAME_LENGTH | pbp_app.c | Length of the Broadcast Name |
aPBPAPP_BroadcastCode | pbp_app.c | Broadcast Code used when BAP_BROADCAST_ENCRYPTION is set to 1. Broadcast Sinks will have to know the Broadcast Code in order to decrypt the stream |
aPBPAPP_BroadcastName | pbp_app.c | Broadcast Name as described in 1.3 |
BAP_BROADCAST_SOURCE_ID | pbp_app.h | ID of the Broadcast Source. This value is ST specific and permits the PBP Sink to identify the PBP Source with a custom static identifier. Not to be confused with the Broadcast ID which is generated randomly by the BAP layer at Broadcast Source creation. |
3.5. PBP Sink configuration
Following is a summary of the main modification possible on the PBP_Sink project
PBP_Sink project configuration |
---|
Setting | File | Description |
---|---|---|
BROADCAST_CONTROLLER_DELAY | pbp_app.c | Controller delay value. Refer to "STM32WBA LC3 codec and audio data path" wiki page[3] |
BAP_BROADCAST_ENCRYPTION | pbp_app.c | 1 to enable broadcast decryption, 0 to disable it |
BIG_HANDLE | pbp_app.c | Handle of the BIG used for the Broadcast |
aPBPAPP_BroadcastCode | pbp_app.c | Broadcast Code used when BAP_BROADCAST_ENCRYPTION is set to 1. Broadcast Code must match the one set on the PBP Source |
aSourceIdList | pbp_app.c | List of Source IDs to cycle through using the joystick |
3.6. PBP Source Advertising details
The following schematic details the content of a Public Broadcast Source advertising Data.
Detail of PBP Source Advertising Data |
---|