1. Introduction
When integrating an RTOS with the Secure Manager, it is crucial to ensure secure and efficient thread management. The following article delves into the necessary steps for successful integration of an RTOS with the Secure Manager and emphasizes the mechanism responsible for ensuring secure and thread-safe function calls.
2. Prerequisite
- Installed Secure Manager
- Have a nonsecure application compatible with the Secure Manager
- Have the RTOS library chosen by the user integrated in the nonsecure application
3. Implementation example
Using the Secure Manager from a nonsecure application can be done in a single thread, which eliminates the possibility of concurrent access.
However, when working with a real-time operating system and a multi-threaded application, it is essential to protect the calls made to the Secure Manager. This protection guarantees that only one call can be made to the Secure Manager at a time, ensuring secure and efficient thread management.
In this section, we will provide an implementation example of how to protect calls made to the Secure Manager in a multi-threaded environment.
3.1. Thread-safe secure calls
To prevent multiple calls from the nonsecure application to the Secure Manager interface functions, a mechanism is included in tfm_ns_interface.c which can be found in the middleware secure_manager_api.
This mechanism, which is based on __weak functions, needs to be re-implemented with a mutex protection to ensure secure and efficient thread management.
The ns_ipc_seq_begin and ns_ipc_seq_end functions, which are declared by default in the Secure Manager, must be re-implemented in the RTOS project to support multi-threaded use.
3.2. Step by step implementation
The following steps outline how to implement mutex in the Secure Manager with RTOS in your project.
- Initialize the mutex
- Create the mutex
- Implement the acquisition and release of the mutex in the interface functions.
3.2.1. Detailed example applied with FreeRTOS.
1. Declare a mutex and initialize it to 0 :
static SemaphoreHandle_t nsIpcMutex = { 0 };
2. Create a function that creates the mutex and assigns it to the nsIpcMutex variable.
void tfm_ns_interface_init( void )
{
nsIpcMutex = xSemaphoreCreateMutex();
if(nsIpcMutex == NULL)
{
// Logging Error
}
}
3. Re-implement the acquisition and release of the mutex with functions defines in semphr.c from library FreeRTOS, in the ns_ipc_seq_begin and ns_ipc_seq_end functions.
void ns_ipc_seq_begin(const ns_ipc_seq_info_t* info)
{
/* Lock mutex */
if(nsIpcMutex != NULL)
{
xSemaphoreTake(nsIpcMutex, portMAX_DELAY );
}
….
}
void ns_ipc_seq_end(const ns_ipc_seq_info_t* info)
{
/* Unlock mutex */
if(nsIpcMutex != NULL)
{
xSemaphoreGive(nsIpcMutex);
}
….
}
For more concrete examples, actual implementations can be found in X-Cube-AWS & X-Cube-Azure using the Secure Manager with a real-time operating system.