This article is a step-by-step guide of how to use STM32Cube.AI Developer Cloud online platform and services.
1. Glossary
- DMZ is a physical or logical subnetwork that contains and exposes an organization's external-facing services to an untrusted, usually larger, network such as the Internet.
- ELF is a common standard format for binary files.
- GUI stands for graphic user interface.
- IOC is the project configuration file for STM32CubeMX
- K-means is a type of machine learning algorithm.
- Keras is an open-source library that provides a Python interface for artificial neural networks.
- MACC stands for multiply-accumulate.
- MATLAB® is a proprietary multi-paradigm programming language and numeric computing environment.
- MCU is an acronym for microcontroller unit.
- Netron is a viewer for neural network, deep learning and machine learning models.
- npz is a binary file format used to store arrays.
- ONNX is an open ecosystem that provides an open source format for AI models.
- PyTorch™ is a machine learning framework.
- RAM stands for random access memory, which is volatile memory.
- REST API stands for stands for representational state transfer application programming interface.
- scikit-learn is a free software machine learning library for the Python programming language.
- STM32 model zoo is a collection of reference machine learning models that are optimized to run on STM32 microcontrollers.
- Support vector machine (SVM) a type of machine learning algorithm.
- TensorFlow™ Lite is a mobile library for deploying models on mobile, microcontrollers and other edge devices.
- TFLiteConverter is the API for converting TensorFlow models to TensorFlow Lite.
- USART stands for Universal Synchronous/Asynchronous Receiver/Transmitter that allows a device to communicate using serial protocols.
- X-CUBE-AI is an STM32Cube Expansion Package, which is part of the STM32Cube.AI ecosystem.
2. Overview
STM32Cube.AI Developer Cloud (STM32CubeAI-DC) is a free-of-charge online platform and service that enables the creation, optimization, benchmarking, and generation of artificial intelligence (AI) for STM32 microcontrollers based on the Arm® Cortex®‑M processor. It is based on the STM32Cube.AI core technology.
The benefits and features of STM32Cube.AI Developer Cloud:
- Online GUI (no installation required) accessible with STMicroelectronics extranet user credentials
- Network optimization and visualization providing the RAM and flash memory sizes required to run on the STM32 target
- Quantization tool to convert a floating-point model into an integer model
- Benchmark service on the STMicroelectronics hosted board farm including various STM32 boards to make the most suited hardware selection
- Code generator including the network C code and optionally the whole STM32 project
- STM32 model zoo:
- Easy access to model selection, training script, and key model metrics, directly available for benchmark
- Application code generator from the user's model with “Getting started” code examples
- Machine learning (ML) workflow automation service with Python™ scripts (REST API)
- Supports all the X-CUBE-AI features, such as:
- Native support for various deep learning frameworks such as Keras and TensorFlow™ Lite, and support for all frameworks that can export to the ONNX standard format such as PyTorch™, MATLAB®, and more
- Support for the 8-bit quantization of Keras networks and TensorFlow™ Lite quantized networks
- Support for various built-in scikit-learn models such as isolation forest, support vector machine (SVM), K-means, and more
- Possibility to use larger networks by storing weights in external flash memory and activation buffers in external RAM
- Easy portability across different STM32 microcontroller series
- User-friendly license terms
3. Begin with login
To begin utilizing the tool, navigate to the home page of the STM32Cube.AI Developer Cloud at https://stm32ai-cs.st.com/. Upon arrival, the welcome page shown below should appear:
Once the page has fully loaded, select the "START NOW" button. This will redirect you to the sign-in page, as shown below:
- If you have a myST account, input your credentials and select the "Login" button.
- If you do not currently have an account, you may create a new one by selecting the "Create Account" button and filling out the required form. This process is entirely free.
4. Creating a project
Upon successfully logging in, you will be directed to the main page. On the main page there are three main zones, as shown below:
4.1. Upload your own model
In the first zone, you can upload any of your pre-trained AI model by pressing the "Upload" button or performing a drag-and-drop action.
4.2. Importing from STM32 model zoo
In the second zone, there is a list of pre-trained AI models, which have been trained for various targeted use cases, currently including five categories:
- Hand posture
- Image classification
- Human activity recognition
- Audio event detection
- Object detection
These models originate from STM32 model zoo. To create a new project, simply press the "Import" button next to the desired model.
4.3. Using saved models
Finally, the third zone functions as a workspace. This area contains all of the AI models that you have previously analyzed and benchmarked in STM32Cube.AI Developer Cloud.
4.4. Start the project
Within this article, we will be using a .h5 model from the model zoo, which was created using the TensorFlow Keras API.
To use the model, scroll down the model list of model zoo and locate the MOBILENET_V2_0.35_128_IMAGE_CLASSIFICATION_PERSON.H5
model. Once located, select the "Import" button adjacent to it.
Upon successful importation, the model will appear within the workspace.
- Press the "Play" button to compute Netron graph. Once the analysis is complete, select the "Netron" icon to open a pop-up window, which displays the model architecture in Neutron. This view allows you to observe all of the layers and components of the model. To exit this view, select the "cross" button located in the top right corner.
- Finally, press the "Start" button to create a new project.
After the project has been created, five action items will be available on the top bar:
- Optimize: to optimize the model with different options.
- Quantize: to quantize the float model using the post-training quantization.
- Benchmark: to benchmark the AI model on different STM32 boards from our board farm.
- Results: to view, analyze and compare the results generated from different benchmarking runs.
- Generate: to generate the code and the projects for the target MCU family and board for the optimized and benchmarked model.
Further details regarding these items will be explored in subsequent chapters.
Within this section, you will also be able to locate the details of the currently selected model. This includes pertinent information such as input and output shape, type, and MACC numbers, among other relevant data.
5. Optimize
Upon entering the optimize flow, a default optimization will be conducted utilizing the balanced optimization option. This will have "use activation buffer for input buffer" and "use activin for output buffer" enabled. You may modify the default setting and press "Optimize" to observe the impact.
5.1. Optimization options
There are three distinct options available for optimizing AI models:
- Balance between RAM size and inference time: this approach seeks to find a tradeoff between minimum RAM and the smallest inference time
- Optimize for RAM size: this approach seeks to identify the smallest RAM size.
- Optimize for inference time: this approach seeks to identify the smallest inference time.
By default, the balanced option is selected to provide users with the best compromise between the smallest footprint and the smallest inference time possible.
5.2. Use activation buffer for input/output buffer
When these options are enabled, it indicates that the “activations” buffer will be also used to handle the input/output buffers. This will only have an impact on memory and not inference time. Depending on the size of the input/output data, the “activations” buffer may be larger but overall less than the sum of the activation buffer plus the input/output buffer.
5.3. Launch the optimization
To initiate the optimization process, select the desired options and press the "Optimize" button. While the optimization is running, you can monitor the terminal, which will provide you with details regarding the optimization run. Any errors will be displayed here.
Multiple optimizations can be launched by selecting different types, allowing you to choose the option that best suits your needs. After each optimization has been performed, the reported numbers in terms of MACC, flash size, and RAM size will be displayed in the terminal.
Once all optimizations have been conducted, you can select the option that best suits your needs. In this example we will use the balanced approach. From here, you can proceed to the next action item. If you are utilizing a float model, the next step will be quantization. However, if you are utilizing a quantized model, you may skip this step and proceed directly to benchmarking. To Initialize the quantization step, simply press the "Go to quantize" button. To skip the quantization step and proceed directly to benchmarking, press the "Go to benchmark" button.
6. Quantize
This panel can be used to create a quantized model (8-bit integer format) from a Keras float model. Quantization is an optimization technique to compress a 32-bit floating-point model by reducing the size (smaller storage size and less memory peak usage at runtime), by improving CPU/MCU usage and latency (including power consumption) with a small degradation of accuracy. A quantized model executes some or all of the operations on tensors with integers rather than floating point values.
The quantize service uses Tensorflow post-training quantization interface offered by TFLiteConverter. You may select any input or output type from the three supported options, including int8, unsigned int8 or float32. To prevent accuracy loss during the quantization process, users are advised to provide their training dataset or a portion thereof. This can be provided in the form of .npz files. If no quantization file is provided, the quantization will be conducted with random data, and the resulting quantized model may only be used for benchmarks to to obtain the necessary flash and RAM size, as well as the inference time. However, no accuracy will be calculated.
Once an .npz file of the dataset has been provided, quantization can be performed by pressing the "Launch quantization" button. For the purposes of this demonstration, we will conduct the quantization without the dataset, utilizing random numbers instead.
Once the quantization has been completed, the quantized model will be listed below. You have the choice to run the "Optimize selected quantized model" by pressing the button and to compare the results with the float model. During the optimization process, the output will also be displayed in the terminal, as seen in the previous step..
After the optimization of the quantized model, the results are displayed in the "History of optimization results" table. In our example, an approximately 70% reduction in both Flash and RAM size from the optimization should be observed:
Once satisfied with the quantization results, you can press the "Go to benchmark" button. This will direct you to the model benchmarking step.
7. Benchmark
In the Benchmark panel, you can find the currently selected model, as well as the current parameters used for optimization.
The benchmark service enables users to remotely run selected AI models on several STM32 boards and obtain the required internal or external Flash and RAM, as well as inference time. These STM32 boards are hosted in ST premises, known as the "board farm" and will be accessible via a waiting queue Some basic information of the boards is listed, including CPU type and frequency, as well as both internal and external memory sizes.
To initiate the benchmark on a given board, simply press the "Start Benchmark" button next to that board. This will start the benchmarking process. For the purposes of this article, we will choose the STM32H735G-DK.
During the benchmarking process, users may observe the progress bar and current status in real-time. A project for system performance application will be created. The tool builds the project with the C code of the AI model and flashes one of the actual physical boards in our board farm. It runs the application on the board and provides users with the memory footprint and inference time. It is important to note that the inference times reported here are actual inference times on real physical boards, rather than mere estimates.
Once the benchmark has been completed, the measured inference time will be reported next to the board..
To obtain further details regarding the resources expended per layer, simply click on the "three-dot" icon and choose the "Show details per layer" option. A dialog of bar chart will appear here.
The bar chart displays the size of each of the layers in bytes. Users may toggle between the bar chart and the pie chart by clicking the "Toggle Pie/Bar Chart" button. While the bar chart displays the actual size, the pie chart displays the distribution.
Users may perform the same action for the execution time. The bar chart displays the duration in the milliseconds spent on each of the layers, while the pie chart displays the distribution of the execution time by each of the layers. To close this view, simply click anywhere outside the dialog.
The tool enables users to launch a benchmark on multiple boards simultaneously. You can launch the benchmarking on all boards by pressing all the "Start Benchmark" buttons. This will repeat the process for all boards and report the inference time on all boards next to them. Once all launched benchmarking runs have been completed, you can go to the Results section.
8. Results
The Results page showcases a table of all benchmarks conducted in the STM32Cube.AI Developer Cloud, which is intuitive for comparing all benchmarks. Users may directly select a benchmark for code generation by pressing the "Generate with this configuration" button. For this demonstration, we will choose the STM32H735G-DK, which provides the smallest inference time.
9. Generate
The Generate page offers various outputs that cater to different needs. These include updating an existing project, creating a new STM32CubeMX project, generating a STM32CubeIDE project with all the sources included, or downloading a compiled firmware to estimate the inference time on your own board.
Upon reaching the "Generate" step, users will be presented with the same header of the currently selected model and current parameters. If coming from the Benchmark or Results step, the target board will already be selected. Otherwise, users will need to filter from CPU types or STM32 series to select their target STM32 board.
Following this, users will have four generation options to choose from:
- Download C Code
- Download STM32CubeMX IOC file
- Download STM32CubeIDE Project
- Download Firmware
9.1. Download C code
This option generates STM32-optimized C Code associated with your pre-trained Neural Network. The ZIP package contains all network.c and .h files, the Cube.AI runtime library files and the stm32ai command line reports and output. Users can replace the existing files in their project with these newly generated files.
9.2. Download STM32CubeMX IOC file
This option generates a ZIP package containing an IOC file and the selected model, which is ready to start a new STM32CubeMX project locally on your machine. Users can open the IOC file with STM32CubeMX v6.6.1 or above and either directly generate the code or add other peripherals required for their application.
9.3. Download STM32CubeIDE Project
This option generates a ZIP package with a STM32CubeIDE project including IOC file, Project File, file tree and STM32-optimized C Code:
- The board is the selected board
- X-CUBE-AI is activated in the project and SystemPerformance application is selected
- The neural network model is configured in the project and is available in the ZIP package
- The USART needed for system performance application is already configured
- The STM32CubeIDE project and all the code and library are generated
Users can open the project with STM32CubeIDE 1.10.0 or above by double-clicking the .project file in the package. Once the project is imported into STM32CubeIDE, users can either edit the code or directly compile and flash the program on their own board.
9.4. Download Firmware
This option generates ELF file(s) associated to the selected board, which can be directly flashed on users' own board using STM32CubeProgrammer. The System Performance application is enabled on the application.
The AI system performance application is a self and bare-metal on-device application that allows the out-of-the-box measurement of the critical system integration aspects of the generated neural network. The accuracy performance aspect is not and cannot be considered here. The reported measurements include CPU cycles by inference (duration in ms, CPU cycles, CPU workload), and used stack and used heap (in bytes).
10. Other information
10.1. Project cannot be saved
Please note that, in some particular circumstances, your progress in the working project may be lost and cannot be retrieved, for example, if the web browser is accidentally closed or if you lose the internet connection. If this happens, you will need to start over.
10.2. Data Protection
STM32Cube.AI Developer Cloud is deployed on the Microsoft Azure Cloud Service.
10.2.1. Customer External access and data upload
- External access to the service is always done through a firewall, a load balancer and a route dispatcher. All accesses are performed using encrypted secured https.
- All users are authenticated using my.st.com authentication.
- There is no direct access to the internal Azure services nor uploaded resources.
- Uploaded data are checked against malicious data.
10.2.2. Model and Data storage
- Uploaded models are stored in an Azure storage service and accessible only by the user that has uploaded the model, the stm32ai micro services and the benchmark farm for the purpose of their service.
- Models are automatically deleted after 6 months of inactivity.
- Uploaded data is kept only for the time of the action.
- Access to the storage is only allowed by private end points not visible outside the DMZ
10.3. Embedded Documentation
Users can open the online documentation anytime by clicking on the "Open documentation" button embedded in the page or clicking on the "Documentation" icon at the top of the page to open it in a new tab/window. To close the documentation, simply press the "close documentation" button.
In certain pages, there are also "Information bubbles" available too. By click on the bubble, users will directly go the corresponding documentation page related to that topic.
10.4. Step-by-step video Tutorial on YouTube
ST has also created a video of a step-by-step guide for STM32Cube.AI Developer Cloud. You can find this video on STMicroelectronics official YouTube channel: Getting started with STM32Cube.AI Developer Cloud