How to use an RTOS with Secure Manager on STM32H5

Revision as of 11:05, 19 December 2023 by Registered User (→‎Implementation example)

1. Introduction

When working with the Secure Manager, incorporating an RTOS can be a valuable approach to ensure secure and efficient thread management. In this wiki article, we will explore the specific steps required to successfully integrate an RTOS with the Secure Manager, with a focus on the mechanism that guarantees secure and thread-safe function calls.

Prerequisite:

  • Installed the Secure Manager
  • Have a nonsecure application compatible with the Secure Manager
  • Have the RTOS library chosen by the user integrated in the nonsecure application

2. Implementation example

Using the Secure Manager from a non-secure application can be done in a single thread, which eliminates the possibility of concurrent access. However, when working with a real-time operating system and a multi-threaded application, it is essential to protect the calls made to the Secure Manager. This protection guarantees that only one call can be made to the Secure Manager at a time, ensuring secure and efficient thread management. In this section, we will provide an implementation example of how to protect calls made to the Secure Manager in a multi-threaded environment.

2.1. Thread-safe secure calls

The implementation will protect from multiple calls via the interface functions from the nonsecure application to Secure Manager.

There is a mechanism in tfm_ns_interface.c in the middleware secure_manager_api that interfacing with the Secure Manager.

Figure 1 : tfm_ns_interface.c directory


This mechanism, based on functions defined as __weak, will have to be re-implemented by integrating a protection, called mutex.

The functions ns_ipc_seq_begin and ns_ipc_seq_end, which are declared by default in the Secure Manager, need to be re-implemented in the RTOS project due to multithreaded use.

Figure 2 : tfm_ns_interface.c functions

2.2. Step by step implementation

Here are the following steps, to implement mutex in the Secure Manager with RTOS in your project in the file where the user decides to reimplement interface function:

  1. Initialize the mutex
  2. Create the mutex
  3. Implement the acquisition and release of the mutex in the interface functions.

2.2.1. Detailed example applied with FreeRTOS.

1. Declare a mutex and initialize it to 0 :

static SemaphoreHandle_t nsIpcMutex = { 0 };

2. Create a function that creates the mutex and assigns it to the nsIpcMutex variable.

void tfm_ns_interface_init( void )
{
  nsIpcMutex = xSemaphoreCreateMutex();
  if(nsIpcMutex == NULL)
  {
   // Logging Error
  }
}

3. Re-implement the acquisition and release of the mutex with functions defines in semphr.c from library FreeRTOS, in the ns_ipc_seq_begin and ns_ipc_seq_end functions reimplemented in your project.

void ns_ipc_seq_begin(const ns_ipc_seq_info_t* info)
{
  /* Lock mutex */
  if(nsIpcMutex != NULL)
  {
    xSemaphoreTake(nsIpcMutex, portMAX_DELAY );
  }
  ….
}
void ns_ipc_seq_end(const ns_ipc_seq_info_t* info)
{
  /* Unlock mutex */
  if(nsIpcMutex != NULL)
  {
    xSemaphoreGive(nsIpcMutex);
  }
  ….
}

For more concrete examples, actual implementations can be found in X-Cube-AWS & X-Cube-Azure using the Secure Manager with a real-time operating system.

No categories assignedEdit