STM32WBA Build Zigbee project

Revision as of 12:55, 12 December 2023 by Registered User (→‎Hardware requirements)

1. Presentation

This page describes how to easily build and install an STM32WBA Zigbee application.
Project examples can be found on STM32CubeWBA MCU package[1], and are available for different platforms.

STMicroelectronics Zigbee project example directory
Connectivity wba zigbee projects.png


2. Requirements

2.1. Software and system requirements

The software requirements are as follows:

The minimum IDEs versions:

  • IAR Embedded Workbench® for Arm (EWARM) toolchain V9.20.1, plus a patch available in the WBA firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/EWARMv8_STM32WBAx_V1.2.zip
  • RealView microcontroller development kit (MDK-ARM) toolchain V5.37, plus a patch available in the WBA firmware package: STM32Cube_FW_WBA_Vx.x.x/Utilities/PC_Software/Keil.STM32WBAx_DFP.1.0.0.zip
  • STM32CubeIDE toolchain V1.12.0 [2].

The required programmer version:

  • STM32CubeProgrammer[3]: To flash the board with an already generated binary

2.2. Hardware requirements

A Nucleo board[4] is necessary to install the application.

Platform illustration
Connectivity STM32WBA52 Board.png


3. Build and install the application

This section describes the build process using IAR and STM32CubeIDE.

3.1. IAR IDE

Select the application that you want to build, open the IAR (EWARM) dedicated directory. Launch Project.eww to open the demonstration project on IDE.

IAR project directory
Connectivity Zigbee IAR.png



Ensure that your project is correctly visible into the project explorer view.

Build your project by reproducing the following steps:

IAR: build
Connectivity Zigbee Build Project.png


You can build and flash the project on your board by clicking on the button illustrated below:

IAR: build and flash
Connectivity Zigbee BuildProject.png

3.2. STM32CubeIDE

Select the application that you want to build, and open the STM32CubeIDE dedicated directory. Launch the STM32CubeIDE, and select the folder .project of the demonstration.

STM32CubeIDE project folder
Connectivity Zigbee IDE.png




Ensure that your project is correctly visible into the project explorer view.
Build your project by reproducing the following steps:

STM32CubeIDE: build
Connectivity Zigbee CubeIDE.png


Flash it on the board.

STM32CubeIDE: flash
Connectivity Zigbee Flash CubeIDE.png

3.3. Install the application from STM32CubeProgrammer

It is possible to flash the previously build binary by using the STM32CubeProgrammer software[5].

Select your device and connect to it.

STM32CubeProgrammer: platform connection
Connectivity Zigbee Build CubeProgrammer.png


Once connected, the device information is displayed on the STM32CubeProgrammer interface. Click on the programming icon in the left column. Then, select the project binary to flash (could be .hex, .elf, or .bin):

  • [...]\Projects\[...]\Applications\Zigbee\Zigbee_Find_Bind_Coord\[...]\ Zigbee_Find_Bind_Coord.elf

Then, click on the Start programming button:

STM32CubeProgrammer: flash project
Connectivity Zigbee CubeProgrammer.png


When the programming is complete, the following logs are displayed:

STM32CubeProgrammer: logs
Connectivity Zigbee log.png

4. References