Zigbee Realistic Use Case Weather Station

Revision as of 16:52, 11 December 2023 by Registered User (→‎Cluster implementation)

1. Introduction

This implementation can be seen as a base to implement home sensors that can be extend to thermostat or others.
Test and verify various functionality and ensure proper functioning.

2. Cluster implementation

For this example, several clusters Measurement are mixed for sensors, like Temperature, Water content and concentration.

  • Temperature Measurement cluster [1], is the basic cluster for the weather station.
  • Water Content Measurement [2], which includes three subclusters:
  • Concentration Measurement, a collection of 33 subclusters [3]. The one used in the application is the CO2 cluster.

3. Acronyms and definitions

Term Definition
ZC Zigbee Coordinator
ZR Zigbee Router
ZED Zigbee End Device
RUC Realistic Use Case
GPIO General Purpose Input Output
PWM Pulse Width Modulation


4. References